1 /* GStreamer
2 * Copyright (C) <1999> Erik Walthinsen <omega@cse.ogi.edu>
3 *
4 * This library is free software; you can redistribute it and/or
5 * modify it under the terms of the GNU Library General Public
6 * License as published by the Free Software Foundation; either
7 * version 2 of the License, or (at your option) any later version.
8 *
9 * This library is distributed in the hope that it will be useful,
10 * but WITHOUT ANY WARRANTY; without even the implied warranty of
11 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
12 * Library General Public License for more details.
13 *
14 * You should have received a copy of the GNU Library General Public
15 * License along with this library; if not, write to the
16 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
17 * Boston, MA 02111-1307, USA.
18 */
20 #include <gst/gst_private.h>
21 #include <gst/gstversion.h>
22 #include <gst/gstplugin.h>
24 #include "gstindexers.h"
26 static gboolean
27 plugin_init (GstPlugin * plugin)
28 {
29 gboolean res = TRUE;
31 res &= gst_mem_index_plugin_init (plugin);
32 #if defined(HAVE_MMAP) && !defined(GST_DISABLE_LOADSAVE)
33 res &= gst_file_index_plugin_init (plugin);
34 #endif
36 return res;
37 }
39 GST_PLUGIN_DEFINE (GST_VERSION_MAJOR,
40 GST_VERSION_MINOR,
41 "coreindexers",
42 "GStreamer core indexers",
43 plugin_init, VERSION, GST_LICENSE, GST_PACKAGE_NAME, GST_PACKAGE_ORIGIN);