gststructure: early out when we know a value cannot be a subset
[glsdk/gstreamer0-10.git] / plugins / indexers / gstindexers.c
1 /* GStreamer
2  * Copyright (C) <1999> Erik Walthinsen <omega@cse.ogi.edu>
3  *
4  * This library is free software; you can redistribute it and/or
5  * modify it under the terms of the GNU Library General Public
6  * License as published by the Free Software Foundation; either
7  * version 2 of the License, or (at your option) any later version.
8  *
9  * This library is distributed in the hope that it will be useful,
10  * but WITHOUT ANY WARRANTY; without even the implied warranty of
11  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
12  * Library General Public License for more details.
13  *
14  * You should have received a copy of the GNU Library General Public
15  * License along with this library; if not, write to the
16  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
17  * Boston, MA 02111-1307, USA.
18  */
20 #include <gst/gst_private.h>
21 #include <gst/gstversion.h>
22 #include <gst/gstplugin.h>
24 #include "gstindexers.h"
26 static gboolean
27 plugin_init (GstPlugin * plugin)
28 {
29   gboolean res = TRUE;
31   res &= gst_mem_index_plugin_init (plugin);
32 #if defined(HAVE_MMAP) && !defined(GST_DISABLE_LOADSAVE)
33   res &= gst_file_index_plugin_init (plugin);
34 #endif
36   return res;
37 }
39 GST_PLUGIN_DEFINE (GST_VERSION_MAJOR,
40     GST_VERSION_MINOR,
41     "coreindexers",
42     "GStreamer core indexers",
43     plugin_init, VERSION, GST_LICENSE, GST_PACKAGE_NAME, GST_PACKAGE_ORIGIN);