Release notes for GStreamer 0.10.35 "Nuclear Fission" The GStreamer team is proud to announce a new release in the 0.10.x stable series of the core of the GStreamer streaming media framework. The 0.10.x series is a stable series targeted at end users. It is not API or ABI compatible with the stable 0.8.x series. It is, however, parallel installable with the 0.8.x series. The 0.10.x series has been reworked for threadsafety. It also features various feature additions and enhancements. This module, gstreamer, only contains core functionality. For actual media playback, you will need other modules. gst-plugins-base contains a basic set of well-supported plug-ins gst-plugins-good contains a set of well-supported plug-ins under our preferred license gst-plugins-ugly contains a set of well-supported plug-ins, but might pose problems for distributors gst-plugins-bad contains a set of less supported plug-ins that haven't passed the rigorous quality testing we expect Features of this release * work around GLib atomic ops API change * some minor win32/mingw fixes * don't use G_CONST_RETURN in public headers Bugs fixed in this release * 652211 : Use const instead G_CONST_RETURN Download You can find source releases of gstreamer in the download directory: http://gstreamer.freedesktop.org/src/gstreamer/ GStreamer Homepage More details can be found on the project's website: http://gstreamer.freedesktop.org/ Support and Bugs We use GNOME's bugzilla for bug reports and feature requests: http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer Developers GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there. Interested developers of the core library, plug-ins, and applications should subscribe to the gstreamer-devel list. If there is sufficient interest we will create more lists as necessary. Applications Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer, Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others. Let us know if you want to be added to this list. Contributors to this release * David Schleef * Javier Jardón * Руслан Ижбулатов