Release notes for GStreamer 0.10.27 "You're Shocked, We Know" The GStreamer team is proud to announce a new release in the 0.10.x stable series of the core of the GStreamer streaming media framework. The 0.10.x series is a stable series targeted at end users. It is not API or ABI compatible with the stable 0.8.x series. It is, however, parallel installable with the 0.8.x series. The 0.10.x series has been reworked for threadsafety. It also features various feature additions and enhancements. This module, gstreamer, only contains core functionality. For actual media playback, you will need other modules. gst-plugins-base contains a basic set of well-supported plug-ins gst-plugins-good contains a set of well-supported plug-ins under our preferred license gst-plugins-ugly contains a set of well-supported plug-ins, but might pose problems for distributors gst-plugins-bad contains a set of less supported plug-ins that haven't passed the rigorous quality testing we expect Features of this release * basesrc: protect segment values from concurrent access from different threads * typefind: protect internal fields from concurrent changes from different threads * typefind: fix pad activation corner-case with have-type already having been emitted * typefind: reset the working mode when going to READY/NULL, fixes re-use from READY state as with decodebin2 * gstpoll: fix crash when logging is enabled for GST_POLL * bytewriter: expose gst_byte_writer_put_{float32|float64}_*() properly in header * basesink: fix emergency rendering timestamp tracking * fdsink, fdsrc: fix compilation with MSVC * memindex: avoid busy loop when doing EXACT lookup Bugs fixed in this release * 610366 : [gstcollectpads][doc] Add a reminder for 'data' doc * 605189 : gst_element_get_state has wrong introspection * 607771 : [API] Add gst_byte_writer_fill * 608036 : [typefind] deadlock when upstream puts caps on buffers on pull mode * 608877 : [typefind] Access to internal fields not threadsafe * 609941 : GStreamer-WARNING **: External plugin loader failed. * 610210 : [PATCH] Fix compilation of fdsink and fdsrc with MSVC * 610246 : [optimization] Speed up _get_range() * 610367 : [memindex] might busy loop upon EXACT lookup * 610444 : [controller] Interpolation control source passes NULL pointers to GSequence API * 611087 : [basesink] emergency rendering of late buffers fails after resuming from PAUSE * 611719 : GST_DEBUG_OBJECT macros not fed with GObject* in gstpoll.c API changed in this release - API additions: * gst_byte_writer_fill() Download You can find source releases of gstreamer in the download directory: http://gstreamer.freedesktop.org/src/gstreamer/ GStreamer Homepage More details can be found on the project's website: http://gstreamer.freedesktop.org/ Support and Bugs We use GNOME's bugzilla for bug reports and feature requests: http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer Developers GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there. Interested developers of the core library, plug-ins, and applications should subscribe to the gstreamer-devel list. If there is sufficient interest we will create more lists as necessary. Applications Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer, Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others. Let us know if you want to be added to this list. Contributors to this release * Andoni Morales Alastruey * Arun Raghavan * Benjamin Otte * Edward Hervey * Johan Bilien * Mark Nauwelaerts * Sebastian Dröge * Stefan Kost * Thiago Santos * Tim-Philipp Müller