/* Convenience header for conditional use of GNU . Copyright (C) 1995-1998, 2000-2002 Free Software Foundation, Inc. This program is free software; you can redistribute it and/or modify it under the terms of the GNU Library General Public License as published by the Free Software Foundation; either version 2, or (at your option) any later version. This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU Library General Public License for more details. You should have received a copy of the GNU Library General Public License along with this program; if not, write to the Free Software Foundation, Inc., 59 Temple Place - Suite 330, Boston, MA 02111-1307, USA. */ #ifndef _LIBGETTEXT_H #define _LIBGETTEXT_H 1 /* NLS can be disabled through the configure --disable-nls option. */ #ifdef ENABLE_NLS /* Get declarations of GNU message catalog functions. */ # include #else /* Solaris /usr/include/locale.h includes /usr/include/libintl.h, which chokes if dcgettext is defined as a macro. So include it now, to make later inclusions of a NOP. We don't include as well because people using "gettext.h" will not include , and also including would fail on SunOS 4, whereas is OK. */ #if defined(__sun) # include #endif /* Disabled NLS. The casts to 'const char *' serve the purpose of producing warnings for invalid uses of the value returned from these functions. On pre-ANSI systems without 'const', the config.h file is supposed to contain "#define const". */ # define gettext(Msgid) ((const char *) (Msgid)) # define dgettext(Domainname, Msgid) ((const char *) (Msgid)) # define dcgettext(Domainname, Msgid, Category) ((const char *) (Msgid)) # define ngettext(Msgid1, Msgid2, N) \ ((N) == 1 ? (const char *) (Msgid1) : (const char *) (Msgid2)) # define dngettext(Domainname, Msgid1, Msgid2, N) \ ((N) == 1 ? (const char *) (Msgid1) : (const char *) (Msgid2)) # define dcngettext(Domainname, Msgid1, Msgid2, N, Category) \ ((N) == 1 ? (const char *) (Msgid1) : (const char *) (Msgid2)) # define textdomain(Domainname) ((const char *) (Domainname)) # define bindtextdomain(Domainname, Dirname) ((const char *) (Dirname)) # define bind_textdomain_codeset(Domainname, Codeset) ((const char *) (Codeset)) #endif /* A pseudo function call that serves as a marker for the automated extraction of messages, but does not call gettext(). The run-time translation is done at a different place in the code. The argument, String, should be a literal string. Concatenated strings and other string expressions won't work. The macro's expansion is not parenthesized, so that it is suitable as initializer for static 'char[]' or 'const char[]' variables. */ #define gettext_noop(String) String #endif /* _LIBGETTEXT_H */