/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * * gst.h: Main header for GStreamer, apps should include this * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GST_H__ #define __GST_H__ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include /* API compatibility stuff */ #include G_BEGIN_DECLS void gst_init (int *argc, char **argv[]); gboolean gst_init_check (int *argc, char **argv[], GError ** err); gboolean gst_is_initialized (void); GOptionGroup * gst_init_get_option_group (void); void gst_deinit (void); void gst_version (guint *major, guint *minor, guint *micro, guint *nano); gchar * gst_version_string (void); gboolean gst_segtrap_is_enabled (void); void gst_segtrap_set_enabled (gboolean enabled); gboolean gst_registry_fork_is_enabled (void); void gst_registry_fork_set_enabled (gboolean enabled); gboolean gst_update_registry (void); G_END_DECLS #endif /* __GST_H__ */