/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000,2004 Wim Taymans * * gstelement.h: Header for GstElement * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GST_ELEMENT_H__ #define __GST_ELEMENT_H__ /* gstelement.h and gstelementfactory.h include eachother */ typedef struct _GstElement GstElement; typedef struct _GstElementClass GstElementClass; /* gstmessage.h needs State */ typedef enum { GST_STATE_VOID_PENDING = 0, /* used for GstElement->pending_state when there is no pending state */ GST_STATE_NULL = 1, GST_STATE_READY = 2, GST_STATE_PAUSED = 3, GST_STATE_PLAYING = 4 } GstState; #include #include #include #include #include #include #include #include #include #include #include #include G_BEGIN_DECLS GST_EXPORT GType _gst_element_type; #define GST_TYPE_ELEMENT (_gst_element_type) #define GST_IS_ELEMENT(obj) (G_TYPE_CHECK_INSTANCE_TYPE ((obj), GST_TYPE_ELEMENT)) #define GST_IS_ELEMENT_CLASS(klass) (G_TYPE_CHECK_CLASS_TYPE ((klass), GST_TYPE_ELEMENT)) #define GST_ELEMENT_GET_CLASS(obj) (G_TYPE_INSTANCE_GET_CLASS ((obj), GST_TYPE_ELEMENT, GstElementClass)) #define GST_ELEMENT(obj) (G_TYPE_CHECK_INSTANCE_CAST ((obj), GST_TYPE_ELEMENT, GstElement)) #define GST_ELEMENT_CLASS(klass) (G_TYPE_CHECK_CLASS_CAST ((klass), GST_TYPE_ELEMENT, GstElementClass)) #define GST_ELEMENT_CAST(obj) ((GstElement*)(obj)) typedef enum { GST_STATE_CHANGE_FAILURE = 0, GST_STATE_CHANGE_SUCCESS = 1, GST_STATE_CHANGE_ASYNC = 2, GST_STATE_CHANGE_NO_PREROLL = 3 } GstStateChangeReturn; /* NOTE: this probably should be done with an #ifdef to decide * whether to safe-cast or to just do the non-checking cast. */ #define GST_STATE(obj) (GST_ELEMENT(obj)->current_state) #define GST_STATE_PENDING(obj) (GST_ELEMENT(obj)->pending_state) #define GST_STATE_FINAL(obj) (GST_ELEMENT(obj)->final_state) #define GST_STATE_ERROR(obj) (GST_ELEMENT(obj)->state_error) #define GST_STATE_NO_PREROLL(obj) (GST_ELEMENT(obj)->no_preroll) #ifndef GST_DEBUG_STATE_CHANGE #define GST_STATE_CHANGE(obj) ((1<<(GST_STATE(obj)+8)) | 1<state < GST_STATE_NULL || e->state > GST_STATE_PLAYING) g_assert_not_reached (); if (e->pending_state < GST_STATE_NULL || e->pending_state > GST_STATE_PLAYING) g_assert_not_reached (); if (e->state - e->pending_state != 1 && e->pending_state - e->state != 1) g_assert_not_reached (); return (1<<(GST_STATE(obj)+8)) | 1<bus) #define GST_ELEMENT_CLOCK(obj) (GST_ELEMENT_CAST(obj)->clock) #define GST_ELEMENT_PADS(obj) (GST_ELEMENT_CAST(obj)->pads) /** * GST_ELEMENT_ERROR: * @el: the element that throws the error * @domain: like CORE, LIBRARY, RESOURCE or STREAM (see #GstError) * @code: error code defined for that domain (see #GstError) * @text: the message to display (format string and args enclosed in parentheses) * @debug: debugging information for the message (format string and args enclosed in parentheses) * * Utility function that elements can use in case they encountered a fatal * data processing error. The pipeline will throw an error signal and the * application will be requested to stop further media processing. */ #define GST_ELEMENT_ERROR(el, domain, code, text, debug) \ G_STMT_START { \ gchar *__txt = _gst_element_error_printf text; \ gchar *__dbg = _gst_element_error_printf debug; \ if (__txt) \ GST_WARNING_OBJECT (el, "error: %s", __txt); \ if (__dbg) \ GST_WARNING_OBJECT (el, "error: %s", __dbg); \ gst_element_message_full (GST_ELEMENT(el), GST_MESSAGE_ERROR, \ GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code, \ __txt, __dbg, __FILE__, GST_FUNCTION, __LINE__); \ } G_STMT_END /* log a (non-fatal) warning message and post it on the bus */ #define GST_ELEMENT_WARNING(el, domain, code, text, debug) \ G_STMT_START { \ gchar *__txt = _gst_element_error_printf text; \ gchar *__dbg = _gst_element_error_printf debug; \ if (__txt) \ GST_WARNING_OBJECT (el, "warning: %s", __txt); \ if (__dbg) \ GST_WARNING_OBJECT (el, "warning: %s", __dbg); \ gst_element_message_full (GST_ELEMENT(el), GST_MESSAGE_WARNING, \ GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code, \ __txt, __dbg, __FILE__, GST_FUNCTION, __LINE__); \ } G_STMT_END /* the state change mutexes and conds */ #define GST_STATE_GET_LOCK(elem) (GST_ELEMENT_CAST(elem)->state_lock) #define GST_STATE_LOCK(elem) g_mutex_lock(GST_STATE_GET_LOCK(elem)) #define GST_STATE_TRYLOCK(elem) g_mutex_trylock(GST_STATE_GET_LOCK(elem)) #define GST_STATE_UNLOCK(elem) g_mutex_unlock(GST_STATE_GET_LOCK(elem)) #define GST_STATE_GET_COND(elem) (GST_ELEMENT_CAST(elem)->state_cond) #define GST_STATE_WAIT(elem) g_cond_wait (GST_STATE_GET_COND (elem), GST_STATE_GET_LOCK (elem)) #define GST_STATE_TIMED_WAIT(elem, timeval) g_cond_timed_wait (GST_STATE_GET_COND (elem), GST_STATE_GET_LOCK (elem),\ timeval) #define GST_STATE_SIGNAL(elem) g_cond_signal (GST_STATE_GET_COND (elem)); #define GST_STATE_BROADCAST(elem) g_cond_broadcast (GST_STATE_GET_COND (elem)); struct _GstElement { GstObject object; /*< public >*/ /* with STATE_LOCK */ /* element state */ GMutex *state_lock; GCond *state_cond; guint8 current_state; guint8 pending_state; guint8 final_state; gboolean state_error; /* flag is set when the element has an error in the last state change. it is cleared when doing another state change. */ gboolean no_preroll; /* flag is set when the element cannot preroll */ /*< public >*/ /* with LOCK */ GstBus *bus; /* allocated clock */ GstClock *clock; GstClockTimeDiff base_time; /* NULL/READY: 0 - PAUSED: current time - PLAYING: difference to clock */ /* element pads, these lists can only be iterated while holding * the LOCK or checking the cookie after each LOCK. */ guint16 numpads; GList *pads; guint16 numsrcpads; GList *srcpads; guint16 numsinkpads; GList *sinkpads; guint32 pads_cookie; /*< private >*/ gpointer _gst_reserved[GST_PADDING]; }; struct _GstElementClass { GstObjectClass parent_class; /*< public >*/ /* the element details */ GstElementDetails details; /* factory that the element was created from */ GstElementFactory *elementfactory; /* templates for our pads */ GList *padtemplates; gint numpadtemplates; guint32 pad_templ_cookie; /*< private >*/ /* signal callbacks */ void (*state_changed) (GstElement *element, GstState old, GstState state); void (*pad_added) (GstElement *element, GstPad *pad); void (*pad_removed) (GstElement *element, GstPad *pad); void (*no_more_pads) (GstElement *element); /*< public >*/ /* virtual methods for subclasses */ /* request/release pads */ GstPad* (*request_new_pad) (GstElement *element, GstPadTemplate *templ, const gchar* name); void (*release_pad) (GstElement *element, GstPad *pad); /* state changes */ GstStateChangeReturn (*get_state) (GstElement * element, GstState * state, GstState * pending, GTimeVal * timeout); GstStateChangeReturn (*change_state) (GstElement *element, GstStateChange transition); /* bus */ void (*set_bus) (GstElement * element, GstBus * bus); /* set/get clocks */ GstClock* (*get_clock) (GstElement *element); void (*set_clock) (GstElement *element, GstClock *clock); /* index */ GstIndex* (*get_index) (GstElement *element); void (*set_index) (GstElement *element, GstIndex *index); /* query functions */ gboolean (*send_event) (GstElement *element, GstEvent *event); const GstQueryType* (*get_query_types) (GstElement *element); gboolean (*query) (GstElement *element, GstQuery *query); /*< private >*/ gpointer _gst_reserved[GST_PADDING]; }; /* element class pad templates */ void gst_element_class_add_pad_template (GstElementClass *klass, GstPadTemplate *templ); GstPadTemplate* gst_element_class_get_pad_template (GstElementClass *element_class, const gchar *name); GList* gst_element_class_get_pad_template_list (GstElementClass *element_class); void gst_element_class_set_details (GstElementClass *klass, const GstElementDetails *details); /* element instance */ GType gst_element_get_type (void); /* basic name and parentage stuff from GstObject */ #define gst_element_get_name(elem) gst_object_get_name(GST_OBJECT(elem)) #define gst_element_set_name(elem,name) gst_object_set_name(GST_OBJECT(elem),name) #define gst_element_get_parent(elem) gst_object_get_parent(GST_OBJECT(elem)) #define gst_element_set_parent(elem,parent) gst_object_set_parent(GST_OBJECT(elem),parent) /* clocking */ gboolean gst_element_requires_clock (GstElement *element); gboolean gst_element_provides_clock (GstElement *element); GstClock* gst_element_get_clock (GstElement *element); void gst_element_set_clock (GstElement *element, GstClock *clock); void gst_element_set_base_time (GstElement *element, GstClockTime time); GstClockTime gst_element_get_base_time (GstElement *element); /* indexes */ gboolean gst_element_is_indexable (GstElement *element); void gst_element_set_index (GstElement *element, GstIndex *index); GstIndex* gst_element_get_index (GstElement *element); /* bus */ void gst_element_set_bus (GstElement * element, GstBus * bus); GstBus * gst_element_get_bus (GstElement * element); /* pad management */ gboolean gst_element_add_pad (GstElement *element, GstPad *pad); gboolean gst_element_remove_pad (GstElement *element, GstPad *pad); void gst_element_no_more_pads (GstElement *element); GstPad* gst_element_get_pad (GstElement *element, const gchar *name); GstPad* gst_element_get_static_pad (GstElement *element, const gchar *name); GstPad* gst_element_get_request_pad (GstElement *element, const gchar *name); void gst_element_release_request_pad (GstElement *element, GstPad *pad); GstIterator * gst_element_iterate_pads (GstElement * element); GstIterator * gst_element_iterate_src_pads (GstElement * element); GstIterator * gst_element_iterate_sink_pads (GstElement * element); /* event/query/format stuff */ gboolean gst_element_send_event (GstElement *element, GstEvent *event); gboolean gst_element_seek (GstElement *element, gdouble rate, GstFormat format, GstSeekFlags flags, GstSeekType cur_type, gint64 cur, GstSeekType stop_type, gint64 stop); G_CONST_RETURN GstQueryType* gst_element_get_query_types (GstElement *element); gboolean gst_element_query (GstElement *element, GstQuery *query); /* messages */ gboolean gst_element_post_message (GstElement * element, GstMessage * message); /* error handling */ gchar * _gst_element_error_printf (const gchar *format, ...); void gst_element_message_full (GstElement * element, GstMessageType type, GQuark domain, gint code, gchar * text, gchar * debug, const gchar * file, const gchar * function, gint line); /* state management */ gboolean gst_element_is_locked_state (GstElement *element); gboolean gst_element_set_locked_state (GstElement *element, gboolean locked_state); gboolean gst_element_sync_state_with_parent (GstElement *element); GstStateChangeReturn gst_element_get_state (GstElement * element, GstState * state, GstState * pending, GTimeVal * timeout); GstStateChangeReturn gst_element_set_state (GstElement *element, GstState state); void gst_element_abort_state (GstElement * element); void gst_element_commit_state (GstElement * element); void gst_element_lost_state (GstElement * element); /* factory management */ GstElementFactory* gst_element_get_factory (GstElement *element); G_END_DECLS #endif /* __GST_ELEMENT_H__ */