/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * 2003 Benjamin Otte * * gstinfo.h: debugging functions * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GSTINFO_H__ #define __GSTINFO_H__ #include #include #include #ifndef M_PI #define M_PI 3.14159265358979323846 #endif G_BEGIN_DECLS /** * GstDebugLevel: * @GST_LEVEL_NONE: No debugging level specified or desired. Used to deactivate * debugging output. * @GST_LEVEL_ERROR: Error messages are to be used only when an error occured * that stops the application from keeping working correctly. * An examples is gst_element_error, which outputs a message with this priority. * It does not mean that the application is terminating as with g_errror. * @GST_LEVEL_WARNING: Warning messages are to inform about abnormal behaviour * that could lead to problems or weird behaviour later on. An example of this * would be clocking issues ("your computer is pretty slow") or broken input * data ("Can't synchronize to stream.") * @GST_LEVEL_INFO: Informational messages should be used to keep the developer * updated about what is happening. * Examples where this should be used are when a typefind function has * successfully determined the type of the stream or when an mp3 plugin detects * the format to be used. ("This file has mono sound.") * @GST_LEVEL_DEBUG: Debugging messages should be used when something common * happens that is not the expected default behavior, or something that's * useful to know but doesn't happen all the time (ie. per loop iteration or * buffer processed or event handled). * An example would be notifications about state changes or receiving/sending * of events. * @GST_LEVEL_LOG: Log messages are messages that are very common but might be * useful to know. As a rule of thumb a pipeline that is iterating as expected * should never output anything else but LOG messages. Use this log level to * log recurring information in chain functions and loop functions, for * example. * @GST_LEVEL_FIXME: Fixme messages are messages that indicate that something * in the executed code path is not fully implemented or handled yet. Note * that this does not replace proper error handling in any way, the purpose * of this message is to make it easier to spot incomplete/unfinished pieces * of code when reading the debug log. (Since: 0.10.23) * @GST_LEVEL_TRACE: Tracing-related messages (Since: 0.10.30) * Examples for this are referencing/dereferencing of objects. * @GST_LEVEL_MEMDUMP: memory dump messages are used to log (small) chunks of * data as memory dumps in the log. They will be displayed as hexdump with * ASCII characters. (Since: 0.10.23) * @GST_LEVEL_COUNT: The number of defined debugging levels. * * The level defines the importance of a debugging message. The more important a * message is, the greater the probability that the debugging system outputs it. */ typedef enum { GST_LEVEL_NONE = 0, GST_LEVEL_ERROR, GST_LEVEL_WARNING, GST_LEVEL_INFO, GST_LEVEL_DEBUG, GST_LEVEL_LOG, GST_LEVEL_FIXME = 6, GST_LEVEL_TRACE = 7, /* add more */ GST_LEVEL_MEMDUMP = 9, /* add more */ GST_LEVEL_COUNT } GstDebugLevel; /** * GST_LEVEL_DEFAULT: * * Defines the default debugging level to be used with GStreamer. It is normally * set to #GST_LEVEL_NONE so nothing get printed. * As it can be configured at compile time, developer builds may chose to * override that though. * You can use this as an argument to gst_debug_set_default_threshold() to * reset the debugging output to default behaviour. */ #ifndef GST_LEVEL_DEFAULT #define GST_LEVEL_DEFAULT GST_LEVEL_NONE #endif /* defines for format (colors etc) * don't change them around, it uses terminal layout * Terminal color strings: * 00=none 01=bold 04=underscore 05=blink 07=reverse 08=concealed * Text color codes: * 30=black 31=red 32=green 33=yellow 34=blue 35=magenta 36=cyan 37=white * Background color codes: * 40=black 41=red 42=green 43=yellow 44=blue 45=magenta 46=cyan 47=white */ /** * GstDebugColorFlags: * @GST_DEBUG_FG_BLACK: Use black as foreground color. * @GST_DEBUG_FG_RED: Use red as foreground color. * @GST_DEBUG_FG_GREEN: Use green as foreground color. * @GST_DEBUG_FG_YELLOW: Use yellow as foreground color. * @GST_DEBUG_FG_BLUE: Use blue as foreground color. * @GST_DEBUG_FG_MAGENTA: Use magenta as foreground color. * @GST_DEBUG_FG_CYAN: Use cyan as foreground color. * @GST_DEBUG_FG_WHITE: Use white as foreground color. * @GST_DEBUG_BG_BLACK: Use black as background color. * @GST_DEBUG_BG_RED: Use red as background color. * @GST_DEBUG_BG_GREEN: Use green as background color. * @GST_DEBUG_BG_YELLOW: Use yellow as background color. * @GST_DEBUG_BG_BLUE: Use blue as background color. * @GST_DEBUG_BG_MAGENTA: Use magenta as background color. * @GST_DEBUG_BG_CYAN: Use cyan as background color. * @GST_DEBUG_BG_WHITE: Use white as background color. * @GST_DEBUG_BOLD: Make the output bold. * @GST_DEBUG_UNDERLINE: Underline the output. * * These are some terminal style flags you can use when creating your * debugging categories to make them stand out in debugging output. */ typedef enum { /* colors */ GST_DEBUG_FG_BLACK = 0x0000, GST_DEBUG_FG_RED = 0x0001, GST_DEBUG_FG_GREEN = 0x0002, GST_DEBUG_FG_YELLOW = 0x0003, GST_DEBUG_FG_BLUE = 0x0004, GST_DEBUG_FG_MAGENTA = 0x0005, GST_DEBUG_FG_CYAN = 0x0006, GST_DEBUG_FG_WHITE = 0x0007, /* background colors */ GST_DEBUG_BG_BLACK = 0x0000, GST_DEBUG_BG_RED = 0x0010, GST_DEBUG_BG_GREEN = 0x0020, GST_DEBUG_BG_YELLOW = 0x0030, GST_DEBUG_BG_BLUE = 0x0040, GST_DEBUG_BG_MAGENTA = 0x0050, GST_DEBUG_BG_CYAN = 0x0060, GST_DEBUG_BG_WHITE = 0x0070, /* other formats */ GST_DEBUG_BOLD = 0x0100, GST_DEBUG_UNDERLINE = 0x0200 } GstDebugColorFlags; #define GST_DEBUG_FG_MASK (0x000F) #define GST_DEBUG_BG_MASK (0x00F0) #define GST_DEBUG_FORMAT_MASK (0xFF00) typedef struct _GstDebugCategory GstDebugCategory; /** * GstDebugCategory: * * This is the struct that describes the categories. Once initialized with * #GST_DEBUG_CATEGORY_INIT, its values can't be changed anymore. */ struct _GstDebugCategory { /*< private >*/ gint threshold; guint color; /* see defines above */ const gchar * name; const gchar * description; }; /********** some convenience macros for debugging **********/ /** * GST_STR_NULL: * @str: The string to check. * * Macro to use when a string must not be NULL, but may be NULL. If the string * is NULL, "(NULL)" is printed instead. * In GStreamer printf string arguments may not be NULL, because on some * platforms (ie Solaris) the libc crashes in that case. This includes debugging * strings. */ #define GST_STR_NULL(str) ((str) ? (str) : "(NULL)") /* FIXME, not MT safe */ /** * GST_DEBUG_PAD_NAME: * @pad: The pad to debug. * * Evaluates to 2 strings, that describe the pad. Often used in debugging * statements. */ #define GST_DEBUG_PAD_NAME(pad) \ (pad != NULL) ? \ ((GST_OBJECT_PARENT(pad) != NULL) ? \ GST_STR_NULL (GST_OBJECT_NAME (GST_OBJECT_PARENT(pad))) : \ "''" ) : "''", \ (pad != NULL) ? GST_STR_NULL (GST_OBJECT_NAME (pad)) : "''" /** * GST_FUNCTION: * * This macro should evaluate to the name of the current function and be should * be defined when configuring your project, as it is compiler dependant. If it * is not defined, some default value is used. It is used to provide debugging * output with the function name of the message. * * Note that this is different from G_STRFUNC as we do not want the full * function signature in C++ code. */ #ifndef GST_FUNCTION #if defined (__GNUC__) || (defined (_MSC_VER) && _MSC_VER >= 1300) # define GST_FUNCTION ((const char*) (__FUNCTION__)) #elif defined (__STDC__) && defined (__STDC_VERSION__) && __STDC_VERSION__ >= 199901L # define GST_FUNCTION ((const char*) (__func__)) #else # define GST_FUNCTION ((const char*) ("???")) #endif #endif /* ifndef GST_FUNCTION */ typedef struct _GstDebugMessage GstDebugMessage; /** * GstLogFunction: * @category: a #GstDebugCategory * @level: a #GstDebugLevel * @file: file name * @function: function name * @line: line number * @object: a #GObject * @message: the message * @data: user data for the log function * * Function prototype for a logging function that can be registered with * gst_debug_add_log_function(). * Use G_GNUC_NO_INSTRUMENT on that function. */ typedef void (*GstLogFunction) (GstDebugCategory * category, GstDebugLevel level, const gchar * file, const gchar * function, gint line, GObject * object, GstDebugMessage * message, gpointer data); /* FIXME 0.11: move this into private headers */ void _gst_debug_init (void); #ifdef GST_USING_PRINTF_EXTENSION /* not using G_GNUC_PRINTF, since gcc will choke on GST_PTR_FORMAT being %P */ void gst_debug_log (GstDebugCategory * category, GstDebugLevel level, const gchar * file, const gchar * function, gint line, GObject * object, const gchar * format, ...) G_GNUC_NO_INSTRUMENT; #else /* GST_USING_PRINTF_EXTENSION */ void gst_debug_log (GstDebugCategory * category, GstDebugLevel level, const gchar * file, const gchar * function, gint line, GObject * object, const gchar * format, ...) G_GNUC_PRINTF (7, 8) G_GNUC_NO_INSTRUMENT; #endif /* GST_USING_PRINTF_EXTENSION */ void gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level, const gchar * file, const gchar * function, gint line, GObject * object, const gchar * format, va_list args) G_GNUC_NO_INSTRUMENT; /* do not use this function, use the GST_DEBUG_CATEGORY_INIT macro */ GstDebugCategory *_gst_debug_category_new (const gchar * name, guint color, const gchar * description); /* do not use this function, use the GST_DEBUG_CATEGORY_GET macro */ GstDebugCategory *_gst_debug_get_category (const gchar *name); /* do not use this function, use the GST_CAT_MEMDUMP_* macros */ void _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file, const gchar * func, gint line, GObject * obj, const gchar * msg, const guint8 * data, guint length); /* we define this to avoid a compiler warning regarding a cast from a function * pointer to a void pointer * (see https://bugzilla.gnome.org/show_bug.cgi?id=309253) */ typedef void (* GstDebugFuncPtr) (void); /* do no use these functions, use the GST_DEBUG*_FUNCPTR macros */ void _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname); G_CONST_RETURN gchar * _gst_debug_nameof_funcptr (GstDebugFuncPtr func) G_GNUC_NO_INSTRUMENT; const gchar * gst_debug_message_get (GstDebugMessage * message); void gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level, const gchar * file, const gchar * function, gint line, GObject * object, GstDebugMessage * message, gpointer unused) G_GNUC_NO_INSTRUMENT; G_CONST_RETURN gchar * gst_debug_level_get_name (GstDebugLevel level); void gst_debug_add_log_function (GstLogFunction func, gpointer data); guint gst_debug_remove_log_function (GstLogFunction func); guint gst_debug_remove_log_function_by_data (gpointer data); void gst_debug_set_active (gboolean active); gboolean gst_debug_is_active (void); void gst_debug_set_colored (gboolean colored); gboolean gst_debug_is_colored (void); void gst_debug_set_default_threshold (GstDebugLevel level); GstDebugLevel gst_debug_get_default_threshold (void); void gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level); void gst_debug_unset_threshold_for_name (const gchar * name); void gst_debug_category_free (GstDebugCategory * category); void gst_debug_category_set_threshold (GstDebugCategory * category, GstDebugLevel level); void gst_debug_category_reset_threshold (GstDebugCategory * category); GstDebugLevel gst_debug_category_get_threshold (GstDebugCategory * category); G_CONST_RETURN gchar * gst_debug_category_get_name (GstDebugCategory * category); guint gst_debug_category_get_color (GstDebugCategory * category); G_CONST_RETURN gchar * gst_debug_category_get_description (GstDebugCategory * category); GSList * gst_debug_get_all_categories (void); gchar * gst_debug_construct_term_color (guint colorinfo); gint gst_debug_construct_win_color (guint colorinfo); #ifndef GST_DISABLE_GST_DEBUG /** * GST_DEBUG_CATEGORY: * @cat: the category * * Defines a GstDebugCategory variable. * This macro expands to nothing if debugging is disabled. */ #define GST_DEBUG_CATEGORY(cat) GstDebugCategory *cat = NULL /** * GST_DEBUG_CATEGORY_EXTERN: * @cat: the category * * Declares a GstDebugCategory variable as extern. Use in header files. * This macro expands to nothing if debugging is disabled. */ #define GST_DEBUG_CATEGORY_EXTERN(cat) extern GstDebugCategory *cat /** * GST_DEBUG_CATEGORY_STATIC: * @cat: the category * * Defines a static GstDebugCategory variable. * This macro expands to nothing if debugging is disabled. */ #define GST_DEBUG_CATEGORY_STATIC(cat) static GstDebugCategory *cat = NULL /** * GST_DEBUG_CATEGORY_INIT: * @cat: the category to initialize. * @name: the name of the category. * @color: the colors to use for a color representation or 0 for no color. * @description: optional description of the category. * * Initializes a new #GstDebugCategory with the given properties and set to * the default threshold. * * * * This macro expands to nothing if debugging is disabled. * * * When naming your category, please follow the following conventions to ensure * that the pattern matching for categories works as expected. It is not * earth-shattering if you don't follow these conventions, but it would be nice * for everyone. * * * If you define a category for a plugin or a feature of it, name the category * like the feature. So if you wanted to write a "filesrc" element, you would * name the category "filesrc". Use lowercase letters only. * If you define more than one category for the same element, append an * underscore and an identifier to your categories, like this: "filesrc_cache" * * * If you create a library or an application using debugging categories, use a * common prefix followed by an underscore for all your categories. GStreamer * uses the GST prefix so GStreamer categories look like "GST_STATES". Be sure * to include uppercase letters. * * */ #define GST_DEBUG_CATEGORY_INIT(cat,name,color,description) G_STMT_START{\ if (cat == NULL) \ cat = _gst_debug_category_new (name,color,description); \ }G_STMT_END /** * GST_DEBUG_CATEGORY_GET: * @cat: the category to initialize. * @name: log category name * * Lookup an exiting #GstDebugCategory by its @name and sets @cat. If category * is not found, but GST_CAT_DEFAULT is defined, that is assigned to @cat. * Otherwise cat will be NULL. * * |[ * GST_DEBUG_CATEGORY_STATIC (gst_myplugin_debug); * #define GST_CAT_DEFAULT gst_myplugin_debug * GST_DEBUG_CATEGORY_STATIC (GST_CAT_PERFORMANCE); * ... * GST_DEBUG_CATEGORY_INIT (gst_myplugin_debug, "myplugin", 0, "nice element"); * GST_DEBUG_CATEGORY_GET (GST_CAT_PERFORMANCE, "performance"); * ]| * * Since: 0.10.24 */ #ifdef GST_CAT_DEFAULT #define GST_DEBUG_CATEGORY_GET(cat,name) G_STMT_START{\ cat = _gst_debug_get_category (name); \ if (!cat) { \ cat = GST_CAT_DEFAULT; \ } \ }G_STMT_END #else #define GST_DEBUG_CATEGORY_GET(cat,name) G_STMT_START{\ cat = _gst_debug_get_category (name); \ }G_STMT_END #endif /** * GST_CAT_DEFAULT: * * Default gstreamer core debug log category. Please define your own. */ GST_EXPORT GstDebugCategory * GST_CAT_DEFAULT; /* this symbol may not be used */ extern gboolean __gst_debug_enabled; /* since 0.10.7, the min debug level, used for quickly discarding debug * messages that fall under the threshold. */ GST_EXPORT GstDebugLevel __gst_debug_min; /** * GST_CAT_LEVEL_LOG: * @cat: category to use * @level: the severity of the message * @object: the #GObject the message belongs to or NULL if none * @...: A printf-style message to output * * Outputs a debugging message. This is the most general macro for outputting * debugging messages. You will probably want to use one of the ones described * below. */ #ifdef G_HAVE_ISO_VARARGS #define GST_CAT_LEVEL_LOG(cat,level,object,...) G_STMT_START{ \ if (G_UNLIKELY (level <= __gst_debug_min)) { \ gst_debug_log ((cat), (level), __FILE__, GST_FUNCTION, __LINE__, \ (GObject *) (object), __VA_ARGS__); \ } \ }G_STMT_END #else /* G_HAVE_GNUC_VARARGS */ #ifdef G_HAVE_GNUC_VARARGS #define GST_CAT_LEVEL_LOG(cat,level,object,args...) G_STMT_START{ \ if (G_UNLIKELY (level <= __gst_debug_min)) { \ gst_debug_log ((cat), (level), __FILE__, GST_FUNCTION, __LINE__, \ (GObject *) (object), ##args ); \ } \ }G_STMT_END #else /* no variadic macros, use inline */ static inline void GST_CAT_LEVEL_LOG_valist (GstDebugCategory * cat, GstDebugLevel level, gpointer object, const char *format, va_list varargs) { if (G_UNLIKELY (level <= __gst_debug_min)) { gst_debug_log_valist (cat, level, "", "", 0, (GObject *) object, format, varargs); } } static inline void GST_CAT_LEVEL_LOG (GstDebugCategory * cat, GstDebugLevel level, gpointer object, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, level, object, format, varargs); va_end (varargs); } #endif #endif /* G_HAVE_ISO_VARARGS */ /* This one doesn't have varargs in the macro, so it's different than all the * other macros and hence in a separate block right here. Docs chunks are * with the other doc chunks below though. */ #define __GST_CAT_MEMDUMP_LOG(cat,object,msg,data,length) G_STMT_START{ \ if (G_UNLIKELY (GST_LEVEL_MEMDUMP <= __gst_debug_min)) { \ _gst_debug_dump_mem ((cat), __FILE__, GST_FUNCTION, __LINE__, \ (GObject *) (object), (msg), (data), (length)); \ } \ }G_STMT_END #define GST_CAT_MEMDUMP_OBJECT(cat,obj,msg,data,length) \ __GST_CAT_MEMDUMP_LOG(cat,obj,msg,data,length) #define GST_CAT_MEMDUMP(cat,msg,data,length) \ __GST_CAT_MEMDUMP_LOG(cat,NULL,msg,data,length) #define GST_MEMDUMP_OBJECT(obj,msg,data,length) \ __GST_CAT_MEMDUMP_LOG(GST_CAT_DEFAULT,obj,msg,data,length) #define GST_MEMDUMP(msg,data,length) \ __GST_CAT_MEMDUMP_LOG(GST_CAT_DEFAULT,NULL,msg,data,length) /** * GST_CAT_ERROR_OBJECT: * @cat: category to use * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output an error message belonging to the given object in the given category. */ /** * GST_CAT_WARNING_OBJECT: * @cat: category to use * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output a warning message belonging to the given object in the given category. */ /** * GST_CAT_INFO_OBJECT: * @cat: category to use * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output an informational message belonging to the given object in the given * category. */ /** * GST_CAT_DEBUG_OBJECT: * @cat: category to use * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output an debugging message belonging to the given object in the given category. */ /** * GST_CAT_LOG_OBJECT: * @cat: category to use * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output an logging message belonging to the given object in the given category. */ /** * GST_CAT_FIXME_OBJECT: * @cat: category to use * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output a fixme message belonging to the given object in the given category. * * Since: 0.10.23 */ /** * GST_CAT_TRACE_OBJECT: * @cat: category to use * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output a tracing message belonging to the given object in the given * category. * * Since: 0.10.30 */ /** * GST_CAT_MEMDUMP_OBJECT: * @cat: category to use * @obj: the #GObject the message belongs to * @msg: message string to log with the data * @data: pointer to the data to output * @length: length of the data to output * * Output a hexdump of @data relating to the given object in the given * category. * * Since: 0.10.23 */ /** * GST_CAT_ERROR: * @cat: category to use * @...: printf-style message to output * * Output an error message in the given category. */ /** * GST_CAT_WARNING: * @cat: category to use * @...: printf-style message to output * * Output an warning message in the given category. */ /** * GST_CAT_INFO: * @cat: category to use * @...: printf-style message to output * * Output an informational message in the given category. */ /** * GST_CAT_DEBUG: * @cat: category to use * @...: printf-style message to output * * Output an debugging message in the given category. */ /** * GST_CAT_LOG: * @cat: category to use * @...: printf-style message to output * * Output an logging message in the given category. */ /** * GST_CAT_FIXME: * @cat: category to use * @...: printf-style message to output * * Output an fixme message in the given category. * * Since: 0.10.23 */ /** * GST_CAT_TRACE: * @cat: category to use * @...: printf-style message to output * * Output a tracing message in the given category. * * Since: 0.10.30 */ /** * GST_CAT_MEMDUMP: * @cat: category to use * @msg: message string to log with the data * @data: pointer to the data to output * @length: length of the data to output * * Output a hexdump of @data in the given category. * * Since: 0.10.23 */ /** * GST_ERROR_OBJECT: * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output an error message belonging to the given object in the default category. */ /** * GST_WARNING_OBJECT: * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output a warning message belonging to the given object in the default category. */ /** * GST_INFO_OBJECT: * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output an informational message belonging to the given object in the default * category. */ /** * GST_DEBUG_OBJECT: * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output a debugging message belonging to the given object in the default * category. */ /** * GST_LOG_OBJECT: * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output a logging message belonging to the given object in the default category. */ /** * GST_FIXME_OBJECT: * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output a fixme message belonging to the given object in the default category. * * Since: 0.10.23 */ /** * GST_TRACE_OBJECT: * @obj: the #GObject the message belongs to * @...: printf-style message to output * * Output a tracing message belonging to the given object in the default category. * * Since: 0.10.30 */ /** * GST_MEMDUMP_OBJECT: * @obj: the #GObject the message belongs to * @msg: message string to log with the data * @data: pointer to the data to output * @length: length of the data to output * * Output a logging message belonging to the given object in the default category. * * Since: 0.10.23 */ /** * GST_ERROR: * @...: printf-style message to output * * Output an error message in the default category. */ /** * GST_WARNING: * @...: printf-style message to output * * Output a warning message in the default category. */ /** * GST_INFO: * @...: printf-style message to output * * Output an informational message in the default category. */ /** * GST_DEBUG: * @...: printf-style message to output * * Output a debugging message in the default category. */ /** * GST_LOG: * @...: printf-style message to output * * Output a logging message in the default category. */ /** * GST_FIXME: * @...: printf-style message to output * * Output a fixme message in the default category. * * Since: 0.10.23 */ /** * GST_TRACE: * @...: printf-style message to output * * Output a tracing message in the default category. * * Since: 0.10.30 */ /** * GST_MEMDUMP: * @msg: message string to log with the data * @data: pointer to the data to output * @length: length of the data to output * * Output a hexdump of @data. * * Since: 0.10.23 */ #ifdef G_HAVE_ISO_VARARGS #define GST_CAT_ERROR_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR, obj, __VA_ARGS__) #define GST_CAT_WARNING_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, obj, __VA_ARGS__) #define GST_CAT_INFO_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO, obj, __VA_ARGS__) #define GST_CAT_DEBUG_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG, obj, __VA_ARGS__) #define GST_CAT_LOG_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG, obj, __VA_ARGS__) #define GST_CAT_FIXME_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME, obj, __VA_ARGS__) #define GST_CAT_TRACE_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE, obj, __VA_ARGS__) #define GST_CAT_ERROR(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR, NULL, __VA_ARGS__) #define GST_CAT_WARNING(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, NULL, __VA_ARGS__) #define GST_CAT_INFO(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO, NULL, __VA_ARGS__) #define GST_CAT_DEBUG(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG, NULL, __VA_ARGS__) #define GST_CAT_LOG(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG, NULL, __VA_ARGS__) #define GST_CAT_FIXME(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME, NULL, __VA_ARGS__) #define GST_CAT_TRACE(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE, NULL, __VA_ARGS__) #define GST_ERROR_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR, obj, __VA_ARGS__) #define GST_WARNING_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj, __VA_ARGS__) #define GST_INFO_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO, obj, __VA_ARGS__) #define GST_DEBUG_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, obj, __VA_ARGS__) #define GST_LOG_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG, obj, __VA_ARGS__) #define GST_FIXME_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME, obj, __VA_ARGS__) #define GST_TRACE_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE, obj, __VA_ARGS__) #define GST_ERROR(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR, NULL, __VA_ARGS__) #define GST_WARNING(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, __VA_ARGS__) #define GST_INFO(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO, NULL, __VA_ARGS__) #define GST_DEBUG(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, NULL, __VA_ARGS__) #define GST_LOG(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG, NULL, __VA_ARGS__) #define GST_FIXME(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME, NULL, __VA_ARGS__) #define GST_TRACE(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE, NULL, __VA_ARGS__) #else #ifdef G_HAVE_GNUC_VARARGS #define GST_CAT_ERROR_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR, obj, ##args ) #define GST_CAT_WARNING_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, obj, ##args ) #define GST_CAT_INFO_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO, obj, ##args ) #define GST_CAT_DEBUG_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG, obj, ##args ) #define GST_CAT_LOG_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG, obj, ##args ) #define GST_CAT_FIXME_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME, obj, ##args ) #define GST_CAT_TRACE_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE, obj, ##args ) #define GST_CAT_ERROR(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR, NULL, ##args ) #define GST_CAT_WARNING(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, NULL, ##args ) #define GST_CAT_INFO(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO, NULL, ##args ) #define GST_CAT_DEBUG(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG, NULL, ##args ) #define GST_CAT_LOG(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG, NULL, ##args ) #define GST_CAT_FIXME(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME, NULL, ##args ) #define GST_CAT_TRACE(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE, NULL, ##args ) #define GST_ERROR_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR, obj, ##args ) #define GST_WARNING_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj, ##args ) #define GST_INFO_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO, obj, ##args ) #define GST_DEBUG_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, obj, ##args ) #define GST_LOG_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG, obj, ##args ) #define GST_FIXME_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME, obj, ##args ) #define GST_TRACE_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE, obj, ##args ) #define GST_ERROR(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR, NULL, ##args ) #define GST_WARNING(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, ##args ) #define GST_INFO(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO, NULL, ##args ) #define GST_DEBUG(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, NULL, ##args ) #define GST_LOG(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG, NULL, ##args ) #define GST_FIXME(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME, NULL, ##args ) #define GST_TRACE(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE, NULL, ##args ) #else /* no variadic macros, use inline */ static inline void GST_CAT_ERROR_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_ERROR, obj, format, varargs); va_end (varargs); } static inline void GST_CAT_WARNING_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_WARNING, obj, format, varargs); va_end (varargs); } static inline void GST_CAT_INFO_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_INFO, obj, format, varargs); va_end (varargs); } static inline void GST_CAT_DEBUG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_DEBUG, obj, format, varargs); va_end (varargs); } static inline void GST_CAT_LOG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_LOG, obj, format, varargs); va_end (varargs); } static inline void GST_CAT_FIXME_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_FIXME, obj, format, varargs); va_end (varargs); } static inline void GST_CAT_TRACE_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_TRACE, obj, format, varargs); va_end (varargs); } static inline void GST_CAT_ERROR (GstDebugCategory * cat, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_ERROR, NULL, format, varargs); va_end (varargs); } static inline void GST_CAT_WARNING (GstDebugCategory * cat, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_WARNING, NULL, format, varargs); va_end (varargs); } static inline void GST_CAT_INFO (GstDebugCategory * cat, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_INFO, NULL, format, varargs); va_end (varargs); } static inline void GST_CAT_DEBUG (GstDebugCategory * cat, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_DEBUG, NULL, format, varargs); va_end (varargs); } static inline void GST_CAT_LOG (GstDebugCategory * cat, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_LOG, NULL, format, varargs); va_end (varargs); } static inline void GST_CAT_FIXME (GstDebugCategory * cat, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_FIXME, NULL, format, varargs); va_end (varargs); } static inline void GST_CAT_TRACE (GstDebugCategory * cat, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_TRACE, NULL, format, varargs); va_end (varargs); } static inline void GST_ERROR_OBJECT (gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_ERROR, obj, format, varargs); va_end (varargs); } static inline void GST_WARNING_OBJECT (gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj, format, varargs); va_end (varargs); } static inline void GST_INFO_OBJECT (gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_INFO, obj, format, varargs); va_end (varargs); } static inline void GST_DEBUG_OBJECT (gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, obj, format, varargs); va_end (varargs); } static inline void GST_LOG_OBJECT (gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_LOG, obj, format, varargs); va_end (varargs); } static inline void GST_FIXME_OBJECT (gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_FIXME, obj, format, varargs); va_end (varargs); } static inline void GST_TRACE_OBJECT (gpointer obj, const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_TRACE, obj, format, varargs); va_end (varargs); } static inline void GST_ERROR (const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_ERROR, NULL, format, varargs); va_end (varargs); } static inline void GST_WARNING (const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, format, varargs); va_end (varargs); } static inline void GST_INFO (const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_INFO, NULL, format, varargs); va_end (varargs); } static inline void GST_DEBUG (const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, NULL, format, varargs); va_end (varargs); } static inline void GST_LOG (const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_LOG, NULL, format, varargs); va_end (varargs); } static inline void GST_FIXME (const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_FIXME, NULL, format, varargs); va_end (varargs); } static inline void GST_TRACE (const char *format, ...) { va_list varargs; va_start (varargs, format); GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_TRACE, NULL, format, varargs); va_end (varargs); } #endif #endif /********** function pointer stuff **********/ /** * GST_DEBUG_REGISTER_FUNCPTR: * @ptr: pointer to the function to register * * Register a pointer to a function with its name, so it can later be used by * GST_DEBUG_FUNCPTR_NAME(). * * Use this variant of #GST_DEBUG_FUNCPTR if you do not need to use @ptr. * * Since: 0.10.26 */ #define GST_DEBUG_REGISTER_FUNCPTR(ptr) \ _gst_debug_register_funcptr((GstDebugFuncPtr)(ptr), #ptr) /** * GST_DEBUG_FUNCPTR: * @ptr: pointer to the function to register * * Register a pointer to a function with its name, so it can later be used by * GST_DEBUG_FUNCPTR_NAME(). * * Returns: the value passed to @ptr. */ #define GST_DEBUG_FUNCPTR(ptr) \ (_gst_debug_register_funcptr((GstDebugFuncPtr)(ptr), #ptr) , ptr) /** * GST_DEBUG_FUNCPTR_NAME: * @ptr: address of the function of which to look up the name * * Retrieves the name of the function, if it was previously registered with * GST_DEBUG_FUNCPTR(). If not, it returns a description of the pointer. * * This macro returns a constant string which must not be modified or * freed by the caller. */ #define GST_DEBUG_FUNCPTR_NAME(ptr) \ _gst_debug_nameof_funcptr((GstDebugFuncPtr)ptr) #else /* GST_DISABLE_GST_DEBUG */ #ifndef GST_INFO_C #if defined(__GNUC__) && __GNUC__ >= 3 # pragma GCC poison gst_debug_log # pragma GCC poison gst_debug_log_valist # pragma GCC poison _gst_debug_category_new #endif #define __gst_debug_min GST_LEVEL_NONE #define _gst_debug_init() G_STMT_START{ }G_STMT_END #define gst_debug_set_default_threshold(level) G_STMT_START{ }G_STMT_END #define gst_debug_get_default_threshold() (GST_LEVEL_NONE) #define gst_debug_level_get_name(level) ("NONE") #define gst_debug_message_get(message) ("") #define gst_debug_add_log_function(func,data) G_STMT_START{ }G_STMT_END #define gst_debug_set_active(active) G_STMT_START{ }G_STMT_END #define gst_debug_is_active() (FALSE) #define gst_debug_set_colored(colored) G_STMT_START{ }G_STMT_END #define gst_debug_is_colored() (FALSE) #define gst_debug_set_default_threshold(level) G_STMT_START{ }G_STMT_END #define gst_debug_get_default_threshold() (GST_LEVEL_NONE) #define gst_debug_set_threshold_for_name(name,level) G_STMT_START{ }G_STMT_END #define gst_debug_unset_threshold_for_name(name) G_STMT_START{ }G_STMT_END /* we are using dummy function prototypes here to eat ';' as these macros are * used outside of functions */ #define GST_DEBUG_CATEGORY(var) void _gst_debug_dummy_##var (void) #define GST_DEBUG_CATEGORY_EXTERN(var) void _gst_debug_dummy_extern_##var (void) #define GST_DEBUG_CATEGORY_STATIC(var) void _gst_debug_dummy_static_##var (void) #define GST_DEBUG_CATEGORY_INIT(var,name,color,desc) G_STMT_START{ }G_STMT_END #define GST_DEBUG_CATEGORY_GET(var,name) G_STMT_START{ }G_STMT_END #define gst_debug_category_free(category) G_STMT_START{ }G_STMT_END #define gst_debug_category_set_threshold(category,level) G_STMT_START{ }G_STMT_END #define gst_debug_category_reset_threshold(category) G_STMT_START{ }G_STMT_END #define gst_debug_category_get_threshold(category) (GST_LEVEL_NONE) #define gst_debug_category_get_name(cat) ("") #define gst_debug_category_get_color(cat) (0) #define gst_debug_category_get_description(cat) ("") #define gst_debug_get_all_categories() (NULL) #define gst_debug_construct_term_color(colorinfo) (g_strdup ("00")) #define gst_debug_construct_win_color(colorinfo) (0) #endif /* !GST_INFO_C */ #ifdef G_HAVE_ISO_VARARGS #define GST_CAT_LEVEL_LOG(cat,level,...) G_STMT_START{ }G_STMT_END #define GST_CAT_ERROR_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_CAT_WARNING_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_CAT_INFO_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_CAT_DEBUG_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_CAT_LOG_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_CAT_FIXME_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_CAT_ERROR(...) G_STMT_START{ }G_STMT_END #define GST_CAT_WARNING(...) G_STMT_START{ }G_STMT_END #define GST_CAT_INFO(...) G_STMT_START{ }G_STMT_END #define GST_CAT_DEBUG(...) G_STMT_START{ }G_STMT_END #define GST_CAT_LOG(...) G_STMT_START{ }G_STMT_END #define GST_CAT_FIXME(...) G_STMT_START{ }G_STMT_END #define GST_ERROR_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_WARNING_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_INFO_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_DEBUG_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_LOG_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_FIXME_OBJECT(...) G_STMT_START{ }G_STMT_END #define GST_ERROR(...) G_STMT_START{ }G_STMT_END #define GST_WARNING(...) G_STMT_START{ }G_STMT_END #define GST_INFO(...) G_STMT_START{ }G_STMT_END #define GST_DEBUG(...) G_STMT_START{ }G_STMT_END #define GST_LOG(...) G_STMT_START{ }G_STMT_END #define GST_FIXME(...) G_STMT_START{ }G_STMT_END #else /* !G_HAVE_ISO_VARARGS */ #ifdef G_HAVE_GNUC_VARARGS #define GST_CAT_LEVEL_LOG(cat,level,args...) G_STMT_START{ }G_STMT_END #define GST_CAT_ERROR_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_WARNING_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_INFO_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_DEBUG_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_LOG_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_FIXME_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_ERROR(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_WARNING(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_INFO(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_DEBUG(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_LOG(args...) G_STMT_START{ }G_STMT_END #define GST_CAT_FIXME(args...) G_STMT_START{ }G_STMT_END #define GST_ERROR_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_WARNING_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_INFO_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_DEBUG_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_LOG_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_FIXME_OBJECT(args...) G_STMT_START{ }G_STMT_END #define GST_ERROR(args...) G_STMT_START{ }G_STMT_END #define GST_WARNING(args...) G_STMT_START{ }G_STMT_END #define GST_INFO(args...) G_STMT_START{ }G_STMT_END #define GST_DEBUG(args...) G_STMT_START{ }G_STMT_END #define GST_LOG(args...) G_STMT_START{ }G_STMT_END #define GST_FIXME(args...) G_STMT_START{ }G_STMT_END #else /* !G_HAVE_GNUC_VARARGS */ static inline void GST_CAT_LEVEL_LOG_valist (GstDebugCategory * cat, GstDebugLevel level, gpointer object, const char *format, va_list varargs) { } static inline void GST_CAT_ERROR_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { } static inline void GST_CAT_WARNING_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { } static inline void GST_CAT_INFO_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { } static inline void GST_CAT_DEBUG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { } static inline void GST_CAT_LOG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { } static inline void GST_CAT_FIXME_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format, ...) { } static inline void GST_CAT_ERROR (GstDebugCategory * cat, const char *format, ...) { } static inline void GST_CAT_WARNING (GstDebugCategory * cat, const char *format, ...) { } static inline void GST_CAT_INFO (GstDebugCategory * cat, const char *format, ...) { } static inline void GST_CAT_DEBUG (GstDebugCategory * cat, const char *format, ...) { } static inline void GST_CAT_LOG (GstDebugCategory * cat, const char *format, ...) { } static inline void GST_CAT_FIXME (GstDebugCategory * cat, const char *format, ...) { } static inline void GST_ERROR_OBJECT (gpointer obj, const char *format, ...) { } static inline void GST_WARNING_OBJECT (gpointer obj, const char *format, ...) { } static inline void GST_INFO_OBJECT (gpointer obj, const char *format, ...) { } static inline void GST_DEBUG_OBJECT (gpointer obj, const char *format, ...) { } static inline void GST_LOG_OBJECT (gpointer obj, const char *format, ...) { } static inline void GST_FIXME_OBJECT (gpointer obj, const char *format, ...) { } static inline void GST_ERROR (const char *format, ...) { } static inline void GST_WARNING (const char *format, ...) { } static inline void GST_INFO (const char *format, ...) { } static inline void GST_DEBUG (const char *format, ...) { } static inline void GST_LOG (const char *format, ...) { } static inline void GST_FIXME (const char *format, ...) { } #endif /* G_HAVE_GNUC_VARARGS */ #endif /* G_HAVE_ISO_VARARGS */ #define GST_DEBUG_REGISTER_FUNCPTR(ptr) G_STMT_START{ }G_STMT_END #define GST_DEBUG_FUNCPTR(ptr) (ptr) #define GST_DEBUG_FUNCPTR_NAME(ptr) (g_strdup_printf ("%p", ptr)) #define GST_CAT_MEMDUMP_OBJECT(cat,obj,msg,data,length) G_STMT_START{ }G_STMT_END #define GST_CAT_MEMDUMP(cat,msg,data,length) G_STMT_START{ }G_STMT_END #define GST_MEMDUMP_OBJECT(obj,msg,data,length) G_STMT_START{ }G_STMT_END #define GST_MEMDUMP(msg,data,length) G_STMT_START{ }G_STMT_END #endif /* GST_DISABLE_GST_DEBUG */ void gst_debug_print_stack_trace (void); G_END_DECLS #endif /* __GSTINFO_H__ */