/* GStreamer * * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * * gstinterface.c: Interface functions * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:gstimplementsinterface * @short_description: Core interface implemented by #GstElement instances that * allows runtime querying of interface availability * @see_also: #GstElement * * Provides interface functionality on per instance basis and not per class * basis, which is the case for gobject. */ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include "gst_private.h" #include "gstinterface.h" static void gst_implements_interface_class_init (GstImplementsInterfaceClass * ifklass); static gboolean gst_implements_interface_supported_default (GstImplementsInterface * iface, GType iface_type); GType gst_implements_interface_get_type (void) { static volatile gsize gst_interface_type = 0; if (g_once_init_enter (&gst_interface_type)) { GType _type; static const GTypeInfo gst_interface_info = { sizeof (GstImplementsInterfaceClass), (GBaseInitFunc) gst_implements_interface_class_init, NULL, NULL, NULL, NULL, 0, 0, NULL, NULL }; _type = g_type_register_static (G_TYPE_INTERFACE, "GstImplementsInterface", &gst_interface_info, 0); g_type_interface_add_prerequisite (_type, GST_TYPE_ELEMENT); g_once_init_leave (&gst_interface_type, _type); } return gst_interface_type; } static void gst_implements_interface_class_init (GstImplementsInterfaceClass * klass) { klass->supported = gst_implements_interface_supported_default; } static gboolean gst_implements_interface_supported_default (GstImplementsInterface * interface, GType iface_type) { /* Well, if someone didn't set the virtual function, * then something is clearly wrong. So big no-no here */ return FALSE; } /** * gst_element_implements_interface: * @element: #GstElement to check for the implementation of the interface * @iface_type: (final) type of the interface which we want to be implemented * * Test whether the given element implements a certain interface of type * iface_type, and test whether it is supported for this specific instance. * * Returns: whether or not the element implements the interface. */ gboolean gst_element_implements_interface (GstElement * element, GType iface_type) { g_return_val_if_fail (GST_IS_ELEMENT (element), FALSE); if (G_TYPE_CHECK_INSTANCE_TYPE (G_OBJECT (element), iface_type)) { GstImplementsInterface *iface; GstImplementsInterfaceClass *ifclass; iface = G_TYPE_CHECK_INSTANCE_CAST (G_OBJECT (element), iface_type, GstImplementsInterface); ifclass = GST_IMPLEMENTS_INTERFACE_GET_CLASS (iface); /* element implements iface_type but not GstImplementsInterface, so * just assume the other interface is implemented unconditionally */ if (ifclass == NULL) return TRUE; if (ifclass->supported != NULL && ifclass->supported (iface, iface_type) == TRUE) { return TRUE; } } return FALSE; } /** * gst_implements_interface_cast: * @from: the object (any sort) from which to cast to the interface * @type: the interface type to cast to * * cast a given object to an interface type, and check whether this * interface is supported for this specific instance. * * Returns: (transfer none): a gpointer to the interface type */ gpointer gst_implements_interface_cast (gpointer from, GType iface_type) { GstImplementsInterface *iface; /* check cast, give warning+fail if it's invalid */ if (!(iface = G_TYPE_CHECK_INSTANCE_CAST (from, iface_type, GstImplementsInterface))) { return NULL; } /* if we're an element, take care that this interface * is actually implemented */ if (GST_IS_ELEMENT (from)) { g_return_val_if_fail (gst_element_implements_interface (GST_ELEMENT (from), iface_type), NULL); } return iface; } /** * gst_implements_interface_check: * @from: the object (any sort) from which to check from for the interface * @type: the interface type to check for * * check a given object for an interface implementation, and check * whether this interface is supported for this specific instance. * * Returns: whether or not the object implements the given interface */ gboolean gst_implements_interface_check (gpointer from, GType type) { /* check cast, return FALSE if it fails, don't give a warning... */ if (!G_TYPE_CHECK_INSTANCE_TYPE (from, type)) { return FALSE; } /* now, if we're an element (or derivative), is this thing * actually implemented for real? */ if (GST_IS_ELEMENT (from)) { if (!gst_element_implements_interface (GST_ELEMENT (from), type)) { return FALSE; } } return TRUE; }