/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * * gstpipeline.h: Header for GstPipeline element * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GST_PIPELINE_H__ #define __GST_PIPELINE_H__ #include G_BEGIN_DECLS #define GST_TYPE_PIPELINE (gst_pipeline_get_type ()) #define GST_PIPELINE(obj) (G_TYPE_CHECK_INSTANCE_CAST ((obj), GST_TYPE_PIPELINE, GstPipeline)) #define GST_IS_PIPELINE(obj) (G_TYPE_CHECK_INSTANCE_TYPE ((obj), GST_TYPE_PIPELINE)) #define GST_PIPELINE_CLASS(klass) (G_TYPE_CHECK_CLASS_CAST ((klass), GST_TYPE_PIPELINE, GstPipelineClass)) #define GST_IS_PIPELINE_CLASS(klass) (G_TYPE_CHECK_CLASS_TYPE ((klass), GST_TYPE_PIPELINE)) #define GST_PIPELINE_GET_CLASS(obj) (G_TYPE_INSTANCE_GET_CLASS ((obj), GST_TYPE_PIPELINE, GstPipelineClass)) #define GST_PIPELINE_CAST(obj) ((GstPipeline*)(obj)) typedef struct _GstPipeline GstPipeline; typedef struct _GstPipelineClass GstPipelineClass; typedef struct _GstPipelinePrivate GstPipelinePrivate; /** * GstPipelineFlags: * @GST_PIPELINE_FLAG_FIXED_CLOCK: this pipeline works with a fixed clock * @GST_PIPELINE_FLAG_LAST: offset to define more flags * * Pipeline flags */ typedef enum { GST_PIPELINE_FLAG_FIXED_CLOCK = (GST_BIN_FLAG_LAST << 0), /* padding */ GST_PIPELINE_FLAG_LAST = (GST_BIN_FLAG_LAST << 4) } GstPipelineFlags; /** * GstPipeline: * @fixed_clock: The fixed clock of the pipeline, used when * GST_PIPELINE_FLAG_FIXED_CLOCK is set. * @stream_time: The stream time of the pipeline. A better name for this * property would be the running_time, the total time spent in the * PLAYING state without being flushed. (deprecated, use the start_time * on GstElement). * @delay: Extra delay added to base_time to compensate for computing delays * when setting elements to PLAYING. * * The #GstPipeline structure. */ struct _GstPipeline { GstBin bin; /*< public >*/ /* with LOCK */ GstClock *fixed_clock; GstClockTime stream_time; GstClockTime delay; /*< private >*/ GstPipelinePrivate *priv; gpointer _gst_reserved[GST_PADDING-1]; }; struct _GstPipelineClass { GstBinClass parent_class; /*< private >*/ gpointer _gst_reserved[GST_PADDING]; }; GType gst_pipeline_get_type (void); GstElement* gst_pipeline_new (const gchar *name); GstBus* gst_pipeline_get_bus (GstPipeline *pipeline); #ifndef GST_DISABLE_DEPRECATED void gst_pipeline_set_new_stream_time (GstPipeline *pipeline, GstClockTime time); GstClockTime gst_pipeline_get_last_stream_time (GstPipeline *pipeline); #endif void gst_pipeline_use_clock (GstPipeline *pipeline, GstClock *clock); gboolean gst_pipeline_set_clock (GstPipeline *pipeline, GstClock *clock); GstClock* gst_pipeline_get_clock (GstPipeline *pipeline); void gst_pipeline_auto_clock (GstPipeline *pipeline); void gst_pipeline_set_delay (GstPipeline *pipeline, GstClockTime delay); GstClockTime gst_pipeline_get_delay (GstPipeline *pipeline); void gst_pipeline_set_auto_flush_bus (GstPipeline *pipeline, gboolean auto_flush); gboolean gst_pipeline_get_auto_flush_bus (GstPipeline *pipeline); G_END_DECLS #endif /* __GST_PIPELINE_H__ */