/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * 2005 Wim Taymans * * gstquery.c: GstQueryType registration and Query parsing/creation * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:gstquery * @short_description: Dynamically register new query types. Provide functions * to create queries, and to set and parse values in them. * @see_also: #GstPad, #GstElement * * GstQuery functions are used to register new query types to the gstreamer * core and use them. * Queries can be performed on pads (gst_pad_query()) and elements * (gst_element_query()). Please note that some queries might need a running * pipeline to work. * * Queries can be created using the gst_query_new_*() functions. * Query values can be set using gst_query_set_*(), and parsed using * gst_query_parse_*() helpers. * * The following example shows how to query the duration of a pipeline: * * * Query duration on a pipeline * * GstQuery *query; * gboolean res; * query = gst_query_new_duration (GST_FORMAT_TIME); * res = gst_element_query (pipeline, query); * if (res) { * gint64 duration; * gst_query_parse_duration (query, NULL, &duration); * g_print ("duration = %"GST_TIME_FORMAT, GST_TIME_ARGS (duration)); * } * else { * g_print ("duration query failed..."); * } * gst_query_unref (query); * * * * Last reviewed on 2006-02-14 (0.10.4) */ #include "gst_private.h" #include "gstinfo.h" #include "gstquery.h" #include "gstvalue.h" #include "gstenumtypes.h" #include "gstquark.h" #include "gsturi.h" GST_DEBUG_CATEGORY_STATIC (gst_query_debug); #define GST_CAT_DEFAULT gst_query_debug static void gst_query_finalize (GstQuery * query); static GstQuery *_gst_query_copy (GstQuery * query); static GStaticMutex mutex = G_STATIC_MUTEX_INIT; static GList *_gst_queries = NULL; static GHashTable *_nick_to_query = NULL; static GHashTable *_query_type_to_nick = NULL; static guint32 _n_values = 1; /* we start from 1 because 0 reserved for NONE */ static GstMiniObjectClass *parent_class = NULL; static GstQueryTypeDefinition standard_definitions[] = { {GST_QUERY_POSITION, "position", "Current position", 0}, {GST_QUERY_DURATION, "duration", "Total duration", 0}, {GST_QUERY_LATENCY, "latency", "Latency", 0}, {GST_QUERY_JITTER, "jitter", "Jitter", 0}, {GST_QUERY_RATE, "rate", "Configured rate 1000000 = 1", 0}, {GST_QUERY_SEEKING, "seeking", "Seeking capabilities and parameters", 0}, {GST_QUERY_SEGMENT, "segment", "currently configured segment", 0}, {GST_QUERY_CONVERT, "convert", "Converting between formats", 0}, {GST_QUERY_FORMATS, "formats", "Supported formats for conversion", 0}, {GST_QUERY_BUFFERING, "buffering", "Buffering status", 0}, {GST_QUERY_CUSTOM, "custom", "Custom query", 0}, {GST_QUERY_URI, "uri", "URI of the source or sink", 0}, {GST_QUERY_BUFFERS, "buffers", "Minimum buffer requirements", 0}, {GST_QUERY_NONE, NULL, NULL, 0} }; void _gst_query_initialize (void) { GstQueryTypeDefinition *standards = standard_definitions; GST_CAT_INFO (GST_CAT_GST_INIT, "init queries"); GST_DEBUG_CATEGORY_INIT (gst_query_debug, "query", 0, "query system"); g_static_mutex_lock (&mutex); if (_nick_to_query == NULL) { _nick_to_query = g_hash_table_new (g_str_hash, g_str_equal); _query_type_to_nick = g_hash_table_new (NULL, NULL); } while (standards->nick) { standards->quark = g_quark_from_static_string (standards->nick); g_hash_table_insert (_nick_to_query, (gpointer) standards->nick, standards); g_hash_table_insert (_query_type_to_nick, GINT_TO_POINTER (standards->value), standards); _gst_queries = g_list_append (_gst_queries, standards); standards++; _n_values++; } g_static_mutex_unlock (&mutex); g_type_class_ref (gst_query_get_type ()); } /** * gst_query_type_get_name: * @query: the query type * * Get a printable name for the given query type. Do not modify or free. * * Returns: a reference to the static name of the query. */ const gchar * gst_query_type_get_name (GstQueryType query) { const GstQueryTypeDefinition *def; def = gst_query_type_get_details (query); return def->nick; } /** * gst_query_type_to_quark: * @query: the query type * * Get the unique quark for the given query type. * * Returns: the quark associated with the query type */ GQuark gst_query_type_to_quark (GstQueryType query) { const GstQueryTypeDefinition *def; def = gst_query_type_get_details (query); return def->quark; } G_DEFINE_TYPE (GstQuery, gst_query, GST_TYPE_MINI_OBJECT); static void gst_query_class_init (GstQueryClass * klass) { parent_class = g_type_class_peek_parent (klass); klass->mini_object_class.copy = (GstMiniObjectCopyFunction) _gst_query_copy; klass->mini_object_class.finalize = (GstMiniObjectFinalizeFunction) gst_query_finalize; } static void gst_query_init (GstQuery * query) { } static void gst_query_finalize (GstQuery * query) { g_return_if_fail (query != NULL); if (query->structure) { gst_structure_set_parent_refcount (query->structure, NULL); gst_structure_free (query->structure); } /* GST_MINI_OBJECT_CLASS (parent_class)->finalize (GST_MINI_OBJECT (query)); */ } static GstQuery * _gst_query_copy (GstQuery * query) { GstQuery *copy; copy = (GstQuery *) gst_mini_object_new (GST_TYPE_QUERY); copy->type = query->type; if (query->structure) { copy->structure = gst_structure_copy (query->structure); gst_structure_set_parent_refcount (copy->structure, &query->mini_object.refcount); } return copy; } /** * gst_query_type_register: * @nick: The nick of the new query * @description: The description of the new query * * Create a new GstQueryType based on the nick or return an * already registered query with that nick * * Returns: A new GstQueryType or an already registered query * with the same nick. */ GstQueryType gst_query_type_register (const gchar * nick, const gchar * description) { GstQueryTypeDefinition *query; GstQueryType lookup; g_return_val_if_fail (nick != NULL, GST_QUERY_NONE); g_return_val_if_fail (description != NULL, GST_QUERY_NONE); lookup = gst_query_type_get_by_nick (nick); if (lookup != GST_QUERY_NONE) return lookup; query = g_slice_new (GstQueryTypeDefinition); query->value = (GstQueryType) _n_values; query->nick = g_strdup (nick); query->description = g_strdup (description); query->quark = g_quark_from_static_string (query->nick); g_static_mutex_lock (&mutex); g_hash_table_insert (_nick_to_query, (gpointer) query->nick, query); g_hash_table_insert (_query_type_to_nick, GINT_TO_POINTER (query->value), query); _gst_queries = g_list_append (_gst_queries, query); _n_values++; g_static_mutex_unlock (&mutex); return query->value; } /** * gst_query_type_get_by_nick: * @nick: The nick of the query * * Get the query type registered with @nick. * * Returns: The query registered with @nick or #GST_QUERY_NONE * if the query was not registered. */ GstQueryType gst_query_type_get_by_nick (const gchar * nick) { GstQueryTypeDefinition *query; g_return_val_if_fail (nick != NULL, GST_QUERY_NONE); g_static_mutex_lock (&mutex); query = g_hash_table_lookup (_nick_to_query, nick); g_static_mutex_unlock (&mutex); if (query != NULL) return query->value; else return GST_QUERY_NONE; } /** * gst_query_types_contains: * @types: The query array to search * @type: the #GstQueryType to find * * See if the given #GstQueryType is inside the @types query types array. * * Returns: TRUE if the type is found inside the array */ gboolean gst_query_types_contains (const GstQueryType * types, GstQueryType type) { if (!types) return FALSE; while (*types) { if (*types == type) return TRUE; types++; } return FALSE; } /** * gst_query_type_get_details: * @type: a #GstQueryType * * Get details about the given #GstQueryType. * * Returns: The #GstQueryTypeDefinition for @type or NULL on failure. */ const GstQueryTypeDefinition * gst_query_type_get_details (GstQueryType type) { const GstQueryTypeDefinition *result; g_static_mutex_lock (&mutex); result = g_hash_table_lookup (_query_type_to_nick, GINT_TO_POINTER (type)); g_static_mutex_unlock (&mutex); return result; } /** * gst_query_type_iterate_definitions: * * Get a #GstIterator of all the registered query types. The definitions * iterated over are read only. * * Free-function: gst_iterator_free * * Returns: (transfer full): a #GstIterator of #GstQueryTypeDefinition. */ GstIterator * gst_query_type_iterate_definitions (void) { GstIterator *result; g_static_mutex_lock (&mutex); /* FIXME: register a boxed type for GstQueryTypeDefinition */ result = gst_iterator_new_list (G_TYPE_POINTER, g_static_mutex_get_mutex (&mutex), &_n_values, &_gst_queries, NULL, NULL, NULL); g_static_mutex_unlock (&mutex); return result; } static GstQuery * gst_query_new (GstQueryType type, GstStructure * structure) { GstQuery *query; query = (GstQuery *) gst_mini_object_new (GST_TYPE_QUERY); GST_DEBUG ("creating new query %p %s", query, gst_query_type_get_name (type)); query->type = type; if (structure) { query->structure = structure; gst_structure_set_parent_refcount (query->structure, &query->mini_object.refcount); } else { query->structure = NULL; } return query; } /** * gst_query_new_position: * @format: the default #GstFormat for the new query * * Constructs a new query stream position query object. Use gst_query_unref() * when done with it. A position query is used to query the current position * of playback in the streams, in some format. * * Free-function: gst_query_unref * * Returns: (transfer full): a new #GstQuery */ GstQuery * gst_query_new_position (GstFormat format) { GstQuery *query; GstStructure *structure; structure = gst_structure_id_new (GST_QUARK (QUERY_POSITION), GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (CURRENT), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL); query = gst_query_new (GST_QUERY_POSITION, structure); return query; } /** * gst_query_set_position: * @query: a #GstQuery with query type GST_QUERY_POSITION * @format: the requested #GstFormat * @cur: the position to set * * Answer a position query by setting the requested value in the given format. */ void gst_query_set_position (GstQuery * query, GstFormat format, gint64 cur) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_POSITION); gst_structure_id_set (query->structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (CURRENT), G_TYPE_INT64, cur, NULL); } /** * gst_query_parse_position: * @query: a #GstQuery * @format: (out) (allow-none): the storage for the #GstFormat of the * position values (may be NULL) * @cur: (out) (allow-none): the storage for the current position (may be NULL) * * Parse a position query, writing the format into @format, and the position * into @cur, if the respective parameters are non-NULL. */ void gst_query_parse_position (GstQuery * query, GstFormat * format, gint64 * cur) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_POSITION); structure = query->structure; if (format) *format = (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (cur) *cur = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (CURRENT))); } /** * gst_query_new_duration: * @format: the #GstFormat for this duration query * * Constructs a new stream duration query object to query in the given format. * Use gst_query_unref() when done with it. A duration query will give the * total length of the stream. * * Free-function: gst_query_unref * * Returns: (transfer full): a new #GstQuery */ GstQuery * gst_query_new_duration (GstFormat format) { GstQuery *query; GstStructure *structure; structure = gst_structure_id_new (GST_QUARK (QUERY_DURATION), GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (DURATION), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL); query = gst_query_new (GST_QUERY_DURATION, structure); return query; } /** * gst_query_set_duration: * @query: a #GstQuery * @format: the #GstFormat for the duration * @duration: the duration of the stream * * Answer a duration query by setting the requested value in the given format. */ void gst_query_set_duration (GstQuery * query, GstFormat format, gint64 duration) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_DURATION); gst_structure_id_set (query->structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (DURATION), G_TYPE_INT64, duration, NULL); } /** * gst_query_parse_duration: * @query: a #GstQuery * @format: (out) (allow-none): the storage for the #GstFormat of the duration * value, or NULL. * @duration: (out) (allow-none): the storage for the total duration, or NULL. * * Parse a duration query answer. Write the format of the duration into @format, * and the value into @duration, if the respective variables are non-NULL. */ void gst_query_parse_duration (GstQuery * query, GstFormat * format, gint64 * duration) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_DURATION); structure = query->structure; if (format) *format = (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (duration) *duration = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (DURATION))); } /** * gst_query_new_latency: * * Constructs a new latency query object. * Use gst_query_unref() when done with it. A latency query is usually performed * by sinks to compensate for additional latency introduced by elements in the * pipeline. * * Free-function: gst_query_unref * * Returns: (transfer full): a #GstQuery * * Since: 0.10.12 */ GstQuery * gst_query_new_latency (void) { GstQuery *query; GstStructure *structure; structure = gst_structure_id_new (GST_QUARK (QUERY_LATENCY), GST_QUARK (LIVE), G_TYPE_BOOLEAN, FALSE, GST_QUARK (MIN_LATENCY), G_TYPE_UINT64, G_GUINT64_CONSTANT (0), GST_QUARK (MAX_LATENCY), G_TYPE_UINT64, G_GUINT64_CONSTANT (-1), NULL); query = gst_query_new (GST_QUERY_LATENCY, structure); return query; } /** * gst_query_set_latency: * @query: a #GstQuery * @live: if there is a live element upstream * @min_latency: the minimal latency of the live element * @max_latency: the maximal latency of the live element * * Answer a latency query by setting the requested values in the given format. * * Since: 0.10.12 */ void gst_query_set_latency (GstQuery * query, gboolean live, GstClockTime min_latency, GstClockTime max_latency) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_LATENCY); gst_structure_id_set (query->structure, GST_QUARK (LIVE), G_TYPE_BOOLEAN, live, GST_QUARK (MIN_LATENCY), G_TYPE_UINT64, min_latency, GST_QUARK (MAX_LATENCY), G_TYPE_UINT64, max_latency, NULL); } /** * gst_query_parse_latency: * @query: a #GstQuery * @live: (out) (allow-none): storage for live or NULL * @min_latency: (out) (allow-none): the storage for the min latency or NULL * @max_latency: (out) (allow-none): the storage for the max latency or NULL * * Parse a latency query answer. * * Since: 0.10.12 */ void gst_query_parse_latency (GstQuery * query, gboolean * live, GstClockTime * min_latency, GstClockTime * max_latency) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_LATENCY); structure = query->structure; if (live) *live = g_value_get_boolean (gst_structure_id_get_value (structure, GST_QUARK (LIVE))); if (min_latency) *min_latency = g_value_get_uint64 (gst_structure_id_get_value (structure, GST_QUARK (MIN_LATENCY))); if (max_latency) *max_latency = g_value_get_uint64 (gst_structure_id_get_value (structure, GST_QUARK (MAX_LATENCY))); } /** * gst_query_new_convert: * @src_format: the source #GstFormat for the new query * @value: the value to convert * @dest_format: the target #GstFormat * * Constructs a new convert query object. Use gst_query_unref() * when done with it. A convert query is used to ask for a conversion between * one format and another. * * Free-function: gst_query_unref * * Returns: (transfer full): a #GstQuery */ GstQuery * gst_query_new_convert (GstFormat src_format, gint64 value, GstFormat dest_format) { GstQuery *query; GstStructure *structure; structure = gst_structure_id_new (GST_QUARK (QUERY_CONVERT), GST_QUARK (SRC_FORMAT), GST_TYPE_FORMAT, src_format, GST_QUARK (SRC_VALUE), G_TYPE_INT64, value, GST_QUARK (DEST_FORMAT), GST_TYPE_FORMAT, dest_format, GST_QUARK (DEST_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL); query = gst_query_new (GST_QUERY_CONVERT, structure); return query; } /** * gst_query_set_convert: * @query: a #GstQuery * @src_format: the source #GstFormat * @src_value: the source value * @dest_format: the destination #GstFormat * @dest_value: the destination value * * Answer a convert query by setting the requested values. */ void gst_query_set_convert (GstQuery * query, GstFormat src_format, gint64 src_value, GstFormat dest_format, gint64 dest_value) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_CONVERT); gst_structure_id_set (query->structure, GST_QUARK (SRC_FORMAT), GST_TYPE_FORMAT, src_format, GST_QUARK (SRC_VALUE), G_TYPE_INT64, src_value, GST_QUARK (DEST_FORMAT), GST_TYPE_FORMAT, dest_format, GST_QUARK (DEST_VALUE), G_TYPE_INT64, dest_value, NULL); } /** * gst_query_parse_convert: * @query: a #GstQuery * @src_format: (out) (allow-none): the storage for the #GstFormat of the * source value, or NULL * @src_value: (out) (allow-none): the storage for the source value, or NULL * @dest_format: (out) (allow-none): the storage for the #GstFormat of the * destination value, or NULL * @dest_value: (out) (allow-none): the storage for the destination value, * or NULL * * Parse a convert query answer. Any of @src_format, @src_value, @dest_format, * and @dest_value may be NULL, in which case that value is omitted. */ void gst_query_parse_convert (GstQuery * query, GstFormat * src_format, gint64 * src_value, GstFormat * dest_format, gint64 * dest_value) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_CONVERT); structure = query->structure; if (src_format) *src_format = (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (SRC_FORMAT))); if (src_value) *src_value = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (SRC_VALUE))); if (dest_format) *dest_format = (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (DEST_FORMAT))); if (dest_value) *dest_value = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (DEST_VALUE))); } /** * gst_query_new_segment: * @format: the #GstFormat for the new query * * Constructs a new segment query object. Use gst_query_unref() * when done with it. A segment query is used to discover information about the * currently configured segment for playback. * * Free-function: gst_query_unref * * Returns: (transfer full): a new #GstQuery */ GstQuery * gst_query_new_segment (GstFormat format) { GstQuery *query; GstStructure *structure; structure = gst_structure_id_new (GST_QUARK (QUERY_SEGMENT), GST_QUARK (RATE), G_TYPE_DOUBLE, (gdouble) 0.0, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (START_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1), GST_QUARK (STOP_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL); query = gst_query_new (GST_QUERY_SEGMENT, structure); return query; } /** * gst_query_set_segment: * @query: a #GstQuery * @rate: the rate of the segment * @format: the #GstFormat of the segment values (@start_value and @stop_value) * @start_value: the start value * @stop_value: the stop value * * Answer a segment query by setting the requested values. The normal * playback segment of a pipeline is 0 to duration at the default rate of * 1.0. If a seek was performed on the pipeline to play a different * segment, this query will return the range specified in the last seek. * * @start_value and @stop_value will respectively contain the configured * playback range start and stop values expressed in @format. * The values are always between 0 and the duration of the media and * @start_value <= @stop_value. @rate will contain the playback rate. For * negative rates, playback will actually happen from @stop_value to * @start_value. */ void gst_query_set_segment (GstQuery * query, gdouble rate, GstFormat format, gint64 start_value, gint64 stop_value) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEGMENT); gst_structure_id_set (query->structure, GST_QUARK (RATE), G_TYPE_DOUBLE, rate, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (START_VALUE), G_TYPE_INT64, start_value, GST_QUARK (STOP_VALUE), G_TYPE_INT64, stop_value, NULL); } /** * gst_query_parse_segment: * @query: a #GstQuery * @rate: (out) (allow-none): the storage for the rate of the segment, or NULL * @format: (out) (allow-none): the storage for the #GstFormat of the values, * or NULL * @start_value: (out) (allow-none): the storage for the start value, or NULL * @stop_value: (out) (allow-none): the storage for the stop value, or NULL * * Parse a segment query answer. Any of @rate, @format, @start_value, and * @stop_value may be NULL, which will cause this value to be omitted. * * See gst_query_set_segment() for an explanation of the function arguments. */ void gst_query_parse_segment (GstQuery * query, gdouble * rate, GstFormat * format, gint64 * start_value, gint64 * stop_value) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEGMENT); structure = query->structure; if (rate) *rate = g_value_get_double (gst_structure_id_get_value (structure, GST_QUARK (RATE))); if (format) *format = (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (start_value) *start_value = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (START_VALUE))); if (stop_value) *stop_value = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (STOP_VALUE))); } /** * gst_query_new_application: * @type: the query type * @structure: a structure for the query * * Constructs a new custom application query object. Use gst_query_unref() * when done with it. * * Free-function: gst_query_unref * * Returns: (transfer full): a new #GstQuery */ GstQuery * gst_query_new_application (GstQueryType type, GstStructure * structure) { g_return_val_if_fail (gst_query_type_get_details (type) != NULL, NULL); g_return_val_if_fail (structure != NULL, NULL); return gst_query_new (type, structure); } /** * gst_query_get_structure: * @query: a #GstQuery * * Get the structure of a query. * * Returns: (transfer none): the #GstStructure of the query. The structure is * still owned by the query and will therefore be freed when the query * is unreffed. */ GstStructure * gst_query_get_structure (GstQuery * query) { g_return_val_if_fail (GST_IS_QUERY (query), NULL); return query->structure; } /** * gst_query_new_seeking: * @format: the default #GstFormat for the new query * * Constructs a new query object for querying seeking properties of * the stream. * * Free-function: gst_query_unref * * Returns: (transfer full): a new #GstQuery */ GstQuery * gst_query_new_seeking (GstFormat format) { GstQuery *query; GstStructure *structure; structure = gst_structure_id_new (GST_QUARK (QUERY_SEEKING), GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (SEEKABLE), G_TYPE_BOOLEAN, FALSE, GST_QUARK (SEGMENT_START), G_TYPE_INT64, G_GINT64_CONSTANT (-1), GST_QUARK (SEGMENT_END), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL); query = gst_query_new (GST_QUERY_SEEKING, structure); return query; } /** * gst_query_set_seeking: * @query: a #GstQuery * @format: the format to set for the @segment_start and @segment_end values * @seekable: the seekable flag to set * @segment_start: the segment_start to set * @segment_end: the segment_end to set * * Set the seeking query result fields in @query. */ void gst_query_set_seeking (GstQuery * query, GstFormat format, gboolean seekable, gint64 segment_start, gint64 segment_end) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEEKING); gst_structure_id_set (query->structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (SEEKABLE), G_TYPE_BOOLEAN, seekable, GST_QUARK (SEGMENT_START), G_TYPE_INT64, segment_start, GST_QUARK (SEGMENT_END), G_TYPE_INT64, segment_end, NULL); } /** * gst_query_parse_seeking: * @query: a GST_QUERY_SEEKING type query #GstQuery * @format: (out) (allow-none): the format to set for the @segment_start * and @segment_end values, or NULL * @seekable: (out) (allow-none): the seekable flag to set, or NULL * @segment_start: (out) (allow-none): the segment_start to set, or NULL * @segment_end: (out) (allow-none): the segment_end to set, or NULL * * Parse a seeking query, writing the format into @format, and * other results into the passed parameters, if the respective parameters * are non-NULL */ void gst_query_parse_seeking (GstQuery * query, GstFormat * format, gboolean * seekable, gint64 * segment_start, gint64 * segment_end) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEEKING); structure = query->structure; if (format) *format = (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (seekable) *seekable = g_value_get_boolean (gst_structure_id_get_value (structure, GST_QUARK (SEEKABLE))); if (segment_start) *segment_start = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (SEGMENT_START))); if (segment_end) *segment_end = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (SEGMENT_END))); } /** * gst_query_new_formats: * * Constructs a new query object for querying formats of * the stream. * * Free-function: gst_query_unref * * Returns: (transfer full): a new #GstQuery * * Since: 0.10.4 */ GstQuery * gst_query_new_formats (void) { GstQuery *query; GstStructure *structure; structure = gst_structure_id_empty_new (GST_QUARK (QUERY_FORMATS)); query = gst_query_new (GST_QUERY_FORMATS, structure); return query; } static void gst_query_list_add_format (GValue * list, GstFormat format) { GValue item = { 0, }; g_value_init (&item, GST_TYPE_FORMAT); g_value_set_enum (&item, format); gst_value_list_append_value (list, &item); g_value_unset (&item); } /** * gst_query_set_formats: * @query: a #GstQuery * @n_formats: the number of formats to set. * @...: A number of @GstFormats equal to @n_formats. * * Set the formats query result fields in @query. The number of formats passed * must be equal to @n_formats. */ void gst_query_set_formats (GstQuery * query, gint n_formats, ...) { va_list ap; GValue list = { 0, }; gint i; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS); g_value_init (&list, GST_TYPE_LIST); va_start (ap, n_formats); for (i = 0; i < n_formats; i++) { gst_query_list_add_format (&list, va_arg (ap, GstFormat)); } va_end (ap); gst_structure_set_value (query->structure, "formats", &list); g_value_unset (&list); } /** * gst_query_set_formatsv: * @query: a #GstQuery * @n_formats: the number of formats to set. * @formats: (in) (array length=n_formats): an array containing @n_formats * @GstFormat values. * * Set the formats query result fields in @query. The number of formats passed * in the @formats array must be equal to @n_formats. * * Since: 0.10.4 */ void gst_query_set_formatsv (GstQuery * query, gint n_formats, const GstFormat * formats) { GValue list = { 0, }; gint i; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS); g_value_init (&list, GST_TYPE_LIST); for (i = 0; i < n_formats; i++) { gst_query_list_add_format (&list, formats[i]); } gst_structure_set_value (query->structure, "formats", &list); g_value_unset (&list); } /** * gst_query_parse_formats_length: * @query: a #GstQuery * @n_formats: (out): the number of formats in this query. * * Parse the number of formats in the formats @query. * * Since: 0.10.4 */ void gst_query_parse_formats_length (GstQuery * query, guint * n_formats) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS); if (n_formats) { const GValue *list; list = gst_structure_get_value (query->structure, "formats"); if (list == NULL) *n_formats = 0; else *n_formats = gst_value_list_get_size (list); } } /** * gst_query_parse_formats_nth: * @query: a #GstQuery * @nth: (out): the nth format to retrieve. * @format: (out): a pointer to store the nth format * * Parse the format query and retrieve the @nth format from it into * @format. If the list contains less elements than @nth, @format will be * set to GST_FORMAT_UNDEFINED. * * Since: 0.10.4 */ void gst_query_parse_formats_nth (GstQuery * query, guint nth, GstFormat * format) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS); if (format) { const GValue *list; list = gst_structure_get_value (query->structure, "formats"); if (list == NULL) { *format = GST_FORMAT_UNDEFINED; } else { if (nth < gst_value_list_get_size (list)) { *format = (GstFormat) g_value_get_enum (gst_value_list_get_value (list, nth)); } else *format = GST_FORMAT_UNDEFINED; } } } /** * gst_query_new_buffering * @format: the default #GstFormat for the new query * * Constructs a new query object for querying the buffering status of * a stream. * * Free-function: gst_query_new * * Returns: (transfer full): a new #GstQuery * * Since: 0.10.20 */ GstQuery * gst_query_new_buffering (GstFormat format) { GstQuery *query; GstStructure *structure; /* by default, we configure the answer as no buffering with a 100% buffering * progress */ structure = gst_structure_id_new (GST_QUARK (QUERY_BUFFERING), GST_QUARK (BUSY), G_TYPE_BOOLEAN, FALSE, GST_QUARK (BUFFER_PERCENT), G_TYPE_INT, 100, GST_QUARK (BUFFERING_MODE), GST_TYPE_BUFFERING_MODE, GST_BUFFERING_STREAM, GST_QUARK (AVG_IN_RATE), G_TYPE_INT, -1, GST_QUARK (AVG_OUT_RATE), G_TYPE_INT, -1, GST_QUARK (BUFFERING_LEFT), G_TYPE_INT64, G_GINT64_CONSTANT (0), GST_QUARK (ESTIMATED_TOTAL), G_TYPE_INT64, G_GINT64_CONSTANT (-1), GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (START_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1), GST_QUARK (STOP_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL); query = gst_query_new (GST_QUERY_BUFFERING, structure); return query; } /** * gst_query_set_buffering_percent * @query: A valid #GstQuery of type GST_QUERY_BUFFERING. * @busy: if buffering is busy * @percent: a buffering percent * * Set the percentage of buffered data. This is a value between 0 and 100. * The @busy indicator is %TRUE when the buffering is in progress. * * Since: 0.10.20 */ void gst_query_set_buffering_percent (GstQuery * query, gboolean busy, gint percent) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING); g_return_if_fail (percent >= 0 && percent <= 100); gst_structure_id_set (query->structure, GST_QUARK (BUSY), G_TYPE_BOOLEAN, busy, GST_QUARK (BUFFER_PERCENT), G_TYPE_INT, percent, NULL); } /** * gst_query_parse_buffering_percent * @query: A valid #GstQuery of type GST_QUERY_BUFFERING. * @busy: (out) (allow-none): if buffering is busy, or NULL * @percent: (out) (allow-none): a buffering percent, or NULL * * Get the percentage of buffered data. This is a value between 0 and 100. * The @busy indicator is %TRUE when the buffering is in progress. * * Since: 0.10.20 */ void gst_query_parse_buffering_percent (GstQuery * query, gboolean * busy, gint * percent) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING); if (busy) *busy = g_value_get_boolean (gst_structure_id_get_value (query->structure, GST_QUARK (BUSY))); if (percent) *percent = g_value_get_int (gst_structure_id_get_value (query->structure, GST_QUARK (BUFFER_PERCENT))); } /** * gst_query_set_buffering_stats: * @query: A valid #GstQuery of type GST_QUERY_BUFFERING. * @mode: a buffering mode * @avg_in: the average input rate * @avg_out: the average output rate * @buffering_left: amount of buffering time left * * Configures the buffering stats values in @query. * * Since: 0.10.20 */ void gst_query_set_buffering_stats (GstQuery * query, GstBufferingMode mode, gint avg_in, gint avg_out, gint64 buffering_left) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING); gst_structure_id_set (query->structure, GST_QUARK (BUFFERING_MODE), GST_TYPE_BUFFERING_MODE, mode, GST_QUARK (AVG_IN_RATE), G_TYPE_INT, avg_in, GST_QUARK (AVG_OUT_RATE), G_TYPE_INT, avg_out, GST_QUARK (BUFFERING_LEFT), G_TYPE_INT64, buffering_left, NULL); } /** * gst_query_parse_buffering_stats: * @query: A valid #GstQuery of type GST_QUERY_BUFFERING. * @mode: (out) (allow-none): a buffering mode, or NULL * @avg_in: (out) (allow-none): the average input rate, or NULL * @avg_out: (out) (allow-none): the average output rat, or NULLe * @buffering_left: (out) (allow-none): amount of buffering time left, or NULL * * Extracts the buffering stats values from @query. * * Since: 0.10.20 */ void gst_query_parse_buffering_stats (GstQuery * query, GstBufferingMode * mode, gint * avg_in, gint * avg_out, gint64 * buffering_left) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING); if (mode) *mode = (GstBufferingMode) g_value_get_enum (gst_structure_id_get_value (query->structure, GST_QUARK (BUFFERING_MODE))); if (avg_in) *avg_in = g_value_get_int (gst_structure_id_get_value (query->structure, GST_QUARK (AVG_IN_RATE))); if (avg_out) *avg_out = g_value_get_int (gst_structure_id_get_value (query->structure, GST_QUARK (AVG_OUT_RATE))); if (buffering_left) *buffering_left = g_value_get_int64 (gst_structure_id_get_value (query->structure, GST_QUARK (BUFFERING_LEFT))); } /** * gst_query_set_buffering_range: * @query: a #GstQuery * @format: the format to set for the @start and @stop values * @start: the start to set * @stop: the stop to set * @estimated_total: estimated total amount of download time * * Set the available query result fields in @query. * * Since: 0.10.20 */ void gst_query_set_buffering_range (GstQuery * query, GstFormat format, gint64 start, gint64 stop, gint64 estimated_total) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING); gst_structure_id_set (query->structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (START_VALUE), G_TYPE_INT64, start, GST_QUARK (STOP_VALUE), G_TYPE_INT64, stop, GST_QUARK (ESTIMATED_TOTAL), G_TYPE_INT64, estimated_total, NULL); } /** * gst_query_parse_buffering_range: * @query: a GST_QUERY_BUFFERING type query #GstQuery * @format: (out) (allow-none): the format to set for the @segment_start * and @segment_end values, or NULL * @start: (out) (allow-none): the start to set, or NULL * @stop: (out) (allow-none): the stop to set, or NULL * @estimated_total: (out) (allow-none): estimated total amount of download * time, or NULL * * Parse an available query, writing the format into @format, and * other results into the passed parameters, if the respective parameters * are non-NULL * * Since: 0.10.20 */ void gst_query_parse_buffering_range (GstQuery * query, GstFormat * format, gint64 * start, gint64 * stop, gint64 * estimated_total) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING); structure = query->structure; if (format) *format = (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (start) *start = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (START_VALUE))); if (stop) *stop = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (STOP_VALUE))); if (estimated_total) *estimated_total = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (ESTIMATED_TOTAL))); } /** * gst_query_add_buffering_range * @query: a GST_QUERY_BUFFERING type query #GstQuery * @start: start position of the range * @stop: stop position of the range * * Set the buffering-ranges array field in @query. The current last * start position of the array should be inferior to @start. * * Returns: a #gboolean indicating if the range was added or not. * * Since: 0.10.31 */ gboolean gst_query_add_buffering_range (GstQuery * query, gint64 start, gint64 stop) { GValueArray *array; GValue *last_array_value; const GValue *value; GValue range_value = { 0 }; g_return_val_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING, FALSE); if (G_UNLIKELY (start >= stop)) return FALSE; value = gst_structure_id_get_value (query->structure, GST_QUARK (BUFFERING_RANGES)); if (value) { array = (GValueArray *) g_value_get_boxed (value); last_array_value = g_value_array_get_nth (array, array->n_values - 1); if (G_UNLIKELY (start <= gst_value_get_int64_range_min (last_array_value))) return FALSE; } else { GValue new_array_val = { 0, }; array = g_value_array_new (0); g_value_init (&new_array_val, G_TYPE_VALUE_ARRAY); g_value_take_boxed (&new_array_val, array); /* set the value array only once, so we then modify (append to) the * existing value array owned by the GstStructure / the field's GValue */ gst_structure_id_take_value (query->structure, GST_QUARK (BUFFERING_RANGES), &new_array_val); } g_value_init (&range_value, GST_TYPE_INT64_RANGE); gst_value_set_int64_range (&range_value, start, stop); g_value_array_append (array, &range_value); /* skip the g_value_unset(&range_value) here, we know it's not needed */ return TRUE; } /** * gst_query_get_n_buffering_ranges * @query: a GST_QUERY_BUFFERING type query #GstQuery * * Retrieve the number of values currently stored in the * buffered-ranges array of the query's structure. * * Returns: the range array size as a #guint. * * Since: 0.10.31 */ guint gst_query_get_n_buffering_ranges (GstQuery * query) { GValueArray *array; const GValue *value; guint size = 0; g_return_val_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING, 0); value = gst_structure_id_get_value (query->structure, GST_QUARK (BUFFERING_RANGES)); if (value) { array = (GValueArray *) g_value_get_boxed (value); size = array->n_values; } return size; } /** * gst_query_parse_nth_buffering_range * @query: a GST_QUERY_BUFFERING type query #GstQuery * @index: position in the buffered-ranges array to read * @start: (out) (allow-none): the start position to set, or NULL * @stop: (out) (allow-none): the stop position to set, or NULL * * Parse an available query and get the start and stop values stored * at the @index of the buffered ranges array. * * Returns: a #gboolean indicating if the parsing succeeded. * * Since: 0.10.31 */ gboolean gst_query_parse_nth_buffering_range (GstQuery * query, guint index, gint64 * start, gint64 * stop) { const GValue *value; GValueArray *ranges; GValue *range_value; gboolean ret = FALSE; g_return_val_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING, ret); value = gst_structure_id_get_value (query->structure, GST_QUARK (BUFFERING_RANGES)); ranges = (GValueArray *) g_value_get_boxed (value); range_value = g_value_array_get_nth (ranges, index); if (range_value) { if (start) *start = gst_value_get_int64_range_min (range_value); if (stop) *stop = gst_value_get_int64_range_max (range_value); ret = TRUE; } return ret; } /** * gst_query_new_uri: * * Constructs a new query URI query object. Use gst_query_unref() * when done with it. An URI query is used to query the current URI * that is used by the source or sink. * * Free-function: gst_query_unref * * Returns: (transfer full): a new #GstQuery * * Since: 0.10.22 */ GstQuery * gst_query_new_uri (void) { GstQuery *query; GstStructure *structure; structure = gst_structure_id_new (GST_QUARK (QUERY_URI), GST_QUARK (URI), G_TYPE_STRING, NULL, NULL); query = gst_query_new (GST_QUERY_URI, structure); return query; } /** * gst_query_set_uri: * @query: a #GstQuery with query type GST_QUERY_URI * @uri: the URI to set * * Answer a URI query by setting the requested URI. * * Since: 0.10.22 */ void gst_query_set_uri (GstQuery * query, const gchar * uri) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_URI); g_return_if_fail (gst_uri_is_valid (uri)); gst_structure_id_set (query->structure, GST_QUARK (URI), G_TYPE_STRING, uri, NULL); } /** * gst_query_parse_uri: * @query: a #GstQuery * @uri: (out callee-allocates) (allow-none): the storage for the current URI * (may be NULL) * * Parse an URI query, writing the URI into @uri as a newly * allocated string, if the respective parameters are non-NULL. * Free the string with g_free() after usage. * * Since: 0.10.22 */ void gst_query_parse_uri (GstQuery * query, gchar ** uri) { g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_URI); if (uri) *uri = g_value_dup_string (gst_structure_id_get_value (query->structure, GST_QUARK (URI))); } /** * gst_query_new_buffers: * @caps: the #GstCaps for the buffers that are going to be allocated * * Constructs a new buffer requirements query object to query buffer * requirements for a particular caps. Use gst_query_unref() when done * with it. * * Returns: A #GstQuery */ GstQuery * gst_query_new_buffers (GstCaps * caps) { GstQuery *query; GstStructure *structure; /* XXX could add size here, for linear (non YUV/RGB) buffers? But I'm not * entirely sure what is the use-case for that.. it should be easy enough * to add more optional reply fields later */ structure = gst_structure_id_new (GST_QUARK (QUERY_BUFFERS), GST_QUARK (CAPS), GST_TYPE_CAPS, caps, GST_QUARK (COUNT), G_TYPE_INT, -1, GST_QUARK (WIDTH), G_TYPE_INT, -1, GST_QUARK (HEIGHT), G_TYPE_INT, -1, NULL); query = gst_query_new (GST_QUERY_BUFFERS, structure); return query; } /** * gst_query_set_buffers_count: * @count: minimum number of buffers required * * Answer a buffers query by setting the minimum number of buffers required. * If there is no minimum buffer count requirement, don't set this field in * the query. */ void gst_query_set_buffers_count (GstQuery * query, gint count) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); structure = gst_query_get_structure (query); gst_structure_id_set (structure, GST_QUARK (COUNT), G_TYPE_INT, count, NULL); } /** * gst_query_set_buffers_dimensions: * @width: minimum buffer width * @height: minimum buffer height * * Answer a buffers query by setting the minimum buffer dimensions required. * If there is no minimum buffer dimensions (beyond the width/height specified * in the #GstCaps), don't set this field in the query. */ void gst_query_set_buffers_dimensions (GstQuery * query, gint width, gint height) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); structure = gst_query_get_structure (query); gst_structure_id_set (structure, GST_QUARK (WIDTH), G_TYPE_INT, width, GST_QUARK (HEIGHT), G_TYPE_INT, height, NULL); } /** * gst_query_parse_buffers_caps: * @query: a #GstQuery * @caps: the storage for the #GstCaps pointer, or NULL * * Parse a buffers query. */ void gst_query_parse_buffers_caps (GstQuery * query, const GstCaps ** caps) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); structure = gst_query_get_structure (query); if (caps) *caps = gst_value_get_caps (gst_structure_id_get_value (structure, GST_QUARK (CAPS))); } /** * gst_query_parse_buffers_count: * @query: a #GstQuery * @count: the storage for minimum number of buffers, or NULL * * Parse a buffers query answer to see the minimum number of buffers * required. A returned value of -1 means there is no minimum requirement */ void gst_query_parse_buffers_count (GstQuery * query, gint * count) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); structure = gst_query_get_structure (query); if (count) *count = g_value_get_int (gst_structure_id_get_value (structure, GST_QUARK (COUNT))); } /** * gst_query_parse_buffers_dimensions: * @query: a #GstQuery * @width: the storage for minimum width, or NULL * @height: the storage for minimum height, or NULL * * Parse a buffers query answer to see the minimum buffer dimensions required. * A returned value of -1 for either dimension means there is no minimum * requirement in that axis */ void gst_query_parse_buffers_dimensions (GstQuery * query, gint * width, gint * height) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); structure = gst_query_get_structure (query); if (width) *width = g_value_get_int (gst_structure_id_get_value (structure, GST_QUARK (WIDTH))); if (height) *height = g_value_get_int (gst_structure_id_get_value (structure, GST_QUARK (HEIGHT))); }