/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * 2005 Wim Taymans * * gstquery.c: GstQueryType registration and Query parsing/creation * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:gstquery * @short_description: Dynamically register new query types. Provide functions * to create queries, and to set and parse values in them. * @see_also: #GstPad, #GstElement * * GstQuery functions are used to register a new query types to the gstreamer * core. * Query types can be used to perform queries on pads and elements. * * Queries can be created using the gst_query_new_xxx() functions. * Query values can be set using gst_query_set_xxx(), and parsed using * gst_query_parse_xxx() helpers. * * The following example shows how to query the duration of a pipeline: * * * Query duration on a pipeline * * GstQuery *query; * gboolean res; * query = gst_query_new_duration (GST_FORMAT_TIME); * res = gst_element_query (pipeline, query); * if (res) { * gint64 duration; * gst_query_parse_duration (query, NULL, &duration); * g_print ("duration = %"GST_TIME_FORMAT, GST_TIME_ARGS (duration)); * } * else { * g_print ("duration query failed..."); * } * gst_query_unref (query); * * * * Last reviewed on 2006-02-14 (0.10.4) */ #include "gst_private.h" #include "gstinfo.h" #include "gstquery.h" #include "gstvalue.h" #include "gstenumtypes.h" #include "gstquark.h" GST_DEBUG_CATEGORY_STATIC (gst_query_debug); #define GST_CAT_DEFAULT gst_query_debug static void gst_query_init (GTypeInstance * instance, gpointer g_class); static void gst_query_class_init (gpointer g_class, gpointer class_data); static void gst_query_finalize (GstQuery * query); static GstQuery *_gst_query_copy (GstQuery * query); static GStaticMutex mutex = G_STATIC_MUTEX_INIT; static GList *_gst_queries = NULL; static GHashTable *_nick_to_query = NULL; static GHashTable *_query_type_to_nick = NULL; static guint32 _n_values = 1; /* we start from 1 because 0 reserved for NONE */ static GstQueryTypeDefinition standard_definitions[] = { {GST_QUERY_POSITION, "position", "Current position", 0}, {GST_QUERY_DURATION, "duration", "Total duration", 0}, {GST_QUERY_LATENCY, "latency", "Latency", 0}, {GST_QUERY_JITTER, "jitter", "Jitter", 0}, {GST_QUERY_RATE, "rate", "Configured rate 1000000 = 1", 0}, {GST_QUERY_SEEKING, "seeking", "Seeking capabilities and parameters", 0}, {GST_QUERY_SEGMENT, "segment", "currently configured segment", 0}, {GST_QUERY_CONVERT, "convert", "Converting between formats", 0}, {GST_QUERY_FORMATS, "formats", "Supported formats for conversion", 0}, {0, NULL, NULL, 0} }; void _gst_query_initialize (void) { GstQueryTypeDefinition *standards = standard_definitions; GST_CAT_INFO (GST_CAT_GST_INIT, "init queries"); GST_DEBUG_CATEGORY_INIT (gst_query_debug, "query", 0, "query system"); g_static_mutex_lock (&mutex); if (_nick_to_query == NULL) { _nick_to_query = g_hash_table_new (g_str_hash, g_str_equal); _query_type_to_nick = g_hash_table_new (NULL, NULL); } while (standards->nick) { standards->quark = g_quark_from_static_string (standards->nick); g_hash_table_insert (_nick_to_query, standards->nick, standards); g_hash_table_insert (_query_type_to_nick, GINT_TO_POINTER (standards->value), standards); _gst_queries = g_list_append (_gst_queries, standards); standards++; _n_values++; } g_static_mutex_unlock (&mutex); gst_query_get_type (); } /** * gst_query_type_get_name: * @query: the query type * * Get a printable name for the given query type. Do not modify or free. * * Returns: a reference to the static name of the query. */ const gchar * gst_query_type_get_name (GstQueryType query) { const GstQueryTypeDefinition *def; def = gst_query_type_get_details (query); return def->nick; } /** * gst_query_type_to_quark: * @query: the query type * * Get the unique quark for the given query type. * * Returns: the quark associated with the query type */ GQuark gst_query_type_to_quark (GstQueryType query) { const GstQueryTypeDefinition *def; def = gst_query_type_get_details (query); return def->quark; } GType gst_query_get_type (void) { static GType _gst_query_type; if (G_UNLIKELY (_gst_query_type == 0)) { static const GTypeInfo query_info = { sizeof (GstQueryClass), NULL, NULL, gst_query_class_init, NULL, NULL, sizeof (GstQuery), 0, gst_query_init, NULL }; _gst_query_type = g_type_register_static (GST_TYPE_MINI_OBJECT, "GstQuery", &query_info, 0); } return _gst_query_type; } static void gst_query_class_init (gpointer g_class, gpointer class_data) { GstQueryClass *query_class = GST_QUERY_CLASS (g_class); query_class->mini_object_class.copy = (GstMiniObjectCopyFunction) _gst_query_copy; query_class->mini_object_class.finalize = (GstMiniObjectFinalizeFunction) gst_query_finalize; } static void gst_query_finalize (GstQuery * query) { g_return_if_fail (query != NULL); if (query->structure) { gst_structure_set_parent_refcount (query->structure, NULL); gst_structure_free (query->structure); } } static void gst_query_init (GTypeInstance * instance, gpointer g_class) { } static GstQuery * _gst_query_copy (GstQuery * query) { GstQuery *copy; copy = (GstQuery *) gst_mini_object_new (GST_TYPE_QUERY); copy->type = query->type; if (query->structure) { copy->structure = gst_structure_copy (query->structure); gst_structure_set_parent_refcount (copy->structure, &query->mini_object.refcount); } return copy; } /** * gst_query_type_register: * @nick: The nick of the new query * @description: The description of the new query * * Create a new GstQueryType based on the nick or return an * already registered query with that nick * * Returns: A new GstQueryType or an already registered query * with the same nick. */ GstQueryType gst_query_type_register (const gchar * nick, const gchar * description) { GstQueryTypeDefinition *query; GstQueryType lookup; g_return_val_if_fail (nick != NULL, 0); g_return_val_if_fail (description != NULL, 0); lookup = gst_query_type_get_by_nick (nick); if (lookup != GST_QUERY_NONE) return lookup; query = g_new0 (GstQueryTypeDefinition, 1); query->value = _n_values; query->nick = g_strdup (nick); query->description = g_strdup (description); query->quark = g_quark_from_static_string (query->nick); g_static_mutex_lock (&mutex); g_hash_table_insert (_nick_to_query, query->nick, query); g_hash_table_insert (_query_type_to_nick, GINT_TO_POINTER (query->value), query); _gst_queries = g_list_append (_gst_queries, query); _n_values++; g_static_mutex_unlock (&mutex); return query->value; } /** * gst_query_type_get_by_nick: * @nick: The nick of the query * * Get the query type registered with @nick. * * Returns: The query registered with @nick or #GST_QUERY_NONE * if the query was not registered. */ GstQueryType gst_query_type_get_by_nick (const gchar * nick) { GstQueryTypeDefinition *query; g_return_val_if_fail (nick != NULL, 0); g_static_mutex_lock (&mutex); query = g_hash_table_lookup (_nick_to_query, nick); g_static_mutex_unlock (&mutex); if (query != NULL) return query->value; else return GST_QUERY_NONE; } /** * gst_query_types_contains: * @types: The query array to search * @type: the #GstQueryType to find * * See if the given #GstQueryType is inside the @types query types array. * * Returns: TRUE if the type is found inside the array */ gboolean gst_query_types_contains (const GstQueryType * types, GstQueryType type) { if (!types) return FALSE; while (*types) { if (*types == type) return TRUE; types++; } return FALSE; } /** * gst_query_type_get_details: * @type: a #GstQueryType * * Get details about the given #GstQueryType. * * Returns: The #GstQueryTypeDefinition for @type or NULL on failure. */ const GstQueryTypeDefinition * gst_query_type_get_details (GstQueryType type) { const GstQueryTypeDefinition *result; g_static_mutex_lock (&mutex); result = g_hash_table_lookup (_query_type_to_nick, GINT_TO_POINTER (type)); g_static_mutex_unlock (&mutex); return result; } /** * gst_query_type_iterate_definitions: * * Get a #GstIterator of all the registered query types. The definitions * iterated over are read only. * * Returns: A #GstIterator of #GstQueryTypeDefinition. */ GstIterator * gst_query_type_iterate_definitions (void) { GstIterator *result; g_static_mutex_lock (&mutex); /* FIXME: register a boxed type for GstQueryTypeDefinition */ result = gst_iterator_new_list (G_TYPE_POINTER, g_static_mutex_get_mutex (&mutex), &_n_values, &_gst_queries, NULL, NULL, NULL); g_static_mutex_unlock (&mutex); return result; } static GstQuery * gst_query_new (GstQueryType type, GstStructure * structure) { GstQuery *query; query = (GstQuery *) gst_mini_object_new (GST_TYPE_QUERY); GST_DEBUG ("creating new query %p %d", query, type); query->type = type; if (structure) { query->structure = structure; gst_structure_set_parent_refcount (query->structure, &query->mini_object.refcount); } else { query->structure = NULL; } return query; } /** * gst_query_new_position: * @format: the default #GstFormat for the new query * * Constructs a new query stream position query object. Use gst_query_unref() * when done with it. A position query is used to query the current position * of playback in the streams, in some format. * * Returns: A #GstQuery */ GstQuery * gst_query_new_position (GstFormat format) { GstQuery *query; GstStructure *structure; structure = gst_structure_empty_new ("GstQueryPosition"); gst_structure_id_set (structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (CURRENT), G_TYPE_INT64, (gint64) - 1, NULL); query = gst_query_new (GST_QUERY_POSITION, structure); return query; } /** * gst_query_set_position: * @query: a #GstQuery with query type GST_QUERY_POSITION * @format: the requested #GstFormat * @cur: the position to set * * Answer a position query by setting the requested value in the given format. */ void gst_query_set_position (GstQuery * query, GstFormat format, gint64 cur) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_POSITION); structure = gst_query_get_structure (query); gst_structure_id_set (structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (CURRENT), G_TYPE_INT64, cur, NULL); } /** * gst_query_parse_position: * @query: a #GstQuery * @format: the storage for the #GstFormat of the position values (may be NULL) * @cur: the storage for the current position (may be NULL) * * Parse a position query, writing the format into @format, and the position * into @cur, if the respective parameters are non-NULL. */ void gst_query_parse_position (GstQuery * query, GstFormat * format, gint64 * cur) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_POSITION); structure = gst_query_get_structure (query); if (format) *format = g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (cur) *cur = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (CURRENT))); } /** * gst_query_new_duration: * @format: the #GstFormat for this duration query * * Constructs a new stream duration query object to query in the given format. * Use gst_query_unref() when done with it. A duration query will give the * total length of the stream. * * Returns: A #GstQuery */ GstQuery * gst_query_new_duration (GstFormat format) { GstQuery *query; GstStructure *structure; structure = gst_structure_empty_new ("GstQueryDuration"); gst_structure_id_set (structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (DURATION), G_TYPE_INT64, (gint64) - 1, NULL); query = gst_query_new (GST_QUERY_DURATION, structure); return query; } /** * gst_query_set_duration: * @query: a #GstQuery * @format: the #GstFormat for the duration * @duration: the duration of the stream * * Answer a duration query by setting the requested value in the given format. */ void gst_query_set_duration (GstQuery * query, GstFormat format, gint64 duration) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_DURATION); structure = gst_query_get_structure (query); gst_structure_id_set (structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (DURATION), G_TYPE_INT64, duration, NULL); } /** * gst_query_parse_duration: * @query: a #GstQuery * @format: the storage for the #GstFormat of the duration value, or NULL. * @duration: the storage for the total duration, or NULL. * * Parse a duration query answer. Write the format of the duration into @format, * and the value into @duration, if the respective variables are non-NULL. */ void gst_query_parse_duration (GstQuery * query, GstFormat * format, gint64 * duration) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_DURATION); structure = gst_query_get_structure (query); if (format) *format = g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (duration) *duration = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (DURATION))); } /** * gst_query_new_convert: * @src_format: the source #GstFormat for the new query * @value: the value to convert * @dest_format: the target #GstFormat * * Constructs a new convert query object. Use gst_query_unref() * when done with it. A convert query is used to ask for a conversion between * one format and another. * * Returns: A #GstQuery */ GstQuery * gst_query_new_convert (GstFormat src_format, gint64 value, GstFormat dest_format) { GstQuery *query; GstStructure *structure; g_return_val_if_fail (value >= 0, NULL); structure = gst_structure_empty_new ("GstQueryConvert"); gst_structure_id_set (structure, GST_QUARK (SRC_FORMAT), GST_TYPE_FORMAT, src_format, GST_QUARK (SRC_VALUE), G_TYPE_INT64, value, GST_QUARK (DEST_FORMAT), GST_TYPE_FORMAT, dest_format, GST_QUARK (DEST_VALUE), G_TYPE_INT64, (gint64) - 1, NULL); query = gst_query_new (GST_QUERY_CONVERT, structure); return query; } /** * gst_query_set_convert: * @query: a #GstQuery * @src_format: the source #GstFormat * @src_value: the source value * @dest_format: the destination #GstFormat * @dest_value: the destination value * * Answer a convert query by setting the requested values. */ void gst_query_set_convert (GstQuery * query, GstFormat src_format, gint64 src_value, GstFormat dest_format, gint64 dest_value) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_CONVERT); structure = gst_query_get_structure (query); gst_structure_id_set (structure, GST_QUARK (SRC_FORMAT), GST_TYPE_FORMAT, src_format, GST_QUARK (SRC_VALUE), G_TYPE_INT64, src_value, GST_QUARK (DEST_FORMAT), GST_TYPE_FORMAT, dest_format, GST_QUARK (DEST_VALUE), G_TYPE_INT64, (gint64) dest_value, NULL); } /** * gst_query_parse_convert: * @query: a #GstQuery * @src_format: the storage for the #GstFormat of the source value, or NULL * @src_value: the storage for the source value, or NULL * @dest_format: the storage for the #GstFormat of the destination value, or NULL * @dest_value: the storage for the destination value, or NULL * * Parse a convert query answer. Any of @src_format, @src_value, @dest_format, * and @dest_value may be NULL, in which case that value is omitted. */ void gst_query_parse_convert (GstQuery * query, GstFormat * src_format, gint64 * src_value, GstFormat * dest_format, gint64 * dest_value) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_CONVERT); structure = gst_query_get_structure (query); if (src_format) *src_format = g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (SRC_FORMAT))); if (src_value) *src_value = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (SRC_VALUE))); if (dest_format) *dest_format = g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (DEST_FORMAT))); if (dest_value) *dest_value = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (DEST_VALUE))); } /** * gst_query_new_segment: * @format: the #GstFormat for the new query * * Constructs a new segment query object. Use gst_query_unref() * when done with it. A segment query is used to discover information about the * currently configured segment for playback. * * Returns: a #GstQuery */ GstQuery * gst_query_new_segment (GstFormat format) { GstQuery *query; GstStructure *structure; structure = gst_structure_empty_new ("GstQuerySegment"); gst_structure_id_set (structure, GST_QUARK (RATE), G_TYPE_DOUBLE, (gdouble) 0.0, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (START_VALUE), G_TYPE_INT64, (gint64) - 1, GST_QUARK (STOP_VALUE), G_TYPE_INT64, (gint64) - 1, NULL); query = gst_query_new (GST_QUERY_SEGMENT, structure); return query; } /** * gst_query_set_segment: * @query: a #GstQuery * @rate: the rate of the segment * @format: the #GstFormat of the segment values (@start_value and @stop_value) * @start_value: the start value * @stop_value: the stop value * * Answer a segment query by setting the requested values. The normal * playback segment of a pipeline is 0 to duration at the default rate of * 1.0. If a seek was performed on the pipeline to play a different * segment, this query will return the range specified in the last seek. * * @start_value and @stop_value will respectively contain the configured * playback range start and stop values expressed in @format. * The values are always between 0 and the duration of the media and * @start_value <= @stop_value. @rate will contain the playback rate. For * negative rates, playback will actually happen from @stop_value to * @start_value. */ void gst_query_set_segment (GstQuery * query, gdouble rate, GstFormat format, gint64 start_value, gint64 stop_value) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEGMENT); structure = gst_query_get_structure (query); gst_structure_id_set (structure, GST_QUARK (RATE), G_TYPE_DOUBLE, rate, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (START_VALUE), G_TYPE_INT64, start_value, GST_QUARK (STOP_VALUE), G_TYPE_INT64, stop_value, NULL); } /** * gst_query_parse_segment: * @query: a #GstQuery * @rate: the storage for the rate of the segment, or NULL * @format: the storage for the #GstFormat of the values, or NULL * @start_value: the storage for the start value, or NULL * @stop_value: the storage for the stop value, or NULL * * Parse a segment query answer. Any of @rate, @format, @start_value, and * @stop_value may be NULL, which will cause this value to be omitted. * * See gst_query_set_segment() for an explanation of the function arguments. */ void gst_query_parse_segment (GstQuery * query, gdouble * rate, GstFormat * format, gint64 * start_value, gint64 * stop_value) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEGMENT); structure = gst_query_get_structure (query); if (rate) *rate = g_value_get_double (gst_structure_id_get_value (structure, GST_QUARK (RATE))); if (format) *format = g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (start_value) *start_value = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (START_VALUE))); if (stop_value) *stop_value = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (STOP_VALUE))); } /** * gst_query_new_application: * @type: the query type * @structure: a structure for the query * * Constructs a new custom application query object. Use gst_query_unref() * when done with it. * * Returns: a #GstQuery */ GstQuery * gst_query_new_application (GstQueryType type, GstStructure * structure) { g_return_val_if_fail (gst_query_type_get_details (type) != NULL, NULL); g_return_val_if_fail (structure != NULL, NULL); return gst_query_new (type, structure); } /** * gst_query_get_structure: * @query: a #GstQuery * * Get the structure of a query. * * Returns: The #GstStructure of the query. The structure is still owned * by the query and will therefore be freed when the query is unreffed. */ GstStructure * gst_query_get_structure (GstQuery * query) { g_return_val_if_fail (GST_IS_QUERY (query), NULL); return query->structure; } /** * gst_query_new_seeking (GstFormat *format) * @format: the default #GstFormat for the new query * * Constructs a new query object for querying seeking properties of * the stream. * * Returns: A #GstQuery */ GstQuery * gst_query_new_seeking (GstFormat format) { GstQuery *query; GstStructure *structure; structure = gst_structure_empty_new ("GstQuerySeeking"); gst_structure_id_set (structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (SEEKABLE), G_TYPE_BOOLEAN, FALSE, GST_QUARK (SEGMENT_START), G_TYPE_INT64, (gint64) - 1, GST_QUARK (SEGMENT_END), G_TYPE_INT64, (gint64) - 1, NULL); query = gst_query_new (GST_QUERY_SEEKING, structure); return query; } /** * gst_query_set_seeking: * @query: a #GstQuery * @format: the format to set for the @segment_start and @segment_end values * @seekable: the seekable flag to set * @segment_start: the segment_start to set * @segment_end: the segment_end to set * * Set the seeking query result fields in @query. */ void gst_query_set_seeking (GstQuery * query, GstFormat format, gboolean seekable, gint64 segment_start, gint64 segment_end) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEEKING); structure = gst_query_get_structure (query); gst_structure_id_set (structure, GST_QUARK (FORMAT), GST_TYPE_FORMAT, format, GST_QUARK (SEEKABLE), G_TYPE_BOOLEAN, seekable, GST_QUARK (SEGMENT_START), G_TYPE_INT64, segment_start, GST_QUARK (SEGMENT_END), G_TYPE_INT64, segment_end, NULL); } /** * gst_query_parse_seeking: * @query: a GST_QUERY_SEEKING type query #GstQuery * @format: the format to set for the @segment_start and @segment_end values * @seekable: the seekable flag to set * @segment_start: the segment_start to set * @segment_end: the segment_end to set * * Parse a seeking query, writing the format into @format, and * other results into the passed parameters, if the respective parameters * are non-NULL */ void gst_query_parse_seeking (GstQuery * query, GstFormat * format, gboolean * seekable, gint64 * segment_start, gint64 * segment_end) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEEKING); structure = gst_query_get_structure (query); if (format) *format = g_value_get_enum (gst_structure_id_get_value (structure, GST_QUARK (FORMAT))); if (seekable) *seekable = g_value_get_boolean (gst_structure_id_get_value (structure, GST_QUARK (SEEKABLE))); if (segment_start) *segment_start = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (SEGMENT_START))); if (segment_end) *segment_end = g_value_get_int64 (gst_structure_id_get_value (structure, GST_QUARK (SEGMENT_END))); } /** * gst_query_new_formats: * * Constructs a new query object for querying formats of * the stream. * * Returns: A #GstQuery * * Since: 0.10.4 */ GstQuery * gst_query_new_formats (void) { GstQuery *query; GstStructure *structure; structure = gst_structure_new ("GstQueryFormats", NULL); query = gst_query_new (GST_QUERY_FORMATS, structure); return query; } static void gst_query_list_add_format (GValue * list, GstFormat format) { GValue item = { 0, }; g_value_init (&item, GST_TYPE_FORMAT); g_value_set_enum (&item, format); gst_value_list_append_value (list, &item); g_value_unset (&item); } /** * gst_query_set_formats: * @query: a #GstQuery * @n_formats: the number of formats to set. * @...: A number of @GstFormats equal to @n_formats. * * Set the formats query result fields in @query. The number of formats passed * must be equal to @n_formats. */ void gst_query_set_formats (GstQuery * query, gint n_formats, ...) { va_list ap; GValue list = { 0, }; GstStructure *structure; gint i; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS); g_value_init (&list, GST_TYPE_LIST); va_start (ap, n_formats); for (i = 0; i < n_formats; i++) { gst_query_list_add_format (&list, va_arg (ap, GstFormat)); } va_end (ap); structure = gst_query_get_structure (query); gst_structure_set_value (structure, "formats", &list); g_value_unset (&list); } /** * gst_query_set_formatsv: * @query: a #GstQuery * @n_formats: the number of formats to set. * @formats: An array containing @n_formats @GstFormat values. * * Set the formats query result fields in @query. The number of formats passed * in the @formats array must be equal to @n_formats. * * Since: 0.10.4 */ void gst_query_set_formatsv (GstQuery * query, gint n_formats, GstFormat * formats) { GValue list = { 0, }; GstStructure *structure; gint i; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS); g_value_init (&list, GST_TYPE_LIST); for (i = 0; i < n_formats; i++) { gst_query_list_add_format (&list, formats[i]); } structure = gst_query_get_structure (query); gst_structure_set_value (structure, "formats", &list); g_value_unset (&list); } /** * gst_query_parse_formats_length: * @query: a #GstQuery * @n_formats: the number of formats in this query. * * Parse the number of formats in the formats @query. * * Since: 0.10.4 */ void gst_query_parse_formats_length (GstQuery * query, guint * n_formats) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS); if (n_formats) { const GValue *list; structure = gst_query_get_structure (query); list = gst_structure_get_value (structure, "formats"); if (list == NULL) *n_formats = 0; else *n_formats = gst_value_list_get_size (list); } } /** * gst_query_parse_formats_nth: * @query: a #GstQuery * @nth: the nth format to retrieve. * @format: a pointer to store the nth format * * Parse the format query and retrieve the @nth format from it into * @format. If the list contains less elements than @nth, @format will be * set to GST_FORMAT_UNDEFINED. * * Since: 0.10.4 */ void gst_query_parse_formats_nth (GstQuery * query, guint nth, GstFormat * format) { GstStructure *structure; g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS); if (format) { const GValue *list; structure = gst_query_get_structure (query); list = gst_structure_get_value (structure, "formats"); if (list == NULL) { *format = GST_FORMAT_UNDEFINED; } else { if (nth < gst_value_list_get_size (list)) { *format = g_value_get_enum (gst_value_list_get_value (list, nth)); } else *format = GST_FORMAT_UNDEFINED; } } }