/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * * gstpad.h: Header for GstPad object * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GST_QUERY_H__ #define __GST_QUERY_H__ #include G_BEGIN_DECLS typedef enum { GST_QUERY_NONE = 0, GST_QUERY_TOTAL, GST_QUERY_POSITION, GST_QUERY_LATENCY, GST_QUERY_JITTER, GST_QUERY_START, GST_QUERY_SEGMENT_END, GST_QUERY_RATE } GstQueryType; /* rate is relative to 1000000LL */ #define GST_QUERY_TYPE_RATE_DEN 1000000LL typedef struct _GstQueryTypeDefinition GstQueryTypeDefinition; struct _GstQueryTypeDefinition { GstQueryType value; gchar *nick; gchar *description; }; #ifdef G_HAVE_ISO_VARARGS #define GST_QUERY_TYPE_FUNCTION(type, functionname, ...) \ static const GstQueryType* \ functionname (type object) \ { \ static const GstQueryType types[] = { \ __VA_ARGS__, \ 0 \ }; \ return types; \ } #elif defined(G_HAVE_GNUC_VARARGS) #define GST_QUERY_TYPE_FUNCTION(type, functionname, a...) \ static const GstQueryType* \ functionname (type object) \ { \ static const GstQueryType types[] = { \ a, \ 0 \ }; \ return types; \ } #endif void _gst_query_type_initialize (void); /* register a new query */ GstQueryType gst_query_type_register (const gchar *nick, const gchar *description); GstQueryType gst_query_type_get_by_nick (const gchar *nick); /* check if a query is in an array of querys */ gboolean gst_query_types_contains (const GstQueryType *types, GstQueryType type); /* query for query details */ const GstQueryTypeDefinition* gst_query_type_get_details (GstQueryType type); const GList* gst_query_type_get_definitions (void); G_END_DECLS #endif /* __GST_QUERY_H__ */