/* GStreamer * Copyright (C) 2005 Wim Taymans * * gstsegment.h: Header for GstSegment subsystem * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GST_SEGMENT_H__ #define __GST_SEGMENT_H__ #include #include G_BEGIN_DECLS #define GST_TYPE_SEGMENT (gst_segment_get_type()) typedef struct _GstSegment GstSegment; /** * GstSegment: * @rate: the rate of the segment * @abs_rate: absolute value of @rate * @format: the format of the segment values * @flags: flags for this segment * @start: the start of the segment * @stop: the stop of the segment * @time: the stream time of the segment * @accum: accumulated segment * @last_stop: last known stop time * @duration: total duration of segment * @applied_rate: the already applied rate to the segment * * A helper structure that holds the configured region of * interest in a media file. */ struct _GstSegment { /*< public >*/ gdouble rate; gdouble abs_rate; GstFormat format; GstSeekFlags flags; gint64 start; gint64 stop; gint64 time; gint64 accum; gint64 last_stop; gint64 duration; /* API added 0.10.6 */ gdouble applied_rate; /*< private >*/ /*gpointer _gst_reserved[GST_PADDING-2];*/ guint8 _gst_reserved[(sizeof (gpointer) * GST_PADDING) - sizeof (gdouble)]; }; GType gst_segment_get_type (void); GstSegment * gst_segment_new (void); GstSegment * gst_segment_copy (GstSegment *segment); void gst_segment_free (GstSegment *segment); void gst_segment_init (GstSegment *segment, GstFormat format); void gst_segment_set_duration (GstSegment *segment, GstFormat format, gint64 duration); void gst_segment_set_last_stop (GstSegment *segment, GstFormat format, gint64 position); void gst_segment_set_seek (GstSegment *segment, gdouble rate, GstFormat format, GstSeekFlags flags, GstSeekType start_type, gint64 start, GstSeekType stop_type, gint64 stop, gboolean *update); void gst_segment_set_newsegment (GstSegment *segment, gboolean update, gdouble rate, GstFormat format, gint64 start, gint64 stop, gint64 time); void gst_segment_set_newsegment_full (GstSegment *segment, gboolean update, gdouble rate, gdouble applied_rate, GstFormat format, gint64 start, gint64 stop, gint64 time); gint64 gst_segment_to_stream_time (GstSegment *segment, GstFormat format, gint64 position); gint64 gst_segment_to_running_time (GstSegment *segment, GstFormat format, gint64 position); gint64 gst_segment_to_position (GstSegment *segment, GstFormat format, gint64 running_time); gboolean gst_segment_clip (GstSegment *segment, GstFormat format, gint64 start, gint64 stop, gint64 *clip_start, gint64 *clip_stop); gboolean gst_segment_set_running_time (GstSegment *segment, GstFormat format, gint64 running_time); G_END_DECLS #endif /* __GST_SEGMENT_H__ */