/* GStreamer * Copyright (C) 2003 David A. Schleef * * gststructure.c: lists of { GQuark, GValue } tuples * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:gststructure * @short_description: Generic structure containing fields of names and values * @see_also: #GstCaps, #GstMessage, #GstEvent, #GstQuery * * A #GstStructure is a collection of key/value pairs. The keys are expressed * as GQuarks and the values can be of any GType. * * In addition to the key/value pairs, a #GstStructure also has a name. The name * starts with a letter and can be folled by letters, numbers and any of "/-_.:". * * #GstStructure is used by various GStreamer subsystems to store information * in a flexible and extensible way. A #GstStructure does not have a refcount * because it usually is part of a higher level object such as #GstCaps. It * provides a means to enforce mutability using the refcount of the parent * with the gst_structure_set_parent_refcount() method. * * A #GstStructure can be created with gst_structure_empty_new() or * gst_structure_new(), which both take a name and an optional set of * key/value pairs along with the types of the values. * * Field values can be changed with gst_structure_set_value() or * gst_structure_set(). * * Field values can be retrieved with gst_structure_get_value() or the more * convenient gst_structure_get_*() functions. * * Fields can be removed with gst_structure_remove_field() or * gst_structure_remove_fields(). * * Strings in structures must be ASCII or UTF-8 encoded. Other encodings are * not allowed. Strings must not be empty either, but may be NULL. * * Last reviewed on 2009-06-08 (0.10.23) */ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include #include "gst_private.h" #include "gstquark.h" #include #include typedef struct _GstStructureField GstStructureField; struct _GstStructureField { GQuark name; GValue value; }; #define GST_STRUCTURE_FIELD(structure, index) \ &g_array_index((structure)->fields, GstStructureField, (index)) #define IS_MUTABLE(structure) \ (!(structure)->parent_refcount || \ g_atomic_int_get ((structure)->parent_refcount) == 1) #define IS_TAGLIST(structure) \ (structure->name == GST_QUARK (TAGLIST)) static void gst_structure_set_field (GstStructure * structure, GstStructureField * field); static GstStructureField *gst_structure_get_field (const GstStructure * structure, const gchar * fieldname); static GstStructureField *gst_structure_id_get_field (const GstStructure * structure, GQuark field); static void gst_structure_transform_to_string (const GValue * src_value, GValue * dest_value); static GstStructure *gst_structure_copy_conditional (const GstStructure * structure); static gboolean gst_structure_parse_value (gchar * str, gchar ** after, GValue * value, GType default_type); static gboolean gst_structure_parse_simple_string (gchar * s, gchar ** end); GType gst_structure_get_type (void) { static GType gst_structure_type = 0; if (G_UNLIKELY (gst_structure_type == 0)) { gst_structure_type = g_boxed_type_register_static ("GstStructure", (GBoxedCopyFunc) gst_structure_copy_conditional, (GBoxedFreeFunc) gst_structure_free); g_value_register_transform_func (gst_structure_type, G_TYPE_STRING, gst_structure_transform_to_string); } return gst_structure_type; } static GstStructure * gst_structure_id_empty_new_with_size (GQuark quark, guint prealloc) { GstStructure *structure; structure = g_slice_new (GstStructure); structure->type = gst_structure_get_type (); structure->name = quark; structure->parent_refcount = NULL; structure->fields = g_array_sized_new (FALSE, FALSE, sizeof (GstStructureField), prealloc); return structure; } /** * gst_structure_id_empty_new: * @quark: name of new structure * * Creates a new, empty #GstStructure with the given name as a GQuark. * * Free-function: gst_structure_free * * Returns: (transfer full): a new, empty #GstStructure */ GstStructure * gst_structure_id_empty_new (GQuark quark) { g_return_val_if_fail (quark != 0, NULL); return gst_structure_id_empty_new_with_size (quark, 0); } #ifndef G_DISABLE_CHECKS static gboolean gst_structure_validate_name (const gchar * name) { const gchar *s; g_return_val_if_fail (name != NULL, FALSE); /* FIXME 0.11: use g_ascii_isalpha() */ if (G_UNLIKELY (!g_ascii_isalnum (*name))) { GST_WARNING ("Invalid character '%c' at offset 0 in structure name: %s", *name, name); return FALSE; } /* FIXME 0.11: don't allow spaces */ /* FIXME: test name string more */ s = &name[1]; while (*s && (g_ascii_isalnum (*s) || strchr ("/-_.:+ ", *s) != NULL)) s++; if (G_UNLIKELY (*s != '\0')) { GST_WARNING ("Invalid character '%c' at offset %lu in structure name: %s", *s, ((gulong) s - (gulong) name), name); return FALSE; } return TRUE; } #endif /** * gst_structure_empty_new: * @name: name of new structure * * Creates a new, empty #GstStructure with the given @name. * * See gst_structure_set_name() for constraints on the @name parameter. * * Free-function: gst_structure_free * * Returns: (transfer full): a new, empty #GstStructure */ GstStructure * gst_structure_empty_new (const gchar * name) { g_return_val_if_fail (gst_structure_validate_name (name), NULL); return gst_structure_id_empty_new_with_size (g_quark_from_string (name), 0); } /** * gst_structure_new: * @name: name of new structure * @firstfield: name of first field to set * @...: additional arguments * * Creates a new #GstStructure with the given name. Parses the * list of variable arguments and sets fields to the values listed. * Variable arguments should be passed as field name, field type, * and value. Last variable argument should be NULL. * * Free-function: gst_structure_free * * Returns: (transfer full): a new #GstStructure */ GstStructure * gst_structure_new (const gchar * name, const gchar * firstfield, ...) { GstStructure *structure; va_list varargs; g_return_val_if_fail (name != NULL, NULL); va_start (varargs, firstfield); structure = gst_structure_new_valist (name, firstfield, varargs); va_end (varargs); return structure; } /** * gst_structure_new_valist: * @name: name of new structure * @firstfield: name of first field to set * @varargs: variable argument list * * Creates a new #GstStructure with the given @name. Structure fields * are set according to the varargs in a manner similar to * gst_structure_new(). * * See gst_structure_set_name() for constraints on the @name parameter. * * Free-function: gst_structure_free * * Returns: (transfer full): a new #GstStructure */ GstStructure * gst_structure_new_valist (const gchar * name, const gchar * firstfield, va_list varargs) { GstStructure *structure; g_return_val_if_fail (name != NULL, NULL); structure = gst_structure_empty_new (name); if (structure) gst_structure_set_valist (structure, firstfield, varargs); return structure; } /** * gst_structure_set_parent_refcount: * @structure: a #GstStructure * @refcount: (in): a pointer to the parent's refcount * * Sets the parent_refcount field of #GstStructure. This field is used to * determine whether a structure is mutable or not. This function should only be * called by code implementing parent objects of #GstStructure, as described in * the MT Refcounting section of the design documents. */ void gst_structure_set_parent_refcount (GstStructure * structure, gint * refcount) { g_return_if_fail (structure != NULL); /* if we have a parent_refcount already, we can only clear * if with a NULL refcount */ if (structure->parent_refcount) g_return_if_fail (refcount == NULL); else g_return_if_fail (refcount != NULL); structure->parent_refcount = refcount; } /** * gst_structure_copy: * @structure: a #GstStructure to duplicate * * Duplicates a #GstStructure and all its fields and values. * * Free-function: gst_structure_free * * Returns: (transfer none): a new #GstStructure. */ GstStructure * gst_structure_copy (const GstStructure * structure) { GstStructure *new_structure; GstStructureField *field; guint i, len; g_return_val_if_fail (structure != NULL, NULL); len = structure->fields->len; new_structure = gst_structure_id_empty_new_with_size (structure->name, len); for (i = 0; i < len; i++) { GstStructureField new_field = { 0 }; field = GST_STRUCTURE_FIELD (structure, i); new_field.name = field->name; gst_value_init_and_copy (&new_field.value, &field->value); g_array_append_val (new_structure->fields, new_field); } return new_structure; } /** * gst_structure_free: * @structure: (in) (transfer full): the #GstStructure to free * * Frees a #GstStructure and all its fields and values. The structure must not * have a parent when this function is called. */ void gst_structure_free (GstStructure * structure) { GstStructureField *field; guint i, len; g_return_if_fail (structure != NULL); g_return_if_fail (structure->parent_refcount == NULL); len = structure->fields->len; for (i = 0; i < len; i++) { field = GST_STRUCTURE_FIELD (structure, i); if (G_IS_VALUE (&field->value)) { g_value_unset (&field->value); } } g_array_free (structure->fields, TRUE); #ifdef USE_POISONING memset (structure, 0xff, sizeof (GstStructure)); #endif g_slice_free (GstStructure, structure); } /** * gst_structure_get_name: * @structure: a #GstStructure * * Get the name of @structure as a string. * * Returns: the name of the structure. */ const gchar * gst_structure_get_name (const GstStructure * structure) { g_return_val_if_fail (structure != NULL, NULL); return g_quark_to_string (structure->name); } /** * gst_structure_has_name: * @structure: a #GstStructure * @name: structure name to check for * * Checks if the structure has the given name * * Returns: TRUE if @name matches the name of the structure. */ gboolean gst_structure_has_name (const GstStructure * structure, const gchar * name) { const gchar *structure_name; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (name != NULL, FALSE); /* getting the string is cheap and comparing short strings is too * should be faster than getting the quark for name and comparing the quarks */ structure_name = g_quark_to_string (structure->name); return (structure_name && strcmp (structure_name, name) == 0); } /** * gst_structure_get_name_id: * @structure: a #GstStructure * * Get the name of @structure as a GQuark. * * Returns: the quark representing the name of the structure. */ GQuark gst_structure_get_name_id (const GstStructure * structure) { g_return_val_if_fail (structure != NULL, 0); return structure->name; } /** * gst_structure_set_name: * @structure: a #GstStructure * @name: the new name of the structure * * Sets the name of the structure to the given @name. The string * provided is copied before being used. It must not be empty, start with a * letter and can be followed by letters, numbers and any of "/-_.:". */ void gst_structure_set_name (GstStructure * structure, const gchar * name) { g_return_if_fail (structure != NULL); g_return_if_fail (IS_MUTABLE (structure)); g_return_if_fail (gst_structure_validate_name (name)); structure->name = g_quark_from_string (name); } static inline void gst_structure_id_set_value_internal (GstStructure * structure, GQuark field, const GValue * value) { GstStructureField gsfield = { 0, {0,} }; gsfield.name = field; gst_value_init_and_copy (&gsfield.value, value); gst_structure_set_field (structure, &gsfield); } /** * gst_structure_id_set_value: * @structure: a #GstStructure * @field: a #GQuark representing a field * @value: the new value of the field * * Sets the field with the given GQuark @field to @value. If the field * does not exist, it is created. If the field exists, the previous * value is replaced and freed. */ void gst_structure_id_set_value (GstStructure * structure, GQuark field, const GValue * value) { g_return_if_fail (structure != NULL); g_return_if_fail (G_IS_VALUE (value)); g_return_if_fail (IS_MUTABLE (structure)); gst_structure_id_set_value_internal (structure, field, value); } /** * gst_structure_set_value: * @structure: a #GstStructure * @fieldname: the name of the field to set * @value: the new value of the field * * Sets the field with the given name @field to @value. If the field * does not exist, it is created. If the field exists, the previous * value is replaced and freed. */ void gst_structure_set_value (GstStructure * structure, const gchar * fieldname, const GValue * value) { g_return_if_fail (structure != NULL); g_return_if_fail (fieldname != NULL); g_return_if_fail (G_IS_VALUE (value)); g_return_if_fail (IS_MUTABLE (structure)); gst_structure_id_set_value_internal (structure, g_quark_from_string (fieldname), value); } static inline void gst_structure_id_take_value_internal (GstStructure * structure, GQuark field, GValue * value) { GstStructureField gsfield = { 0, {0,} }; gsfield.name = field; gsfield.value = *value; gst_structure_set_field (structure, &gsfield); /* we took ownership */ #ifdef USE_POISONING memset (value, 0, sizeof (GValue)); #else value->g_type = G_TYPE_INVALID; #endif } /** * gst_structure_id_take_value: * @structure: a #GstStructure * @field: a #GQuark representing a field * @value: (transfer full): the new value of the field * * Sets the field with the given GQuark @field to @value. If the field * does not exist, it is created. If the field exists, the previous * value is replaced and freed. * * Since: 0.10.31 */ void gst_structure_id_take_value (GstStructure * structure, GQuark field, GValue * value) { g_return_if_fail (structure != NULL); g_return_if_fail (G_IS_VALUE (value)); g_return_if_fail (IS_MUTABLE (structure)); gst_structure_id_take_value_internal (structure, field, value); } /** * gst_structure_take_value: * @structure: a #GstStructure * @fieldname: the name of the field to set * @value: (transfer full): the new value of the field * * Sets the field with the given name @field to @value. If the field * does not exist, it is created. If the field exists, the previous * value is replaced and freed. The function will take ownership of @value. * * Since: 0.10.31 */ void gst_structure_take_value (GstStructure * structure, const gchar * fieldname, GValue * value) { g_return_if_fail (structure != NULL); g_return_if_fail (fieldname != NULL); g_return_if_fail (G_IS_VALUE (value)); g_return_if_fail (IS_MUTABLE (structure)); gst_structure_id_take_value_internal (structure, g_quark_from_string (fieldname), value); } static void gst_structure_set_valist_internal (GstStructure * structure, const gchar * fieldname, va_list varargs) { gchar *err = NULL; GType type; while (fieldname) { GstStructureField field = { 0 }; field.name = g_quark_from_string (fieldname); type = va_arg (varargs, GType); if (G_UNLIKELY (type == G_TYPE_DATE)) { g_warning ("Don't use G_TYPE_DATE, use GST_TYPE_DATE instead\n"); type = GST_TYPE_DATE; } #if GLIB_CHECK_VERSION(2,23,3) G_VALUE_COLLECT_INIT (&field.value, type, varargs, 0, &err); #else g_value_init (&field.value, type); G_VALUE_COLLECT (&field.value, varargs, 0, &err); #endif if (G_UNLIKELY (err)) { g_critical ("%s", err); return; } gst_structure_set_field (structure, &field); fieldname = va_arg (varargs, gchar *); } } /** * gst_structure_set: * @structure: a #GstStructure * @fieldname: the name of the field to set * @...: variable arguments * * Parses the variable arguments and sets fields accordingly. * Variable arguments should be in the form field name, field type * (as a GType), value(s). The last variable argument should be NULL. */ void gst_structure_set (GstStructure * structure, const gchar * field, ...) { va_list varargs; g_return_if_fail (structure != NULL); g_return_if_fail (IS_MUTABLE (structure) || field == NULL); va_start (varargs, field); gst_structure_set_valist_internal (structure, field, varargs); va_end (varargs); } /** * gst_structure_set_valist: * @structure: a #GstStructure * @fieldname: the name of the field to set * @varargs: variable arguments * * va_list form of gst_structure_set(). */ void gst_structure_set_valist (GstStructure * structure, const gchar * fieldname, va_list varargs) { g_return_if_fail (structure != NULL); g_return_if_fail (IS_MUTABLE (structure)); gst_structure_set_valist_internal (structure, fieldname, varargs); } static void gst_structure_id_set_valist_internal (GstStructure * structure, GQuark fieldname, va_list varargs) { gchar *err = NULL; GType type; while (fieldname) { GstStructureField field = { 0 }; field.name = fieldname; type = va_arg (varargs, GType); if (G_UNLIKELY (type == G_TYPE_DATE)) { g_warning ("Don't use G_TYPE_DATE, use GST_TYPE_DATE instead\n"); type = GST_TYPE_DATE; } #ifndef G_VALUE_COLLECT_INIT g_value_init (&field.value, type); G_VALUE_COLLECT (&field.value, varargs, 0, &err); #else G_VALUE_COLLECT_INIT (&field.value, type, varargs, 0, &err); #endif if (G_UNLIKELY (err)) { g_critical ("%s", err); return; } gst_structure_set_field (structure, &field); fieldname = va_arg (varargs, GQuark); } } /** * gst_structure_id_set: * @structure: a #GstStructure * @fieldname: the GQuark for the name of the field to set * @...: variable arguments * * Identical to gst_structure_set, except that field names are * passed using the GQuark for the field name. This allows more efficient * setting of the structure if the caller already knows the associated * quark values. * The last variable argument must be NULL. * * Since: 0.10.10 */ void gst_structure_id_set (GstStructure * structure, GQuark field, ...) { va_list varargs; g_return_if_fail (structure != NULL); va_start (varargs, field); gst_structure_id_set_valist_internal (structure, field, varargs); va_end (varargs); } /** * gst_structure_id_set_valist: * @structure: a #GstStructure * @fieldname: the name of the field to set * @varargs: variable arguments * * va_list form of gst_structure_id_set(). * * Since: 0.10.10 */ void gst_structure_id_set_valist (GstStructure * structure, GQuark fieldname, va_list varargs) { g_return_if_fail (structure != NULL); g_return_if_fail (IS_MUTABLE (structure)); gst_structure_id_set_valist_internal (structure, fieldname, varargs); } /** * gst_structure_id_new: * @name_quark: name of new structure * @field_quark: the GQuark for the name of the field to set * @...: variable arguments * * Creates a new #GstStructure with the given name as a GQuark, followed by * fieldname quark, GType, argument(s) "triplets" in the same format as * gst_structure_id_set(). Basically a convenience wrapper around * gst_structure_id_empty_new() and gst_structure_id_set(). * * The last variable argument must be NULL (or 0). * * Free-function: gst_structure_free * * Returns: (transfer full): a new #GstStructure * * Since: 0.10.24 */ GstStructure * gst_structure_id_new (GQuark name_quark, GQuark field_quark, ...) { GstStructure *s; va_list varargs; g_return_val_if_fail (name_quark != 0, NULL); g_return_val_if_fail (field_quark != 0, NULL); s = gst_structure_id_empty_new (name_quark); va_start (varargs, field_quark); gst_structure_id_set_valist_internal (s, field_quark, varargs); va_end (varargs); return s; } #if GST_VERSION_NANO == 1 #define GIT_G_WARNING g_warning #else #define GIT_G_WARNING GST_WARNING #endif /* If the structure currently contains a field with the same name, it is * replaced with the provided field. Otherwise, the field is added to the * structure. The field's value is not deeply copied. */ static void gst_structure_set_field (GstStructure * structure, GstStructureField * field) { GstStructureField *f; guint i, len = structure->fields->len; if (G_UNLIKELY (G_VALUE_HOLDS_STRING (&field->value))) { const gchar *s; s = g_value_get_string (&field->value); /* only check for NULL strings in taglists, as they are allowed in message * structs, e.g. error message debug strings */ if (G_UNLIKELY (IS_TAGLIST (structure) && (s == NULL || *s == '\0'))) { if (s == NULL) { GIT_G_WARNING ("Trying to set NULL string on field '%s' on taglist. " "Please file a bug.", g_quark_to_string (field->name)); g_value_unset (&field->value); return; } else { /* empty strings never make sense */ GIT_G_WARNING ("Trying to set empty string on taglist field '%s'. " "Please file a bug.", g_quark_to_string (field->name)); g_value_unset (&field->value); return; } } else if (G_UNLIKELY (s != NULL && !g_utf8_validate (s, -1, NULL))) { g_warning ("Trying to set string on %s field '%s', but string is not " "valid UTF-8. Please file a bug.", IS_TAGLIST (structure) ? "taglist" : "structure", g_quark_to_string (field->name)); g_value_unset (&field->value); return; } } for (i = 0; i < len; i++) { f = GST_STRUCTURE_FIELD (structure, i); if (G_UNLIKELY (f->name == field->name)) { g_value_unset (&f->value); memcpy (f, field, sizeof (GstStructureField)); return; } } g_array_append_val (structure->fields, *field); } /* If there is no field with the given ID, NULL is returned. */ static GstStructureField * gst_structure_id_get_field (const GstStructure * structure, GQuark field_id) { GstStructureField *field; guint i, len; len = structure->fields->len; for (i = 0; i < len; i++) { field = GST_STRUCTURE_FIELD (structure, i); if (G_UNLIKELY (field->name == field_id)) return field; } return NULL; } /* If there is no field with the given ID, NULL is returned. */ static GstStructureField * gst_structure_get_field (const GstStructure * structure, const gchar * fieldname) { g_return_val_if_fail (structure != NULL, NULL); g_return_val_if_fail (fieldname != NULL, NULL); return gst_structure_id_get_field (structure, g_quark_from_string (fieldname)); } /** * gst_structure_get_value: * @structure: a #GstStructure * @fieldname: the name of the field to get * * Get the value of the field with name @fieldname. * * Returns: the #GValue corresponding to the field with the given name. */ const GValue * gst_structure_get_value (const GstStructure * structure, const gchar * fieldname) { GstStructureField *field; g_return_val_if_fail (structure != NULL, NULL); g_return_val_if_fail (fieldname != NULL, NULL); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return NULL; return &field->value; } /** * gst_structure_id_get_value: * @structure: a #GstStructure * @field: the #GQuark of the field to get * * Get the value of the field with GQuark @field. * * Returns: the #GValue corresponding to the field with the given name * identifier. */ const GValue * gst_structure_id_get_value (const GstStructure * structure, GQuark field) { GstStructureField *gsfield; g_return_val_if_fail (structure != NULL, NULL); gsfield = gst_structure_id_get_field (structure, field); if (gsfield == NULL) return NULL; return &gsfield->value; } /** * gst_structure_remove_field: * @structure: a #GstStructure * @fieldname: the name of the field to remove * * Removes the field with the given name. If the field with the given * name does not exist, the structure is unchanged. */ void gst_structure_remove_field (GstStructure * structure, const gchar * fieldname) { GstStructureField *field; GQuark id; guint i, len; g_return_if_fail (structure != NULL); g_return_if_fail (fieldname != NULL); g_return_if_fail (IS_MUTABLE (structure)); id = g_quark_from_string (fieldname); len = structure->fields->len; for (i = 0; i < len; i++) { field = GST_STRUCTURE_FIELD (structure, i); if (field->name == id) { if (G_IS_VALUE (&field->value)) { g_value_unset (&field->value); } structure->fields = g_array_remove_index (structure->fields, i); return; } } } /** * gst_structure_remove_fields: * @structure: a #GstStructure * @fieldname: the name of the field to remove * @...: NULL-terminated list of more fieldnames to remove * * Removes the fields with the given names. If a field does not exist, the * argument is ignored. */ void gst_structure_remove_fields (GstStructure * structure, const gchar * fieldname, ...) { va_list varargs; g_return_if_fail (structure != NULL); g_return_if_fail (fieldname != NULL); /* mutability checked in remove_field */ va_start (varargs, fieldname); gst_structure_remove_fields_valist (structure, fieldname, varargs); va_end (varargs); } /** * gst_structure_remove_fields_valist: * @structure: a #GstStructure * @fieldname: the name of the field to remove * @varargs: NULL-terminated list of more fieldnames to remove * * va_list form of gst_structure_remove_fields(). */ void gst_structure_remove_fields_valist (GstStructure * structure, const gchar * fieldname, va_list varargs) { gchar *field = (gchar *) fieldname; g_return_if_fail (structure != NULL); g_return_if_fail (fieldname != NULL); /* mutability checked in remove_field */ while (field) { gst_structure_remove_field (structure, field); field = va_arg (varargs, char *); } } /** * gst_structure_remove_all_fields: * @structure: a #GstStructure * * Removes all fields in a GstStructure. */ void gst_structure_remove_all_fields (GstStructure * structure) { GstStructureField *field; int i; g_return_if_fail (structure != NULL); g_return_if_fail (IS_MUTABLE (structure)); for (i = structure->fields->len - 1; i >= 0; i--) { field = GST_STRUCTURE_FIELD (structure, i); if (G_IS_VALUE (&field->value)) { g_value_unset (&field->value); } structure->fields = g_array_remove_index (structure->fields, i); } } /** * gst_structure_get_field_type: * @structure: a #GstStructure * @fieldname: the name of the field * * Finds the field with the given name, and returns the type of the * value it contains. If the field is not found, G_TYPE_INVALID is * returned. * * Returns: the #GValue of the field */ GType gst_structure_get_field_type (const GstStructure * structure, const gchar * fieldname) { GstStructureField *field; g_return_val_if_fail (structure != NULL, G_TYPE_INVALID); g_return_val_if_fail (fieldname != NULL, G_TYPE_INVALID); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return G_TYPE_INVALID; return G_VALUE_TYPE (&field->value); } /** * gst_structure_n_fields: * @structure: a #GstStructure * * Get the number of fields in the structure. * * Returns: the number of fields in the structure */ gint gst_structure_n_fields (const GstStructure * structure) { g_return_val_if_fail (structure != NULL, 0); return structure->fields->len; } /** * gst_structure_nth_field_name: * @structure: a #GstStructure * @index: the index to get the name of * * Get the name of the given field number, counting from 0 onwards. * * Returns: the name of the given field number */ const gchar * gst_structure_nth_field_name (const GstStructure * structure, guint index) { GstStructureField *field; g_return_val_if_fail (structure != NULL, NULL); g_return_val_if_fail (index < structure->fields->len, NULL); field = GST_STRUCTURE_FIELD (structure, index); return g_quark_to_string (field->name); } /** * gst_structure_foreach: * @structure: a #GstStructure * @func: a function to call for each field * @user_data: (closure): private data * * Calls the provided function once for each field in the #GstStructure. The * function must not modify the fields. Also see gst_structure_map_in_place(). * * Returns: TRUE if the supplied function returns TRUE For each of the fields, * FALSE otherwise. */ gboolean gst_structure_foreach (const GstStructure * structure, GstStructureForeachFunc func, gpointer user_data) { guint i, len; GstStructureField *field; gboolean ret; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (func != NULL, FALSE); len = structure->fields->len; for (i = 0; i < len; i++) { field = GST_STRUCTURE_FIELD (structure, i); ret = func (field->name, &field->value, user_data); if (G_UNLIKELY (!ret)) return FALSE; } return TRUE; } /** * gst_structure_map_in_place: * @structure: a #GstStructure * @func: a function to call for each field * @user_data: (closure): private data * * Calls the provided function once for each field in the #GstStructure. In * contrast to gst_structure_foreach(), the function may modify but not delete the * fields. The structure must be mutable. * * Returns: TRUE if the supplied function returns TRUE For each of the fields, * FALSE otherwise. */ gboolean gst_structure_map_in_place (GstStructure * structure, GstStructureMapFunc func, gpointer user_data) { guint i, len; GstStructureField *field; gboolean ret; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (IS_MUTABLE (structure), FALSE); g_return_val_if_fail (func != NULL, FALSE); len = structure->fields->len; for (i = 0; i < len; i++) { field = GST_STRUCTURE_FIELD (structure, i); ret = func (field->name, &field->value, user_data); if (!ret) return FALSE; } return TRUE; } /** * gst_structure_id_has_field: * @structure: a #GstStructure * @field: #GQuark of the field name * * Check if @structure contains a field named @field. * * Returns: TRUE if the structure contains a field with the given name * * Since: 0.10.26 */ gboolean gst_structure_id_has_field (const GstStructure * structure, GQuark field) { GstStructureField *f; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (field != 0, FALSE); f = gst_structure_id_get_field (structure, field); return (f != NULL); } /** * gst_structure_has_field: * @structure: a #GstStructure * @fieldname: the name of a field * * Check if @structure contains a field named @fieldname. * * Returns: TRUE if the structure contains a field with the given name */ gboolean gst_structure_has_field (const GstStructure * structure, const gchar * fieldname) { g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); return gst_structure_id_has_field (structure, g_quark_from_string (fieldname)); } /** * gst_structure_id_has_field_typed: * @structure: a #GstStructure * @field: #GQuark of the field name * @type: the type of a value * * Check if @structure contains a field named @field and with GType @type. * * Returns: TRUE if the structure contains a field with the given name and type * * Since: 0.10.26 */ gboolean gst_structure_id_has_field_typed (const GstStructure * structure, GQuark field, GType type) { GstStructureField *f; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (field != 0, FALSE); f = gst_structure_id_get_field (structure, field); if (f == NULL) return FALSE; return (G_VALUE_TYPE (&f->value) == type); } /** * gst_structure_has_field_typed: * @structure: a #GstStructure * @fieldname: the name of a field * @type: the type of a value * * Check if @structure contains a field named @fieldname and with GType @type. * * Returns: TRUE if the structure contains a field with the given name and type */ gboolean gst_structure_has_field_typed (const GstStructure * structure, const gchar * fieldname, GType type) { g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); return gst_structure_id_has_field_typed (structure, g_quark_from_string (fieldname), type); } /* utility functions */ /** * gst_structure_get_boolean: * @structure: a #GstStructure * @fieldname: the name of a field * @value: (out): a pointer to a #gboolean to set * * Sets the boolean pointed to by @value corresponding to the value of the * given field. Caller is responsible for making sure the field exists * and has the correct type. * * Returns: TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain a boolean, this * function returns FALSE. */ gboolean gst_structure_get_boolean (const GstStructure * structure, const gchar * fieldname, gboolean * value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!G_VALUE_HOLDS_BOOLEAN (&field->value)) return FALSE; *value = gst_g_value_get_boolean_unchecked (&field->value); return TRUE; } /** * gst_structure_get_int: * @structure: a #GstStructure * @fieldname: the name of a field * @value: (out): a pointer to an int to set * * Sets the int pointed to by @value corresponding to the value of the * given field. Caller is responsible for making sure the field exists * and has the correct type. * * Returns: %TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain an int, this function * returns %FALSE. */ gboolean gst_structure_get_int (const GstStructure * structure, const gchar * fieldname, gint * value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (value != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!G_VALUE_HOLDS_INT (&field->value)) return FALSE; *value = gst_g_value_get_int_unchecked (&field->value); return TRUE; } /** * gst_structure_get_uint: * @structure: a #GstStructure * @fieldname: the name of a field * @value: (out): a pointer to a uint to set * * Sets the uint pointed to by @value corresponding to the value of the * given field. Caller is responsible for making sure the field exists * and has the correct type. * * Returns: %TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain a uint, this function * returns %FALSE. * * Since: 0.10.15 */ gboolean gst_structure_get_uint (const GstStructure * structure, const gchar * fieldname, guint * value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (value != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!G_VALUE_HOLDS_UINT (&field->value)) return FALSE; *value = gst_g_value_get_uint_unchecked (&field->value); return TRUE; } /** * gst_structure_get_fourcc: * @structure: a #GstStructure * @fieldname: the name of a field * @value: (out): a pointer to a 32bit unsigned int to set * * Sets the Fourcc pointed to by @value corresponding to the value of the * given field. Caller is responsible for making sure the field exists * and has the correct type. * * Returns: TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain a fourcc, this function * returns FALSE. */ gboolean gst_structure_get_fourcc (const GstStructure * structure, const gchar * fieldname, guint32 * value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (value != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!GST_VALUE_HOLDS_FOURCC (&field->value)) return FALSE; *value = gst_value_get_fourcc (&field->value); return TRUE; } /** * gst_structure_get_date: * @structure: a #GstStructure * @fieldname: the name of a field * @value: (out callee-allocates): a pointer to a #GDate to set * * Sets the date pointed to by @value corresponding to the date of the * given field. Caller is responsible for making sure the field exists * and has the correct type. * * On success @value will point to a newly-allocated copy of the date which * should be freed with g_date_free() when no longer needed (note: this is * inconsistent with e.g. gst_structure_get_string() which doesn't return a * copy of the string). * * Returns: TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain a data, this function * returns FALSE. */ gboolean gst_structure_get_date (const GstStructure * structure, const gchar * fieldname, GDate ** value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (value != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!GST_VALUE_HOLDS_DATE (&field->value)) return FALSE; /* FIXME: 0.11 g_value_dup_boxed() -> g_value_get_boxed() */ *value = g_value_dup_boxed (&field->value); return TRUE; } /** * gst_structure_get_date_time: * @structure: a #GstStructure * @fieldname: the name of a field * @value: (out callee-allocates): a pointer to a #GstDateTime to set * * Sets the datetime pointed to by @value corresponding to the datetime of the * given field. Caller is responsible for making sure the field exists * and has the correct type. * * On success @value will point to a reference of the datetime which * should be unreffed with gst_date_time_unref() when no longer needed * (note: this is inconsistent with e.g. gst_structure_get_string() * which doesn't return a copy of the string). * * Returns: TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain a data, this function * returns FALSE. * * Since: 0.10.31 */ gboolean gst_structure_get_date_time (const GstStructure * structure, const gchar * fieldname, GstDateTime ** value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (value != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!GST_VALUE_HOLDS_DATE_TIME (&field->value)) return FALSE; /* FIXME: 0.11 g_value_dup_boxed() -> g_value_get_boxed() */ *value = g_value_dup_boxed (&field->value); return TRUE; } /** * gst_structure_get_clock_time: * @structure: a #GstStructure * @fieldname: the name of a field * @value: (out): a pointer to a #GstClockTime to set * * Sets the clock time pointed to by @value corresponding to the clock time * of the given field. Caller is responsible for making sure the field exists * and has the correct type. * * Returns: TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain a #GstClockTime, this * function returns FALSE. */ gboolean gst_structure_get_clock_time (const GstStructure * structure, const gchar * fieldname, GstClockTime * value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (value != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!G_VALUE_HOLDS_UINT64 (&field->value)) return FALSE; *value = gst_g_value_get_uint64_unchecked (&field->value); return TRUE; } /** * gst_structure_get_double: * @structure: a #GstStructure * @fieldname: the name of a field * @value: (out): a pointer to a gdouble to set * * Sets the double pointed to by @value corresponding to the value of the * given field. Caller is responsible for making sure the field exists * and has the correct type. * * Returns: TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain a double, this * function returns FALSE. */ gboolean gst_structure_get_double (const GstStructure * structure, const gchar * fieldname, gdouble * value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (value != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!G_VALUE_HOLDS_DOUBLE (&field->value)) return FALSE; *value = gst_g_value_get_double_unchecked (&field->value); return TRUE; } /** * gst_structure_get_string: * @structure: a #GstStructure * @fieldname: the name of a field * * Finds the field corresponding to @fieldname, and returns the string * contained in the field's value. Caller is responsible for making * sure the field exists and has the correct type. * * The string should not be modified, and remains valid until the next * call to a gst_structure_*() function with the given structure. * * Returns: a pointer to the string or NULL when the field did not exist * or did not contain a string. */ const gchar * gst_structure_get_string (const GstStructure * structure, const gchar * fieldname) { GstStructureField *field; g_return_val_if_fail (structure != NULL, NULL); g_return_val_if_fail (fieldname != NULL, NULL); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return NULL; if (!G_VALUE_HOLDS_STRING (&field->value)) return NULL; return gst_g_value_get_string_unchecked (&field->value); } /** * gst_structure_get_enum: * @structure: a #GstStructure * @fieldname: the name of a field * @enumtype: the enum type of a field * @value: (out): a pointer to an int to set * * Sets the int pointed to by @value corresponding to the value of the * given field. Caller is responsible for making sure the field exists, * has the correct type and that the enumtype is correct. * * Returns: TRUE if the value could be set correctly. If there was no field * with @fieldname or the existing field did not contain an enum of the given * type, this function returns FALSE. */ gboolean gst_structure_get_enum (const GstStructure * structure, const gchar * fieldname, GType enumtype, gint * value) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (enumtype != G_TYPE_INVALID, FALSE); g_return_val_if_fail (value != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!G_TYPE_CHECK_VALUE_TYPE (&field->value, enumtype)) return FALSE; *value = g_value_get_enum (&field->value); return TRUE; } /** * gst_structure_get_fraction: * @structure: a #GstStructure * @fieldname: the name of a field * @value_numerator: (out): a pointer to an int to set * @value_denominator: (out): a pointer to an int to set * * Sets the integers pointed to by @value_numerator and @value_denominator * corresponding to the value of the given field. Caller is responsible * for making sure the field exists and has the correct type. * * Returns: TRUE if the values could be set correctly. If there was no field * with @fieldname or the existing field did not contain a GstFraction, this * function returns FALSE. */ gboolean gst_structure_get_fraction (const GstStructure * structure, const gchar * fieldname, gint * value_numerator, gint * value_denominator) { GstStructureField *field; g_return_val_if_fail (structure != NULL, FALSE); g_return_val_if_fail (fieldname != NULL, FALSE); g_return_val_if_fail (value_numerator != NULL, FALSE); g_return_val_if_fail (value_denominator != NULL, FALSE); field = gst_structure_get_field (structure, fieldname); if (field == NULL) return FALSE; if (!GST_VALUE_HOLDS_FRACTION (&field->value)) return FALSE; *value_numerator = gst_value_get_fraction_numerator (&field->value); *value_denominator = gst_value_get_fraction_denominator (&field->value); return TRUE; } typedef struct _GstStructureAbbreviation { const gchar *type_name; GType type; } GstStructureAbbreviation; /* return a copy of an array of GstStructureAbbreviation containing all the * known type_string, GType maps, including abbreviations for common types */ static GstStructureAbbreviation * gst_structure_get_abbrs (gint * n_abbrs) { static GstStructureAbbreviation *abbrs = NULL; static volatile gsize num = 0; if (g_once_init_enter (&num)) { /* dynamically generate the array */ gsize _num; GstStructureAbbreviation dyn_abbrs[] = { {"int", G_TYPE_INT} , {"i", G_TYPE_INT} , {"uint", G_TYPE_UINT} , {"u", G_TYPE_UINT} , {"float", G_TYPE_FLOAT} , {"f", G_TYPE_FLOAT} , {"double", G_TYPE_DOUBLE} , {"d", G_TYPE_DOUBLE} , {"buffer", GST_TYPE_BUFFER} , {"fourcc", GST_TYPE_FOURCC} , {"4", GST_TYPE_FOURCC} , {"fraction", GST_TYPE_FRACTION} , {"boolean", G_TYPE_BOOLEAN} , {"bool", G_TYPE_BOOLEAN} , {"b", G_TYPE_BOOLEAN} , {"string", G_TYPE_STRING} , {"str", G_TYPE_STRING} , {"s", G_TYPE_STRING} , {"structure", GST_TYPE_STRUCTURE} , {"datetime", GST_TYPE_DATE_TIME} }; _num = G_N_ELEMENTS (dyn_abbrs); /* permanently allocate and copy the array now */ abbrs = g_new0 (GstStructureAbbreviation, _num); memcpy (abbrs, dyn_abbrs, sizeof (GstStructureAbbreviation) * _num); g_once_init_leave (&num, _num); } *n_abbrs = num; return abbrs; } /* given a type_name that could be a type abbreviation or a registered GType, * return a matching GType */ static GType gst_structure_gtype_from_abbr (const char *type_name) { int i; GstStructureAbbreviation *abbrs; gint n_abbrs; g_return_val_if_fail (type_name != NULL, G_TYPE_INVALID); abbrs = gst_structure_get_abbrs (&n_abbrs); for (i = 0; i < n_abbrs; i++) { if (strcmp (type_name, abbrs[i].type_name) == 0) { return abbrs[i].type; } } /* this is the fallback */ return g_type_from_name (type_name); } static const char * gst_structure_to_abbr (GType type) { int i; GstStructureAbbreviation *abbrs; gint n_abbrs; g_return_val_if_fail (type != G_TYPE_INVALID, NULL); abbrs = gst_structure_get_abbrs (&n_abbrs); for (i = 0; i < n_abbrs; i++) { if (type == abbrs[i].type) { return abbrs[i].type_name; } } return g_type_name (type); } static GType gst_structure_value_get_generic_type (GValue * val) { if (G_VALUE_TYPE (val) == GST_TYPE_LIST || G_VALUE_TYPE (val) == GST_TYPE_ARRAY) { GArray *array = g_value_peek_pointer (val); if (array->len > 0) { GValue *value = &g_array_index (array, GValue, 0); return gst_structure_value_get_generic_type (value); } else { return G_TYPE_INT; } } else if (G_VALUE_TYPE (val) == GST_TYPE_INT_RANGE) { return G_TYPE_INT; } else if (G_VALUE_TYPE (val) == GST_TYPE_INT64_RANGE) { return G_TYPE_INT64; } else if (G_VALUE_TYPE (val) == GST_TYPE_DOUBLE_RANGE) { return G_TYPE_DOUBLE; } else if (G_VALUE_TYPE (val) == GST_TYPE_FRACTION_RANGE) { return GST_TYPE_FRACTION; } return G_VALUE_TYPE (val); } gboolean priv_gst_structure_append_to_gstring (const GstStructure * structure, GString * s) { GstStructureField *field; guint i, len; g_return_val_if_fail (s != NULL, FALSE); g_string_append (s, g_quark_to_string (structure->name)); len = structure->fields->len; for (i = 0; i < len; i++) { char *t; GType type; field = GST_STRUCTURE_FIELD (structure, i); t = gst_value_serialize (&field->value); type = gst_structure_value_get_generic_type (&field->value); g_string_append_len (s, ", ", 2); /* FIXME: do we need to escape fieldnames? */ g_string_append (s, g_quark_to_string (field->name)); g_string_append_len (s, "=(", 2); g_string_append (s, gst_structure_to_abbr (type)); g_string_append_c (s, ')'); g_string_append (s, t == NULL ? "NULL" : t); g_free (t); } g_string_append_c (s, ';'); return TRUE; } /** * gst_structure_to_string: * @structure: a #GstStructure * * Converts @structure to a human-readable string representation. * * For debugging purposes its easier to do something like this: * |[ * GST_LOG ("structure is %" GST_PTR_FORMAT, structure); * ]| * This prints the structure in human readble form. * * Free-function: g_free * * Returns: (transfer full)L a pointer to string allocated by g_malloc(). * g_free() after usage. */ gchar * gst_structure_to_string (const GstStructure * structure) { GString *s; /* NOTE: This function is potentially called by the debug system, * so any calls to gst_log() (and GST_DEBUG(), GST_LOG(), etc.) * should be careful to avoid recursion. This includes any functions * called by gst_structure_to_string. In particular, calls should * not use the GST_PTR_FORMAT extension. */ g_return_val_if_fail (structure != NULL, NULL); /* we estimate a minimum size based on the number of fields in order to * avoid unnecessary reallocs within GString */ s = g_string_sized_new (STRUCTURE_ESTIMATED_STRING_LEN (structure)); priv_gst_structure_append_to_gstring (structure, s); return g_string_free (s, FALSE); } /* * r will still point to the string. if end == next, the string will not be * null-terminated. In all other cases it will be. * end = pointer to char behind end of string, next = pointer to start of * unread data. * THIS FUNCTION MODIFIES THE STRING AND DETECTS INSIDE A NONTERMINATED STRING */ static gboolean gst_structure_parse_string (gchar * s, gchar ** end, gchar ** next, gboolean unescape) { gchar *w; if (*s == 0) return FALSE; if (*s != '"') { int ret; ret = gst_structure_parse_simple_string (s, end); *next = *end; return ret; } if (unescape) { w = s; s++; while (*s != '"') { if (G_UNLIKELY (*s == 0)) return FALSE; if (G_UNLIKELY (*s == '\\')) s++; *w = *s; w++; s++; } s++; } else { /* Find the closing quotes */ s++; while (*s != '"') { if (G_UNLIKELY (*s == 0)) return FALSE; if (G_UNLIKELY (*s == '\\')) s++; s++; } s++; w = s; } *end = w; *next = s; return TRUE; } static gboolean gst_structure_parse_range (gchar * s, gchar ** after, GValue * value, GType type) { GValue value1 = { 0 }; GValue value2 = { 0 }; GType range_type; gboolean ret; if (*s != '[') return FALSE; s++; ret = gst_structure_parse_value (s, &s, &value1, type); if (ret == FALSE) return FALSE; while (g_ascii_isspace (*s)) s++; if (*s != ',') return FALSE; s++; while (g_ascii_isspace (*s)) s++; ret = gst_structure_parse_value (s, &s, &value2, type); if (ret == FALSE) return FALSE; while (g_ascii_isspace (*s)) s++; if (*s != ']') return FALSE; s++; if (G_VALUE_TYPE (&value1) != G_VALUE_TYPE (&value2)) return FALSE; if (G_VALUE_TYPE (&value1) == G_TYPE_DOUBLE) { range_type = GST_TYPE_DOUBLE_RANGE; g_value_init (value, range_type); gst_value_set_double_range (value, gst_g_value_get_double_unchecked (&value1), gst_g_value_get_double_unchecked (&value2)); } else if (G_VALUE_TYPE (&value1) == G_TYPE_INT) { range_type = GST_TYPE_INT_RANGE; g_value_init (value, range_type); gst_value_set_int_range (value, gst_g_value_get_int_unchecked (&value1), gst_g_value_get_int_unchecked (&value2)); } else if (G_VALUE_TYPE (&value1) == G_TYPE_INT64) { range_type = GST_TYPE_INT64_RANGE; g_value_init (value, range_type); gst_value_set_int64_range (value, gst_g_value_get_int64_unchecked (&value1), gst_g_value_get_int64_unchecked (&value2)); } else if (G_VALUE_TYPE (&value1) == GST_TYPE_FRACTION) { range_type = GST_TYPE_FRACTION_RANGE; g_value_init (value, range_type); gst_value_set_fraction_range (value, &value1, &value2); } else { return FALSE; } *after = s; return TRUE; } static gboolean gst_structure_parse_any_list (gchar * s, gchar ** after, GValue * value, GType type, GType list_type, char begin, char end) { GValue list_value = { 0 }; gboolean ret; GArray *array; g_value_init (value, list_type); array = g_value_peek_pointer (value); if (*s != begin) return FALSE; s++; while (g_ascii_isspace (*s)) s++; if (*s == end) { s++; *after = s; return TRUE; } ret = gst_structure_parse_value (s, &s, &list_value, type); if (ret == FALSE) return FALSE; g_array_append_val (array, list_value); while (g_ascii_isspace (*s)) s++; while (*s != end) { if (*s != ',') return FALSE; s++; while (g_ascii_isspace (*s)) s++; memset (&list_value, 0, sizeof (list_value)); ret = gst_structure_parse_value (s, &s, &list_value, type); if (ret == FALSE) return FALSE; g_array_append_val (array, list_value); while (g_ascii_isspace (*s)) s++; } s++; *after = s; return TRUE; } static gboolean gst_structure_parse_list (gchar * s, gchar ** after, GValue * value, GType type) { return gst_structure_parse_any_list (s, after, value, type, GST_TYPE_LIST, '{', '}'); } static gboolean gst_structure_parse_array (gchar * s, gchar ** after, GValue * value, GType type) { return gst_structure_parse_any_list (s, after, value, type, GST_TYPE_ARRAY, '<', '>'); } static gboolean gst_structure_parse_simple_string (gchar * str, gchar ** end) { char *s = str; while (G_LIKELY (GST_ASCII_IS_STRING (*s))) { s++; } *end = s; return (s != str); } static gboolean gst_structure_parse_field (gchar * str, gchar ** after, GstStructureField * field) { gchar *name; gchar *name_end; gchar *s; gchar c; s = str; while (g_ascii_isspace (*s) || (s[0] == '\\' && g_ascii_isspace (s[1]))) s++; name = s; if (G_UNLIKELY (!gst_structure_parse_simple_string (s, &name_end))) { GST_WARNING ("failed to parse simple string, str=%s", str); return FALSE; } s = name_end; while (g_ascii_isspace (*s) || (s[0] == '\\' && g_ascii_isspace (s[1]))) s++; if (G_UNLIKELY (*s != '=')) { GST_WARNING ("missing assignment operator in the field, str=%s", str); return FALSE; } s++; c = *name_end; *name_end = '\0'; field->name = g_quark_from_string (name); GST_DEBUG ("trying field name '%s'", name); *name_end = c; if (G_UNLIKELY (!gst_structure_parse_value (s, &s, &field->value, G_TYPE_INVALID))) { GST_WARNING ("failed to parse value %s", str); return FALSE; } *after = s; return TRUE; } static gboolean gst_structure_parse_value (gchar * str, gchar ** after, GValue * value, GType default_type) { gchar *type_name; gchar *type_end; gchar *value_s; gchar *value_end; gchar *s; gchar c; int ret = 0; GType type = default_type; s = str; while (g_ascii_isspace (*s)) s++; /* check if there's a (type_name) 'cast' */ type_name = NULL; if (*s == '(') { s++; while (g_ascii_isspace (*s)) s++; type_name = s; if (G_UNLIKELY (!gst_structure_parse_simple_string (s, &type_end))) return FALSE; s = type_end; while (g_ascii_isspace (*s)) s++; if (G_UNLIKELY (*s != ')')) return FALSE; s++; while (g_ascii_isspace (*s)) s++; c = *type_end; *type_end = 0; type = gst_structure_gtype_from_abbr (type_name); GST_DEBUG ("trying type name '%s'", type_name); *type_end = c; if (G_UNLIKELY (type == G_TYPE_INVALID)) { GST_WARNING ("invalid type"); return FALSE; } } while (g_ascii_isspace (*s)) s++; if (*s == '[') { ret = gst_structure_parse_range (s, &s, value, type); } else if (*s == '{') { ret = gst_structure_parse_list (s, &s, value, type); } else if (*s == '<') { ret = gst_structure_parse_array (s, &s, value, type); } else { value_s = s; if (G_UNLIKELY (type == G_TYPE_INVALID)) { GType try_types[] = { G_TYPE_INT, G_TYPE_DOUBLE, GST_TYPE_FRACTION, G_TYPE_BOOLEAN, G_TYPE_STRING }; int i; if (G_UNLIKELY (!gst_structure_parse_string (s, &value_end, &s, TRUE))) return FALSE; /* Set NULL terminator for deserialization */ c = *value_end; *value_end = '\0'; for (i = 0; i < G_N_ELEMENTS (try_types); i++) { g_value_init (value, try_types[i]); ret = gst_value_deserialize (value, value_s); if (ret) break; g_value_unset (value); } } else { g_value_init (value, type); if (G_UNLIKELY (!gst_structure_parse_string (s, &value_end, &s, (type != G_TYPE_STRING)))) return FALSE; /* Set NULL terminator for deserialization */ c = *value_end; *value_end = '\0'; ret = gst_value_deserialize (value, value_s); if (G_UNLIKELY (!ret)) g_value_unset (value); } *value_end = c; } *after = s; return ret; } /** * gst_structure_from_string: * @string: a string representation of a #GstStructure. * @end: (out) (allow-none): pointer to store the end of the string in. * * Creates a #GstStructure from a string representation. * If end is not NULL, a pointer to the place inside the given string * where parsing ended will be returned. * * Free-function: gst_structure_free * * Returns: (transfer full): a new #GstStructure or NULL when the string could * not be parsed. Free with gst_structure_free() after use. */ GstStructure * gst_structure_from_string (const gchar * string, gchar ** end) { char *name; char *copy; char *w; char *r; char save; GstStructure *structure = NULL; GstStructureField field; g_return_val_if_fail (string != NULL, NULL); copy = g_strdup (string); r = copy; /* skip spaces (FIXME: _isspace treats tabs and newlines as space!) */ while (*r && (g_ascii_isspace (*r) || (r[0] == '\\' && g_ascii_isspace (r[1])))) r++; name = r; if (G_UNLIKELY (!gst_structure_parse_string (r, &w, &r, TRUE))) { GST_WARNING ("Failed to parse structure string '%s'", string); goto error; } save = *w; *w = '\0'; structure = gst_structure_empty_new (name); *w = save; if (G_UNLIKELY (structure == NULL)) goto error; do { while (*r && (g_ascii_isspace (*r) || (r[0] == '\\' && g_ascii_isspace (r[1])))) r++; if (*r == ';') { /* end of structure, get the next char and finish */ r++; break; } if (*r == '\0') { /* accept \0 as end delimiter */ break; } if (G_UNLIKELY (*r != ',')) { GST_WARNING ("Failed to find delimiter, r=%s", r); goto error; } r++; while (*r && (g_ascii_isspace (*r) || (r[0] == '\\' && g_ascii_isspace (r[1])))) r++; memset (&field, 0, sizeof (field)); if (G_UNLIKELY (!gst_structure_parse_field (r, &r, &field))) { GST_WARNING ("Failed to parse field, r=%s", r); goto error; } gst_structure_set_field (structure, &field); } while (TRUE); if (end) *end = (char *) string + (r - copy); else if (*r) g_warning ("gst_structure_from_string did not consume whole string," " but caller did not provide end pointer (\"%s\")", string); g_free (copy); return structure; error: if (structure) gst_structure_free (structure); g_free (copy); return NULL; } static void gst_structure_transform_to_string (const GValue * src_value, GValue * dest_value) { g_return_if_fail (src_value != NULL); g_return_if_fail (dest_value != NULL); dest_value->data[0].v_pointer = gst_structure_to_string (src_value->data[0].v_pointer); } static GstStructure * gst_structure_copy_conditional (const GstStructure * structure) { if (structure) return gst_structure_copy (structure); return NULL; } /* fixate utility functions */ /** * gst_structure_fixate_field_nearest_int: * @structure: a #GstStructure * @field_name: a field in @structure * @target: the target value of the fixation * * Fixates a #GstStructure by changing the given field to the nearest * integer to @target that is a subset of the existing field. * * Returns: TRUE if the structure could be fixated */ gboolean gst_structure_fixate_field_nearest_int (GstStructure * structure, const char *field_name, int target) { const GValue *value; g_return_val_if_fail (gst_structure_has_field (structure, field_name), FALSE); g_return_val_if_fail (IS_MUTABLE (structure), FALSE); value = gst_structure_get_value (structure, field_name); if (G_VALUE_TYPE (value) == G_TYPE_INT) { /* already fixed */ return FALSE; } else if (G_VALUE_TYPE (value) == GST_TYPE_INT_RANGE) { int x; x = gst_value_get_int_range_min (value); if (target < x) target = x; x = gst_value_get_int_range_max (value); if (target > x) target = x; gst_structure_set (structure, field_name, G_TYPE_INT, target, NULL); return TRUE; } else if (G_VALUE_TYPE (value) == GST_TYPE_LIST) { const GValue *list_value; int i, n; int best = 0; int best_index = -1; n = gst_value_list_get_size (value); for (i = 0; i < n; i++) { list_value = gst_value_list_get_value (value, i); if (G_VALUE_TYPE (list_value) == G_TYPE_INT) { int x = gst_g_value_get_int_unchecked (list_value); if (best_index == -1 || (ABS (target - x) < ABS (target - best))) { best_index = i; best = x; } } } if (best_index != -1) { gst_structure_set (structure, field_name, G_TYPE_INT, best, NULL); return TRUE; } return FALSE; } return FALSE; } /** * gst_structure_fixate_field_nearest_double: * @structure: a #GstStructure * @field_name: a field in @structure * @target: the target value of the fixation * * Fixates a #GstStructure by changing the given field to the nearest * double to @target that is a subset of the existing field. * * Returns: TRUE if the structure could be fixated */ gboolean gst_structure_fixate_field_nearest_double (GstStructure * structure, const char *field_name, double target) { const GValue *value; g_return_val_if_fail (gst_structure_has_field (structure, field_name), FALSE); g_return_val_if_fail (IS_MUTABLE (structure), FALSE); value = gst_structure_get_value (structure, field_name); if (G_VALUE_TYPE (value) == G_TYPE_DOUBLE) { /* already fixed */ return FALSE; } else if (G_VALUE_TYPE (value) == GST_TYPE_DOUBLE_RANGE) { double x; x = gst_value_get_double_range_min (value); if (target < x) target = x; x = gst_value_get_double_range_max (value); if (target > x) target = x; gst_structure_set (structure, field_name, G_TYPE_DOUBLE, target, NULL); return TRUE; } else if (G_VALUE_TYPE (value) == GST_TYPE_LIST) { const GValue *list_value; int i, n; double best = 0; int best_index = -1; n = gst_value_list_get_size (value); for (i = 0; i < n; i++) { list_value = gst_value_list_get_value (value, i); if (G_VALUE_TYPE (list_value) == G_TYPE_DOUBLE) { double x = gst_g_value_get_double_unchecked (list_value); if (best_index == -1 || (ABS (target - x) < ABS (target - best))) { best_index = i; best = x; } } } if (best_index != -1) { gst_structure_set (structure, field_name, G_TYPE_DOUBLE, best, NULL); return TRUE; } return FALSE; } return FALSE; } /** * gst_structure_fixate_field_boolean: * @structure: a #GstStructure * @field_name: a field in @structure * @target: the target value of the fixation * * Fixates a #GstStructure by changing the given @field_name field to the given * @target boolean if that field is not fixed yet. * * Returns: TRUE if the structure could be fixated */ gboolean gst_structure_fixate_field_boolean (GstStructure * structure, const char *field_name, gboolean target) { const GValue *value; g_return_val_if_fail (gst_structure_has_field (structure, field_name), FALSE); g_return_val_if_fail (IS_MUTABLE (structure), FALSE); value = gst_structure_get_value (structure, field_name); if (G_VALUE_TYPE (value) == G_TYPE_BOOLEAN) { /* already fixed */ return FALSE; } else if (G_VALUE_TYPE (value) == GST_TYPE_LIST) { const GValue *list_value; int i, n; int best = 0; int best_index = -1; n = gst_value_list_get_size (value); for (i = 0; i < n; i++) { list_value = gst_value_list_get_value (value, i); if (G_VALUE_TYPE (list_value) == G_TYPE_BOOLEAN) { gboolean x = gst_g_value_get_boolean_unchecked (list_value); if (best_index == -1 || x == target) { best_index = i; best = x; } } } if (best_index != -1) { gst_structure_set (structure, field_name, G_TYPE_BOOLEAN, best, NULL); return TRUE; } return FALSE; } return FALSE; } /** * gst_structure_fixate_field_string: * @structure: a #GstStructure * @field_name: a field in @structure * @target: the target value of the fixation * * Fixates a #GstStructure by changing the given @field_name field to the given * @target string if that field is not fixed yet. * * Returns: TRUE if the structure could be fixated * * Since: 0.10.30 */ gboolean gst_structure_fixate_field_string (GstStructure * structure, const gchar * field_name, const gchar * target) { const GValue *value; g_return_val_if_fail (gst_structure_has_field (structure, field_name), FALSE); g_return_val_if_fail (IS_MUTABLE (structure), FALSE); value = gst_structure_get_value (structure, field_name); if (G_VALUE_TYPE (value) == G_TYPE_STRING) { /* already fixed */ return FALSE; } else if (G_VALUE_TYPE (value) == GST_TYPE_LIST) { const GValue *list_value; int i, n; const gchar *best = NULL; int best_index = -1; n = gst_value_list_get_size (value); for (i = 0; i < n; i++) { list_value = gst_value_list_get_value (value, i); if (G_VALUE_TYPE (list_value) == G_TYPE_STRING) { const gchar *x = g_value_get_string (list_value); if (best_index == -1 || g_str_equal (x, target)) { best_index = i; best = x; } } } if (best_index != -1) { gst_structure_set (structure, field_name, G_TYPE_STRING, best, NULL); return TRUE; } return FALSE; } return FALSE; } /** * gst_structure_fixate_field_nearest_fraction: * @structure: a #GstStructure * @field_name: a field in @structure * @target_numerator: The numerator of the target value of the fixation * @target_denominator: The denominator of the target value of the fixation * * Fixates a #GstStructure by changing the given field to the nearest * fraction to @target_numerator/@target_denominator that is a subset * of the existing field. * * Returns: TRUE if the structure could be fixated */ gboolean gst_structure_fixate_field_nearest_fraction (GstStructure * structure, const char *field_name, const gint target_numerator, const gint target_denominator) { const GValue *value; g_return_val_if_fail (gst_structure_has_field (structure, field_name), FALSE); g_return_val_if_fail (IS_MUTABLE (structure), FALSE); value = gst_structure_get_value (structure, field_name); if (G_VALUE_TYPE (value) == GST_TYPE_FRACTION) { /* already fixed */ return FALSE; } else if (G_VALUE_TYPE (value) == GST_TYPE_FRACTION_RANGE) { const GValue *x, *new_value; GValue target = { 0 }; g_value_init (&target, GST_TYPE_FRACTION); gst_value_set_fraction (&target, target_numerator, target_denominator); new_value = ⌖ x = gst_value_get_fraction_range_min (value); if (gst_value_compare (&target, x) == GST_VALUE_LESS_THAN) new_value = x; x = gst_value_get_fraction_range_max (value); if (gst_value_compare (&target, x) == GST_VALUE_GREATER_THAN) new_value = x; gst_structure_set_value (structure, field_name, new_value); g_value_unset (&target); return TRUE; } else if (G_VALUE_TYPE (value) == GST_TYPE_LIST) { const GValue *list_value; int i, n; const GValue *best = NULL; gdouble target; gdouble cur_diff; gdouble best_diff = G_MAXDOUBLE; target = (gdouble) target_numerator / (gdouble) target_denominator; GST_DEBUG ("target %g, best %g", target, best_diff); best = NULL; n = gst_value_list_get_size (value); for (i = 0; i < n; i++) { list_value = gst_value_list_get_value (value, i); if (G_VALUE_TYPE (list_value) == GST_TYPE_FRACTION) { gint num, denom; gdouble list_double; num = gst_value_get_fraction_numerator (list_value); denom = gst_value_get_fraction_denominator (list_value); list_double = ((gdouble) num / (gdouble) denom); cur_diff = target - list_double; GST_DEBUG ("curr diff %g, list %g", cur_diff, list_double); if (cur_diff < 0) cur_diff = -cur_diff; if (!best || cur_diff < best_diff) { GST_DEBUG ("new best %g", list_double); best = list_value; best_diff = cur_diff; } } } if (best != NULL) { gst_structure_set_value (structure, field_name, best); return TRUE; } } return FALSE; } /* our very own version of G_VALUE_LCOPY that allows NULL return locations * (useful for message parsing functions where the return location is user * supplied and the user may pass NULL if the value isn't of interest) */ #define GST_VALUE_LCOPY(value, var_args, flags, __error, fieldname) \ G_STMT_START { \ const GValue *_value = (value); \ guint _flags = (flags); \ GType _value_type = G_VALUE_TYPE (_value); \ GTypeValueTable *_vtable = g_type_value_table_peek (_value_type); \ gchar *_lcopy_format = _vtable->lcopy_format; \ GTypeCValue _cvalues[G_VALUE_COLLECT_FORMAT_MAX_LENGTH] = { { 0, }, }; \ guint _n_values = 0; \ \ while (*_lcopy_format != '\0') { \ g_assert (*_lcopy_format == G_VALUE_COLLECT_POINTER); \ _cvalues[_n_values++].v_pointer = va_arg ((var_args), gpointer); \ _lcopy_format++; \ } \ if (_n_values == 2 && !!_cvalues[0].v_pointer != !!_cvalues[1].v_pointer) { \ *(__error) = g_strdup_printf ("either all or none of the return " \ "locations for field '%s' need to be NULL", fieldname); \ } else if (_cvalues[0].v_pointer != NULL) { \ *(__error) = _vtable->lcopy_value (_value, _n_values, _cvalues, _flags); \ } \ } G_STMT_END /** * gst_structure_get_valist: * @structure: a #GstStructure * @first_fieldname: the name of the first field to read * @args: variable arguments * * Parses the variable arguments and reads fields from @structure accordingly. * valist-variant of gst_structure_get(). Look at the documentation of * gst_structure_get() for more details. * * Returns: TRUE, or FALSE if there was a problem reading any of the fields * * Since: 0.10.24 */ gboolean gst_structure_get_valist (const GstStructure * structure, const char *first_fieldname, va_list args) { const char *field_name; GType expected_type = G_TYPE_INVALID; g_return_val_if_fail (GST_IS_STRUCTURE (structure), FALSE); g_return_val_if_fail (first_fieldname != NULL, FALSE); field_name = first_fieldname; while (field_name) { const GValue *val = NULL; gchar *err = NULL; expected_type = va_arg (args, GType); val = gst_structure_get_value (structure, field_name); if (val == NULL) goto no_such_field; if (G_VALUE_TYPE (val) != expected_type) goto wrong_type; GST_VALUE_LCOPY (val, args, 0, &err, field_name); if (err) { g_warning ("%s: %s", G_STRFUNC, err); g_free (err); return FALSE; } field_name = va_arg (args, const gchar *); } return TRUE; /* ERRORS */ no_such_field: { GST_WARNING ("Expected field '%s' in structure: %" GST_PTR_FORMAT, field_name, structure); return FALSE; } wrong_type: { GST_WARNING ("Expected field '%s' in structure to be of type '%s', but " "field was of type '%s': %" GST_PTR_FORMAT, field_name, GST_STR_NULL (g_type_name (expected_type)), G_VALUE_TYPE_NAME (gst_structure_get_value (structure, field_name)), structure); return FALSE; } } /** * gst_structure_id_get_valist: * @structure: a #GstStructure * @first_field_id: the quark of the first field to read * @args: variable arguments * * Parses the variable arguments and reads fields from @structure accordingly. * valist-variant of gst_structure_id_get(). Look at the documentation of * gst_structure_id_get() for more details. * * Returns: TRUE, or FALSE if there was a problem reading any of the fields * * Since: 0.10.24 */ gboolean gst_structure_id_get_valist (const GstStructure * structure, GQuark first_field_id, va_list args) { GQuark field_id; GType expected_type = G_TYPE_INVALID; g_return_val_if_fail (GST_IS_STRUCTURE (structure), FALSE); g_return_val_if_fail (first_field_id != 0, FALSE); field_id = first_field_id; while (field_id) { const GValue *val = NULL; gchar *err = NULL; expected_type = va_arg (args, GType); val = gst_structure_id_get_value (structure, field_id); if (val == NULL) goto no_such_field; if (G_VALUE_TYPE (val) != expected_type) goto wrong_type; GST_VALUE_LCOPY (val, args, 0, &err, g_quark_to_string (field_id)); if (err) { g_warning ("%s: %s", G_STRFUNC, err); g_free (err); return FALSE; } field_id = va_arg (args, GQuark); } return TRUE; /* ERRORS */ no_such_field: { GST_WARNING ("Expected field '%s' in structure: %" GST_PTR_FORMAT, GST_STR_NULL (g_quark_to_string (field_id)), structure); return FALSE; } wrong_type: { GST_WARNING ("Expected field '%s' in structure to be of type '%s', but " "field was of type '%s': %" GST_PTR_FORMAT, g_quark_to_string (field_id), GST_STR_NULL (g_type_name (expected_type)), G_VALUE_TYPE_NAME (gst_structure_id_get_value (structure, field_id)), structure); return FALSE; } } /** * gst_structure_get: * @structure: a #GstStructure * @first_fieldname: the name of the first field to read * @...: variable arguments * * Parses the variable arguments and reads fields from @structure accordingly. * Variable arguments should be in the form field name, field type * (as a GType), pointer(s) to a variable(s) to hold the return value(s). * The last variable argument should be NULL. * * For refcounted (mini)objects you will acquire your own reference which * you must release with a suitable _unref() when no longer needed. For * strings and boxed types you will acquire a copy which you will need to * release with either g_free() or the suiteable function for the boxed type. * * Returns: FALSE if there was a problem reading any of the fields (e.g. * because the field requested did not exist, or was of a type other * than the type specified), otherwise TRUE. * * Since: 0.10.24 */ gboolean gst_structure_get (const GstStructure * structure, const char *first_fieldname, ...) { gboolean ret; va_list args; g_return_val_if_fail (GST_IS_STRUCTURE (structure), FALSE); g_return_val_if_fail (first_fieldname != NULL, FALSE); va_start (args, first_fieldname); ret = gst_structure_get_valist (structure, first_fieldname, args); va_end (args); return ret; } /** * gst_structure_id_get: * @structure: a #GstStructure * @first_field_id: the quark of the first field to read * @...: variable arguments * * Parses the variable arguments and reads fields from @structure accordingly. * Variable arguments should be in the form field id quark, field type * (as a GType), pointer(s) to a variable(s) to hold the return value(s). * The last variable argument should be NULL (technically it should be a * 0 quark, but we require NULL so compilers that support it can check for * the NULL terminator and warn if it's not there). * * This function is just like gst_structure_get() only that it is slightly * more efficient since it saves the string-to-quark lookup in the global * quark hashtable. * * For refcounted (mini)objects you will acquire your own reference which * you must release with a suitable _unref() when no longer needed. For * strings and boxed types you will acquire a copy which you will need to * release with either g_free() or the suiteable function for the boxed type. * * Returns: FALSE if there was a problem reading any of the fields (e.g. * because the field requested did not exist, or was of a type other * than the type specified), otherwise TRUE. * * Since: 0.10.24 */ gboolean gst_structure_id_get (const GstStructure * structure, GQuark first_field_id, ...) { gboolean ret; va_list args; g_return_val_if_fail (GST_IS_STRUCTURE (structure), FALSE); g_return_val_if_fail (first_field_id != 0, FALSE); va_start (args, first_field_id); ret = gst_structure_id_get_valist (structure, first_field_id, args); va_end (args); return ret; }