/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2004 Wim Taymans * * gstsystemclock.c: Default clock, uses the system clock * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:gstsystemclock * @short_description: Default clock that uses the current system time * @see_also: #GstClock * * The GStreamer core provides a GstSystemClock based on the system time. * Asynchronous callbacks are scheduled from an internal thread. * * Clock implementors are encouraged to subclass this systemclock as it * implements the async notification. * * Subclasses can however override all of the important methods for sync and * async notifications to implement their own callback methods or blocking * wait operations. * * Last reviewed on 2006-03-08 (0.10.4) */ #include "gst_private.h" #include "gstinfo.h" #include "gstsystemclock.h" #include "gstenumtypes.h" #include "gstpoll.h" #include "gstutils.h" #include #ifdef G_OS_WIN32 # define WIN32_LEAN_AND_MEAN /* prevents from including too many things */ # include /* QueryPerformance* stuff */ # undef WIN32_LEAN_AND_MEAN # define EWOULDBLOCK EAGAIN /* This is just to placate gcc */ #endif /* G_OS_WIN32 */ #define GET_ENTRY_STATUS(e) (g_atomic_int_get(&GST_CLOCK_ENTRY_STATUS(e))) #define SET_ENTRY_STATUS(e,val) (g_atomic_int_set(&GST_CLOCK_ENTRY_STATUS(e),(val))) #define CAS_ENTRY_STATUS(e,old,val) (g_atomic_int_compare_and_exchange(\ ((volatile gint *)&GST_CLOCK_ENTRY_STATUS(e)), (old), (val))) /* Define this to get some extra debug about jitter from each clock_wait */ #undef WAIT_DEBUGGING struct _GstSystemClockPrivate { GstClockType clock_type; GstPoll *timer; gint wakeup_count; /* the number of entries with a pending wakeup */ gboolean async_wakeup; /* if the wakeup was because of a async list change */ #ifdef G_OS_WIN32 LARGE_INTEGER start; LARGE_INTEGER frequency; #endif /* G_OS_WIN32 */ }; #define GST_SYSTEM_CLOCK_GET_PRIVATE(obj) \ (G_TYPE_INSTANCE_GET_PRIVATE ((obj), GST_TYPE_SYSTEM_CLOCK, \ GstSystemClockPrivate)) #ifdef HAVE_POSIX_TIMERS # ifdef HAVE_MONOTONIC_CLOCK # define DEFAULT_CLOCK_TYPE GST_CLOCK_TYPE_MONOTONIC # else # define DEFAULT_CLOCK_TYPE GST_CLOCK_TYPE_REALTIME # endif #else #define DEFAULT_CLOCK_TYPE GST_CLOCK_TYPE_REALTIME #endif enum { PROP_0, PROP_CLOCK_TYPE, /* FILL ME */ }; /* the one instance of the systemclock */ static GstClock *_the_system_clock = NULL; static void gst_system_clock_dispose (GObject * object); static void gst_system_clock_set_property (GObject * object, guint prop_id, const GValue * value, GParamSpec * pspec); static void gst_system_clock_get_property (GObject * object, guint prop_id, GValue * value, GParamSpec * pspec); static GstClockTime gst_system_clock_get_internal_time (GstClock * clock); static guint64 gst_system_clock_get_resolution (GstClock * clock); static GstClockReturn gst_system_clock_id_wait_jitter (GstClock * clock, GstClockEntry * entry, GstClockTimeDiff * jitter); static GstClockReturn gst_system_clock_id_wait_jitter_unlocked (GstClock * clock, GstClockEntry * entry, GstClockTimeDiff * jitter, gboolean restart); static GstClockReturn gst_system_clock_id_wait_async (GstClock * clock, GstClockEntry * entry); static void gst_system_clock_id_unschedule (GstClock * clock, GstClockEntry * entry); static void gst_system_clock_async_thread (GstClock * clock); static gboolean gst_system_clock_start_async (GstSystemClock * clock); static void gst_system_clock_add_wakeup (GstSystemClock * sysclock); static GStaticMutex _gst_sysclock_mutex = G_STATIC_MUTEX_INIT; static GstClockClass *parent_class = NULL; /* static guint gst_system_clock_signals[LAST_SIGNAL] = { 0 }; */ G_DEFINE_TYPE (GstSystemClock, gst_system_clock, GST_TYPE_CLOCK); static void gst_system_clock_class_init (GstSystemClockClass * klass) { GObjectClass *gobject_class; GstClockClass *gstclock_class; gobject_class = (GObjectClass *) klass; gstclock_class = (GstClockClass *) klass; parent_class = g_type_class_peek_parent (klass); g_type_class_add_private (klass, sizeof (GstSystemClockPrivate)); gobject_class->dispose = gst_system_clock_dispose; gobject_class->set_property = gst_system_clock_set_property; gobject_class->get_property = gst_system_clock_get_property; g_object_class_install_property (gobject_class, PROP_CLOCK_TYPE, g_param_spec_enum ("clock-type", "Clock type", "The type of underlying clock implementation used", GST_TYPE_CLOCK_TYPE, DEFAULT_CLOCK_TYPE, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); gstclock_class->get_internal_time = gst_system_clock_get_internal_time; gstclock_class->get_resolution = gst_system_clock_get_resolution; gstclock_class->wait_jitter = gst_system_clock_id_wait_jitter; gstclock_class->wait_async = gst_system_clock_id_wait_async; gstclock_class->unschedule = gst_system_clock_id_unschedule; } static void gst_system_clock_init (GstSystemClock * clock) { GST_OBJECT_FLAG_SET (clock, GST_CLOCK_FLAG_CAN_DO_SINGLE_SYNC | GST_CLOCK_FLAG_CAN_DO_SINGLE_ASYNC | GST_CLOCK_FLAG_CAN_DO_PERIODIC_SYNC | GST_CLOCK_FLAG_CAN_DO_PERIODIC_ASYNC); clock->priv = GST_SYSTEM_CLOCK_GET_PRIVATE (clock); clock->priv->clock_type = DEFAULT_CLOCK_TYPE; clock->priv->timer = gst_poll_new_timer (); #ifdef G_OS_WIN32 QueryPerformanceFrequency (&clock->priv->frequency); /* can be 0 if the hardware does not have hardware support */ if (clock->priv->frequency.QuadPart != 0) /* we take a base time so that time starts from 0 to ease debugging */ QueryPerformanceCounter (&clock->priv->start); #endif /* G_OS_WIN32 */ #if 0 /* Uncomment this to start the async clock thread straight away */ GST_OBJECT_LOCK (clock); gst_system_clock_start_async (clock); GST_OBJECT_UNLOCK (clock); #endif } static void gst_system_clock_dispose (GObject * object) { GstClock *clock = (GstClock *) object; GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock); GList *entries; /* else we have to stop the thread */ GST_OBJECT_LOCK (clock); sysclock->stopping = TRUE; /* unschedule all entries */ for (entries = clock->entries; entries; entries = g_list_next (entries)) { GstClockEntry *entry = (GstClockEntry *) entries->data; GST_CAT_DEBUG (GST_CAT_CLOCK, "unscheduling entry %p", entry); SET_ENTRY_STATUS (entry, GST_CLOCK_UNSCHEDULED); } GST_CLOCK_BROADCAST (clock); gst_system_clock_add_wakeup (sysclock); GST_OBJECT_UNLOCK (clock); if (sysclock->thread) g_thread_join (sysclock->thread); sysclock->thread = NULL; GST_CAT_DEBUG (GST_CAT_CLOCK, "joined thread"); g_list_foreach (clock->entries, (GFunc) gst_clock_id_unref, NULL); g_list_free (clock->entries); clock->entries = NULL; gst_poll_free (sysclock->priv->timer); G_OBJECT_CLASS (parent_class)->dispose (object); if (_the_system_clock == clock) { _the_system_clock = NULL; GST_CAT_DEBUG (GST_CAT_CLOCK, "disposed system clock"); } } static void gst_system_clock_set_property (GObject * object, guint prop_id, const GValue * value, GParamSpec * pspec) { GstSystemClock *sysclock = GST_SYSTEM_CLOCK (object); switch (prop_id) { case PROP_CLOCK_TYPE: sysclock->priv->clock_type = g_value_get_enum (value); GST_CAT_DEBUG (GST_CAT_CLOCK, "clock-type set to %d", sysclock->priv->clock_type); break; default: G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec); break; } } static void gst_system_clock_get_property (GObject * object, guint prop_id, GValue * value, GParamSpec * pspec) { GstSystemClock *sysclock = GST_SYSTEM_CLOCK (object); switch (prop_id) { case PROP_CLOCK_TYPE: g_value_set_enum (value, sysclock->priv->clock_type); break; default: G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec); break; } } /** * gst_system_clock_obtain: * * Get a handle to the default system clock. The refcount of the * clock will be increased so you need to unref the clock after * usage. * * Returns: (transfer full): the default clock. * * MT safe. */ GstClock * gst_system_clock_obtain (void) { GstClock *clock; g_static_mutex_lock (&_gst_sysclock_mutex); clock = _the_system_clock; if (clock == NULL) { GST_CAT_DEBUG (GST_CAT_CLOCK, "creating new static system clock"); clock = g_object_new (GST_TYPE_SYSTEM_CLOCK, "name", "GstSystemClock", NULL); /* we created the global clock; take ownership so * we can hand out instances later */ gst_object_ref_sink (clock); _the_system_clock = clock; g_static_mutex_unlock (&_gst_sysclock_mutex); } else { g_static_mutex_unlock (&_gst_sysclock_mutex); GST_CAT_DEBUG (GST_CAT_CLOCK, "returning static system clock"); } /* we ref it since we are a clock factory. */ gst_object_ref (clock); return clock; } static void gst_system_clock_remove_wakeup (GstSystemClock * sysclock) { g_return_if_fail (sysclock->priv->wakeup_count > 0); sysclock->priv->wakeup_count--; if (sysclock->priv->wakeup_count == 0) { /* read the control socket byte when we removed the last wakeup count */ GST_CAT_DEBUG (GST_CAT_CLOCK, "reading control"); while (!gst_poll_read_control (sysclock->priv->timer)) { g_warning ("gstsystemclock: read control failed, trying again\n"); } GST_CLOCK_BROADCAST (sysclock); } GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup count %d", sysclock->priv->wakeup_count); } static void gst_system_clock_add_wakeup (GstSystemClock * sysclock) { /* only write the control socket for the first wakeup */ if (sysclock->priv->wakeup_count == 0) { GST_CAT_DEBUG (GST_CAT_CLOCK, "writing control"); while (!gst_poll_write_control (sysclock->priv->timer)) { if (errno == EAGAIN || errno == EWOULDBLOCK || errno == EINTR) { g_warning ("gstsystemclock: write control failed in wakeup_async, trying again: %d:%s\n", errno, g_strerror (errno)); } else { g_critical ("gstsystemclock: write control failed in wakeup_async: %d:%s\n", errno, g_strerror (errno)); return; } } } sysclock->priv->wakeup_count++; GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup count %d", sysclock->priv->wakeup_count); } static void gst_system_clock_wait_wakeup (GstSystemClock * sysclock) { while (sysclock->priv->wakeup_count > 0) { GST_CLOCK_WAIT (sysclock); } } /* this thread reads the sorted clock entries from the queue. * * It waits on each of them and fires the callback when the timeout occurs. * * When an entry in the queue was canceled before we wait for it, it is * simply skipped. * * When waiting for an entry, it can become canceled, in that case we don't * call the callback but move to the next item in the queue. * * MT safe. */ static void gst_system_clock_async_thread (GstClock * clock) { GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock); GST_CAT_DEBUG (GST_CAT_CLOCK, "enter system clock thread"); GST_OBJECT_LOCK (clock); /* signal spinup */ GST_CLOCK_BROADCAST (clock); /* now enter our (almost) infinite loop */ while (!sysclock->stopping) { GstClockEntry *entry; GstClockTime requested; GstClockReturn res; /* check if something to be done */ while (clock->entries == NULL) { GST_CAT_DEBUG (GST_CAT_CLOCK, "no clock entries, waiting.."); /* wait for work to do */ GST_CLOCK_WAIT (clock); GST_CAT_DEBUG (GST_CAT_CLOCK, "got signal"); /* clock was stopping, exit */ if (sysclock->stopping) goto exit; } /* see if we have a pending wakeup because the order of the list * changed. */ if (sysclock->priv->async_wakeup) { GST_CAT_DEBUG (GST_CAT_CLOCK, "clear async wakeup"); gst_system_clock_remove_wakeup (sysclock); sysclock->priv->async_wakeup = FALSE; } /* pick the next entry */ entry = clock->entries->data; GST_OBJECT_UNLOCK (clock); requested = entry->time; /* now wait for the entry, we already hold the lock */ res = gst_system_clock_id_wait_jitter_unlocked (clock, (GstClockID) entry, NULL, FALSE); GST_OBJECT_LOCK (clock); switch (res) { case GST_CLOCK_UNSCHEDULED: /* entry was unscheduled, move to the next */ GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry %p unscheduled", entry); goto next_entry; case GST_CLOCK_OK: case GST_CLOCK_EARLY: { /* entry timed out normally, fire the callback and move to the next * entry */ GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry %p timed out", entry); if (entry->func) { /* unlock before firing the callback */ GST_OBJECT_UNLOCK (clock); entry->func (clock, entry->time, (GstClockID) entry, entry->user_data); GST_OBJECT_LOCK (clock); } if (entry->type == GST_CLOCK_ENTRY_PERIODIC) { GST_CAT_DEBUG (GST_CAT_CLOCK, "updating periodic entry %p", entry); /* adjust time now */ entry->time = requested + entry->interval; /* and resort the list now */ clock->entries = g_list_sort (clock->entries, gst_clock_id_compare_func); /* and restart */ continue; } else { GST_CAT_DEBUG (GST_CAT_CLOCK, "moving to next entry"); goto next_entry; } } case GST_CLOCK_BUSY: /* somebody unlocked the entry but is was not canceled, This means that * either a new entry was added in front of the queue or some other entry * was canceled. Whatever it is, pick the head entry of the list and * continue waiting. */ GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry %p needs restart", entry); /* we set the entry back to the OK state. This is needed so that the * _unschedule() code can see if an entry is currently being waited * on (when its state is BUSY). */ SET_ENTRY_STATUS (entry, GST_CLOCK_OK); continue; default: GST_CAT_DEBUG (GST_CAT_CLOCK, "strange result %d waiting for %p, skipping", res, entry); g_warning ("%s: strange result %d waiting for %p, skipping", GST_OBJECT_NAME (clock), res, entry); goto next_entry; } next_entry: /* we remove the current entry and unref it */ clock->entries = g_list_remove (clock->entries, entry); gst_clock_id_unref ((GstClockID) entry); } exit: /* signal exit */ GST_CLOCK_BROADCAST (clock); GST_OBJECT_UNLOCK (clock); GST_CAT_DEBUG (GST_CAT_CLOCK, "exit system clock thread"); } #ifdef HAVE_POSIX_TIMERS static inline clockid_t clock_type_to_posix_id (GstClockType clock_type) { #ifdef HAVE_MONOTONIC_CLOCK if (clock_type == GST_CLOCK_TYPE_MONOTONIC) return CLOCK_MONOTONIC; else #endif return CLOCK_REALTIME; } #endif /* MT safe */ static GstClockTime gst_system_clock_get_internal_time (GstClock * clock) { #ifdef G_OS_WIN32 GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock); if (sysclock->priv->frequency.QuadPart != 0) { LARGE_INTEGER now; /* we prefer the highly accurate performance counters on windows */ QueryPerformanceCounter (&now); return gst_util_uint64_scale (now.QuadPart - sysclock->priv->start.QuadPart, GST_SECOND, sysclock->priv->frequency.QuadPart); } else #endif /* G_OS_WIN32 */ #if !defined HAVE_POSIX_TIMERS { GTimeVal timeval; g_get_current_time (&timeval); return GST_TIMEVAL_TO_TIME (timeval); } #else { GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock); clockid_t ptype; struct timespec ts; ptype = clock_type_to_posix_id (sysclock->priv->clock_type); if (G_UNLIKELY (clock_gettime (ptype, &ts))) return GST_CLOCK_TIME_NONE; return GST_TIMESPEC_TO_TIME (ts); } #endif } static guint64 gst_system_clock_get_resolution (GstClock * clock) { #ifdef G_OS_WIN32 GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock); if (sysclock->priv->frequency.QuadPart != 0) { return GST_SECOND / sysclock->priv->frequency.QuadPart; } else #endif /* G_OS_WIN32 */ #ifdef HAVE_POSIX_TIMERS { GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock); clockid_t ptype; struct timespec ts; ptype = clock_type_to_posix_id (sysclock->priv->clock_type); if (G_UNLIKELY (clock_getres (ptype, &ts))) return GST_CLOCK_TIME_NONE; return GST_TIMESPEC_TO_TIME (ts); } #else { return 1 * GST_USECOND; } #endif } /* synchronously wait on the given GstClockEntry. * * We do this by blocking on the global GstPoll timer with * the requested timeout. This allows us to unblock the * entry by writing on the control fd. * * Note that writing the global GstPoll unlocks all waiting entries. So * we need to check if an unlocked entry has changed when it unlocks. * * Entries that arrive too late are simply not waited on and a * GST_CLOCK_EARLY result is returned. * * MT safe. */ static GstClockReturn gst_system_clock_id_wait_jitter_unlocked (GstClock * clock, GstClockEntry * entry, GstClockTimeDiff * jitter, gboolean restart) { GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock); GstClockTime entryt, now; GstClockTimeDiff diff; GstClockReturn status; if (G_UNLIKELY (GET_ENTRY_STATUS (entry) == GST_CLOCK_UNSCHEDULED)) return GST_CLOCK_UNSCHEDULED; /* need to call the overridden method because we want to sync against the time * of the clock, whatever the subclass uses as a clock. */ now = gst_clock_get_time (clock); /* get the time of the entry */ entryt = GST_CLOCK_ENTRY_TIME (entry); /* the diff of the entry with the clock is the amount of time we have to * wait */ diff = GST_CLOCK_DIFF (now, entryt); if (G_LIKELY (jitter)) *jitter = -diff; GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p" " time %" GST_TIME_FORMAT " now %" GST_TIME_FORMAT " diff (time-now) %" G_GINT64_FORMAT, entry, GST_TIME_ARGS (entryt), GST_TIME_ARGS (now), diff); if (G_LIKELY (diff > 0)) { #ifdef WAIT_DEBUGGING GstClockTime final; #endif while (TRUE) { gint pollret; do { status = GET_ENTRY_STATUS (entry); /* stop when we are unscheduled */ if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED)) goto done; /* mark the entry as busy but watch out for intermediate unscheduled * statuses */ } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status, GST_CLOCK_BUSY))); /* now wait on the entry, it either times out or the fd is written. The * status of the entry is only BUSY around the poll. */ pollret = gst_poll_wait (sysclock->priv->timer, diff); /* get the new status, mark as DONE. We do this so that the unschedule * function knows when we left the poll and doesn't need to wakeup the * poll anymore. */ do { status = GET_ENTRY_STATUS (entry); /* we were unscheduled, exit immediately */ if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED)) break; } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status, GST_CLOCK_DONE))); GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p unlocked, status %d, ret %d", entry, status, pollret); if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED)) { /* try to clean up The unschedule function managed to set the status to * unscheduled. We now take the lock and mark the entry as unscheduled. * This makes sure that the unschedule function doesn't perform a * wakeup anymore. If the unschedule function has a change to perform * the wakeup before us, we clean up here */ GST_OBJECT_LOCK (sysclock); entry->unscheduled = TRUE; if (entry->woken_up) { gst_system_clock_remove_wakeup (sysclock); } GST_OBJECT_UNLOCK (sysclock); goto done; } else { if (G_UNLIKELY (pollret != 0)) { /* some other id got unlocked */ if (!restart) { /* this can happen if the entry got unlocked because of an async * entry was added to the head of the async queue. */ GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup waiting for entry %p", entry); goto done; } /* wait till all the entries got woken up */ GST_OBJECT_LOCK (sysclock); gst_system_clock_wait_wakeup (sysclock); GST_OBJECT_UNLOCK (sysclock); GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p needs to be restarted", entry); } else { GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p unlocked after timeout", entry); } /* reschedule if gst_poll_wait returned early or we have to reschedule after * an unlock*/ now = gst_clock_get_time (clock); diff = GST_CLOCK_DIFF (now, entryt); if (diff <= 0) { /* timeout, this is fine, we can report success now */ status = GST_CLOCK_OK; SET_ENTRY_STATUS (entry, status); GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p finished, diff %" G_GINT64_FORMAT, entry, diff); #ifdef WAIT_DEBUGGING final = gst_system_clock_get_internal_time (clock); GST_CAT_DEBUG (GST_CAT_CLOCK, "Waited for %" G_GINT64_FORMAT " got %" G_GINT64_FORMAT " diff %" G_GINT64_FORMAT " %g target-offset %" G_GINT64_FORMAT " %g", entryt, now, now - entryt, (double) (GstClockTimeDiff) (now - entryt) / GST_SECOND, (final - target), ((double) (GstClockTimeDiff) (final - target)) / GST_SECOND); #endif goto done; } else { GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p restart, diff %" G_GINT64_FORMAT, entry, diff); } } } } else { /* we are right on time or too late */ if (G_UNLIKELY (diff == 0)) status = GST_CLOCK_OK; else status = GST_CLOCK_EARLY; SET_ENTRY_STATUS (entry, status); } done: return status; } static GstClockReturn gst_system_clock_id_wait_jitter (GstClock * clock, GstClockEntry * entry, GstClockTimeDiff * jitter) { return gst_system_clock_id_wait_jitter_unlocked (clock, entry, jitter, TRUE); } /* Start the async clock thread. Must be called with the object lock * held */ static gboolean gst_system_clock_start_async (GstSystemClock * clock) { GError *error = NULL; if (G_LIKELY (clock->thread != NULL)) return TRUE; /* Thread already running. Nothing to do */ clock->thread = g_thread_create ((GThreadFunc) gst_system_clock_async_thread, clock, TRUE, &error); if (G_UNLIKELY (error)) goto no_thread; /* wait for it to spin up */ GST_CLOCK_WAIT (clock); return TRUE; /* ERRORS */ no_thread: { g_warning ("could not create async clock thread: %s", error->message); g_error_free (error); } return FALSE; } /* Add an entry to the list of pending async waits. The entry is inserted * in sorted order. If we inserted the entry at the head of the list, we * need to signal the thread as it might either be waiting on it or waiting * for a new entry. * * MT safe. */ static GstClockReturn gst_system_clock_id_wait_async (GstClock * clock, GstClockEntry * entry) { GstSystemClock *sysclock; GstClockEntry *head; sysclock = GST_SYSTEM_CLOCK_CAST (clock); GST_CAT_DEBUG (GST_CAT_CLOCK, "adding async entry %p", entry); GST_OBJECT_LOCK (clock); /* Start the clock async thread if needed */ if (G_UNLIKELY (!gst_system_clock_start_async (sysclock))) goto thread_error; if (G_UNLIKELY (GET_ENTRY_STATUS (entry) == GST_CLOCK_UNSCHEDULED)) goto was_unscheduled; if (clock->entries) head = clock->entries->data; else head = NULL; /* need to take a ref */ gst_clock_id_ref ((GstClockID) entry); /* insert the entry in sorted order */ clock->entries = g_list_insert_sorted (clock->entries, entry, gst_clock_id_compare_func); /* only need to send the signal if the entry was added to the * front, else the thread is just waiting for another entry and * will get to this entry automatically. */ if (clock->entries->data == entry) { GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry added to head %p", head); if (head == NULL) { /* the list was empty before, signal the cond so that the async thread can * start taking a look at the queue */ GST_CAT_DEBUG (GST_CAT_CLOCK, "first entry, sending signal"); GST_CLOCK_BROADCAST (clock); } else { GstClockReturn status; status = GET_ENTRY_STATUS (head); GST_CAT_DEBUG (GST_CAT_CLOCK, "head entry %p status %d", head, status); if (status == GST_CLOCK_BUSY) { GST_CAT_DEBUG (GST_CAT_CLOCK, "head entry is busy"); /* the async thread was waiting for an entry, unlock the wait so that it * looks at the new head entry instead, we only need to do this once */ if (!sysclock->priv->async_wakeup) { GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup async thread"); sysclock->priv->async_wakeup = TRUE; gst_system_clock_add_wakeup (sysclock); } } } } GST_OBJECT_UNLOCK (clock); return GST_CLOCK_OK; /* ERRORS */ thread_error: { /* Could not start the async clock thread */ GST_OBJECT_UNLOCK (clock); return GST_CLOCK_ERROR; } was_unscheduled: { GST_OBJECT_UNLOCK (clock); return GST_CLOCK_UNSCHEDULED; } } /* unschedule an entry. This will set the state of the entry to GST_CLOCK_UNSCHEDULED * and will signal any thread waiting for entries to recheck their entry. * We cannot really decide if the signal is needed or not because the entry * could be waited on in async or sync mode. * * MT safe. */ static void gst_system_clock_id_unschedule (GstClock * clock, GstClockEntry * entry) { GstSystemClock *sysclock; GstClockReturn status; sysclock = GST_SYSTEM_CLOCK_CAST (clock); GST_CAT_DEBUG (GST_CAT_CLOCK, "unscheduling entry %p", entry); GST_OBJECT_LOCK (clock); /* change the entry status to unscheduled */ do { status = GET_ENTRY_STATUS (entry); } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status, GST_CLOCK_UNSCHEDULED))); if (G_LIKELY (status == GST_CLOCK_BUSY)) { /* the entry was being busy, wake up all entries so that they recheck their * status. We cannot wake up just one entry because allocating such a * datastructure for each entry would be too heavy and unlocking an entry * is usually done when shutting down or some other exceptional case. */ GST_CAT_DEBUG (GST_CAT_CLOCK, "entry was BUSY, doing wakeup"); if (!entry->unscheduled && !entry->woken_up) { gst_system_clock_add_wakeup (sysclock); entry->woken_up = TRUE; } } GST_OBJECT_UNLOCK (clock); }