/* GStreamer * Copyright (C) 2003 Benjamin Otte * * gsttypefind.c: typefinding subsystem * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:gsttypefind * @short_description: Stream type detection * * The following functions allow you to detect the media type of an unknown * stream. * * Last reviewed on 2005-11-09 (0.9.4) */ #include "gst_private.h" #include "gstinfo.h" #include "gsttypefind.h" #include "gstregistry.h" #include "gsttypefindfactory.h" GST_DEBUG_CATEGORY_EXTERN (type_find_debug); #define GST_CAT_DEFAULT type_find_debug GType gst_type_find_get_type (void) { static GType typefind_type = 0; if (G_UNLIKELY (typefind_type == 0)) { typefind_type = g_pointer_type_register_static ("GstTypeFind"); } return typefind_type; } /** * gst_type_find_register: * @plugin: A #GstPlugin, or NULL for a static typefind function (note that * passing NULL only works in GStreamer 0.10.16 and later) * @name: The name for registering * @rank: The rank (or importance) of this typefind function * @func: The #GstTypeFindFunction to use * @extensions: (transfer none) (array zero-terminated=1) (element-type utf8): * Optional extensions that could belong to this type * @possible_caps: Optionally the caps that could be returned when typefinding * succeeds * @data: Optional user data. This user data must be available until the plugin * is unloaded. * @data_notify: a #GDestroyNotify that will be called on @data when the plugin * is unloaded. * * Registers a new typefind function to be used for typefinding. After * registering this function will be available for typefinding. * This function is typically called during an element's plugin initialization. * * Returns: TRUE on success, FALSE otherwise */ gboolean gst_type_find_register (GstPlugin * plugin, const gchar * name, guint rank, GstTypeFindFunction func, gchar ** extensions, const GstCaps * possible_caps, gpointer data, GDestroyNotify data_notify) { GstTypeFindFactory *factory; g_return_val_if_fail (name != NULL, FALSE); GST_INFO ("registering typefind function for %s", name); factory = g_object_newv (GST_TYPE_TYPE_FIND_FACTORY, 0, NULL); GST_DEBUG_OBJECT (factory, "using new typefind factory for %s", name); g_assert (GST_IS_TYPE_FIND_FACTORY (factory)); gst_plugin_feature_set_name (GST_PLUGIN_FEATURE_CAST (factory), name); gst_plugin_feature_set_rank (GST_PLUGIN_FEATURE_CAST (factory), rank); if (factory->extensions) g_strfreev (factory->extensions); factory->extensions = g_strdupv (extensions); gst_caps_replace (&factory->caps, (GstCaps *) possible_caps); factory->function = func; factory->user_data = data; factory->user_data_notify = data_notify; if (plugin && plugin->desc.name) { GST_PLUGIN_FEATURE_CAST (factory)->plugin_name = plugin->desc.name; /* interned string */ GST_PLUGIN_FEATURE_CAST (factory)->plugin = plugin; g_object_add_weak_pointer ((GObject *) plugin, (gpointer *) & GST_PLUGIN_FEATURE_CAST (factory)->plugin); } else { GST_PLUGIN_FEATURE_CAST (factory)->plugin_name = "NULL"; GST_PLUGIN_FEATURE_CAST (factory)->plugin = NULL; } GST_PLUGIN_FEATURE_CAST (factory)->loaded = TRUE; gst_registry_add_feature (gst_registry_get_default (), GST_PLUGIN_FEATURE_CAST (factory)); return TRUE; } /*** typefind function interface **********************************************/ /** * gst_type_find_peek: * @find: The #GstTypeFind object the function was called with * @offset: The offset * @size: The number of bytes to return * * Returns the @size bytes of the stream to identify beginning at offset. If * offset is a positive number, the offset is relative to the beginning of the * stream, if offset is a negative number the offset is relative to the end of * the stream. The returned memory is valid until the typefinding function * returns and must not be freed. * * Returns: (transfer none) (array length=size): the requested data, or NULL * if that data is not available. */ guint8 * gst_type_find_peek (GstTypeFind * find, gint64 offset, guint size) { g_return_val_if_fail (find->peek != NULL, NULL); return find->peek (find->data, offset, size); } /** * gst_type_find_suggest: * @find: The #GstTypeFind object the function was called with * @probability: The probability in percent that the suggestion is right * @caps: The fixed #GstCaps to suggest * * If a #GstTypeFindFunction calls this function it suggests the caps with the * given probability. A #GstTypeFindFunction may supply different suggestions * in one call. * It is up to the caller of the #GstTypeFindFunction to interpret these values. */ void gst_type_find_suggest (GstTypeFind * find, guint probability, const GstCaps * caps) { g_return_if_fail (find->suggest != NULL); g_return_if_fail (probability <= 100); g_return_if_fail (caps != NULL); g_return_if_fail (gst_caps_is_fixed (caps)); find->suggest (find->data, probability, caps); } /** * gst_type_find_suggest_simple: * @find: The #GstTypeFind object the function was called with * @probability: The probability in percent that the suggestion is right * @media_type: the media type of the suggested caps * @fieldname: first field of the suggested caps, or NULL * @...: additional arguments to the suggested caps in the same format as the * arguments passed to gst_structure_new() (ie. triplets of field name, * field GType and field value) * * If a #GstTypeFindFunction calls this function it suggests the caps with the * given probability. A #GstTypeFindFunction may supply different suggestions * in one call. It is up to the caller of the #GstTypeFindFunction to interpret * these values. * * This function is similar to gst_type_find_suggest(), only that instead of * passing a #GstCaps argument you can create the caps on the fly in the same * way as you can with gst_caps_new_simple(). * * Make sure you terminate the list of arguments with a NULL argument and that * the values passed have the correct type (in terms of width in bytes when * passed to the vararg function - this applies particularly to gdouble and * guint64 arguments). * * Since: 0.10.20 */ void gst_type_find_suggest_simple (GstTypeFind * find, guint probability, const char *media_type, const char *fieldname, ...) { GstStructure *structure; va_list var_args; GstCaps *caps; g_return_if_fail (find->suggest != NULL); g_return_if_fail (probability <= 100); g_return_if_fail (media_type != NULL); caps = gst_caps_new_empty (); va_start (var_args, fieldname); structure = gst_structure_new_valist (media_type, fieldname, var_args); va_end (var_args); gst_caps_append_structure (caps, structure); g_return_if_fail (gst_caps_is_fixed (caps)); find->suggest (find->data, probability, caps); gst_caps_unref (caps); } /** * gst_type_find_get_length: * @find: The #GstTypeFind the function was called with * * Get the length of the data stream. * * Returns: The length of the data stream, or 0 if it is not available. */ guint64 gst_type_find_get_length (GstTypeFind * find) { if (find->get_length == NULL) return 0; return find->get_length (find->data); }