/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * * gsturi.h: Header for uri to element mappings * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GST_URI_H__ #define __GST_URI_H__ #include #include #include G_BEGIN_DECLS /** * GstURIType: * @GST_URI_UNKNOWN : The URI direction is unknown * @GST_URI_SINK : The URI is a consumer. * @GST_URI_SRC : The URI is a producer. * * The different types of URI direction. */ typedef enum { GST_URI_UNKNOWN, GST_URI_SINK, GST_URI_SRC } GstURIType; /** * GST_URI_TYPE_IS_VALID: * @type: A #GstURIType * * Tests if the type direction is valid. */ #define GST_URI_TYPE_IS_VALID(type) ((type) == GST_URI_SRC || (type) == GST_URI_SINK) /* uri handler functions */ #define GST_TYPE_URI_HANDLER (gst_uri_handler_get_type ()) #define GST_URI_HANDLER(obj) (G_TYPE_CHECK_INSTANCE_CAST ((obj), GST_TYPE_URI_HANDLER, GstURIHandler)) #define GST_IS_URI_HANDLER(obj) (G_TYPE_CHECK_INSTANCE_TYPE ((obj), GST_TYPE_URI_HANDLER)) #define GST_URI_HANDLER_GET_INTERFACE(obj) (G_TYPE_INSTANCE_GET_INTERFACE ((obj), GST_TYPE_URI_HANDLER, GstURIHandlerInterface)) /** * GstURIHandler: * * Opaque #GstURIHandler structure. */ typedef struct _GstURIHandler GstURIHandler; typedef struct _GstURIHandlerInterface GstURIHandlerInterface; /** * GstURIHandlerInterface: * @parent: The parent interface type * @get_type: Method to tell whether the element handles source or sink URI. * @get_protocols: Method to return the list of protocols handled by the element. * @get_uri: Method to return the URI currently handled by the element. * @set_uri: Method to set a new URI. * @get_type_full: Variant of get_type which takes a GType argument. This is * for use by bindings that need to pass context when creating a URI Handler. * If implemented, get_type will be used in preference to get_type_full. * Since: 0.10.15. * @get_protocols_full: Variant of get_protocols which takes a GType argument. * This is for use by bindings that need to pass context when creating a URI * Handler. If implemented, get_protocols will be used in preference to * get_protocols_full. Since: 0.10.15. * * Any #GstElement using this interface should implement these methods. */ struct _GstURIHandlerInterface { GTypeInterface parent; /*< private >*/ /* signals */ void (* new_uri) (GstURIHandler * handler, const gchar * uri); /* idea for the future ? gboolean (* require_password) (GstURIHandler * handler, gchar ** username, gchar ** password); */ /* vtable */ /*< public >*/ /* querying capabilities */ GstURIType (* get_type) (void); gchar ** (* get_protocols) (void); /* using the interface */ const gchar * (* get_uri) (GstURIHandler * handler); gboolean (* set_uri) (GstURIHandler * handler, const gchar * uri); GstURIType (* get_type_full) (GType type); gchar ** (* get_protocols_full) (GType type); /*< private >*/ /* we might want to add functions here to query features, * someone with gnome-vfs knowledge go ahead */ gpointer _gst_reserved[GST_PADDING - 2]; }; /* general URI functions */ gboolean gst_uri_protocol_is_valid (const gchar * protocol); gboolean gst_uri_protocol_is_supported (const GstURIType type, const gchar *protocol); gboolean gst_uri_is_valid (const gchar * uri); gchar * gst_uri_get_protocol (const gchar * uri) G_GNUC_MALLOC; gboolean gst_uri_has_protocol (const gchar * uri, const gchar * protocol); gchar * gst_uri_get_location (const gchar * uri) G_GNUC_MALLOC; gchar * gst_uri_construct (const gchar * protocol, const gchar * location) G_GNUC_MALLOC; gchar * gst_filename_to_uri (const gchar * filename, GError ** error) G_GNUC_MALLOC; GstElement * gst_element_make_from_uri (const GstURIType type, const gchar * uri, const gchar * elementname) G_GNUC_MALLOC; /* accessing the interface */ GType gst_uri_handler_get_type (void); guint gst_uri_handler_get_uri_type (GstURIHandler * handler); gchar ** gst_uri_handler_get_protocols (GstURIHandler * handler); const gchar * gst_uri_handler_get_uri (GstURIHandler * handler); gboolean gst_uri_handler_set_uri (GstURIHandler * handler, const gchar * uri); void gst_uri_handler_new_uri (GstURIHandler * handler, const gchar * uri); G_END_DECLS #endif /* __GST_URI_H__ */