%define majorminor @GST_MAJORMINOR@ %define gstreamer gstreamer09 Name: %{gstreamer} Version: @VERSION@ Release: @GST_VERSION_RELEASE@ Summary: GStreamer streaming media framework runtime Group: Applications/Multimedia License: LGPL URL: http://gstreamer.freedesktop.org/ Vendor: GStreamer Backpackers Team Source: http://gstreamer.freedesktop.org/src/gstreamer/gstreamer-%{version}.tar.gz BuildRoot: %{_tmppath}/%{name}-%{version}-%{release}-root-%(%{__id_u} -n) %define _glib2 @GLIB2_REQ@ %define _libxml2 @LIBXML2_REQ@ Requires: glib2 >= %_glib2 Requires: libxml2 >= %_libxml2 Requires: popt > 1.6 # Provides: gstreamer =%{version}-%{release} BuildRequires: glib2-devel >= %_glib2 BuildRequires: libxml2-devel >= %_libxml2 BuildRequires: bison BuildRequires: flex BuildRequires: m4 BuildRequires: check BuildRequires: gtk-doc >= 1.1 BuildRequires: gcc BuildRequires: gettext BuildRequires: zlib-devel BuildRequires: popt > 1.6 Requires(pre): /sbin/ldconfig Requires(post): /sbin/ldconfig ### documentation requirements BuildRequires: python2 BuildRequires: openjade BuildRequires: jadetex BuildRequires: libxslt BuildRequires: docbook-style-dsssl BuildRequires: docbook-style-xsl BuildRequires: docbook-utils BuildRequires: transfig BuildRequires: xfig BuildRequires: netpbm-progs BuildRequires: ghostscript %description GStreamer is a streaming media framework, based on graphs of filters which operate on media data. Applications using this library can do anything from real-time sound processing to playing videos, and just about anything else media-related. Its plugin-based architecture means that new data types or processing capabilities can be added simply by installing new plugins. %package devel Summary: Libraries/include files for GStreamer streaming media framework Group: Development/Libraries Requires: %{name} = %{version}-%{release} Requires: glib2-devel >= %_glib2 Requires: libxml2-devel >= %_libxml2 %description devel GStreamer is a streaming-media framework, based on graphs of filters which operate on media data. Applications using this library can do anything from real-time sound processing to playing videos, and just about anything else media-related. Its plugin-based architecture means that new data types or processing capabilities can be added simply by installing new plugins. This package contains the libraries and includes files necessary to develop applications and plugins for GStreamer. %package -n gstreamer09-tools Summary: tools for GStreamer streaming media framework Group: Applications/Multimedia %description -n gstreamer-tools GStreamer is a streaming-media framework, based on graphs of filters which operate on media data. Applications using this library can do anything from real-time sound processing to playing videos, and just about anything else media-related. Its plugin-based architecture means that new data types or processing capabilities can be added simply by installing new plugins. This package contains wrapper scripts for the command-line tools that work with different major/minor versions of GStreamer. %prep %setup -q -n gstreamer-%{version} %build %configure \ --with-cachedir=%{_localstatedir}/cache/gstreamer-%{majorminor} \ --enable-gtk-doc --enable-docbook \ --disable-tests --disable-examples make %install rm -rf $RPM_BUILD_ROOT # Install doc temporarily in order to be included later by rpm %makeinstall docdir="`pwd`/installed-doc" %find_lang gstreamer-%{majorminor} # Clean out files that should not be part of the rpm. rm -f $RPM_BUILD_ROOT%{_libdir}/gstreamer-%{majorminor}/*.la rm -f $RPM_BUILD_ROOT%{_libdir}/gstreamer-%{majorminor}/*.a rm -f $RPM_BUILD_ROOT%{_libdir}/*.a rm -f $RPM_BUILD_ROOT%{_libdir}/*.la # Create empty cache directory mkdir -p $RPM_BUILD_ROOT%{_localstatedir}/cache/gstreamer-%{majorminor} %clean rm -rf $RPM_BUILD_ROOT %post /sbin/ldconfig %postun -p /sbin/ldconfig %files -f gstreamer-%{majorminor}.lang %defattr(-, root, root, -) %doc AUTHORS COPYING NEWS README TODO RELEASE %doc ABOUT-NLS REQUIREMENTS DOCBUILDING %{_libdir}/libgstreamer-%{majorminor}.so.* %{_libdir}/libgstbase-%{majorminor}.so.* %{_libdir}/libgstcontroller-%{majorminor}.so.* %{_libdir}/libgstdataprotocol-%{majorminor}.so.* %dir %{_libdir}/gstreamer-%{majorminor} %{_libdir}/gstreamer-%{majorminor}/libgstelements.so %{_libdir}/gstreamer-%{majorminor}/libgstindexers.so %{_bindir}/gst-complete-%{majorminor} %{_bindir}/gst-compprep-%{majorminor} %{_bindir}/gst-feedback-%{majorminor} %{_bindir}/gst-inspect-%{majorminor} %{_bindir}/gst-launch-%{majorminor} %{_bindir}/gst-md5sum-%{majorminor} %{_bindir}/gst-typefind-%{majorminor} %{_bindir}/gst-xmlinspect-%{majorminor} %{_bindir}/gst-xmllaunch-%{majorminor} %{_mandir}/man1/gst-complete-%{majorminor}.* %{_mandir}/man1/gst-compprep-%{majorminor}.* %{_mandir}/man1/gst-feedback-%{majorminor}.* %{_mandir}/man1/gst-inspect-%{majorminor}.* %{_mandir}/man1/gst-launch-%{majorminor}.* %{_mandir}/man1/gst-md5sum-%{majorminor}.* %{_mandir}/man1/gst-typefind-%{majorminor}.* %{_mandir}/man1/gst-xmlinspect-%{majorminor}.* %{_mandir}/man1/gst-xmllaunch-%{majorminor}.* %dir %{_localstatedir}/cache/gstreamer-%{majorminor} %files -n gstreamer-tools %defattr(-, root, root, -) %{_bindir}/gst-complete %{_bindir}/gst-compprep %{_bindir}/gst-feedback %{_bindir}/gst-inspect %{_bindir}/gst-launch %{_bindir}/gst-md5sum %{_bindir}/gst-typefind %{_bindir}/gst-xmlinspect %{_bindir}/gst-xmllaunch %files devel %defattr(-, root, root, -) %doc installed-doc/faq installed-doc/pwg installed-doc/manual %dir %{_includedir}/gstreamer-%{majorminor} %dir %{_includedir}/gstreamer-%{majorminor}/gst %{_includedir}/gstreamer-%{majorminor}/gst/*.h %{_includedir}/gstreamer-%{majorminor}/gst/controller/gstcontroller.h %{_includedir}/gstreamer-%{majorminor}/gst/base %{_includedir}/gstreamer-%{majorminor}/gst/dataprotocol %{_libdir}/libgstreamer-%{majorminor}.so %{_libdir}/libgstdataprotocol-%{majorminor}.so %{_libdir}/libgstbase-%{majorminor}.so %{_libdir}/libgstcontroller-%{majorminor}.so %{_datadir}/aclocal/gst-element-check-%{majorminor}.m4 %{_libdir}/pkgconfig/gstreamer-%{majorminor}.pc %{_libdir}/pkgconfig/gstreamer-base-%{majorminor}.pc %{_libdir}/pkgconfig/gstreamer-dataprotocol-%{majorminor}.pc %{_libdir}/pkgconfig/gstreamer-controller-%{majorminor}.pc %doc %{_datadir}/gtk-doc/html/gstreamer-%{majorminor} %doc %{_datadir}/gtk-doc/html/gstreamer-libs-%{majorminor} %changelog * Fri Sep 02 2005 Thomas Vander Stichele - clean up a little * Thu Jun 09 2005 Thomas Vander Stichele - clean up spec for 0.9 builds * Thu Feb 12 2004 Thomas Vander Stichele - sync with 0.7.4 fedora spec * Thu Feb 05 2004 Thomas Vander Stichele - bump gtk-doc required version to 1.0 for the new options used * Wed Feb 04 2004 Thomas Vander Stichele - add -common package containing frontend wrapper binaries * Mon Dec 01 2003 Thomas Vander Stichele - changed documentation buildrequires * Sun Nov 09 2003 Christian Schaller - Fix spec to handle new bytestream library * Sun Aug 17 2003 Christian Schaller - Remove docs build from RPM as the build is broken - Fix stuff since more files are versioned now - Remove wingo schedulers - Remove putbits stuff * Sun May 18 2003 Thomas Vander Stichele - devhelp files are now generated by gtk-doc, changed accordingly * Sun Mar 16 2003 Christian F.K. Schaller - Add gthread scheduler * Sat Dec 07 2002 Thomas Vander Stichele - define majorminor and use it everywhere - full parallel installability * Tue Nov 05 2002 Christian Schaller - Add optwingo scheduler * Sat Oct 12 2002 Christian Schaller - Updated to work better with default RH8 rpm - Added missing unspeced files - Removed .a and .la files from buildroot * Sat Sep 21 2002 Thomas Vander Stichele - added gst-md5sum * Tue Sep 17 2002 Thomas Vander Stichele - adding flex to buildrequires * Fri Sep 13 2002 Christian F.K. Schaller - Fixed the schedulers after the renaming * Sun Sep 08 2002 Thomas Vander Stichele - added transfig to the BuildRequires: * Sat Jun 22 2002 Thomas Vander Stichele - moved header location * Mon Jun 17 2002 Thomas Vander Stichele - added popt - removed .la * Fri Jun 07 2002 Thomas Vander Stichele - added release of gstreamer to req of gstreamer-devel - changed location of API docs to be in gtk-doc like other gtk-doc stuff - reordered SPEC file * Mon Apr 29 2002 Thomas Vander Stichele - moved html docs to gtk-doc standard directory * Tue Mar 5 2002 Thomas Vander Stichele - move version defines of glib2 and libxml2 to configure.ac - add BuildRequires for these two libs * Sun Mar 3 2002 Thomas Vander Stichele - put html docs in canonical place, avoiding %doc erasure - added devhelp support, current install of it is hackish * Sat Mar 2 2002 Christian Schaller - Added documentation to build * Mon Feb 11 2002 Thomas Vander Stichele - added libgstbasicscheduler - renamed libgst to libgstreamer * Fri Jan 04 2002 Christian Schaller - Added configdir parameter as it seems the configdir gets weird otherwise * Thu Jan 03 2002 Thomas Vander Stichele - split off gstreamer-editor from core - removed gstreamer-gnome-apps * Sat Dec 29 2001 Rodney Dawes - Cleaned up the spec file for the gstreamer core/plug-ins split - Improve spec file * Sat Dec 15 2001 Christian Schaller - Split of more plugins from the core and put them into their own modules - Includes colorspace, xfree and wav - Improved package Require lines - Added mp3encode (lame based) to the SPEC * Wed Dec 12 2001 Christian Schaller - Thomas merged mpeg plugins into one * Sat Dec 08 2001 Christian Schaller - More minor cleanups including some fixed descriptions from Andrew Mitchell * Fri Dec 07 2001 Christian Schaller - Added logging to the make statement * Wed Dec 05 2001 Christian Schaller - Updated in preparation for 0.3.0 release * Fri Jun 29 2001 Christian Schaller - Updated for 0.2.1 release - Split out the GUI packages into their own RPM - added new plugins (FLAC, festival, quicktime etc.) * Sat Jun 09 2001 Christian Schaller - Visualisation plugins bundled out togheter - Moved files sections up close to their respective descriptions * Sat Jun 02 2001 Christian Schaller - Split the package into separate RPMS, putting most plugins out by themselves. * Fri Jun 01 2001 Christian Schaller - Updated with change suggestions from Dennis Bjorklund * Tue Jan 09 2001 Erik Walthinsen - updated to build -devel package as well * Sun Jan 30 2000 Erik Walthinsen - first draft of spec file