/* GStreamer * Copyright (C) 2004 Benjamin Otte * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #include #ifndef __GST_ADAPTER_H__ #define __GST_ADAPTER_H__ G_BEGIN_DECLS #define GST_TYPE_ADAPTER \ (gst_adapter_get_type()) #define GST_ADAPTER(obj) \ (G_TYPE_CHECK_INSTANCE_CAST((obj), GST_TYPE_ADAPTER, GstAdapter)) #define GST_ADAPTER_CLASS(klass) \ (G_TYPE_CHECK_CLASS_CAST((klass), GST_TYPE_ADAPTER, GstAdapterClass)) #define GST_ADAPTER_GET_CLASS(obj) \ (G_TYPE_INSTANCE_GET_CLASS ((obj), GST_TYPE_ADAPTER, GstAdapterClass)) #define GST_IS_ADAPTER(obj) \ (G_TYPE_CHECK_INSTANCE_TYPE((obj), GST_TYPE_ADAPTER)) #define GST_IS_ADAPTER_CLASS(klass) \ (G_TYPE_CHECK_CLASS_TYPE((klass), GST_TYPE_ADAPTER)) typedef struct _GstAdapter GstAdapter; typedef struct _GstAdapterClass GstAdapterClass; typedef struct _GstAdapterPrivate GstAdapterPrivate; /** * GstAdapter: * * The opaque #GstAdapter data structure. */ struct _GstAdapter { GObject object; /*< private >*/ GSList * buflist; guint size; guint skip; /* we keep state of assembled pieces */ guint8 * assembled_data; guint assembled_size; guint assembled_len; /* ABI added */ /* Remember where the end of our buffer list is to * speed up the push */ GSList *buflist_end; GstAdapterPrivate *priv; gpointer _gst_reserved[GST_PADDING - 2]; }; struct _GstAdapterClass { GObjectClass parent_class; /*< private >*/ gpointer _gst_reserved[GST_PADDING]; }; GType gst_adapter_get_type (void); GstAdapter * gst_adapter_new (void) G_GNUC_MALLOC; void gst_adapter_clear (GstAdapter *adapter); void gst_adapter_push (GstAdapter *adapter, GstBuffer* buf); const guint8 * gst_adapter_peek (GstAdapter *adapter, guint size); void gst_adapter_copy (GstAdapter *adapter, guint8 *dest, guint offset, guint size); void gst_adapter_flush (GstAdapter *adapter, guint flush); guint8* gst_adapter_take (GstAdapter *adapter, guint nbytes); GstBuffer* gst_adapter_take_buffer (GstAdapter *adapter, guint nbytes); GList* gst_adapter_take_list (GstAdapter *adapter, guint nbytes); guint gst_adapter_available (GstAdapter *adapter); guint gst_adapter_available_fast (GstAdapter *adapter); GstClockTime gst_adapter_prev_timestamp (GstAdapter *adapter, guint64 *distance); guint gst_adapter_masked_scan_uint32 (GstAdapter * adapter, guint32 mask, guint32 pattern, guint offset, guint size); guint gst_adapter_masked_scan_uint32_peek (GstAdapter * adapter, guint32 mask, guint32 pattern, guint offset, guint size, guint32 * value); G_END_DECLS #endif /* __GST_ADAPTER_H__ */