/* GStreamer * * Common code for GStreamer unittests * * Copyright (C) <2004> Thomas Vander Stichele * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GST_CHECK_H__ #define __GST_CHECK_H__ #include #include #include #include #include GST_DEBUG_CATEGORY_EXTERN (check_debug); #define GST_CAT_DEFAULT check_debug /* logging function for tests * a test uses g_message() to log a debug line * a gst unit test can be run with GST_TEST_DEBUG env var set to see the * messages */ extern gboolean _gst_check_threads_running; extern gboolean _gst_check_raised_critical; extern gboolean _gst_check_raised_warning; extern gboolean _gst_check_expecting_log; /* global variables used in test methods */ GList * buffers; GMutex *check_mutex; GCond *check_cond; typedef struct { char *name; int size; int abi_size; } GstCheckABIStruct; void gst_check_init (int *argc, char **argv[]); GstFlowReturn gst_check_chain_func (GstPad *pad, GstBuffer *buffer); void gst_check_message_error (GstMessage *message, GstMessageType type, GQuark domain, gint code); GstElement * gst_check_setup_element (const gchar *factory); void gst_check_teardown_element (GstElement *element); GstPad * gst_check_setup_src_pad (GstElement *element, GstStaticPadTemplate *template, GstCaps *caps); void gst_check_teardown_src_pad (GstElement *element); GstPad * gst_check_setup_sink_pad (GstElement *element, GstStaticPadTemplate *template, GstCaps *caps); void gst_check_teardown_sink_pad (GstElement *element); void gst_check_abi_list (GstCheckABIStruct list[], gboolean have_abi_sizes); gint gst_check_run_suite (Suite *suite, const gchar *name, const gchar *fname); #define fail_unless_message_error(msg, domain, code) \ gst_check_message_error (msg, GST_MESSAGE_ERROR, \ GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code) #define assert_message_error(m, d, c) fail_unless_message_error(m, d, c) /*** * wrappers for START_TEST and END_TEST */ #define GST_START_TEST(__testname) \ static void __testname (void)\ {\ GST_DEBUG ("test start"); \ tcase_fn_start (""# __testname, __FILE__, __LINE__); #define GST_END_TEST END_TEST /* additional fail macros */ #define fail_unless_equals_int(a, b) \ G_STMT_START { \ int first = a; \ int second = b; \ fail_unless(first == second, \ "'" #a "' (%d) is not equal to '" #b"' (%d)", first, second); \ } G_STMT_END; #define assert_equals_int(a, b) fail_unless_equals_int(a, b) #define fail_unless_equals_uint64(a, b) \ G_STMT_START { \ guint64 first = a; \ guint64 second = b; \ fail_unless(first == second, \ "'" #a "' (%" G_GUINT64_FORMAT ") is not equal to '" #b"' (%" \ G_GUINT64_FORMAT ")", first, second); \ } G_STMT_END; #define assert_equals_uint64(a, b) fail_unless_equals_uint64(a, b) #define fail_unless_equals_string(a, b) \ G_STMT_START { \ gchar * first = a; \ gchar * second = b; \ fail_unless(strcmp (first, second) == 0, \ "'" #a "' (%s) is not equal to '" #b"' (%s)", first, second); \ } G_STMT_END; #define assert_equals_string(a, b) fail_unless_equals_string(a, b) /*** * thread test macros and variables */ extern GList *thread_list; extern GMutex *mutex; extern GCond *start_cond; /* used to notify main thread of thread startups */ extern GCond *sync_cond; /* used to synchronize all threads and main thread */ #define MAIN_START_THREADS(count, function, data) \ MAIN_INIT(); \ MAIN_START_THREAD_FUNCTIONS(count, function, data); \ MAIN_SYNCHRONIZE(); #define MAIN_INIT() \ G_STMT_START { \ _gst_check_threads_running = TRUE; \ \ mutex = g_mutex_new (); \ start_cond = g_cond_new (); \ sync_cond = g_cond_new (); \ } G_STMT_END; #define MAIN_START_THREAD_FUNCTIONS(count, function, data) \ G_STMT_START { \ int i; \ for (i = 0; i < count; ++i) { \ MAIN_START_THREAD_FUNCTION (i, function, data); \ } \ } G_STMT_END; #define MAIN_START_THREAD_FUNCTION(i, function, data) \ G_STMT_START { \ GThread *thread = NULL; \ GST_DEBUG ("MAIN: creating thread %d", i); \ g_mutex_lock (mutex); \ thread = g_thread_create ((GThreadFunc) function, data, \ TRUE, NULL); \ /* wait for thread to signal us that it's ready */ \ GST_DEBUG ("MAIN: waiting for thread %d", i); \ g_cond_wait (start_cond, mutex); \ g_mutex_unlock (mutex); \ \ thread_list = g_list_append (thread_list, thread); \ } G_STMT_END; #define MAIN_SYNCHRONIZE() \ G_STMT_START { \ GST_DEBUG ("MAIN: synchronizing"); \ g_cond_broadcast (sync_cond); \ GST_DEBUG ("MAIN: synchronized"); \ } G_STMT_END; #define MAIN_STOP_THREADS() \ G_STMT_START { \ _gst_check_threads_running = FALSE; \ \ /* join all threads */ \ GST_DEBUG ("MAIN: joining"); \ g_list_foreach (thread_list, (GFunc) g_thread_join, NULL); \ GST_DEBUG ("MAIN: joined"); \ } G_STMT_END; #define THREAD_START() \ THREAD_STARTED(); \ THREAD_SYNCHRONIZE(); #define THREAD_STARTED() \ G_STMT_START { \ /* signal main thread that we started */ \ GST_DEBUG ("THREAD %p: started", g_thread_self ()); \ g_mutex_lock (mutex); \ g_cond_signal (start_cond); \ } G_STMT_END; #define THREAD_SYNCHRONIZE() \ G_STMT_START { \ /* synchronize everyone */ \ GST_DEBUG ("THREAD %p: syncing", g_thread_self ()); \ g_cond_wait (sync_cond, mutex); \ GST_DEBUG ("THREAD %p: synced", g_thread_self ()); \ g_mutex_unlock (mutex); \ } G_STMT_END; #define THREAD_SWITCH() \ G_STMT_START { \ /* a minimal sleep is a context switch */ \ g_usleep (1); \ } G_STMT_END; #define THREAD_TEST_RUNNING() (_gst_check_threads_running == TRUE) /* additional assertions */ #define ASSERT_CRITICAL(code) \ G_STMT_START { \ _gst_check_expecting_log = TRUE; \ _gst_check_raised_critical = FALSE; \ code; \ _fail_unless (_gst_check_raised_critical, __FILE__, __LINE__, \ "Expected g_critical, got nothing", NULL); \ _gst_check_expecting_log = FALSE; \ } G_STMT_END #define ASSERT_WARNING(code) \ G_STMT_START { \ _gst_check_expecting_log = TRUE; \ _gst_check_raised_warning = FALSE; \ code; \ _fail_unless (_gst_check_raised_warning, __FILE__, __LINE__, \ "Expected g_warning, got nothing", NULL); \ _gst_check_expecting_log = FALSE; \ } G_STMT_END #define ASSERT_OBJECT_REFCOUNT(object, name, value) \ G_STMT_START { \ int rc; \ rc = GST_OBJECT_REFCOUNT_VALUE (object); \ fail_unless (rc == value, \ "%s (%p) refcount is %d instead of %d", \ name, object, rc, value); \ } G_STMT_END #define ASSERT_OBJECT_REFCOUNT_BETWEEN(object, name, lower, upper) \ G_STMT_START { \ int rc = GST_OBJECT_REFCOUNT_VALUE (object); \ int lo = lower; \ int hi = upper; \ \ fail_unless (rc >= lo, \ "%s (%p) refcount %d is smaller than %d", \ name, object, rc, lo); \ fail_unless (rc <= hi, \ "%s (%p) refcount %d is bigger than %d", \ name, object, rc, hi); \ } G_STMT_END #define ASSERT_CAPS_REFCOUNT(caps, name, value) \ ASSERT_MINI_OBJECT_REFCOUNT(caps, name, value) #define ASSERT_BUFFER_REFCOUNT(buffer, name, value) \ ASSERT_MINI_OBJECT_REFCOUNT(buffer, name, value) #define ASSERT_MINI_OBJECT_REFCOUNT(caps, name, value) \ G_STMT_START { \ int rc; \ rc = GST_MINI_OBJECT_REFCOUNT_VALUE (caps); \ fail_unless (rc == value, \ name " refcount is %d instead of %d", rc, value);\ } G_STMT_END #define ASSERT_SET_STATE(element, state, ret) \ fail_unless (gst_element_set_state (element, \ state) == ret, \ "could not change state to " #state); #endif /* __GST_CHECK_H__ */ #define GST_CHECK_MAIN(name) \ int main (int argc, char **argv) \ { \ Suite *s = name ## _suite (); \ gst_check_init (&argc, &argv); \ return gst_check_run_suite (s, # name, __FILE__); \ }