/* GStreamer * Copyright (C) <1999> Erik Walthinsen * Copyright (C) <2004> Thomas Vander Stichele * * dataprotocol.c: Functions implementing the GStreamer Data Protocol * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include #include #include /* g_sprintf */ #include /* strlen */ #include "dp-private.h" /* debug category */ GST_DEBUG_CATEGORY (data_protocol_debug); #define GST_CAT_DEFAULT data_protocol_debug /* calculate a CCITT 16 bit CRC check value for a given byte array */ /* * this code snippet is adapted from a web page I found * it is identical except for cleanups, and a final XOR with 0xffff * as outlined in the uecp spec * * XMODEM x^16 + x^12 + x^5 + 1 */ #define POLY 0x1021 #define CRC_INIT 0xFFFF static guint16 gst_dp_crc (const guint8 * buffer, register guint length) { static gboolean initialized = FALSE; static guint16 crc_table[256]; guint16 crc_register; unsigned long i, j, k; if (!initialized) { for (i = 0; i < 256; i++) { j = i << 8; for (k = 8; k--;) { j = j & 0x8000 ? (j << 1) ^ POLY : j << 1; } crc_table[i] = (guint16) j; } initialized = TRUE; } crc_register = CRC_INIT; /* always init register */ /* calc CRC */ for (; length--;) { crc_register = (guint16) ((crc_register << 8) ^ crc_table[((crc_register >> 8) & 0x00ff) ^ *buffer++]); } return (0xffff ^ crc_register); } /* debugging function; dumps byte array values per 8 bytes */ /* FIXME: would be nice to merge this with gst_util_dump_mem () */ void gst_dp_dump_byte_array (guint8 * array, guint length) { int i; int n = 8; /* number of bytes per line */ gchar *line = g_malloc (3 * n + 1); GST_LOG ("dumping byte array of length %d", length); for (i = 0; i < length; ++i) { g_sprintf (line + 3 * (i % n), "%02x ", array[i]); if (i % n == (n - 1)) { GST_LOG ("%03d: %s", i - (n - 1), line); } } if (i % n != 0) { GST_LOG ("%03d: %s", (i / n) * n, line); } g_free (line); } /** * gst_dp_init: * * Initialize GStreamer Data Protocol library. * * Should be called before using these functions from source linking * to this source file. */ void gst_dp_init (void) { static gboolean _gst_dp_initialized = FALSE; if (_gst_dp_initialized) return; _gst_dp_initialized = TRUE; GST_DEBUG_CATEGORY_INIT (data_protocol_debug, "gdp", 0, "GStreamer Data Protocol"); } /*** PUBLIC FUNCTIONS ***/ /** * gst_dp_header_payload_length: * @header: the byte header of the packet array * * Returns: the length of the payload this header describes. */ guint32 gst_dp_header_payload_length (const guint8 * header) { return GST_DP_HEADER_PAYLOAD_LENGTH (header); } /** * gst_dp_header_payload_type: * @header: the byte header of the packet array * * Returns: the #GstDPPayloadType the payload this header describes. */ GstDPPayloadType gst_dp_header_payload_type (const guint8 * header) { return GST_DP_HEADER_PAYLOAD_TYPE (header); } /** * gst_dp_header_from_buffer: * @buffer: a #GstBuffer to create a header for * @flags: the #GDPHeaderFlags to create the header with * @length: a guint pointer to store the header length in * @header: a guint8 * pointer to store a newly allocated header byte array in * * Creates a GDP header from the given buffer. * * Returns: %TRUE if the header was successfully created. */ gboolean gst_dp_header_from_buffer (const GstBuffer * buffer, GstDPHeaderFlag flags, guint * length, guint8 ** header) { guint8 *h; guint16 crc; guint16 flags_mask; g_return_val_if_fail (GST_IS_BUFFER (buffer), FALSE); g_return_val_if_fail (header, FALSE); *length = GST_DP_HEADER_LENGTH; h = g_malloc (GST_DP_HEADER_LENGTH); /* version, flags, type */ h[0] = (guint8) GST_DP_VERSION_MAJOR; h[1] = (guint8) GST_DP_VERSION_MINOR; h[2] = (guint8) flags; h[3] = 0; /* padding byte */ GST_WRITE_UINT16_BE (h + 4, GST_DP_PAYLOAD_BUFFER); /* buffer properties */ GST_WRITE_UINT32_BE (h + 6, GST_BUFFER_SIZE (buffer)); GST_WRITE_UINT64_BE (h + 10, GST_BUFFER_TIMESTAMP (buffer)); GST_WRITE_UINT64_BE (h + 18, GST_BUFFER_DURATION (buffer)); GST_WRITE_UINT64_BE (h + 26, GST_BUFFER_OFFSET (buffer)); GST_WRITE_UINT64_BE (h + 34, GST_BUFFER_OFFSET_END (buffer)); /* data flags */ /* we only copy KEY_UNIT,DELTA_UNIT and IN_CAPS flags */ flags_mask = GST_BUFFER_FLAG_PREROLL | GST_BUFFER_FLAG_IN_CAPS | GST_BUFFER_FLAG_DELTA_UNIT; GST_WRITE_UINT16_BE (h + 42, GST_BUFFER_FLAGS (buffer) & flags_mask); /* ABI padding */ GST_WRITE_UINT32_BE (h + 44, (guint64) 0); GST_WRITE_UINT64_BE (h + 48, (guint64) 0); /* CRC */ crc = 0; if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) { /* we don't crc the last four bytes of the header since they are crc's */ crc = gst_dp_crc (h, 58); } GST_WRITE_UINT16_BE (h + 58, crc); crc = 0; if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) { crc = gst_dp_crc (GST_BUFFER_DATA (buffer), GST_BUFFER_SIZE (buffer)); } GST_WRITE_UINT16_BE (h + 60, crc); GST_LOG ("created header from buffer:"); gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH); *header = h; return TRUE; } /** * gst_dp_packet_from_caps: * @caps: a #GstCaps to create a packet for * @flags: the #GDPHeaderFlags to create the header with * @length: a guint pointer to store the header length in * @header: a guint8 pointer to store a newly allocated header byte array in * @payload: a guint8 pointer to store a newly allocated payload byte array in * * Creates a GDP packet from the given caps. * * Returns: %TRUE if the packet was successfully created. */ gboolean gst_dp_packet_from_caps (const GstCaps * caps, GstDPHeaderFlag flags, guint * length, guint8 ** header, guint8 ** payload) { guint8 *h; guint16 crc; guchar *string; /* FIXME: GST_IS_CAPS doesn't work g_return_val_if_fail (GST_IS_CAPS (caps), FALSE); */ g_return_val_if_fail (caps, FALSE); g_return_val_if_fail (header, FALSE); g_return_val_if_fail (payload, FALSE); *length = GST_DP_HEADER_LENGTH; h = g_malloc (GST_DP_HEADER_LENGTH); string = (guchar *) gst_caps_to_string (caps); /* version, flags, type */ h[0] = (guint8) GST_DP_VERSION_MAJOR; h[1] = (guint8) GST_DP_VERSION_MINOR; h[2] = (guint8) flags; h[3] = 0; /* padding bytes */ GST_WRITE_UINT16_BE (h + 4, GST_DP_PAYLOAD_CAPS); /* buffer properties */ GST_WRITE_UINT32_BE (h + 8, strlen ((gchar *) string) + 1); /* include trailing 0 */ GST_WRITE_UINT64_BE (h + 10, (guint64) 0); GST_WRITE_UINT64_BE (h + 18, (guint64) 0); GST_WRITE_UINT64_BE (h + 26, (guint64) 0); GST_WRITE_UINT64_BE (h + 34, (guint64) 0); /* ABI padding */ GST_WRITE_UINT64_BE (h + 42, (guint64) 0); GST_WRITE_UINT64_BE (h + 50, (guint64) 0); /* CRC */ crc = 0; if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) { crc = gst_dp_crc (h, 58); } GST_WRITE_UINT16_BE (h + 58, crc); crc = 0; if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) { crc = gst_dp_crc (string, strlen ((gchar *) string) + 1); } GST_WRITE_UINT16_BE (h + 60, crc); GST_LOG ("created header from caps:"); gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH); *header = h; *payload = string; return TRUE; } /** * gst_dp_packet_from_event: * @event: a #GstEvent to create a packet for * @flags: the #GDPHeaderFlags to create the header with * @length: a guint pointer to store the header length in * @header: a guint8 pointer to store a newly allocated header byte array in * @payload: a guint8 pointer to store a newly allocated payload byte array in * * Creates a GDP packet from the given event. * * Returns: %TRUE if the packet was successfully created. */ gboolean gst_dp_packet_from_event (const GstEvent * event, GstDPHeaderFlag flags, guint * length, guint8 ** header, guint8 ** payload) { guint8 *h; guint16 crc; guint pl_length; /* length of payload */ g_return_val_if_fail (event, FALSE); g_return_val_if_fail (GST_IS_EVENT (event), FALSE); g_return_val_if_fail (header, FALSE); g_return_val_if_fail (payload, FALSE); *length = GST_DP_HEADER_LENGTH; h = g_malloc0 (GST_DP_HEADER_LENGTH); /* first construct payload, since we need the length */ switch (GST_EVENT_TYPE (event)) { case GST_EVENT_UNKNOWN: g_warning ("Unknown event, ignoring"); *length = 0; g_free (h); return FALSE; case GST_EVENT_EOS: case GST_EVENT_FLUSH_START: case GST_EVENT_FLUSH_STOP: case GST_EVENT_NEWSEGMENT: pl_length = 0; *payload = NULL; break; case GST_EVENT_SEEK: { gdouble rate; GstFormat format; GstSeekFlags flags; GstSeekType cur_type, stop_type; gint64 cur, stop; gst_event_parse_seek ((GstEvent *) event, &rate, &format, &flags, &cur_type, &cur, &stop_type, &stop); pl_length = 4 + 4 + 4 + 8 + 4 + 8; *payload = g_malloc0 (pl_length); /* FIXME write rate */ GST_WRITE_UINT32_BE (*payload, (guint32) format); GST_WRITE_UINT32_BE (*payload + 4, (guint32) flags); GST_WRITE_UINT32_BE (*payload + 8, (guint32) cur_type); GST_WRITE_UINT64_BE (*payload + 12, (guint64) cur); GST_WRITE_UINT32_BE (*payload + 20, (guint32) stop_type); GST_WRITE_UINT64_BE (*payload + 24, (guint64) stop); break; } case GST_EVENT_QOS: case GST_EVENT_NAVIGATION: case GST_EVENT_TAG: g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event)); return FALSE; default: g_warning ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event)); *length = 0; g_free (h); return FALSE; } /* version, flags, type */ h[0] = (guint8) GST_DP_VERSION_MAJOR; h[1] = (guint8) GST_DP_VERSION_MINOR; h[2] = (guint8) flags; h[3] = 0; /* padding byte */ GST_WRITE_UINT16_BE (h + 4, GST_DP_PAYLOAD_EVENT_NONE + GST_EVENT_TYPE (event)); /* length */ GST_WRITE_UINT32_BE (h + 6, (guint32) pl_length); /* timestamp */ GST_WRITE_UINT64_BE (h + 10, GST_EVENT_TIMESTAMP (event)); /* ABI padding */ GST_WRITE_UINT64_BE (h + 42, (guint64) 0); GST_WRITE_UINT64_BE (h + 50, (guint64) 0); /* CRC */ crc = 0; if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) { crc = gst_dp_crc (h, 58); } GST_WRITE_UINT16_BE (h + 58, crc); crc = 0; /* events can have a NULL payload */ if (*payload && flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) { crc = gst_dp_crc (*payload, strlen ((gchar *) * payload) + 1); } GST_WRITE_UINT16_BE (h + 60, crc); GST_LOG ("created header from event:"); gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH); *header = h; return TRUE; } /** * gst_dp_buffer_from_header: * @header_length: the length of the packet header * @header: the byte array of the packet header * * Creates a newly allocated #GstBuffer from the given header. * The buffer data needs to be copied into it before validating. * * Use this function if you want to pre-allocate a buffer based on the * packet header to read the packet payload in to. * * Returns: %TRUE if the buffer was successfully created. */ GstBuffer * gst_dp_buffer_from_header (guint header_length, const guint8 * header) { GstBuffer *buffer; g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) == GST_DP_PAYLOAD_BUFFER, NULL); buffer = gst_buffer_new_and_alloc ((guint) GST_DP_HEADER_PAYLOAD_LENGTH (header)); GST_BUFFER_TIMESTAMP (buffer) = GST_DP_HEADER_TIMESTAMP (header); GST_BUFFER_DURATION (buffer) = GST_DP_HEADER_DURATION (header); GST_BUFFER_OFFSET (buffer) = GST_DP_HEADER_OFFSET (header); GST_BUFFER_OFFSET_END (buffer) = GST_DP_HEADER_OFFSET_END (header); GST_BUFFER_FLAGS (buffer) = GST_DP_HEADER_BUFFER_FLAGS (header); return buffer; } /** * gst_dp_caps_from_packet: * @header_length: the length of the packet header * @header: the byte array of the packet header * @payload: the byte array of the packet payload * * Creates a newly allocated #GstCaps from the given packet. * * Returns: %TRUE if the caps was successfully created. */ GstCaps * gst_dp_caps_from_packet (guint header_length, const guint8 * header, const guint8 * payload) { GstCaps *caps; const gchar *string; g_return_val_if_fail (header, NULL); g_return_val_if_fail (payload, NULL); g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) == GST_DP_PAYLOAD_CAPS, NULL); string = (gchar *) payload; caps = gst_caps_from_string (string); return caps; } /** * gst_dp_event_from_packet: * @header_length: the length of the packet header * @header: the byte array of the packet header * @payload: the byte array of the packet payload * * Creates a newly allocated #GstEvent from the given packet. * * Returns: %TRUE if the event was successfully created. */ GstEvent * gst_dp_event_from_packet (guint header_length, const guint8 * header, const guint8 * payload) { GstEvent *event = NULL; GstEventType type; g_return_val_if_fail (header, NULL); /* payload can be NULL, e.g. for an EOS event */ type = GST_DP_HEADER_PAYLOAD_TYPE (header) - GST_DP_PAYLOAD_EVENT_NONE; switch (type) { case GST_EVENT_UNKNOWN: g_warning ("Unknown event, ignoring"); return FALSE; case GST_EVENT_EOS: case GST_EVENT_FLUSH_START: case GST_EVENT_FLUSH_STOP: case GST_EVENT_NEWSEGMENT: event = gst_event_new_custom (type, NULL); GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header); break; case GST_EVENT_SEEK: { gdouble rate; GstFormat format; GstSeekFlags flags; GstSeekType cur_type, stop_type; gint64 cur, stop; /* FIXME, read rate */ rate = 1.0; format = (GstFormat) GST_READ_UINT32_BE (payload); flags = (GstSeekFlags) GST_READ_UINT32_BE (payload + 4); cur_type = (GstSeekType) GST_READ_UINT32_BE (payload + 8); cur = (gint64) GST_READ_UINT64_BE (payload + 12); stop_type = (GstSeekType) GST_READ_UINT32_BE (payload + 20); stop = (gint64) GST_READ_UINT64_BE (payload + 24); event = gst_event_new_seek (rate, format, flags, cur_type, cur, stop_type, stop); GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header); break; } case GST_EVENT_QOS: case GST_EVENT_NAVIGATION: case GST_EVENT_TAG: g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event)); return FALSE; default: g_warning ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event)); return FALSE; } return event; } /** * gst_dp_validate_header: * @header_length: the length of the packet header * @header: the byte array of the packet header * * Validates the given packet header by checking the CRC checksum. * * Returns: %TRUE if the CRC matches, or no CRC checksum is present. */ gboolean gst_dp_validate_header (guint header_length, const guint8 * header) { guint16 crc_read, crc_calculated; if (!(GST_DP_HEADER_FLAGS (header) & GST_DP_HEADER_FLAG_CRC_HEADER)) return TRUE; crc_read = GST_DP_HEADER_CRC_HEADER (header); /* don't included the last two crc fields for the crc check */ crc_calculated = gst_dp_crc (header, header_length - 4); if (crc_read != crc_calculated) { GST_WARNING ("header crc mismatch: read %02x, calculated %02x", crc_read, crc_calculated); return FALSE; } GST_LOG ("header crc validation: %02x", crc_read); return TRUE; } /** * gst_dp_validate_payload: * @header_length: the length of the packet header * @header: the byte array of the packet header * @payload: the byte array of the packet payload * * Validates the given packet payload using the given packet header * by checking the CRC checksum. * * Returns: %TRUE if the CRC matches, or no CRC checksum is present. */ gboolean gst_dp_validate_payload (guint header_length, const guint8 * header, const guint8 * payload) { guint16 crc_read, crc_calculated; if (!(GST_DP_HEADER_FLAGS (header) & GST_DP_HEADER_FLAG_CRC_PAYLOAD)) return TRUE; crc_read = GST_DP_HEADER_CRC_PAYLOAD (header); crc_calculated = gst_dp_crc (payload, GST_DP_HEADER_PAYLOAD_LENGTH (header)); if (crc_read != crc_calculated) { GST_WARNING ("payload crc mismatch: read %02x, calculated %02x", crc_read, crc_calculated); return FALSE; } GST_LOG ("payload crc validation: %02x", crc_read); return TRUE; } /** * gst_dp_validate_packet: * @header_length: the length of the packet header * @header: the byte array of the packet header * @payload: the byte array of the packet payload * * Validates the given packet by checking version information and checksums. * * Returns: %TRUE if the packet validates. */ gboolean gst_dp_validate_packet (guint header_length, const guint8 * header, const guint8 * payload) { if (!gst_dp_validate_header (header_length, header)) return FALSE; if (!gst_dp_validate_payload (header_length, header, payload)) return FALSE; return TRUE; }