/* GStreamer * Copyright (C) <1999> Erik Walthinsen * Copyright (C) <2004> Thomas Vander Stichele * * dp-private.h: private defines/macros for dataprotocol implementation * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifndef __GST_DP_PRIVATE_H__ #define __GST_DP_PRIVATE_H__ #include #include #include G_BEGIN_DECLS /* accessor defines */ #define GST_DP_HEADER_MAJOR_VERSION(x) ((x)[0]) #define GST_DP_HEADER_MINOR_VERSION(x) ((x)[1]) #define GST_DP_HEADER_FLAGS(x) ((x)[2]) /* free byte here to align */ #define GST_DP_HEADER_PAYLOAD_TYPE(x) GST_READ_UINT16_BE (x + 4) #define GST_DP_HEADER_PAYLOAD_LENGTH(x) GST_READ_UINT32_BE (x + 6) #define GST_DP_HEADER_TIMESTAMP(x) GST_READ_UINT64_BE (x + 10) #define GST_DP_HEADER_DURATION(x) GST_READ_UINT64_BE (x + 18) #define GST_DP_HEADER_OFFSET(x) GST_READ_UINT64_BE (x + 26) #define GST_DP_HEADER_OFFSET_END(x) GST_READ_UINT64_BE (x + 34) #define GST_DP_HEADER_BUFFER_FLAGS(x) GST_READ_UINT16_BE (x + 42) #define GST_DP_HEADER_CRC_HEADER(x) GST_READ_UINT16_BE (x + 58) #define GST_DP_HEADER_CRC_PAYLOAD(x) GST_READ_UINT16_BE (x + 60) void gst_dp_dump_byte_array (guint8 *array, guint length); G_END_DECLS #endif /* __GST_DP_PRIVATE_H__ */