/* GStreamer * Copyright (C) 2005 Andy Wingo * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:gstnettimeprovider * @short_description: Special object that exposed the time of a clock * on the network. * @see_also: #GstClock, #GstNetClientClock, #GstPipeline * * This object exposes the time of a #GstClock on the network. * * A #GstNetTimeProvider is created with gst_net_time_provider_new() which * takes a #GstClock, an address and a port number as arguments. * * After creating the object, a client clock such as #GstNetClientClock can * query the exposed clock over the network for its values. * * The #GstNetTimeProvider typically wraps the clock used by a #GstPipeline. * * Last reviewed on 2005-11-23 (0.9.5) */ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include "gstnettimeprovider.h" #include "gstnettimepacket.h" #include #ifdef HAVE_UNISTD_H #include #endif #if defined (_MSC_VER) && _MSC_VER >= 1400 #include #endif #ifndef G_OS_WIN32 #include #endif #ifdef HAVE_FIONREAD_IN_SYS_FILIO #include #endif GST_DEBUG_CATEGORY_STATIC (ntp_debug); #define GST_CAT_DEFAULT (ntp_debug) #ifdef G_OS_WIN32 #define close(sock) closesocket(sock) #endif #define DEFAULT_ADDRESS "0.0.0.0" #define DEFAULT_PORT 5637 #define IS_ACTIVE(self) (g_atomic_int_get (&((self)->active.active))) #ifdef G_OS_WIN32 #define setsockopt(sock, sol_flags, reuse_flags, ru, sizeofru) setsockopt (sock, sol_flags, reuse_flags, (char *)ru, sizeofru) #endif enum { PROP_0, PROP_PORT, PROP_ADDRESS, PROP_CLOCK, PROP_ACTIVE /* FILL ME */ }; #define GST_NET_TIME_PROVIDER_GET_PRIVATE(obj) \ (G_TYPE_INSTANCE_GET_PRIVATE ((obj), GST_TYPE_NET_TIME_PROVIDER, GstNetTimeProviderPrivate)) struct _GstNetTimeProviderPrivate { GstPollFD sock; GstPoll *fdset; }; static gboolean gst_net_time_provider_start (GstNetTimeProvider * bself); static void gst_net_time_provider_stop (GstNetTimeProvider * bself); static gpointer gst_net_time_provider_thread (gpointer data); static void gst_net_time_provider_finalize (GObject * object); static void gst_net_time_provider_set_property (GObject * object, guint prop_id, const GValue * value, GParamSpec * pspec); static void gst_net_time_provider_get_property (GObject * object, guint prop_id, GValue * value, GParamSpec * pspec); #define _do_init(type) \ GST_DEBUG_CATEGORY_INIT (ntp_debug, "nettime", 0, "Network time provider"); GST_BOILERPLATE_FULL (GstNetTimeProvider, gst_net_time_provider, GstObject, GST_TYPE_OBJECT, _do_init); #ifdef G_OS_WIN32 static int inet_aton (const char *c, struct in_addr *paddr) { paddr->s_addr = inet_addr (c); if (paddr->s_addr == INADDR_NONE) return 0; return 1; } #endif static void gst_net_time_provider_base_init (gpointer g_class) { /* Do nothing here */ } static void gst_net_time_provider_class_init (GstNetTimeProviderClass * klass) { GObjectClass *gobject_class; gobject_class = G_OBJECT_CLASS (klass); g_assert (sizeof (GstClockTime) == 8); g_type_class_add_private (klass, sizeof (GstNetTimeProviderPrivate)); gobject_class->finalize = gst_net_time_provider_finalize; gobject_class->set_property = gst_net_time_provider_set_property; gobject_class->get_property = gst_net_time_provider_get_property; g_object_class_install_property (gobject_class, PROP_PORT, g_param_spec_int ("port", "port", "The port to receive the packets from, 0=allocate", 0, G_MAXUINT16, DEFAULT_PORT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_ADDRESS, g_param_spec_string ("address", "address", "The address to bind on, as a dotted quad (x.x.x.x)", DEFAULT_ADDRESS, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_CLOCK, g_param_spec_object ("clock", "Clock", "The clock to export over the network", GST_TYPE_CLOCK, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_ACTIVE, g_param_spec_boolean ("active", "Active", "TRUE if the clock will respond to queries over the network", TRUE, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); } static void gst_net_time_provider_init (GstNetTimeProvider * self, GstNetTimeProviderClass * g_class) { #ifdef G_OS_WIN32 WSADATA w; int error = WSAStartup (0x0202, &w); if (error) { GST_DEBUG_OBJECT (self, "Error on WSAStartup"); } if (w.wVersion != 0x0202) { WSACleanup (); } #endif self->priv = GST_NET_TIME_PROVIDER_GET_PRIVATE (self); self->port = DEFAULT_PORT; self->priv->sock.fd = -1; self->address = g_strdup (DEFAULT_ADDRESS); self->thread = NULL; self->active.active = TRUE; } static void gst_net_time_provider_finalize (GObject * object) { GstNetTimeProvider *self = GST_NET_TIME_PROVIDER (object); if (self->thread) { gst_net_time_provider_stop (self); g_assert (self->thread == NULL); } if (self->priv->fdset) { gst_poll_free (self->priv->fdset); self->priv->fdset = NULL; } g_free (self->address); self->address = NULL; if (self->clock) gst_object_unref (self->clock); self->clock = NULL; #ifdef G_OS_WIN32 WSACleanup (); #endif G_OBJECT_CLASS (parent_class)->finalize (object); } static gpointer gst_net_time_provider_thread (gpointer data) { GstNetTimeProvider *self = data; struct sockaddr_in tmpaddr; socklen_t len; GstNetTimePacket *packet; gint ret; while (TRUE) { GST_LOG_OBJECT (self, "doing select"); ret = gst_poll_wait (self->priv->fdset, GST_CLOCK_TIME_NONE); GST_LOG_OBJECT (self, "select returned %d", ret); if (ret <= 0) { if (errno == EBUSY) { GST_LOG_OBJECT (self, "stop"); goto stopped; } else if (errno != EAGAIN && errno != EINTR) goto select_error; else continue; } else { /* got data in */ len = sizeof (struct sockaddr); packet = gst_net_time_packet_receive (self->priv->sock.fd, (struct sockaddr *) &tmpaddr, &len); if (!packet) goto receive_error; if (IS_ACTIVE (self)) { /* do what we were asked to and send the packet back */ packet->remote_time = gst_clock_get_time (self->clock); /* ignore errors */ gst_net_time_packet_send (packet, self->priv->sock.fd, (struct sockaddr *) &tmpaddr, len); } g_free (packet); continue; } g_assert_not_reached (); /* log errors and keep going */ select_error: { GST_DEBUG_OBJECT (self, "select error %d: %s (%d)", ret, g_strerror (errno), errno); continue; } stopped: { GST_DEBUG_OBJECT (self, "shutting down"); /* close socket */ return NULL; } receive_error: { GST_DEBUG_OBJECT (self, "receive error"); continue; } g_assert_not_reached (); } g_assert_not_reached (); return NULL; } static void gst_net_time_provider_set_property (GObject * object, guint prop_id, const GValue * value, GParamSpec * pspec) { GstNetTimeProvider *self = GST_NET_TIME_PROVIDER (object); GstClock **clock_p = &self->clock; switch (prop_id) { case PROP_PORT: self->port = g_value_get_int (value); break; case PROP_ADDRESS: g_free (self->address); if (g_value_get_string (value) == NULL) self->address = g_strdup (DEFAULT_ADDRESS); else self->address = g_strdup (g_value_get_string (value)); break; case PROP_CLOCK: gst_object_replace ((GstObject **) clock_p, (GstObject *) g_value_get_object (value)); break; case PROP_ACTIVE: g_atomic_int_set (&self->active.active, g_value_get_boolean (value)); break; default: G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec); break; } } static void gst_net_time_provider_get_property (GObject * object, guint prop_id, GValue * value, GParamSpec * pspec) { GstNetTimeProvider *self = GST_NET_TIME_PROVIDER (object); switch (prop_id) { case PROP_PORT: g_value_set_int (value, self->port); break; case PROP_ADDRESS: g_value_set_string (value, self->address); break; case PROP_CLOCK: g_value_set_object (value, self->clock); break; case PROP_ACTIVE: g_value_set_boolean (value, IS_ACTIVE (self)); break; default: G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec); break; } } static gboolean gst_net_time_provider_start (GstNetTimeProvider * self) { gint ru; struct sockaddr_in my_addr; guint len; int port; gint ret; GError *error; if ((ret = socket (AF_INET, SOCK_DGRAM, 0)) < 0) goto no_socket; self->priv->sock.fd = ret; ru = 1; ret = setsockopt (self->priv->sock.fd, SOL_SOCKET, SO_REUSEADDR, &ru, sizeof (ru)); if (ret < 0) goto setsockopt_error; memset (&my_addr, 0, sizeof (my_addr)); my_addr.sin_family = AF_INET; /* host byte order */ my_addr.sin_port = htons ((gint16) self->port); /* short, network byte order */ my_addr.sin_addr.s_addr = INADDR_ANY; if (self->address) inet_aton (self->address, &my_addr.sin_addr); GST_DEBUG_OBJECT (self, "binding on port %d", self->port); ret = bind (self->priv->sock.fd, (struct sockaddr *) &my_addr, sizeof (my_addr)); if (ret < 0) goto bind_error; len = sizeof (my_addr); ret = getsockname (self->priv->sock.fd, (struct sockaddr *) &my_addr, &len); if (ret < 0) goto getsockname_error; port = ntohs (my_addr.sin_port); GST_DEBUG_OBJECT (self, "bound, on port %d", port); if (port != self->port) { self->port = port; GST_DEBUG_OBJECT (self, "notifying %d", port); g_object_notify (G_OBJECT (self), "port"); } gst_poll_add_fd (self->priv->fdset, &self->priv->sock); gst_poll_fd_ctl_read (self->priv->fdset, &self->priv->sock, TRUE); self->thread = g_thread_create (gst_net_time_provider_thread, self, TRUE, &error); if (!self->thread) goto no_thread; return TRUE; /* ERRORS */ no_socket: { GST_ERROR_OBJECT (self, "socket failed %d: %s (%d)", ret, g_strerror (errno), errno); return FALSE; } setsockopt_error: { close (self->priv->sock.fd); self->priv->sock.fd = -1; GST_ERROR_OBJECT (self, "setsockopt failed %d: %s (%d)", ret, g_strerror (errno), errno); return FALSE; } bind_error: { close (self->priv->sock.fd); self->priv->sock.fd = -1; GST_ERROR_OBJECT (self, "bind failed %d: %s (%d)", ret, g_strerror (errno), errno); return FALSE; } getsockname_error: { close (self->priv->sock.fd); self->priv->sock.fd = -1; GST_ERROR_OBJECT (self, "getsockname failed %d: %s (%d)", ret, g_strerror (errno), errno); return FALSE; } no_thread: { gst_poll_remove_fd (self->priv->fdset, &self->priv->sock); close (self->priv->sock.fd); self->priv->sock.fd = -1; GST_ERROR_OBJECT (self, "could not create thread: %s", error->message); g_error_free (error); return FALSE; } } static void gst_net_time_provider_stop (GstNetTimeProvider * self) { gst_poll_set_flushing (self->priv->fdset, TRUE); g_thread_join (self->thread); self->thread = NULL; if (self->priv->sock.fd != -1) { gst_poll_remove_fd (self->priv->fdset, &self->priv->sock); close (self->priv->sock.fd); self->priv->sock.fd = -1; } } /** * gst_net_time_provider_new: * @clock: a #GstClock to export over the network * @address: an address to bind on as a dotted quad (xxx.xxx.xxx.xxx), or NULL * to bind to all addresses * @port: a port to bind on, or 0 to let the kernel choose * * Allows network clients to get the current time of @clock. * * Returns: the new #GstNetTimeProvider, or NULL on error */ GstNetTimeProvider * gst_net_time_provider_new (GstClock * clock, const gchar * address, gint port) { GstNetTimeProvider *ret; g_return_val_if_fail (clock && GST_IS_CLOCK (clock), NULL); g_return_val_if_fail (port >= 0 && port <= G_MAXUINT16, NULL); ret = g_object_new (GST_TYPE_NET_TIME_PROVIDER, "clock", clock, "address", address, "port", port, NULL); if ((ret->priv->fdset = gst_poll_new (TRUE)) == NULL) goto no_fdset; if (!gst_net_time_provider_start (ret)) goto failed_start; /* all systems go, cap'n */ return ret; no_fdset: { GST_ERROR_OBJECT (ret, "could not create an fdset: %s (%d)", g_strerror (errno), errno); gst_object_unref (ret); return NULL; } failed_start: { /* already printed a nice error */ gst_object_unref (ret); return NULL; } }