/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2000 Wim Taymans * 2005 Philippe Khalaf * * gstfdsrc.c: * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:element-fdsrc * @see_also: #GstFdSink * * Read data from a unix file descriptor. * * To generate data, enter some data on the console folowed by enter. * The above mentioned pipeline should dump data packets to the console. * * If the #GstFdSrc:timeout property is set to a value bigger than 0, fdsrc will * generate an element message named * "GstFdSrcTimeout" * if no data was recieved in the given timeout. * The message's structure contains one field: * * * * #guint64 * "timeout": the timeout in microseconds that * expired when waiting for data. * * * * * * Example launch line * |[ * echo "Hello GStreamer" | gst-launch -v fdsrc ! fakesink dump=true * ]| A simple pipeline to read from the standard input and dump the data * with a fakesink as hex ascii block. * * * Last reviewed on 2008-06-20 (0.10.21) */ #ifdef HAVE_CONFIG_H # include "config.h" #endif #include "gst/gst_private.h" #include #ifdef G_OS_WIN32 #include /* lseek, open, close, read */ #undef lseek #define lseek _lseeki64 #undef off_t #define off_t guint64 #endif #include #ifdef HAVE_SYS_SOCKET_H #include #endif #include #include #ifdef HAVE_UNISTD_H #include #endif #ifdef _MSC_VER #undef stat #define stat _stat #define fstat _fstat #define S_ISREG(m) (((m)&S_IFREG)==S_IFREG) #endif #include #include #include "gstfdsrc.h" static GstStaticPadTemplate srctemplate = GST_STATIC_PAD_TEMPLATE ("src", GST_PAD_SRC, GST_PAD_ALWAYS, GST_STATIC_CAPS_ANY); GST_DEBUG_CATEGORY_STATIC (gst_fd_src_debug); #define GST_CAT_DEFAULT gst_fd_src_debug #define DEFAULT_FD 0 #define DEFAULT_TIMEOUT 0 enum { PROP_0, PROP_FD, PROP_TIMEOUT, PROP_LAST }; static void gst_fd_src_uri_handler_init (gpointer g_iface, gpointer iface_data); static void _do_init (GType fd_src_type) { static const GInterfaceInfo urihandler_info = { gst_fd_src_uri_handler_init, NULL, NULL }; g_type_add_interface_static (fd_src_type, GST_TYPE_URI_HANDLER, &urihandler_info); GST_DEBUG_CATEGORY_INIT (gst_fd_src_debug, "fdsrc", 0, "fdsrc element"); } GST_BOILERPLATE_FULL (GstFdSrc, gst_fd_src, GstPushSrc, GST_TYPE_PUSH_SRC, _do_init); static void gst_fd_src_set_property (GObject * object, guint prop_id, const GValue * value, GParamSpec * pspec); static void gst_fd_src_get_property (GObject * object, guint prop_id, GValue * value, GParamSpec * pspec); static void gst_fd_src_dispose (GObject * obj); static gboolean gst_fd_src_start (GstBaseSrc * bsrc); static gboolean gst_fd_src_stop (GstBaseSrc * bsrc); static gboolean gst_fd_src_unlock (GstBaseSrc * bsrc); static gboolean gst_fd_src_unlock_stop (GstBaseSrc * bsrc); static gboolean gst_fd_src_is_seekable (GstBaseSrc * bsrc); static gboolean gst_fd_src_get_size (GstBaseSrc * src, guint64 * size); static gboolean gst_fd_src_do_seek (GstBaseSrc * src, GstSegment * segment); static gboolean gst_fd_src_query (GstBaseSrc * src, GstQuery * query); static GstFlowReturn gst_fd_src_create (GstPushSrc * psrc, GstBuffer ** outbuf); static void gst_fd_src_base_init (gpointer g_class) { GstElementClass *gstelement_class = GST_ELEMENT_CLASS (g_class); gst_element_class_set_details_simple (gstelement_class, "Filedescriptor Source", "Source/File", "Read from a file descriptor", "Erik Walthinsen "); gst_element_class_add_pad_template (gstelement_class, gst_static_pad_template_get (&srctemplate)); } static void gst_fd_src_class_init (GstFdSrcClass * klass) { GObjectClass *gobject_class; GstBaseSrcClass *gstbasesrc_class; GstPushSrcClass *gstpush_src_class; gobject_class = G_OBJECT_CLASS (klass); gstbasesrc_class = GST_BASE_SRC_CLASS (klass); gstpush_src_class = GST_PUSH_SRC_CLASS (klass); gobject_class->set_property = gst_fd_src_set_property; gobject_class->get_property = gst_fd_src_get_property; gobject_class->dispose = gst_fd_src_dispose; g_object_class_install_property (gobject_class, PROP_FD, g_param_spec_int ("fd", "fd", "An open file descriptor to read from", 0, G_MAXINT, DEFAULT_FD, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); /** * GstFdSrc:timeout * * Post a message after timeout microseconds * * Since: 0.10.21 */ g_object_class_install_property (G_OBJECT_CLASS (klass), PROP_TIMEOUT, g_param_spec_uint64 ("timeout", "Timeout", "Post a message after timeout microseconds (0 = disabled)", 0, G_MAXUINT64, DEFAULT_TIMEOUT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); gstbasesrc_class->start = GST_DEBUG_FUNCPTR (gst_fd_src_start); gstbasesrc_class->stop = GST_DEBUG_FUNCPTR (gst_fd_src_stop); gstbasesrc_class->unlock = GST_DEBUG_FUNCPTR (gst_fd_src_unlock); gstbasesrc_class->unlock_stop = GST_DEBUG_FUNCPTR (gst_fd_src_unlock_stop); gstbasesrc_class->is_seekable = GST_DEBUG_FUNCPTR (gst_fd_src_is_seekable); gstbasesrc_class->get_size = GST_DEBUG_FUNCPTR (gst_fd_src_get_size); gstbasesrc_class->do_seek = GST_DEBUG_FUNCPTR (gst_fd_src_do_seek); gstbasesrc_class->query = GST_DEBUG_FUNCPTR (gst_fd_src_query); gstpush_src_class->create = GST_DEBUG_FUNCPTR (gst_fd_src_create); } static void gst_fd_src_init (GstFdSrc * fdsrc, GstFdSrcClass * klass) { fdsrc->new_fd = DEFAULT_FD; fdsrc->seekable_fd = FALSE; fdsrc->fd = -1; fdsrc->size = -1; fdsrc->timeout = DEFAULT_TIMEOUT; fdsrc->uri = g_strdup_printf ("fd://0"); fdsrc->curoffset = 0; } static void gst_fd_src_dispose (GObject * obj) { GstFdSrc *src = GST_FD_SRC (obj); g_free (src->uri); src->uri = NULL; G_OBJECT_CLASS (parent_class)->dispose (obj); } static void gst_fd_src_update_fd (GstFdSrc * src, guint64 size) { struct stat stat_results; GST_DEBUG_OBJECT (src, "fdset %p, old_fd %d, new_fd %d", src->fdset, src->fd, src->new_fd); /* we need to always update the fdset since it may not have existed when * gst_fd_src_update_fd () was called earlier */ if (src->fdset != NULL) { GstPollFD fd = GST_POLL_FD_INIT; if (src->fd >= 0) { fd.fd = src->fd; /* this will log a harmless warning, if it was never added */ gst_poll_remove_fd (src->fdset, &fd); } fd.fd = src->new_fd; gst_poll_add_fd (src->fdset, &fd); gst_poll_fd_ctl_read (src->fdset, &fd, TRUE); } if (src->fd != src->new_fd) { GST_INFO_OBJECT (src, "Updating to fd %d", src->new_fd); src->fd = src->new_fd; GST_INFO_OBJECT (src, "Setting size to fd %" G_GUINT64_FORMAT, size); src->size = size; g_free (src->uri); src->uri = g_strdup_printf ("fd://%d", src->fd); if (fstat (src->fd, &stat_results) < 0) goto not_seekable; if (!S_ISREG (stat_results.st_mode)) goto not_seekable; /* Try a seek of 0 bytes offset to check for seekability */ if (lseek (src->fd, 0, SEEK_CUR) < 0) goto not_seekable; GST_INFO_OBJECT (src, "marking fd %d as seekable", src->fd); src->seekable_fd = TRUE; gst_base_src_set_dynamic_size (GST_BASE_SRC (src), TRUE); } return; not_seekable: { GST_INFO_OBJECT (src, "marking fd %d as NOT seekable", src->fd); src->seekable_fd = FALSE; gst_base_src_set_dynamic_size (GST_BASE_SRC (src), FALSE); } } static gboolean gst_fd_src_start (GstBaseSrc * bsrc) { GstFdSrc *src = GST_FD_SRC (bsrc); src->curoffset = 0; if ((src->fdset = gst_poll_new (TRUE)) == NULL) goto socket_pair; gst_fd_src_update_fd (src, -1); return TRUE; /* ERRORS */ socket_pair: { GST_ELEMENT_ERROR (src, RESOURCE, OPEN_READ_WRITE, (NULL), GST_ERROR_SYSTEM); return FALSE; } } static gboolean gst_fd_src_stop (GstBaseSrc * bsrc) { GstFdSrc *src = GST_FD_SRC (bsrc); if (src->fdset) { gst_poll_free (src->fdset); src->fdset = NULL; } return TRUE; } static gboolean gst_fd_src_unlock (GstBaseSrc * bsrc) { GstFdSrc *src = GST_FD_SRC (bsrc); GST_LOG_OBJECT (src, "Flushing"); GST_OBJECT_LOCK (src); gst_poll_set_flushing (src->fdset, TRUE); GST_OBJECT_UNLOCK (src); return TRUE; } static gboolean gst_fd_src_unlock_stop (GstBaseSrc * bsrc) { GstFdSrc *src = GST_FD_SRC (bsrc); GST_LOG_OBJECT (src, "No longer flushing"); GST_OBJECT_LOCK (src); gst_poll_set_flushing (src->fdset, FALSE); GST_OBJECT_UNLOCK (src); return TRUE; } static void gst_fd_src_set_property (GObject * object, guint prop_id, const GValue * value, GParamSpec * pspec) { GstFdSrc *src = GST_FD_SRC (object); switch (prop_id) { case PROP_FD: src->new_fd = g_value_get_int (value); /* If state is ready or below, update the current fd immediately * so it is reflected in get_properties and uri */ GST_OBJECT_LOCK (object); if (GST_STATE (GST_ELEMENT (src)) <= GST_STATE_READY) { GST_DEBUG_OBJECT (src, "state ready or lower, updating to use new fd"); gst_fd_src_update_fd (src, -1); } else { GST_DEBUG_OBJECT (src, "state above ready, not updating to new fd yet"); } GST_OBJECT_UNLOCK (object); break; case PROP_TIMEOUT: src->timeout = g_value_get_uint64 (value); GST_DEBUG_OBJECT (src, "poll timeout set to %" GST_TIME_FORMAT, GST_TIME_ARGS (src->timeout)); break; default: G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec); break; } } static void gst_fd_src_get_property (GObject * object, guint prop_id, GValue * value, GParamSpec * pspec) { GstFdSrc *src = GST_FD_SRC (object); switch (prop_id) { case PROP_FD: g_value_set_int (value, src->fd); break; case PROP_TIMEOUT: g_value_set_uint64 (value, src->timeout); break; default: G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec); break; } } static GstFlowReturn gst_fd_src_create (GstPushSrc * psrc, GstBuffer ** outbuf) { GstFdSrc *src; GstBuffer *buf; gssize readbytes; guint blocksize; GstClockTime timeout; #ifndef HAVE_WIN32 gboolean try_again; gint retval; #endif src = GST_FD_SRC (psrc); if (src->timeout > 0) { timeout = src->timeout * GST_USECOND; } else { timeout = GST_CLOCK_TIME_NONE; } #ifndef HAVE_WIN32 do { try_again = FALSE; GST_LOG_OBJECT (src, "doing poll, timeout %" GST_TIME_FORMAT, GST_TIME_ARGS (src->timeout)); retval = gst_poll_wait (src->fdset, timeout); GST_LOG_OBJECT (src, "poll returned %d", retval); if (G_UNLIKELY (retval == -1)) { if (errno == EINTR || errno == EAGAIN) { /* retry if interrupted */ try_again = TRUE; } else if (errno == EBUSY) { goto stopped; } else { goto poll_error; } } else if (G_UNLIKELY (retval == 0)) { try_again = TRUE; /* timeout, post element message */ gst_element_post_message (GST_ELEMENT_CAST (src), gst_message_new_element (GST_OBJECT_CAST (src), gst_structure_new ("GstFdSrcTimeout", "timeout", G_TYPE_UINT64, src->timeout, NULL))); } } while (G_UNLIKELY (try_again)); /* retry if interrupted or timeout */ #endif blocksize = GST_BASE_SRC (src)->blocksize; /* create the buffer */ buf = gst_buffer_try_new_and_alloc (blocksize); if (G_UNLIKELY (buf == NULL)) { GST_ERROR_OBJECT (src, "Failed to allocate %u bytes", blocksize); return GST_FLOW_ERROR; } do { readbytes = read (src->fd, GST_BUFFER_DATA (buf), blocksize); GST_LOG_OBJECT (src, "read %" G_GSSIZE_FORMAT, readbytes); } while (readbytes == -1 && errno == EINTR); /* retry if interrupted */ if (readbytes < 0) goto read_error; if (readbytes == 0) goto eos; GST_BUFFER_OFFSET (buf) = src->curoffset; GST_BUFFER_SIZE (buf) = readbytes; GST_BUFFER_TIMESTAMP (buf) = GST_CLOCK_TIME_NONE; src->curoffset += readbytes; GST_LOG_OBJECT (psrc, "Read buffer of size %" G_GSSIZE_FORMAT, readbytes); /* we're done, return the buffer */ *outbuf = buf; return GST_FLOW_OK; /* ERRORS */ #ifndef HAVE_WIN32 poll_error: { GST_ELEMENT_ERROR (src, RESOURCE, READ, (NULL), ("poll on file descriptor: %s.", g_strerror (errno))); GST_DEBUG_OBJECT (psrc, "Error during poll"); return GST_FLOW_ERROR; } stopped: { GST_DEBUG_OBJECT (psrc, "Poll stopped"); return GST_FLOW_WRONG_STATE; } #endif eos: { GST_DEBUG_OBJECT (psrc, "Read 0 bytes. EOS."); gst_buffer_unref (buf); return GST_FLOW_UNEXPECTED; } read_error: { GST_ELEMENT_ERROR (src, RESOURCE, READ, (NULL), ("read on file descriptor: %s.", g_strerror (errno))); GST_DEBUG_OBJECT (psrc, "Error reading from fd"); gst_buffer_unref (buf); return GST_FLOW_ERROR; } } static gboolean gst_fd_src_query (GstBaseSrc * basesrc, GstQuery * query) { gboolean ret = FALSE; GstFdSrc *src = GST_FD_SRC (basesrc); switch (GST_QUERY_TYPE (query)) { case GST_QUERY_URI: gst_query_set_uri (query, src->uri); ret = TRUE; break; default: ret = FALSE; break; } if (!ret) ret = GST_BASE_SRC_CLASS (parent_class)->query (basesrc, query); return ret; } static gboolean gst_fd_src_is_seekable (GstBaseSrc * bsrc) { GstFdSrc *src = GST_FD_SRC (bsrc); return src->seekable_fd; } static gboolean gst_fd_src_get_size (GstBaseSrc * bsrc, guint64 * size) { GstFdSrc *src = GST_FD_SRC (bsrc); struct stat stat_results; if (src->size != -1) { *size = src->size; return TRUE; } if (!src->seekable_fd) { /* If it isn't seekable, we won't know the length (but fstat will still * succeed, and wrongly say our length is zero. */ return FALSE; } if (fstat (src->fd, &stat_results) < 0) goto could_not_stat; *size = stat_results.st_size; return TRUE; /* ERROR */ could_not_stat: { return FALSE; } } static gboolean gst_fd_src_do_seek (GstBaseSrc * bsrc, GstSegment * segment) { gint res; gint64 offset; GstFdSrc *src = GST_FD_SRC (bsrc); offset = segment->start; /* No need to seek to the current position */ if (offset == src->curoffset) return TRUE; res = lseek (src->fd, offset, SEEK_SET); if (G_UNLIKELY (res < 0 || res != offset)) goto seek_failed; segment->last_stop = segment->start; segment->time = segment->start; return TRUE; seek_failed: GST_DEBUG_OBJECT (src, "lseek returned %" G_GINT64_FORMAT, offset); return FALSE; } /*** GSTURIHANDLER INTERFACE *************************************************/ static GstURIType gst_fd_src_uri_get_type (void) { return GST_URI_SRC; } static gchar ** gst_fd_src_uri_get_protocols (void) { static gchar *protocols[] = { (char *) "fd", NULL }; return protocols; } static const gchar * gst_fd_src_uri_get_uri (GstURIHandler * handler) { GstFdSrc *src = GST_FD_SRC (handler); return src->uri; } static gboolean gst_fd_src_uri_set_uri (GstURIHandler * handler, const gchar * uri) { gchar *protocol, *q; GstFdSrc *src = GST_FD_SRC (handler); gint fd; guint64 size = -1; GST_INFO_OBJECT (src, "checking uri %s", uri); protocol = gst_uri_get_protocol (uri); if (strcmp (protocol, "fd") != 0) { g_free (protocol); return FALSE; } g_free (protocol); if (sscanf (uri, "fd://%d", &fd) != 1 || fd < 0) return FALSE; if ((q = g_strstr_len (uri, -1, "?"))) { gchar *sp; GST_INFO_OBJECT (src, "found ?"); if ((sp = g_strstr_len (q, -1, "size="))) { if (sscanf (sp, "size=%" G_GUINT64_FORMAT, &size) != 1) { GST_INFO_OBJECT (src, "parsing size failed"); size = -1; } else { GST_INFO_OBJECT (src, "found size %" G_GUINT64_FORMAT, size); } } } src->new_fd = fd; GST_OBJECT_LOCK (src); if (GST_STATE (GST_ELEMENT (src)) <= GST_STATE_READY) { gst_fd_src_update_fd (src, size); } GST_OBJECT_UNLOCK (src); return TRUE; } static void gst_fd_src_uri_handler_init (gpointer g_iface, gpointer iface_data) { GstURIHandlerInterface *iface = (GstURIHandlerInterface *) g_iface; iface->get_type = gst_fd_src_uri_get_type; iface->get_protocols = gst_fd_src_uri_get_protocols; iface->get_uri = gst_fd_src_uri_get_uri; iface->set_uri = gst_fd_src_uri_set_uri; }