/* GStreamer * Copyright (C) 1999,2000 Erik Walthinsen * 2003 Colin Walters * 2000,2005,2007 Wim Taymans * 2007 Thiago Sousa Santos * SA 2010 ST-Ericsson * * gstqueue2.c: * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /** * SECTION:element-queue2 * * Data is queued until one of the limits specified by the * #GstQueue2:max-size-buffers, #GstQueue2:max-size-bytes and/or * #GstQueue2:max-size-time properties has been reached. Any attempt to push * more buffers into the queue will block the pushing thread until more space * becomes available. * * The queue will create a new thread on the source pad to decouple the * processing on sink and source pad. * * You can query how many buffers are queued by reading the * #GstQueue2:current-level-buffers property. * * The default queue size limits are 100 buffers, 2MB of data, or * two seconds worth of data, whichever is reached first. * * If you set temp-tmpl to a value such as /tmp/gstreamer-XXXXXX, the element * will allocate a random free filename and buffer data in the file. * By using this, it will buffer the entire stream data on the file independently * of the queue size limits, they will only be used for buffering statistics. * * Since 0.10.24, setting the temp-location property with a filename is deprecated * because it's impossible to securely open a temporary file in this way. The * property will still be used to notify the application of the allocated * filename, though. * * Last reviewed on 2009-07-10 (0.10.24) */ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include "gstqueue2.h" #include #include "gst/gst-i18n-lib.h" #include #ifdef G_OS_WIN32 #include /* lseek, open, close, read */ #undef lseek #define lseek _lseeki64 #undef off_t #define off_t guint64 #else #include #endif static GstStaticPadTemplate sinktemplate = GST_STATIC_PAD_TEMPLATE ("sink", GST_PAD_SINK, GST_PAD_ALWAYS, GST_STATIC_CAPS_ANY); static GstStaticPadTemplate srctemplate = GST_STATIC_PAD_TEMPLATE ("src", GST_PAD_SRC, GST_PAD_ALWAYS, GST_STATIC_CAPS_ANY); GST_DEBUG_CATEGORY_STATIC (queue_debug); #define GST_CAT_DEFAULT (queue_debug) GST_DEBUG_CATEGORY_STATIC (queue_dataflow); enum { LAST_SIGNAL }; /* other defines */ #define DEFAULT_BUFFER_SIZE 4096 #define QUEUE_IS_USING_TEMP_FILE(queue) ((queue)->temp_location_set || (queue)->temp_template != NULL) #define QUEUE_IS_USING_RING_BUFFER(queue) ((queue)->use_ring_buffer) /* for consistency with the above macro */ #define QUEUE_IS_USING_QUEUE(queue) (!QUEUE_IS_USING_TEMP_FILE(queue) && !QUEUE_IS_USING_RING_BUFFER (queue)) #define QUEUE_MAX_BYTES(queue) MIN((queue)->max_level.bytes, (queue)->ring_buffer_max_size) /* default property values */ #define DEFAULT_MAX_SIZE_BUFFERS 100 /* 100 buffers */ #define DEFAULT_MAX_SIZE_BYTES (2 * 1024 * 1024) /* 2 MB */ #define DEFAULT_MAX_SIZE_TIME 2 * GST_SECOND /* 2 seconds */ #define DEFAULT_USE_BUFFERING FALSE #define DEFAULT_USE_RATE_ESTIMATE TRUE #define DEFAULT_LOW_PERCENT 10 #define DEFAULT_HIGH_PERCENT 99 #define DEFAULT_TEMP_REMOVE TRUE #define DEFAULT_RING_BUFFER_MAX_SIZE 0 enum { PROP_0, PROP_CUR_LEVEL_BUFFERS, PROP_CUR_LEVEL_BYTES, PROP_CUR_LEVEL_TIME, PROP_MAX_SIZE_BUFFERS, PROP_MAX_SIZE_BYTES, PROP_MAX_SIZE_TIME, PROP_USE_BUFFERING, PROP_USE_RATE_ESTIMATE, PROP_LOW_PERCENT, PROP_HIGH_PERCENT, PROP_TEMP_TEMPLATE, PROP_TEMP_LOCATION, PROP_TEMP_REMOVE, PROP_RING_BUFFER_MAX_SIZE, PROP_LAST }; #define GST_QUEUE2_CLEAR_LEVEL(l) G_STMT_START { \ l.buffers = 0; \ l.bytes = 0; \ l.time = 0; \ l.rate_time = 0; \ } G_STMT_END #define STATUS(queue, pad, msg) \ GST_CAT_LOG_OBJECT (queue_dataflow, queue, \ "(%s:%s) " msg ": %u of %u buffers, %u of %u " \ "bytes, %" G_GUINT64_FORMAT " of %" G_GUINT64_FORMAT \ " ns, %"G_GUINT64_FORMAT" items", \ GST_DEBUG_PAD_NAME (pad), \ queue->cur_level.buffers, \ queue->max_level.buffers, \ queue->cur_level.bytes, \ queue->max_level.bytes, \ queue->cur_level.time, \ queue->max_level.time, \ (guint64) (!QUEUE_IS_USING_QUEUE(queue) ? \ queue->current->writing_pos - queue->current->max_reading_pos : \ queue->queue->length)) #define GST_QUEUE2_MUTEX_LOCK(q) G_STMT_START { \ g_mutex_lock (q->qlock); \ } G_STMT_END #define GST_QUEUE2_MUTEX_LOCK_CHECK(q,res,label) G_STMT_START { \ GST_QUEUE2_MUTEX_LOCK (q); \ if (res != GST_FLOW_OK) \ goto label; \ } G_STMT_END #define GST_QUEUE2_MUTEX_UNLOCK(q) G_STMT_START { \ g_mutex_unlock (q->qlock); \ } G_STMT_END #define GST_QUEUE2_WAIT_DEL_CHECK(q, res, label) G_STMT_START { \ STATUS (queue, q->sinkpad, "wait for DEL"); \ q->waiting_del = TRUE; \ g_cond_wait (q->item_del, queue->qlock); \ q->waiting_del = FALSE; \ if (res != GST_FLOW_OK) { \ STATUS (queue, q->srcpad, "received DEL wakeup"); \ goto label; \ } \ STATUS (queue, q->sinkpad, "received DEL"); \ } G_STMT_END #define GST_QUEUE2_WAIT_ADD_CHECK(q, res, label) G_STMT_START { \ STATUS (queue, q->srcpad, "wait for ADD"); \ q->waiting_add = TRUE; \ g_cond_wait (q->item_add, q->qlock); \ q->waiting_add = FALSE; \ if (res != GST_FLOW_OK) { \ STATUS (queue, q->srcpad, "received ADD wakeup"); \ goto label; \ } \ STATUS (queue, q->srcpad, "received ADD"); \ } G_STMT_END #define GST_QUEUE2_SIGNAL_DEL(q) G_STMT_START { \ if (q->waiting_del) { \ STATUS (q, q->srcpad, "signal DEL"); \ g_cond_signal (q->item_del); \ } \ } G_STMT_END #define GST_QUEUE2_SIGNAL_ADD(q) G_STMT_START { \ if (q->waiting_add) { \ STATUS (q, q->sinkpad, "signal ADD"); \ g_cond_signal (q->item_add); \ } \ } G_STMT_END #define _do_init(bla) \ GST_DEBUG_CATEGORY_INIT (queue_debug, "queue2", 0, "queue element"); \ GST_DEBUG_CATEGORY_INIT (queue_dataflow, "queue2_dataflow", 0, \ "dataflow inside the queue element"); GST_BOILERPLATE_FULL (GstQueue2, gst_queue2, GstElement, GST_TYPE_ELEMENT, _do_init); static void gst_queue2_finalize (GObject * object); static void gst_queue2_set_property (GObject * object, guint prop_id, const GValue * value, GParamSpec * pspec); static void gst_queue2_get_property (GObject * object, guint prop_id, GValue * value, GParamSpec * pspec); static GstFlowReturn gst_queue2_chain (GstPad * pad, GstBuffer * buffer); static GstFlowReturn gst_queue2_bufferalloc (GstPad * pad, guint64 offset, guint size, GstCaps * caps, GstBuffer ** buf); static GstFlowReturn gst_queue2_push_one (GstQueue2 * queue); static void gst_queue2_loop (GstPad * pad); static gboolean gst_queue2_handle_sink_event (GstPad * pad, GstEvent * event); static gboolean gst_queue2_handle_src_event (GstPad * pad, GstEvent * event); static gboolean gst_queue2_handle_src_query (GstPad * pad, GstQuery * query); static gboolean gst_queue2_handle_query (GstElement * element, GstQuery * query); static GstCaps *gst_queue2_getcaps (GstPad * pad); static gboolean gst_queue2_acceptcaps (GstPad * pad, GstCaps * caps); static GstFlowReturn gst_queue2_get_range (GstPad * pad, guint64 offset, guint length, GstBuffer ** buffer); static gboolean gst_queue2_src_checkgetrange_function (GstPad * pad); static gboolean gst_queue2_src_activate_pull (GstPad * pad, gboolean active); static gboolean gst_queue2_src_activate_push (GstPad * pad, gboolean active); static gboolean gst_queue2_sink_activate_push (GstPad * pad, gboolean active); static GstStateChangeReturn gst_queue2_change_state (GstElement * element, GstStateChange transition); static gboolean gst_queue2_is_empty (GstQueue2 * queue); static gboolean gst_queue2_is_filled (GstQueue2 * queue); static void update_cur_level (GstQueue2 * queue, GstQueue2Range * range); /* static guint gst_queue2_signals[LAST_SIGNAL] = { 0 }; */ static void gst_queue2_base_init (gpointer g_class) { GstElementClass *gstelement_class = GST_ELEMENT_CLASS (g_class); gst_element_class_add_pad_template (gstelement_class, gst_static_pad_template_get (&srctemplate)); gst_element_class_add_pad_template (gstelement_class, gst_static_pad_template_get (&sinktemplate)); gst_element_class_set_details_simple (gstelement_class, "Queue 2", "Generic", "Simple data queue", "Erik Walthinsen , " "Wim Taymans "); } static void gst_queue2_class_init (GstQueue2Class * klass) { GObjectClass *gobject_class = G_OBJECT_CLASS (klass); GstElementClass *gstelement_class = GST_ELEMENT_CLASS (klass); parent_class = g_type_class_peek_parent (klass); gobject_class->set_property = gst_queue2_set_property; gobject_class->get_property = gst_queue2_get_property; /* properties */ g_object_class_install_property (gobject_class, PROP_CUR_LEVEL_BYTES, g_param_spec_uint ("current-level-bytes", "Current level (kB)", "Current amount of data in the queue (bytes)", 0, G_MAXUINT, 0, G_PARAM_READABLE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_CUR_LEVEL_BUFFERS, g_param_spec_uint ("current-level-buffers", "Current level (buffers)", "Current number of buffers in the queue", 0, G_MAXUINT, 0, G_PARAM_READABLE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_CUR_LEVEL_TIME, g_param_spec_uint64 ("current-level-time", "Current level (ns)", "Current amount of data in the queue (in ns)", 0, G_MAXUINT64, 0, G_PARAM_READABLE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_MAX_SIZE_BYTES, g_param_spec_uint ("max-size-bytes", "Max. size (kB)", "Max. amount of data in the queue (bytes, 0=disable)", 0, G_MAXUINT, DEFAULT_MAX_SIZE_BYTES, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_MAX_SIZE_BUFFERS, g_param_spec_uint ("max-size-buffers", "Max. size (buffers)", "Max. number of buffers in the queue (0=disable)", 0, G_MAXUINT, DEFAULT_MAX_SIZE_BUFFERS, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_MAX_SIZE_TIME, g_param_spec_uint64 ("max-size-time", "Max. size (ns)", "Max. amount of data in the queue (in ns, 0=disable)", 0, G_MAXUINT64, DEFAULT_MAX_SIZE_TIME, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_USE_BUFFERING, g_param_spec_boolean ("use-buffering", "Use buffering", "Emit GST_MESSAGE_BUFFERING based on low-/high-percent thresholds", DEFAULT_USE_BUFFERING, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_USE_RATE_ESTIMATE, g_param_spec_boolean ("use-rate-estimate", "Use Rate Estimate", "Estimate the bitrate of the stream to calculate time level", DEFAULT_USE_RATE_ESTIMATE, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_LOW_PERCENT, g_param_spec_int ("low-percent", "Low percent", "Low threshold for buffering to start", 0, 100, DEFAULT_LOW_PERCENT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_HIGH_PERCENT, g_param_spec_int ("high-percent", "High percent", "High threshold for buffering to finish", 0, 100, DEFAULT_HIGH_PERCENT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_TEMP_TEMPLATE, g_param_spec_string ("temp-template", "Temporary File Template", "File template to store temporary files in, should contain directory " "and XXXXXX. (NULL == disabled)", NULL, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); g_object_class_install_property (gobject_class, PROP_TEMP_LOCATION, g_param_spec_string ("temp-location", "Temporary File Location", "Location to store temporary files in (Deprecated: Only read this " "property, use temp-template to configure the name template)", NULL, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); /** * GstQueue2:temp-remove * * When temp-template is set, remove the temporary file when going to READY. * * Since: 0.10.26 */ g_object_class_install_property (gobject_class, PROP_TEMP_REMOVE, g_param_spec_boolean ("temp-remove", "Remove the Temporary File", "Remove the temp-location after use", DEFAULT_TEMP_REMOVE, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); /** * GstQueue2:ring-buffer-max-size * * The maximum size of the ring buffer in bytes. If set to 0, the ring * buffer is disabled. Default 0. * * Since: 0.10.30 */ g_object_class_install_property (gobject_class, PROP_RING_BUFFER_MAX_SIZE, g_param_spec_uint64 ("ring-buffer-max-size", "Max. ring buffer size (bytes)", "Max. amount of data in the ring buffer (bytes, 0 = disabled", 0, G_MAXUINT, DEFAULT_RING_BUFFER_MAX_SIZE, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS)); /* set several parent class virtual functions */ gobject_class->finalize = gst_queue2_finalize; gstelement_class->change_state = GST_DEBUG_FUNCPTR (gst_queue2_change_state); gstelement_class->query = GST_DEBUG_FUNCPTR (gst_queue2_handle_query); } static void gst_queue2_init (GstQueue2 * queue, GstQueue2Class * g_class) { queue->sinkpad = gst_pad_new_from_static_template (&sinktemplate, "sink"); gst_pad_set_chain_function (queue->sinkpad, GST_DEBUG_FUNCPTR (gst_queue2_chain)); gst_pad_set_activatepush_function (queue->sinkpad, GST_DEBUG_FUNCPTR (gst_queue2_sink_activate_push)); gst_pad_set_event_function (queue->sinkpad, GST_DEBUG_FUNCPTR (gst_queue2_handle_sink_event)); gst_pad_set_getcaps_function (queue->sinkpad, GST_DEBUG_FUNCPTR (gst_queue2_getcaps)); gst_pad_set_acceptcaps_function (queue->sinkpad, GST_DEBUG_FUNCPTR (gst_queue2_acceptcaps)); gst_pad_set_bufferalloc_function (queue->sinkpad, GST_DEBUG_FUNCPTR (gst_queue2_bufferalloc)); gst_element_add_pad (GST_ELEMENT (queue), queue->sinkpad); queue->srcpad = gst_pad_new_from_static_template (&srctemplate, "src"); gst_pad_set_activatepull_function (queue->srcpad, GST_DEBUG_FUNCPTR (gst_queue2_src_activate_pull)); gst_pad_set_activatepush_function (queue->srcpad, GST_DEBUG_FUNCPTR (gst_queue2_src_activate_push)); gst_pad_set_getrange_function (queue->srcpad, GST_DEBUG_FUNCPTR (gst_queue2_get_range)); gst_pad_set_checkgetrange_function (queue->srcpad, GST_DEBUG_FUNCPTR (gst_queue2_src_checkgetrange_function)); gst_pad_set_getcaps_function (queue->srcpad, GST_DEBUG_FUNCPTR (gst_queue2_getcaps)); gst_pad_set_acceptcaps_function (queue->srcpad, GST_DEBUG_FUNCPTR (gst_queue2_acceptcaps)); gst_pad_set_event_function (queue->srcpad, GST_DEBUG_FUNCPTR (gst_queue2_handle_src_event)); gst_pad_set_query_function (queue->srcpad, GST_DEBUG_FUNCPTR (gst_queue2_handle_src_query)); gst_element_add_pad (GST_ELEMENT (queue), queue->srcpad); /* levels */ GST_QUEUE2_CLEAR_LEVEL (queue->cur_level); queue->max_level.buffers = DEFAULT_MAX_SIZE_BUFFERS; queue->max_level.bytes = DEFAULT_MAX_SIZE_BYTES; queue->max_level.time = DEFAULT_MAX_SIZE_TIME; queue->max_level.rate_time = DEFAULT_MAX_SIZE_TIME; queue->use_buffering = DEFAULT_USE_BUFFERING; queue->use_rate_estimate = DEFAULT_USE_RATE_ESTIMATE; queue->low_percent = DEFAULT_LOW_PERCENT; queue->high_percent = DEFAULT_HIGH_PERCENT; gst_segment_init (&queue->sink_segment, GST_FORMAT_TIME); gst_segment_init (&queue->src_segment, GST_FORMAT_TIME); queue->srcresult = GST_FLOW_WRONG_STATE; queue->sinkresult = GST_FLOW_WRONG_STATE; queue->is_eos = FALSE; queue->in_timer = g_timer_new (); queue->out_timer = g_timer_new (); queue->qlock = g_mutex_new (); queue->waiting_add = FALSE; queue->item_add = g_cond_new (); queue->waiting_del = FALSE; queue->item_del = g_cond_new (); queue->queue = g_queue_new (); /* tempfile related */ queue->temp_template = NULL; queue->temp_location = NULL; queue->temp_location_set = FALSE; queue->temp_remove = DEFAULT_TEMP_REMOVE; queue->use_ring_buffer = FALSE; queue->ring_buffer = NULL; queue->ring_buffer_max_size = DEFAULT_RING_BUFFER_MAX_SIZE; GST_DEBUG_OBJECT (queue, "initialized queue's not_empty & not_full conditions"); } /* called only once, as opposed to dispose */ static void gst_queue2_finalize (GObject * object) { GstQueue2 *queue = GST_QUEUE2 (object); GST_DEBUG_OBJECT (queue, "finalizing queue"); while (!g_queue_is_empty (queue->queue)) { GstMiniObject *data = g_queue_pop_head (queue->queue); gst_mini_object_unref (data); } g_queue_free (queue->queue); g_mutex_free (queue->qlock); g_cond_free (queue->item_add); g_cond_free (queue->item_del); g_timer_destroy (queue->in_timer); g_timer_destroy (queue->out_timer); /* temp_file path cleanup */ g_free (queue->temp_template); g_free (queue->temp_location); G_OBJECT_CLASS (parent_class)->finalize (object); } static void debug_ranges (GstQueue2 * queue) { GstQueue2Range *walk; for (walk = queue->ranges; walk; walk = walk->next) { GST_DEBUG_OBJECT (queue, "range %" G_GUINT64_FORMAT "-%" G_GUINT64_FORMAT ", reading %" G_GUINT64_FORMAT, walk->offset, walk->writing_pos, walk->reading_pos); } } /* clear all the downloaded ranges */ static void clean_ranges (GstQueue2 * queue) { GST_DEBUG_OBJECT (queue, "clean queue ranges"); g_slice_free_chain (GstQueue2Range, queue->ranges, next); queue->ranges = NULL; queue->current = NULL; } /* find a range that contains @offset or NULL when nothing does */ static GstQueue2Range * find_range (GstQueue2 * queue, guint64 offset, guint64 length) { GstQueue2Range *range = NULL; GstQueue2Range *walk; /* first do a quick check for the current range */ for (walk = queue->ranges; walk; walk = walk->next) { if (offset >= walk->offset && offset <= walk->writing_pos) { /* we can reuse an existing range */ range = walk; break; } } return range; } static void update_cur_level (GstQueue2 * queue, GstQueue2Range * range) { guint64 max_reading_pos, writing_pos; writing_pos = range->writing_pos; max_reading_pos = range->max_reading_pos; if (writing_pos > max_reading_pos) queue->cur_level.bytes = writing_pos - max_reading_pos; else queue->cur_level.bytes = 0; } /* make a new range for @offset or reuse an existing range */ static GstQueue2Range * add_range (GstQueue2 * queue, guint64 offset) { GstQueue2Range *range, *prev, *next; GST_DEBUG_OBJECT (queue, "find range for %" G_GUINT64_FORMAT, offset); if ((range = find_range (queue, offset, 0))) { GST_DEBUG_OBJECT (queue, "reusing range %" G_GUINT64_FORMAT "-%" G_GUINT64_FORMAT, range->offset, range->writing_pos); range->writing_pos = offset; } else { GST_DEBUG_OBJECT (queue, "new range %" G_GUINT64_FORMAT "-%" G_GUINT64_FORMAT, offset, offset); range = g_slice_new0 (GstQueue2Range); range->offset = offset; /* we want to write to the next location in the ring buffer */ range->rb_offset = queue->current ? queue->current->rb_writing_pos : 0; range->writing_pos = offset; range->rb_writing_pos = range->rb_offset; range->reading_pos = offset; range->max_reading_pos = offset; /* insert sorted */ prev = NULL; next = queue->ranges; while (next) { if (next->offset > offset) { /* insert before next */ GST_DEBUG_OBJECT (queue, "insert before range %p, offset %" G_GUINT64_FORMAT, next, next->offset); break; } /* try next */ prev = next; next = next->next; } range->next = next; if (prev) prev->next = range; else queue->ranges = range; } debug_ranges (queue); /* update the stats for this range */ update_cur_level (queue, range); return range; } /* clear and init the download ranges for offset 0 */ static void init_ranges (GstQueue2 * queue) { GST_DEBUG_OBJECT (queue, "init queue ranges"); /* get rid of all the current ranges */ clean_ranges (queue); /* make a range for offset 0 */ queue->current = add_range (queue, 0); } static gboolean gst_queue2_acceptcaps (GstPad * pad, GstCaps * caps) { GstQueue2 *queue; GstPad *otherpad; gboolean result; queue = GST_QUEUE2 (GST_PAD_PARENT (pad)); otherpad = (pad == queue->srcpad ? queue->sinkpad : queue->srcpad); result = gst_pad_peer_accept_caps (otherpad, caps); return result; } static GstCaps * gst_queue2_getcaps (GstPad * pad) { GstQueue2 *queue; GstPad *otherpad; GstCaps *result; queue = GST_QUEUE2 (GST_PAD_PARENT (pad)); otherpad = (pad == queue->srcpad ? queue->sinkpad : queue->srcpad); result = gst_pad_peer_get_caps (otherpad); if (result == NULL) result = gst_caps_new_any (); return result; } static GstFlowReturn gst_queue2_bufferalloc (GstPad * pad, guint64 offset, guint size, GstCaps * caps, GstBuffer ** buf) { GstQueue2 *queue; GstFlowReturn result; queue = GST_QUEUE2 (GST_PAD_PARENT (pad)); /* Forward to src pad, without setting caps on the src pad */ result = gst_pad_alloc_buffer (queue->srcpad, offset, size, caps, buf); return result; } /* calculate the diff between running time on the sink and src of the queue. * This is the total amount of time in the queue. */ static void update_time_level (GstQueue2 * queue) { gint64 sink_time, src_time; sink_time = gst_segment_to_running_time (&queue->sink_segment, GST_FORMAT_TIME, queue->sink_segment.last_stop); src_time = gst_segment_to_running_time (&queue->src_segment, GST_FORMAT_TIME, queue->src_segment.last_stop); GST_DEBUG_OBJECT (queue, "sink %" GST_TIME_FORMAT ", src %" GST_TIME_FORMAT, GST_TIME_ARGS (sink_time), GST_TIME_ARGS (src_time)); if (sink_time >= src_time) queue->cur_level.time = sink_time - src_time; else queue->cur_level.time = 0; } /* take a NEWSEGMENT event and apply the values to segment, updating the time * level of queue. */ static void apply_segment (GstQueue2 * queue, GstEvent * event, GstSegment * segment) { gboolean update; GstFormat format; gdouble rate, arate; gint64 start, stop, time; gst_event_parse_new_segment_full (event, &update, &rate, &arate, &format, &start, &stop, &time); GST_DEBUG_OBJECT (queue, "received NEWSEGMENT update %d, rate %lf, applied rate %lf, " "format %d, " "%" G_GINT64_FORMAT " -- %" G_GINT64_FORMAT ", time %" G_GINT64_FORMAT, update, rate, arate, format, start, stop, time); if (format == GST_FORMAT_BYTES) { if (QUEUE_IS_USING_TEMP_FILE (queue)) { /* start is where we'll be getting from and as such writing next */ queue->current = add_range (queue, start); /* update the stats for this range */ update_cur_level (queue, queue->current); } } /* now configure the values, we use these to track timestamps on the * sinkpad. */ if (format != GST_FORMAT_TIME) { /* non-time format, pretent the current time segment is closed with a * 0 start and unknown stop time. */ update = FALSE; format = GST_FORMAT_TIME; start = 0; stop = -1; time = 0; } gst_segment_set_newsegment_full (segment, update, rate, arate, format, start, stop, time); GST_DEBUG_OBJECT (queue, "configured NEWSEGMENT %" GST_SEGMENT_FORMAT, segment); /* segment can update the time level of the queue */ update_time_level (queue); } /* take a buffer and update segment, updating the time level of the queue. */ static void apply_buffer (GstQueue2 * queue, GstBuffer * buffer, GstSegment * segment) { GstClockTime duration, timestamp; timestamp = GST_BUFFER_TIMESTAMP (buffer); duration = GST_BUFFER_DURATION (buffer); /* if no timestamp is set, assume it's continuous with the previous * time */ if (timestamp == GST_CLOCK_TIME_NONE) timestamp = segment->last_stop; /* add duration */ if (duration != GST_CLOCK_TIME_NONE) timestamp += duration; GST_DEBUG_OBJECT (queue, "last_stop updated to %" GST_TIME_FORMAT, GST_TIME_ARGS (timestamp)); gst_segment_set_last_stop (segment, GST_FORMAT_TIME, timestamp); /* calc diff with other end */ update_time_level (queue); } static void update_buffering (GstQueue2 * queue) { gint64 percent; gboolean post = FALSE; if (!queue->use_buffering || queue->high_percent <= 0) return; #define GET_PERCENT(format,alt_max) ((queue->max_level.format) > 0 ? (queue->cur_level.format) * 100 / ((alt_max) > 0 ? MIN ((alt_max), (queue->max_level.format)) : (queue->max_level.format)) : 0) if (queue->is_eos) { /* on EOS we are always 100% full, we set the var here so that it we can * reuse the logic below to stop buffering */ percent = 100; } else { /* figure out the percent we are filled, we take the max of all formats. */ if (!QUEUE_IS_USING_RING_BUFFER (queue)) { percent = GET_PERCENT (bytes, 0); } else { guint64 rb_size = queue->ring_buffer_max_size; percent = GET_PERCENT (bytes, rb_size); } percent = MAX (percent, GET_PERCENT (time, 0)); percent = MAX (percent, GET_PERCENT (buffers, 0)); /* also apply the rate estimate when we need to */ if (queue->use_rate_estimate) percent = MAX (percent, GET_PERCENT (rate_time, 0)); } if (queue->is_buffering) { post = TRUE; /* if we were buffering see if we reached the high watermark */ if (percent >= queue->high_percent) queue->is_buffering = FALSE; } else { /* we were not buffering, check if we need to start buffering if we drop * below the low threshold */ if (percent < queue->low_percent) { queue->is_buffering = TRUE; queue->buffering_iteration++; post = TRUE; } } if (post) { GstMessage *message; GstBufferingMode mode; gint64 buffering_left = -1; /* scale to high percent so that it becomes the 100% mark */ percent = percent * 100 / queue->high_percent; /* clip */ if (percent > 100) percent = 100; queue->buffering_percent = percent; if (!QUEUE_IS_USING_QUEUE (queue)) { GstFormat fmt = GST_FORMAT_BYTES; gint64 duration; if (QUEUE_IS_USING_RING_BUFFER (queue)) mode = GST_BUFFERING_TIMESHIFT; else mode = GST_BUFFERING_DOWNLOAD; if (queue->byte_in_rate > 0) { if (gst_pad_query_peer_duration (queue->sinkpad, &fmt, &duration)) buffering_left = (gdouble) ((duration - queue->current->writing_pos) * 1000) / queue->byte_in_rate; } else { buffering_left = G_MAXINT64; } } else { mode = GST_BUFFERING_STREAM; } GST_DEBUG_OBJECT (queue, "buffering %d percent", (gint) percent); message = gst_message_new_buffering (GST_OBJECT_CAST (queue), (gint) percent); gst_message_set_buffering_stats (message, mode, queue->byte_in_rate, queue->byte_out_rate, buffering_left); gst_element_post_message (GST_ELEMENT_CAST (queue), message); } else { GST_DEBUG_OBJECT (queue, "filled %d percent", (gint) percent); } #undef GET_PERCENT } static void reset_rate_timer (GstQueue2 * queue) { queue->bytes_in = 0; queue->bytes_out = 0; queue->byte_in_rate = 0.0; queue->byte_out_rate = 0.0; queue->last_in_elapsed = 0.0; queue->last_out_elapsed = 0.0; queue->in_timer_started = FALSE; queue->out_timer_started = FALSE; } /* the interval in seconds to recalculate the rate */ #define RATE_INTERVAL 0.2 /* Tuning for rate estimation. We use a large window for the input rate because * it should be stable when connected to a network. The output rate is less * stable (the elements preroll, queues behind a demuxer fill, ...) and should * therefore adapt more quickly. */ #define AVG_IN(avg,val) ((avg) * 15.0 + (val)) / 16.0 #define AVG_OUT(avg,val) ((avg) * 3.0 + (val)) / 4.0 static void update_in_rates (GstQueue2 * queue) { gdouble elapsed, period; gdouble byte_in_rate; if (!queue->in_timer_started) { queue->in_timer_started = TRUE; g_timer_start (queue->in_timer); return; } elapsed = g_timer_elapsed (queue->in_timer, NULL); /* recalc after each interval. */ if (queue->last_in_elapsed + RATE_INTERVAL < elapsed) { period = elapsed - queue->last_in_elapsed; GST_DEBUG_OBJECT (queue, "rates: period %f, in %" G_GUINT64_FORMAT, period, queue->bytes_in); byte_in_rate = queue->bytes_in / period; if (queue->byte_in_rate == 0.0) queue->byte_in_rate = byte_in_rate; else queue->byte_in_rate = AVG_IN (queue->byte_in_rate, byte_in_rate); /* reset the values to calculate rate over the next interval */ queue->last_in_elapsed = elapsed; queue->bytes_in = 0; } if (queue->byte_in_rate > 0.0) { queue->cur_level.rate_time = queue->cur_level.bytes / queue->byte_in_rate * GST_SECOND; } GST_DEBUG_OBJECT (queue, "rates: in %f, time %" GST_TIME_FORMAT, queue->byte_in_rate, GST_TIME_ARGS (queue->cur_level.rate_time)); } static void update_out_rates (GstQueue2 * queue) { gdouble elapsed, period; gdouble byte_out_rate; if (!queue->out_timer_started) { queue->out_timer_started = TRUE; g_timer_start (queue->out_timer); return; } elapsed = g_timer_elapsed (queue->out_timer, NULL); /* recalc after each interval. */ if (queue->last_out_elapsed + RATE_INTERVAL < elapsed) { period = elapsed - queue->last_out_elapsed; GST_DEBUG_OBJECT (queue, "rates: period %f, out %" G_GUINT64_FORMAT, period, queue->bytes_out); byte_out_rate = queue->bytes_out / period; if (queue->byte_out_rate == 0.0) queue->byte_out_rate = byte_out_rate; else queue->byte_out_rate = AVG_OUT (queue->byte_out_rate, byte_out_rate); /* reset the values to calculate rate over the next interval */ queue->last_out_elapsed = elapsed; queue->bytes_out = 0; } if (queue->byte_in_rate > 0.0) { queue->cur_level.rate_time = queue->cur_level.bytes / queue->byte_in_rate * GST_SECOND; } GST_DEBUG_OBJECT (queue, "rates: out %f, time %" GST_TIME_FORMAT, queue->byte_out_rate, GST_TIME_ARGS (queue->cur_level.rate_time)); } static void update_cur_pos (GstQueue2 * queue, GstQueue2Range * range, guint64 pos) { guint64 reading_pos, max_reading_pos; reading_pos = pos; max_reading_pos = range->max_reading_pos; max_reading_pos = MAX (max_reading_pos, reading_pos); GST_DEBUG_OBJECT (queue, "updating max_reading_pos to %" G_GUINT64_FORMAT " from %" G_GUINT64_FORMAT, max_reading_pos, range->max_reading_pos); range->max_reading_pos = max_reading_pos; update_cur_level (queue, range); } static gboolean perform_seek_to_offset (GstQueue2 * queue, guint64 offset) { GstEvent *event; gboolean res; GST_DEBUG_OBJECT (queue, "Seeking to %" G_GUINT64_FORMAT, offset); event = gst_event_new_seek (1.0, GST_FORMAT_BYTES, GST_SEEK_FLAG_FLUSH | GST_SEEK_FLAG_ACCURATE, GST_SEEK_TYPE_SET, offset, GST_SEEK_TYPE_NONE, -1); GST_QUEUE2_MUTEX_UNLOCK (queue); res = gst_pad_push_event (queue->sinkpad, event); GST_QUEUE2_MUTEX_LOCK (queue); if (res) queue->current = add_range (queue, offset); return res; } /* see if there is enough data in the file to read a full buffer */ static gboolean gst_queue2_have_data (GstQueue2 * queue, guint64 offset, guint length) { GstQueue2Range *range; GST_DEBUG_OBJECT (queue, "looking for offset %" G_GUINT64_FORMAT ", len %u", offset, length); if ((range = find_range (queue, offset, length))) { if (queue->current != range) { GST_DEBUG_OBJECT (queue, "switching ranges, do seek to range position"); perform_seek_to_offset (queue, range->writing_pos); } GST_INFO_OBJECT (queue, "cur_level.bytes %u (max %u)", queue->cur_level.bytes, QUEUE_MAX_BYTES (queue)); /* we have a range for offset */ GST_DEBUG_OBJECT (queue, "we have a range %p, offset %" G_GUINT64_FORMAT ", writing_pos %" G_GUINT64_FORMAT, range, range->offset, range->writing_pos); if (!QUEUE_IS_USING_RING_BUFFER (queue) && queue->is_eos) return TRUE; if (offset + length <= range->writing_pos) return TRUE; else GST_DEBUG_OBJECT (queue, "Need more data (%" G_GUINT64_FORMAT " bytes more)", (offset + length) - range->writing_pos); } else { GST_INFO_OBJECT (queue, "not found in any range"); /* we don't have the range, see how far away we are, FIXME, find a good * threshold based on the incomming rate. */ if (!queue->is_eos && queue->current) { if (QUEUE_IS_USING_RING_BUFFER (queue)) { if (offset < queue->current->offset || offset > queue->current->writing_pos + queue->max_level.bytes - queue->cur_level.bytes) { perform_seek_to_offset (queue, offset); } } else if (offset < queue->current->writing_pos + 200000) { update_cur_pos (queue, queue->current, offset + length); GST_INFO_OBJECT (queue, "wait for data"); } return FALSE; } /* too far away, do a seek */ perform_seek_to_offset (queue, offset); } return FALSE; } #ifdef HAVE_FSEEKO #define FSEEK_FILE(file,offset) (fseeko (file, (off_t) offset, SEEK_SET) != 0) #elif defined (G_OS_UNIX) || defined (G_OS_WIN32) #define FSEEK_FILE(file,offset) (lseek (fileno (file), (off_t) offset, SEEK_SET) == (off_t) -1) #else #define FSEEK_FILE(file,offset) (fseek (file, offset, SEEK_SET) != 0) #endif static gint64 gst_queue2_read_data_at_offset (GstQueue2 * queue, guint64 offset, guint length, guint8 * dst) { guint8 *ring_buffer; size_t res; ring_buffer = queue->ring_buffer; if (QUEUE_IS_USING_TEMP_FILE (queue) && FSEEK_FILE (queue->temp_file, offset)) goto seek_failed; /* this should not block */ GST_LOG_OBJECT (queue, "Reading %d bytes from offset %" G_GUINT64_FORMAT, length, offset); if (QUEUE_IS_USING_TEMP_FILE (queue)) { res = fread (dst, 1, length, queue->temp_file); } else { memcpy (dst, ring_buffer + offset, length); res = length; } GST_LOG_OBJECT (queue, "read %" G_GSIZE_FORMAT " bytes", res); if (G_UNLIKELY (res < length)) { if (!QUEUE_IS_USING_TEMP_FILE (queue)) goto could_not_read; /* check for errors or EOF */ if (ferror (queue->temp_file)) goto could_not_read; if (feof (queue->temp_file) && length > 0) goto eos; } return res; seek_failed: { GST_ELEMENT_ERROR (queue, RESOURCE, SEEK, (NULL), GST_ERROR_SYSTEM); return GST_FLOW_ERROR; } could_not_read: { GST_ELEMENT_ERROR (queue, RESOURCE, READ, (NULL), GST_ERROR_SYSTEM); return GST_FLOW_ERROR; } eos: { GST_DEBUG ("non-regular file hits EOS"); return GST_FLOW_UNEXPECTED; } } static GstFlowReturn gst_queue2_create_read (GstQueue2 * queue, guint64 offset, guint length, GstBuffer ** buffer) { GstBuffer *buf; guint8 *data; guint64 file_offset; guint block_length, remaining, read_length; gint64 read_return; guint64 rb_size; guint64 rpos; /* allocate the output buffer of the requested size */ buf = gst_buffer_new_and_alloc (length); data = GST_BUFFER_DATA (buf); GST_DEBUG_OBJECT (queue, "Reading %u bytes from %" G_GUINT64_FORMAT, length, offset); rpos = offset; rb_size = queue->ring_buffer_max_size; remaining = length; while (remaining > 0) { /* configure how much/whether to read */ if (!gst_queue2_have_data (queue, rpos, remaining)) { read_length = 0; queue->current->reading_pos = rpos; if (QUEUE_IS_USING_RING_BUFFER (queue)) { guint64 level; /* calculate how far away the offset is */ if (queue->current->writing_pos > rpos) level = queue->current->writing_pos - rpos; else level = 0; GST_DEBUG_OBJECT (queue, "reading %" G_GUINT64_FORMAT ", writing %" G_GUINT64_FORMAT ", level %" G_GUINT64_FORMAT, queue->current->reading_pos, queue->current->writing_pos, level); if (level >= rb_size) { /* we don't have the data but if we have a ring buffer that is full, we * need to read */ GST_DEBUG_OBJECT (queue, "ring buffer full, reading ring-buffer-max-size %d bytes", rb_size); read_length = rb_size; } } if (read_length == 0) { if (QUEUE_IS_USING_RING_BUFFER (queue)) { /* protect cached data (data between offset and max_reading_pos) * and update current level */ GST_DEBUG_OBJECT (queue, "protecting cached data [%" G_GUINT64_FORMAT "-%" G_GUINT64_FORMAT "]", rpos, queue->current->max_reading_pos); queue->current->max_reading_pos = rpos; update_cur_level (queue, queue->current); } GST_QUEUE2_WAIT_ADD_CHECK (queue, queue->srcresult, out_flushing); continue; } } else { /* we have the requested data so read it */ read_length = remaining; } /* congfigure how much and from where to read */ if (QUEUE_IS_USING_RING_BUFFER (queue)) { file_offset = (queue->current->rb_offset + (rpos - queue->current->offset)) % rb_size; if (file_offset + read_length > rb_size) { block_length = rb_size - file_offset; } else { block_length = read_length; } } else { file_offset = rpos; block_length = read_length; } /* while we still have data to read, we loop */ while (read_length > 0) { read_return = gst_queue2_read_data_at_offset (queue, file_offset, block_length, data); if (read_return < 0) goto read_error; file_offset += read_return; if (QUEUE_IS_USING_RING_BUFFER (queue)) file_offset %= rb_size; data += read_return; read_length -= read_return; block_length = read_length; remaining -= read_return; rpos = (queue->current->reading_pos += read_return); update_cur_pos (queue, queue->current, queue->current->reading_pos); } GST_QUEUE2_SIGNAL_DEL (queue); GST_DEBUG_OBJECT (queue, "%u bytes left to read", remaining); } GST_BUFFER_SIZE (buf) = length; GST_BUFFER_OFFSET (buf) = offset; GST_BUFFER_OFFSET_END (buf) = offset + length; *buffer = buf; return GST_FLOW_OK; /* ERRORS */ out_flushing: { GST_DEBUG_OBJECT (queue, "we are flushing"); return GST_FLOW_WRONG_STATE; } read_error: { GST_DEBUG_OBJECT (queue, "we have a read error"); gst_buffer_unref (buf); return read_return; } } /* should be called with QUEUE_LOCK */ static GstMiniObject * gst_queue2_read_item_from_file (GstQueue2 * queue) { GstMiniObject *item; if (queue->starting_segment != NULL) { item = GST_MINI_OBJECT_CAST (queue->starting_segment); queue->starting_segment = NULL; } else { GstFlowReturn ret; GstBuffer *buffer; guint64 reading_pos; reading_pos = queue->current->reading_pos; ret = gst_queue2_create_read (queue, reading_pos, DEFAULT_BUFFER_SIZE, &buffer); switch (ret) { case GST_FLOW_OK: item = GST_MINI_OBJECT_CAST (buffer); break; case GST_FLOW_UNEXPECTED: item = GST_MINI_OBJECT_CAST (gst_event_new_eos ()); break; default: item = NULL; break; } } return item; } static gboolean gst_queue2_open_temp_location_file (GstQueue2 * queue) { gint fd = -1; gchar *name = NULL; if (queue->temp_file) goto already_opened; GST_DEBUG_OBJECT (queue, "opening temp file %s", queue->temp_template); /* we have two cases: * - temp_location was set to something !NULL (Deprecated). in this case we * open the specified filename. * - temp_template was set, allocate a filename and open that filename */ if (!queue->temp_location_set) { /* nothing to do */ if (queue->temp_template == NULL) goto no_directory; /* make copy of the template, we don't want to change this */ name = g_strdup (queue->temp_template); fd = g_mkstemp (name); if (fd == -1) goto mkstemp_failed; /* open the file for update/writing */ queue->temp_file = fdopen (fd, "wb+"); /* error creating file */ if (queue->temp_file == NULL) goto open_failed; g_free (queue->temp_location); queue->temp_location = name; g_object_notify (G_OBJECT (queue), "temp-location"); } else { /* open the file for update/writing, this is deprecated but we still need to * support it for API/ABI compatibility */ queue->temp_file = g_fopen (queue->temp_location, "wb+"); /* error creating file */ if (queue->temp_file == NULL) goto open_failed; } GST_DEBUG_OBJECT (queue, "opened temp file %s", queue->temp_template); return TRUE; /* ERRORS */ already_opened: { GST_DEBUG_OBJECT (queue, "temp file was already open"); return TRUE; } no_directory: { GST_ELEMENT_ERROR (queue, RESOURCE, NOT_FOUND, (_("No Temp directory specified.")), (NULL)); return FALSE; } mkstemp_failed: { GST_ELEMENT_ERROR (queue, RESOURCE, OPEN_READ, (_("Could not create temp file \"%s\"."), queue->temp_template), GST_ERROR_SYSTEM); g_free (name); return FALSE; } open_failed: { GST_ELEMENT_ERROR (queue, RESOURCE, OPEN_READ, (_("Could not open file \"%s\" for reading."), name), GST_ERROR_SYSTEM); g_free (name); if (fd != -1) close (fd); return FALSE; } } static void gst_queue2_close_temp_location_file (GstQueue2 * queue) { /* nothing to do */ if (queue->temp_file == NULL) return; GST_DEBUG_OBJECT (queue, "closing temp file"); fflush (queue->temp_file); fclose (queue->temp_file); if (queue->temp_remove) remove (queue->temp_location); queue->temp_file = NULL; clean_ranges (queue); } static void gst_queue2_flush_temp_file (GstQueue2 * queue) { if (queue->temp_file == NULL) return; GST_DEBUG_OBJECT (queue, "flushing temp file"); queue->temp_file = g_freopen (queue->temp_location, "wb+", queue->temp_file); } static void gst_queue2_locked_flush (GstQueue2 * queue) { if (!QUEUE_IS_USING_QUEUE (queue)) { if (QUEUE_IS_USING_TEMP_FILE (queue)) gst_queue2_flush_temp_file (queue); init_ranges (queue); } else { while (!g_queue_is_empty (queue->queue)) { GstMiniObject *data = g_queue_pop_head (queue->queue); /* Then lose another reference because we are supposed to destroy that data when flushing */ gst_mini_object_unref (data); } } GST_QUEUE2_CLEAR_LEVEL (queue->cur_level); gst_segment_init (&queue->sink_segment, GST_FORMAT_TIME); gst_segment_init (&queue->src_segment, GST_FORMAT_TIME); if (queue->starting_segment != NULL) gst_event_unref (queue->starting_segment); queue->starting_segment = NULL; queue->segment_event_received = FALSE; /* we deleted a lot of something */ GST_QUEUE2_SIGNAL_DEL (queue); } static gboolean gst_queue2_wait_free_space (GstQueue2 * queue) { /* We make space available if we're "full" according to whatever * the user defined as "full". */ if (gst_queue2_is_filled (queue)) { gboolean started; /* pause the timer while we wait. The fact that we are waiting does not mean * the byterate on the input pad is lower */ if ((started = queue->in_timer_started)) g_timer_stop (queue->in_timer); GST_CAT_DEBUG_OBJECT (queue_dataflow, queue, "queue is full, waiting for free space"); do { /* Wait for space to be available, we could be unlocked because of a flush. */ GST_QUEUE2_WAIT_DEL_CHECK (queue, queue->sinkresult, out_flushing); } while (gst_queue2_is_filled (queue)); /* and continue if we were running before */ if (started) g_timer_continue (queue->in_timer); } return TRUE; /* ERRORS */ out_flushing: { GST_CAT_DEBUG_OBJECT (queue_dataflow, queue, "queue is flushing"); return FALSE; } } static gboolean gst_queue2_create_write (GstQueue2 * queue, GstBuffer * buffer) { guint8 *data, *ring_buffer; guint size, rb_size; guint64 writing_pos, new_writing_pos, max_reading_pos; gint64 space; GstQueue2Range *range, *prev, *next; if (QUEUE_IS_USING_RING_BUFFER (queue)) writing_pos = queue->current->rb_writing_pos; else writing_pos = queue->current->writing_pos; max_reading_pos = queue->current->max_reading_pos; ring_buffer = queue->ring_buffer; rb_size = queue->ring_buffer_max_size; size = GST_BUFFER_SIZE (buffer); data = GST_BUFFER_DATA (buffer); while (size > 0) { guint to_write; if (QUEUE_IS_USING_RING_BUFFER (queue)) { /* calculate the space in the ring buffer not used by data from * the current range */ while (QUEUE_MAX_BYTES (queue) <= queue->cur_level.bytes) { /* wait until there is some free space */ GST_QUEUE2_WAIT_DEL_CHECK (queue, queue->sinkresult, out_flushing); } /* get the amount of space we have */ space = QUEUE_MAX_BYTES (queue) - queue->cur_level.bytes; /* calculate if we need to split or if we can write the entire * buffer now */ to_write = MIN (size, space); /* the writing position in the ring buffer after writing (part * or all of) the buffer */ new_writing_pos = (writing_pos + to_write) % rb_size; prev = NULL; range = queue->ranges; /* if we need to overwrite data in the ring buffer, we need to * update the ranges * * warning: this code is complicated and includes some * simplifications - pen, paper and diagrams for the cases * recommended! */ while (range) { guint64 range_data_start, range_data_end; GstQueue2Range *range_to_destroy = NULL; /* we don't edit the current range here */ if (range == queue->current) goto next_range; range_data_start = range->rb_offset; range_data_end = range->rb_writing_pos; if (range_data_end > range_data_start) { if (writing_pos >= range_data_end && new_writing_pos >= writing_pos) goto next_range; if (new_writing_pos > range_data_start) { if (new_writing_pos >= range_data_end) { GST_DEBUG_OBJECT (queue, "Removing range: offset %" G_GUINT64_FORMAT ", wpos %" G_GUINT64_FORMAT, range->offset, range->writing_pos); /* remove range */ range_to_destroy = range; if (prev) prev->next = range->next; } else { GST_DEBUG_OBJECT (queue, "advancing offsets from %" G_GUINT64_FORMAT " (%" G_GUINT64_FORMAT ") to %" G_GUINT64_FORMAT " (%" G_GUINT64_FORMAT ")", range->offset, range->rb_offset, range->offset + new_writing_pos - range_data_start, new_writing_pos); range->offset += (new_writing_pos - range_data_start); range->rb_offset = new_writing_pos; } } } else { guint64 new_wpos_virt = writing_pos + to_write; if (new_wpos_virt <= range_data_start) goto next_range; if (new_wpos_virt > rb_size && new_writing_pos >= range_data_end) { GST_DEBUG_OBJECT (queue, "Removing range: offset %" G_GUINT64_FORMAT ", wpos %" G_GUINT64_FORMAT, range->offset, range->writing_pos); /* remove range */ range_to_destroy = range; if (prev) prev->next = range->next; } else { GST_DEBUG_OBJECT (queue, "advancing offsets from %" G_GUINT64_FORMAT " (%" G_GUINT64_FORMAT ") to %" G_GUINT64_FORMAT " (%" G_GUINT64_FORMAT ")", range->offset, range->rb_offset, range->offset + new_writing_pos - range_data_start, new_writing_pos); range->offset += (new_wpos_virt - range_data_start); range->rb_offset = new_writing_pos; } } next_range: if (!range_to_destroy) prev = range; range = range->next; if (range_to_destroy) { if (range_to_destroy == queue->ranges) queue->ranges = range; g_slice_free (GstQueue2Range, range_to_destroy); range_to_destroy = NULL; } } } else { space = to_write = size; new_writing_pos = writing_pos + to_write; } if (QUEUE_IS_USING_TEMP_FILE (queue) && FSEEK_FILE (queue->temp_file, writing_pos)) goto seek_failed; if (new_writing_pos > writing_pos) { GST_INFO_OBJECT (queue, "writing %u bytes", to_write); /* either not using ring buffer or no wrapping, just write */ if (QUEUE_IS_USING_TEMP_FILE (queue)) { if (fwrite (data, to_write, 1, queue->temp_file) != 1) goto handle_error; } else { memcpy (ring_buffer + writing_pos, data, to_write); } if (!QUEUE_IS_USING_RING_BUFFER (queue)) { /* try to merge with next range */ while ((next = queue->current->next)) { GST_INFO_OBJECT (queue, "checking merge with next range %" G_GUINT64_FORMAT " < %" G_GUINT64_FORMAT, new_writing_pos, next->offset); if (new_writing_pos < next->offset) break; GST_DEBUG_OBJECT (queue, "merging ranges %" G_GUINT64_FORMAT, next->writing_pos); /* remove the group, we could choose to not read the data in this range * again. This would involve us doing a seek to the current writing position * in the range. FIXME, It would probably make sense to do a seek when there * is a lot of data in the range we merged with to avoid reading it all * again. */ queue->current->next = next->next; g_slice_free (GstQueue2Range, next); debug_ranges (queue); } goto update_and_signal; } } else { /* wrapping */ guint block_one, block_two; block_one = rb_size - writing_pos; block_two = to_write - block_one; if (block_one > 0) { GST_INFO_OBJECT (queue, "writing %u bytes", block_one); /* write data to end of ring buffer */ if (QUEUE_IS_USING_TEMP_FILE (queue)) { if (fwrite (data, block_one, 1, queue->temp_file) != 1) goto handle_error; } else { memcpy (ring_buffer + writing_pos, data, block_one); } } if (QUEUE_IS_USING_TEMP_FILE (queue) && FSEEK_FILE (queue->temp_file, 0)) goto seek_failed; if (block_two > 0) { GST_INFO_OBJECT (queue, "writing %u bytes", block_two); if (QUEUE_IS_USING_TEMP_FILE (queue)) { if (fwrite (data + block_one, block_two, 1, queue->temp_file) != 1) goto handle_error; } else { memcpy (ring_buffer, data + block_one, block_two); } } } update_and_signal: /* update the writing positions */ size -= to_write; GST_INFO_OBJECT (queue, "wrote %u bytes to %" G_GUINT64_FORMAT " (%u bytes remaining to write)", to_write, writing_pos, size); if (QUEUE_IS_USING_RING_BUFFER (queue)) { data += to_write; queue->current->writing_pos += to_write; queue->current->rb_writing_pos = writing_pos = new_writing_pos; } else { queue->current->writing_pos = writing_pos = new_writing_pos; } update_cur_level (queue, queue->current); /* update the buffering status */ update_buffering (queue); GST_INFO_OBJECT (queue, "cur_level.bytes %u (max %u)", queue->cur_level.bytes, QUEUE_MAX_BYTES (queue)); GST_QUEUE2_SIGNAL_ADD (queue); }; return TRUE; /* ERRORS */ out_flushing: { GST_DEBUG_OBJECT (queue, "we are flushing"); /* FIXME - GST_FLOW_UNEXPECTED ? */ return FALSE; } seek_failed: { GST_ELEMENT_ERROR (queue, RESOURCE, SEEK, (NULL), GST_ERROR_SYSTEM); return FALSE; } handle_error: { switch (errno) { case ENOSPC:{ GST_ELEMENT_ERROR (queue, RESOURCE, NO_SPACE_LEFT, (NULL), (NULL)); break; } default:{ GST_ELEMENT_ERROR (queue, RESOURCE, WRITE, (_("Error while writing to download file.")), ("%s", g_strerror (errno))); } } return FALSE; } } /* enqueue an item an update the level stats */ static void gst_queue2_locked_enqueue (GstQueue2 * queue, gpointer item) { if (GST_IS_BUFFER (item)) { GstBuffer *buffer; guint size; buffer = GST_BUFFER_CAST (item); size = GST_BUFFER_SIZE (buffer); /* add buffer to the statistics */ if (QUEUE_IS_USING_QUEUE (queue)) { queue->cur_level.buffers++; queue->cur_level.bytes += size; } queue->bytes_in += size; /* apply new buffer to segment stats */ apply_buffer (queue, buffer, &queue->sink_segment); /* update the byterate stats */ update_in_rates (queue); if (!QUEUE_IS_USING_QUEUE (queue)) { /* FIXME - check return value? */ gst_queue2_create_write (queue, buffer); } } else if (GST_IS_EVENT (item)) { GstEvent *event; event = GST_EVENT_CAST (item); switch (GST_EVENT_TYPE (event)) { case GST_EVENT_EOS: /* Zero the thresholds, this makes sure the queue is completely * filled and we can read all data from the queue. */ GST_DEBUG_OBJECT (queue, "we have EOS"); queue->is_eos = TRUE; break; case GST_EVENT_NEWSEGMENT: apply_segment (queue, event, &queue->sink_segment); /* This is our first new segment, we hold it * as we can't save it on the temp file */ if (!QUEUE_IS_USING_QUEUE (queue)) { if (queue->segment_event_received) goto unexpected_event; queue->segment_event_received = TRUE; if (queue->starting_segment != NULL) gst_event_unref (queue->starting_segment); queue->starting_segment = event; item = NULL; } /* a new segment allows us to accept more buffers if we got UNEXPECTED * from downstream */ queue->unexpected = FALSE; break; default: if (!QUEUE_IS_USING_QUEUE (queue)) goto unexpected_event; break; } } else { g_warning ("Unexpected item %p added in queue %s (refcounting problem?)", item, GST_OBJECT_NAME (queue)); /* we can't really unref since we don't know what it is */ item = NULL; } if (item) { if (QUEUE_IS_USING_QUEUE (queue)) { /* update the buffering status */ update_buffering (queue); g_queue_push_tail (queue->queue, item); } else { gst_mini_object_unref (GST_MINI_OBJECT_CAST (item)); } if (!QUEUE_IS_USING_RING_BUFFER (queue)) GST_QUEUE2_SIGNAL_ADD (queue); } return; /* ERRORS */ unexpected_event: { g_warning ("Unexpected event of kind %s can't be added in temp file of queue %s ", gst_event_type_get_name (GST_EVENT_TYPE (item)), GST_OBJECT_NAME (queue)); gst_event_unref (GST_EVENT_CAST (item)); return; } } /* dequeue an item from the queue and update level stats */ static GstMiniObject * gst_queue2_locked_dequeue (GstQueue2 * queue) { GstMiniObject *item; if (!QUEUE_IS_USING_QUEUE (queue)) item = gst_queue2_read_item_from_file (queue); else item = g_queue_pop_head (queue->queue); if (item == NULL) goto no_item; if (GST_IS_BUFFER (item)) { GstBuffer *buffer; guint size; buffer = GST_BUFFER_CAST (item); size = GST_BUFFER_SIZE (buffer); GST_CAT_LOG_OBJECT (queue_dataflow, queue, "retrieved buffer %p from queue", buffer); if (QUEUE_IS_USING_QUEUE (queue)) { queue->cur_level.buffers--; queue->cur_level.bytes -= size; } queue->bytes_out += size; apply_buffer (queue, buffer, &queue->src_segment); /* update the byterate stats */ update_out_rates (queue); /* update the buffering */ update_buffering (queue); } else if (GST_IS_EVENT (item)) { GstEvent *event = GST_EVENT_CAST (item); GST_CAT_LOG_OBJECT (queue_dataflow, queue, "retrieved event %p from queue", event); switch (GST_EVENT_TYPE (event)) { case GST_EVENT_EOS: /* queue is empty now that we dequeued the EOS */ GST_QUEUE2_CLEAR_LEVEL (queue->cur_level); break; case GST_EVENT_NEWSEGMENT: apply_segment (queue, event, &queue->src_segment); break; default: break; } } else { g_warning ("Unexpected item %p dequeued from queue %s (refcounting problem?)", item, GST_OBJECT_NAME (queue)); item = NULL; } GST_QUEUE2_SIGNAL_DEL (queue); return item; /* ERRORS */ no_item: { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "the queue is empty"); return NULL; } } static gboolean gst_queue2_handle_sink_event (GstPad * pad, GstEvent * event) { GstQueue2 *queue; queue = GST_QUEUE2 (GST_OBJECT_PARENT (pad)); switch (GST_EVENT_TYPE (event)) { case GST_EVENT_FLUSH_START: { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "received flush start event"); if (QUEUE_IS_USING_QUEUE (queue)) { /* forward event */ gst_pad_push_event (queue->srcpad, event); /* now unblock the chain function */ GST_QUEUE2_MUTEX_LOCK (queue); queue->srcresult = GST_FLOW_WRONG_STATE; queue->sinkresult = GST_FLOW_WRONG_STATE; /* unblock the loop and chain functions */ GST_QUEUE2_SIGNAL_ADD (queue); GST_QUEUE2_SIGNAL_DEL (queue); GST_QUEUE2_MUTEX_UNLOCK (queue); /* make sure it pauses, this should happen since we sent * flush_start downstream. */ gst_pad_pause_task (queue->srcpad); GST_CAT_LOG_OBJECT (queue_dataflow, queue, "loop stopped"); } else { GST_QUEUE2_MUTEX_LOCK (queue); /* flush the sink pad */ queue->sinkresult = GST_FLOW_WRONG_STATE; GST_QUEUE2_SIGNAL_DEL (queue); GST_QUEUE2_MUTEX_UNLOCK (queue); gst_event_unref (event); } goto done; } case GST_EVENT_FLUSH_STOP: { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "received flush stop event"); if (QUEUE_IS_USING_QUEUE (queue)) { /* forward event */ gst_pad_push_event (queue->srcpad, event); GST_QUEUE2_MUTEX_LOCK (queue); gst_queue2_locked_flush (queue); queue->srcresult = GST_FLOW_OK; queue->sinkresult = GST_FLOW_OK; queue->is_eos = FALSE; queue->unexpected = FALSE; /* reset rate counters */ reset_rate_timer (queue); gst_pad_start_task (queue->srcpad, (GstTaskFunction) gst_queue2_loop, queue->srcpad); GST_QUEUE2_MUTEX_UNLOCK (queue); } else { GST_QUEUE2_MUTEX_LOCK (queue); queue->segment_event_received = FALSE; queue->is_eos = FALSE; queue->unexpected = FALSE; queue->sinkresult = GST_FLOW_OK; GST_QUEUE2_MUTEX_UNLOCK (queue); gst_event_unref (event); } goto done; } default: if (GST_EVENT_IS_SERIALIZED (event)) { /* serialized events go in the queue */ GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->sinkresult, out_flushing); /* refuse more events on EOS */ if (queue->is_eos) goto out_eos; gst_queue2_locked_enqueue (queue, event); GST_QUEUE2_MUTEX_UNLOCK (queue); } else { /* non-serialized events are passed upstream. */ gst_pad_push_event (queue->srcpad, event); } break; } done: return TRUE; /* ERRORS */ out_flushing: { GST_DEBUG_OBJECT (queue, "refusing event, we are flushing"); GST_QUEUE2_MUTEX_UNLOCK (queue); gst_event_unref (event); return FALSE; } out_eos: { GST_DEBUG_OBJECT (queue, "refusing event, we are EOS"); GST_QUEUE2_MUTEX_UNLOCK (queue); gst_event_unref (event); return FALSE; } } static gboolean gst_queue2_is_empty (GstQueue2 * queue) { /* never empty on EOS */ if (queue->is_eos) return FALSE; if (!QUEUE_IS_USING_QUEUE (queue) && queue->current) { return queue->current->writing_pos <= queue->current->max_reading_pos; } else { if (queue->queue->length == 0) return TRUE; } return FALSE; } static gboolean gst_queue2_is_filled (GstQueue2 * queue) { gboolean res; /* always filled on EOS */ if (queue->is_eos) return TRUE; #define CHECK_FILLED(format,alt_max) ((queue->max_level.format) > 0 && \ (queue->cur_level.format) >= ((alt_max) ? \ MIN ((queue->max_level.format), (alt_max)) : (queue->max_level.format))) /* if using a ring buffer we're filled if all ring buffer space is used * _by the current range_ */ if (QUEUE_IS_USING_RING_BUFFER (queue)) { guint max_bytes = queue->max_level.bytes; guint64 rb_size = queue->ring_buffer_max_size; GST_DEBUG_OBJECT (queue, "max bytes %u, rb size %" G_GUINT64_FORMAT ", cur bytes %u", max_bytes, rb_size, queue->cur_level.bytes); return CHECK_FILLED (bytes, rb_size); } /* if using file, we're never filled if we don't have EOS */ if (QUEUE_IS_USING_TEMP_FILE (queue)) return FALSE; /* we are never filled when we have no buffers at all */ if (queue->cur_level.buffers == 0) return FALSE; /* we are filled if one of the current levels exceeds the max */ res = CHECK_FILLED (buffers, 0) || CHECK_FILLED (bytes, 0) || CHECK_FILLED (time, 0); /* if we need to, use the rate estimate to check against the max time we are * allowed to queue */ if (queue->use_rate_estimate) res |= CHECK_FILLED (rate_time, 0); #undef CHECK_FILLED return res; } static GstFlowReturn gst_queue2_chain (GstPad * pad, GstBuffer * buffer) { GstQueue2 *queue; queue = GST_QUEUE2 (GST_OBJECT_PARENT (pad)); GST_CAT_LOG_OBJECT (queue_dataflow, queue, "received buffer %p of size %d, time %" GST_TIME_FORMAT ", duration %" GST_TIME_FORMAT, buffer, GST_BUFFER_SIZE (buffer), GST_TIME_ARGS (GST_BUFFER_TIMESTAMP (buffer)), GST_TIME_ARGS (GST_BUFFER_DURATION (buffer))); /* we have to lock the queue since we span threads */ GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->sinkresult, out_flushing); /* when we received EOS, we refuse more data */ if (queue->is_eos) goto out_eos; /* when we received unexpected from downstream, refuse more buffers */ if (queue->unexpected) goto out_unexpected; if (!gst_queue2_wait_free_space (queue)) goto out_flushing; /* put buffer in queue now */ gst_queue2_locked_enqueue (queue, buffer); GST_QUEUE2_MUTEX_UNLOCK (queue); return GST_FLOW_OK; /* special conditions */ out_flushing: { GstFlowReturn ret = queue->sinkresult; GST_CAT_LOG_OBJECT (queue_dataflow, queue, "exit because task paused, reason: %s", gst_flow_get_name (ret)); GST_QUEUE2_MUTEX_UNLOCK (queue); gst_buffer_unref (buffer); return ret; } out_eos: { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "exit because we received EOS"); GST_QUEUE2_MUTEX_UNLOCK (queue); gst_buffer_unref (buffer); return GST_FLOW_UNEXPECTED; } out_unexpected: { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "exit because we received UNEXPECTED"); GST_QUEUE2_MUTEX_UNLOCK (queue); gst_buffer_unref (buffer); return GST_FLOW_UNEXPECTED; } } /* dequeue an item from the queue an push it downstream. This functions returns * the result of the push. */ static GstFlowReturn gst_queue2_push_one (GstQueue2 * queue) { GstFlowReturn result = GST_FLOW_OK; GstMiniObject *data; data = gst_queue2_locked_dequeue (queue); if (data == NULL) goto no_item; next: if (GST_IS_BUFFER (data)) { GstBuffer *buffer; GstCaps *caps; buffer = GST_BUFFER_CAST (data); caps = GST_BUFFER_CAPS (buffer); GST_QUEUE2_MUTEX_UNLOCK (queue); /* set caps before pushing the buffer so that core does not try to do * something fancy to check if this is possible. */ if (caps && caps != GST_PAD_CAPS (queue->srcpad)) gst_pad_set_caps (queue->srcpad, caps); result = gst_pad_push (queue->srcpad, buffer); /* need to check for srcresult here as well */ GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing); if (result == GST_FLOW_UNEXPECTED) { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "got UNEXPECTED from downstream"); /* stop pushing buffers, we dequeue all items until we see an item that we * can push again, which is EOS or NEWSEGMENT. If there is nothing in the * queue we can push, we set a flag to make the sinkpad refuse more * buffers with an UNEXPECTED return value until we receive something * pushable again or we get flushed. */ while ((data = gst_queue2_locked_dequeue (queue))) { if (GST_IS_BUFFER (data)) { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "dropping UNEXPECTED buffer %p", data); gst_buffer_unref (GST_BUFFER_CAST (data)); } else if (GST_IS_EVENT (data)) { GstEvent *event = GST_EVENT_CAST (data); GstEventType type = GST_EVENT_TYPE (event); if (type == GST_EVENT_EOS || type == GST_EVENT_NEWSEGMENT) { /* we found a pushable item in the queue, push it out */ GST_CAT_LOG_OBJECT (queue_dataflow, queue, "pushing pushable event %s after UNEXPECTED", GST_EVENT_TYPE_NAME (event)); goto next; } GST_CAT_LOG_OBJECT (queue_dataflow, queue, "dropping UNEXPECTED event %p", event); gst_event_unref (event); } } /* no more items in the queue. Set the unexpected flag so that upstream * make us refuse any more buffers on the sinkpad. Since we will still * accept EOS and NEWSEGMENT we return _FLOW_OK to the caller so that the * task function does not shut down. */ queue->unexpected = TRUE; result = GST_FLOW_OK; } } else if (GST_IS_EVENT (data)) { GstEvent *event = GST_EVENT_CAST (data); GstEventType type = GST_EVENT_TYPE (event); GST_QUEUE2_MUTEX_UNLOCK (queue); gst_pad_push_event (queue->srcpad, event); GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing); /* if we're EOS, return UNEXPECTED so that the task pauses. */ if (type == GST_EVENT_EOS) { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "pushed EOS event %p, return UNEXPECTED", event); result = GST_FLOW_UNEXPECTED; } } return result; /* ERRORS */ no_item: { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "exit because we have no item in the queue"); return GST_FLOW_ERROR; } out_flushing: { GST_CAT_LOG_OBJECT (queue_dataflow, queue, "exit because we are flushing"); return GST_FLOW_WRONG_STATE; } } /* called repeadedly with @pad as the source pad. This function should push out * data to the peer element. */ static void gst_queue2_loop (GstPad * pad) { GstQueue2 *queue; GstFlowReturn ret; queue = GST_QUEUE2 (GST_PAD_PARENT (pad)); /* have to lock for thread-safety */ GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing); if (gst_queue2_is_empty (queue)) { gboolean started; /* pause the timer while we wait. The fact that we are waiting does not mean * the byterate on the output pad is lower */ if ((started = queue->out_timer_started)) g_timer_stop (queue->out_timer); GST_CAT_DEBUG_OBJECT (queue_dataflow, queue, "queue is empty, waiting for new data"); do { /* Wait for data to be available, we could be unlocked because of a flush. */ GST_QUEUE2_WAIT_ADD_CHECK (queue, queue->srcresult, out_flushing); } while (gst_queue2_is_empty (queue)); /* and continue if we were running before */ if (started) g_timer_continue (queue->out_timer); } ret = gst_queue2_push_one (queue); queue->srcresult = ret; queue->sinkresult = ret; if (ret != GST_FLOW_OK) goto out_flushing; GST_QUEUE2_MUTEX_UNLOCK (queue); return; /* ERRORS */ out_flushing: { gboolean eos = queue->is_eos; GstFlowReturn ret = queue->srcresult; gst_pad_pause_task (queue->srcpad); GST_CAT_LOG_OBJECT (queue_dataflow, queue, "pause task, reason: %s", gst_flow_get_name (queue->srcresult)); GST_QUEUE2_MUTEX_UNLOCK (queue); /* let app know about us giving up if upstream is not expected to do so */ /* UNEXPECTED is already taken care of elsewhere */ if (eos && (GST_FLOW_IS_FATAL (ret) || ret == GST_FLOW_NOT_LINKED) && (ret != GST_FLOW_UNEXPECTED)) { GST_ELEMENT_ERROR (queue, STREAM, FAILED, (_("Internal data flow error.")), ("streaming task paused, reason %s (%d)", gst_flow_get_name (ret), ret)); gst_pad_push_event (queue->srcpad, gst_event_new_eos ()); } return; } } static gboolean gst_queue2_handle_src_event (GstPad * pad, GstEvent * event) { gboolean res = TRUE; GstQueue2 *queue = GST_QUEUE2 (GST_PAD_PARENT (pad)); #ifndef GST_DISABLE_GST_DEBUG GST_CAT_DEBUG_OBJECT (queue_dataflow, queue, "got event %p (%s)", event, GST_EVENT_TYPE_NAME (event)); #endif switch (GST_EVENT_TYPE (event)) { case GST_EVENT_FLUSH_START: if (QUEUE_IS_USING_QUEUE (queue)) { /* just forward upstream */ res = gst_pad_push_event (queue->sinkpad, event); } else { /* now unblock the getrange function */ GST_QUEUE2_MUTEX_LOCK (queue); GST_DEBUG_OBJECT (queue, "flushing"); queue->srcresult = GST_FLOW_WRONG_STATE; GST_QUEUE2_SIGNAL_ADD (queue); GST_QUEUE2_MUTEX_UNLOCK (queue); /* when using a temp file, we eat the event */ res = TRUE; gst_event_unref (event); } break; case GST_EVENT_FLUSH_STOP: if (QUEUE_IS_USING_QUEUE (queue)) { /* just forward upstream */ res = gst_pad_push_event (queue->sinkpad, event); } else { /* now unblock the getrange function */ GST_QUEUE2_MUTEX_LOCK (queue); queue->srcresult = GST_FLOW_OK; if (queue->current) { /* forget the highest read offset, we'll calculate a new one when we * get the next getrange request. We need to do this in order to reset * the buffering percentage */ queue->current->max_reading_pos = 0; } GST_QUEUE2_MUTEX_UNLOCK (queue); /* when using a temp file, we eat the event */ res = TRUE; gst_event_unref (event); } break; default: res = gst_pad_push_event (queue->sinkpad, event); break; } return res; } static gboolean gst_queue2_peer_query (GstQueue2 * queue, GstPad * pad, GstQuery * query) { gboolean ret = FALSE; GstPad *peer; if ((peer = gst_pad_get_peer (pad))) { ret = gst_pad_query (peer, query); gst_object_unref (peer); } return ret; } static gboolean gst_queue2_handle_src_query (GstPad * pad, GstQuery * query) { GstQueue2 *queue; queue = GST_QUEUE2 (GST_PAD_PARENT (pad)); switch (GST_QUERY_TYPE (query)) { case GST_QUERY_POSITION: { gint64 peer_pos; GstFormat format; if (!gst_queue2_peer_query (queue, queue->sinkpad, query)) goto peer_failed; /* get peer position */ gst_query_parse_position (query, &format, &peer_pos); /* FIXME: this code assumes that there's no discont in the queue */ switch (format) { case GST_FORMAT_BYTES: peer_pos -= queue->cur_level.bytes; break; case GST_FORMAT_TIME: peer_pos -= queue->cur_level.time; break; default: GST_WARNING_OBJECT (queue, "dropping query in %s format, don't " "know how to adjust value", gst_format_get_name (format)); return FALSE; } /* set updated position */ gst_query_set_position (query, format, peer_pos); break; } case GST_QUERY_DURATION: { GST_DEBUG_OBJECT (queue, "doing peer query"); if (!gst_queue2_peer_query (queue, queue->sinkpad, query)) goto peer_failed; GST_DEBUG_OBJECT (queue, "peer query success"); break; } case GST_QUERY_BUFFERING: { GstFormat format; GST_DEBUG_OBJECT (queue, "query buffering"); /* FIXME - is this condition correct? what should ring buffer do? */ if (QUEUE_IS_USING_QUEUE (queue)) { /* no temp file, just forward to the peer */ if (!gst_queue2_peer_query (queue, queue->sinkpad, query)) goto peer_failed; GST_DEBUG_OBJECT (queue, "buffering forwarded to peer"); } else { gint64 start, stop; guint64 writing_pos; gint percent; gint64 estimated_total, buffering_left; GstFormat peer_fmt; gint64 duration; gboolean peer_res, is_buffering, is_eos; gdouble byte_in_rate, byte_out_rate; /* we need a current download region */ if (queue->current == NULL) return FALSE; writing_pos = queue->current->writing_pos; byte_in_rate = queue->byte_in_rate; byte_out_rate = queue->byte_out_rate; is_buffering = queue->is_buffering; is_eos = queue->is_eos; percent = queue->buffering_percent; if (is_eos) { /* we're EOS, we know the duration in bytes now */ peer_res = TRUE; duration = writing_pos; } else { /* get duration of upstream in bytes */ peer_fmt = GST_FORMAT_BYTES; peer_res = gst_pad_query_peer_duration (queue->sinkpad, &peer_fmt, &duration); } /* calculate remaining and total download time */ if (peer_res && byte_in_rate > 0.0) { estimated_total = (duration * 1000) / byte_in_rate; buffering_left = ((duration - writing_pos) * 1000) / byte_in_rate; } else { estimated_total = -1; buffering_left = -1; } GST_DEBUG_OBJECT (queue, "estimated %" G_GINT64_FORMAT ", left %" G_GINT64_FORMAT, estimated_total, buffering_left); gst_query_parse_buffering_range (query, &format, NULL, NULL, NULL); switch (format) { case GST_FORMAT_PERCENT: /* we need duration */ if (!peer_res) goto peer_failed; GST_DEBUG_OBJECT (queue, "duration %" G_GINT64_FORMAT ", writing %" G_GINT64_FORMAT, duration, writing_pos); start = 0; /* get our available data relative to the duration */ if (duration != -1) stop = GST_FORMAT_PERCENT_MAX * writing_pos / duration; else stop = -1; break; case GST_FORMAT_BYTES: start = 0; stop = writing_pos; break; default: start = -1; stop = -1; break; } gst_query_set_buffering_percent (query, is_buffering, percent); gst_query_set_buffering_range (query, format, start, stop, estimated_total); gst_query_set_buffering_stats (query, GST_BUFFERING_DOWNLOAD, byte_in_rate, byte_out_rate, buffering_left); } break; } default: /* peer handled other queries */ if (!gst_queue2_peer_query (queue, queue->sinkpad, query)) goto peer_failed; break; } return TRUE; /* ERRORS */ peer_failed: { GST_DEBUG_OBJECT (queue, "failed peer query"); return FALSE; } } static gboolean gst_queue2_handle_query (GstElement * element, GstQuery * query) { /* simply forward to the srcpad query function */ return gst_queue2_handle_src_query (GST_QUEUE2_CAST (element)->srcpad, query); } static GstFlowReturn gst_queue2_get_range (GstPad * pad, guint64 offset, guint length, GstBuffer ** buffer) { GstQueue2 *queue; GstFlowReturn ret; queue = GST_QUEUE2_CAST (gst_pad_get_parent (pad)); GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing); length = (length == -1) ? DEFAULT_BUFFER_SIZE : length; offset = (offset == -1) ? queue->current->reading_pos : offset; GST_DEBUG_OBJECT (queue, "Getting range: offset %" G_GUINT64_FORMAT ", length %u", offset, length); /* FIXME - function will block when the range is not yet available */ ret = gst_queue2_create_read (queue, offset, length, buffer); GST_QUEUE2_MUTEX_UNLOCK (queue); gst_object_unref (queue); return ret; /* ERRORS */ out_flushing: { ret = queue->srcresult; GST_DEBUG_OBJECT (queue, "we are flushing"); GST_QUEUE2_MUTEX_UNLOCK (queue); return ret; } } static gboolean gst_queue2_src_checkgetrange_function (GstPad * pad) { GstQueue2 *queue; gboolean ret; queue = GST_QUEUE2 (gst_pad_get_parent (pad)); /* we can operate in pull mode when we are using a tempfile */ ret = !QUEUE_IS_USING_QUEUE (queue); gst_object_unref (GST_OBJECT (queue)); return ret; } /* sink currently only operates in push mode */ static gboolean gst_queue2_sink_activate_push (GstPad * pad, gboolean active) { gboolean result = TRUE; GstQueue2 *queue; queue = GST_QUEUE2 (gst_pad_get_parent (pad)); if (active) { GST_QUEUE2_MUTEX_LOCK (queue); GST_DEBUG_OBJECT (queue, "activating push mode"); queue->srcresult = GST_FLOW_OK; queue->sinkresult = GST_FLOW_OK; queue->is_eos = FALSE; queue->unexpected = FALSE; reset_rate_timer (queue); GST_QUEUE2_MUTEX_UNLOCK (queue); } else { /* unblock chain function */ GST_QUEUE2_MUTEX_LOCK (queue); GST_DEBUG_OBJECT (queue, "deactivating push mode"); queue->srcresult = GST_FLOW_WRONG_STATE; queue->sinkresult = GST_FLOW_WRONG_STATE; gst_queue2_locked_flush (queue); GST_QUEUE2_MUTEX_UNLOCK (queue); } gst_object_unref (queue); return result; } /* src operating in push mode, we start a task on the source pad that pushes out * buffers from the queue */ static gboolean gst_queue2_src_activate_push (GstPad * pad, gboolean active) { gboolean result = FALSE; GstQueue2 *queue; queue = GST_QUEUE2 (gst_pad_get_parent (pad)); if (active) { GST_QUEUE2_MUTEX_LOCK (queue); GST_DEBUG_OBJECT (queue, "activating push mode"); queue->srcresult = GST_FLOW_OK; queue->sinkresult = GST_FLOW_OK; queue->is_eos = FALSE; queue->unexpected = FALSE; result = gst_pad_start_task (pad, (GstTaskFunction) gst_queue2_loop, pad); GST_QUEUE2_MUTEX_UNLOCK (queue); } else { /* unblock loop function */ GST_QUEUE2_MUTEX_LOCK (queue); GST_DEBUG_OBJECT (queue, "deactivating push mode"); queue->srcresult = GST_FLOW_WRONG_STATE; queue->sinkresult = GST_FLOW_WRONG_STATE; /* the item add signal will unblock */ GST_QUEUE2_SIGNAL_ADD (queue); GST_QUEUE2_MUTEX_UNLOCK (queue); /* step 2, make sure streaming finishes */ result = gst_pad_stop_task (pad); } gst_object_unref (queue); return result; } /* pull mode, downstream will call our getrange function */ static gboolean gst_queue2_src_activate_pull (GstPad * pad, gboolean active) { gboolean result; GstQueue2 *queue; queue = GST_QUEUE2 (gst_pad_get_parent (pad)); if (active) { if (!QUEUE_IS_USING_QUEUE (queue)) { if (QUEUE_IS_USING_TEMP_FILE (queue)) { /* open the temp file now */ result = gst_queue2_open_temp_location_file (queue); } else if (!queue->ring_buffer) { queue->ring_buffer = malloc (queue->ring_buffer_max_size); result = ! !queue->ring_buffer; } GST_QUEUE2_MUTEX_LOCK (queue); GST_DEBUG_OBJECT (queue, "activating pull mode"); init_ranges (queue); queue->srcresult = GST_FLOW_OK; queue->sinkresult = GST_FLOW_OK; queue->is_eos = FALSE; queue->unexpected = FALSE; GST_QUEUE2_MUTEX_UNLOCK (queue); } else { GST_QUEUE2_MUTEX_LOCK (queue); GST_DEBUG_OBJECT (queue, "no temp file, cannot activate pull mode"); /* this is not allowed, we cannot operate in pull mode without a temp * file. */ queue->srcresult = GST_FLOW_WRONG_STATE; queue->sinkresult = GST_FLOW_WRONG_STATE; result = FALSE; GST_QUEUE2_MUTEX_UNLOCK (queue); } } else { GST_QUEUE2_MUTEX_LOCK (queue); GST_DEBUG_OBJECT (queue, "deactivating pull mode"); queue->srcresult = GST_FLOW_WRONG_STATE; queue->sinkresult = GST_FLOW_WRONG_STATE; /* this will unlock getrange */ GST_QUEUE2_SIGNAL_ADD (queue); result = TRUE; GST_QUEUE2_MUTEX_UNLOCK (queue); } gst_object_unref (queue); return result; } static GstStateChangeReturn gst_queue2_change_state (GstElement * element, GstStateChange transition) { GstQueue2 *queue; GstStateChangeReturn ret = GST_STATE_CHANGE_SUCCESS; queue = GST_QUEUE2 (element); switch (transition) { case GST_STATE_CHANGE_NULL_TO_READY: break; case GST_STATE_CHANGE_READY_TO_PAUSED: if (!QUEUE_IS_USING_QUEUE (queue)) { if (QUEUE_IS_USING_TEMP_FILE (queue)) { if (!gst_queue2_open_temp_location_file (queue)) ret = GST_STATE_CHANGE_FAILURE; } else { if (queue->ring_buffer) { free (queue->ring_buffer); queue->ring_buffer = NULL; } if (!(queue->ring_buffer = malloc (queue->ring_buffer_max_size))) ret = GST_STATE_CHANGE_FAILURE; } init_ranges (queue); } queue->segment_event_received = FALSE; queue->starting_segment = NULL; break; case GST_STATE_CHANGE_PAUSED_TO_PLAYING: break; default: break; } if (ret == GST_STATE_CHANGE_FAILURE) return ret; ret = GST_ELEMENT_CLASS (parent_class)->change_state (element, transition); if (ret == GST_STATE_CHANGE_FAILURE) return ret; switch (transition) { case GST_STATE_CHANGE_PLAYING_TO_PAUSED: break; case GST_STATE_CHANGE_PAUSED_TO_READY: if (!QUEUE_IS_USING_QUEUE (queue)) { if (QUEUE_IS_USING_TEMP_FILE (queue)) { gst_queue2_close_temp_location_file (queue); } else if (queue->ring_buffer) { free (queue->ring_buffer); queue->ring_buffer = NULL; } } if (queue->starting_segment != NULL) { gst_event_unref (queue->starting_segment); queue->starting_segment = NULL; } break; case GST_STATE_CHANGE_READY_TO_NULL: break; default: break; } return ret; } /* changing the capacity of the queue must wake up * the _chain function, it might have more room now * to store the buffer/event in the queue */ #define QUEUE_CAPACITY_CHANGE(q)\ GST_QUEUE2_SIGNAL_DEL (queue); /* Changing the minimum required fill level must * wake up the _loop function as it might now * be able to preceed. */ #define QUEUE_THRESHOLD_CHANGE(q)\ GST_QUEUE2_SIGNAL_ADD (queue); static void gst_queue2_set_temp_template (GstQueue2 * queue, const gchar * template) { GstState state; /* the element must be stopped in order to do this */ GST_OBJECT_LOCK (queue); state = GST_STATE (queue); if (state != GST_STATE_READY && state != GST_STATE_NULL) goto wrong_state; GST_OBJECT_UNLOCK (queue); /* set new location */ g_free (queue->temp_template); queue->temp_template = g_strdup (template); return; /* ERROR */ wrong_state: { GST_WARNING_OBJECT (queue, "setting temp-template property in wrong state"); GST_OBJECT_UNLOCK (queue); } } static void gst_queue2_set_property (GObject * object, guint prop_id, const GValue * value, GParamSpec * pspec) { GstQueue2 *queue = GST_QUEUE2 (object); /* someone could change levels here, and since this * affects the get/put funcs, we need to lock for safety. */ GST_QUEUE2_MUTEX_LOCK (queue); switch (prop_id) { case PROP_MAX_SIZE_BYTES: queue->max_level.bytes = g_value_get_uint (value); QUEUE_CAPACITY_CHANGE (queue); break; case PROP_MAX_SIZE_BUFFERS: queue->max_level.buffers = g_value_get_uint (value); QUEUE_CAPACITY_CHANGE (queue); break; case PROP_MAX_SIZE_TIME: queue->max_level.time = g_value_get_uint64 (value); /* set rate_time to the same value. We use an extra field in the level * structure so that we can easily access and compare it */ queue->max_level.rate_time = queue->max_level.time; QUEUE_CAPACITY_CHANGE (queue); break; case PROP_USE_BUFFERING: queue->use_buffering = g_value_get_boolean (value); break; case PROP_USE_RATE_ESTIMATE: queue->use_rate_estimate = g_value_get_boolean (value); break; case PROP_LOW_PERCENT: queue->low_percent = g_value_get_int (value); break; case PROP_HIGH_PERCENT: queue->high_percent = g_value_get_int (value); break; case PROP_TEMP_TEMPLATE: gst_queue2_set_temp_template (queue, g_value_get_string (value)); break; case PROP_TEMP_LOCATION: g_free (queue->temp_location); queue->temp_location = g_value_dup_string (value); /* you can set the property back to NULL to make it use the temp-tmpl * property. */ queue->temp_location_set = queue->temp_location != NULL; break; case PROP_TEMP_REMOVE: queue->temp_remove = g_value_get_boolean (value); break; case PROP_RING_BUFFER_MAX_SIZE: queue->ring_buffer_max_size = g_value_get_uint64 (value); queue->use_ring_buffer = ! !queue->ring_buffer_max_size; break; default: G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec); break; } GST_QUEUE2_MUTEX_UNLOCK (queue); } static void gst_queue2_get_property (GObject * object, guint prop_id, GValue * value, GParamSpec * pspec) { GstQueue2 *queue = GST_QUEUE2 (object); GST_QUEUE2_MUTEX_LOCK (queue); switch (prop_id) { case PROP_CUR_LEVEL_BYTES: g_value_set_uint (value, queue->cur_level.bytes); break; case PROP_CUR_LEVEL_BUFFERS: g_value_set_uint (value, queue->cur_level.buffers); break; case PROP_CUR_LEVEL_TIME: g_value_set_uint64 (value, queue->cur_level.time); break; case PROP_MAX_SIZE_BYTES: g_value_set_uint (value, queue->max_level.bytes); break; case PROP_MAX_SIZE_BUFFERS: g_value_set_uint (value, queue->max_level.buffers); break; case PROP_MAX_SIZE_TIME: g_value_set_uint64 (value, queue->max_level.time); break; case PROP_USE_BUFFERING: g_value_set_boolean (value, queue->use_buffering); break; case PROP_USE_RATE_ESTIMATE: g_value_set_boolean (value, queue->use_rate_estimate); break; case PROP_LOW_PERCENT: g_value_set_int (value, queue->low_percent); break; case PROP_HIGH_PERCENT: g_value_set_int (value, queue->high_percent); break; case PROP_TEMP_TEMPLATE: g_value_set_string (value, queue->temp_template); break; case PROP_TEMP_LOCATION: g_value_set_string (value, queue->temp_location); break; case PROP_TEMP_REMOVE: g_value_set_boolean (value, queue->temp_remove); break; case PROP_RING_BUFFER_MAX_SIZE: g_value_set_uint64 (value, queue->ring_buffer_max_size); break; default: G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec); break; } GST_QUEUE2_MUTEX_UNLOCK (queue); }