#!/bin/bash -i # # this script is in git as gstreamer/scripts/gst-uninstalled # # It will set up the environment to use and develop gstreamer and projects # that use gstreamer with an uninstalled git checkout of gstreamer and the # plugin modules. # # It will set up LD_LIBRARY_PATH, DYLD_LIBRARY_PATH, PKG_CONFIG_PATH, # GST_PLUGIN_PATH, GST_PLUGIN_SYSTEM_PATH, GST_REGISTRY, MANPATH, PYTHONPATH # to prefer the uninstalled versions but also contain the installed ones. # The only exception to this is, that no system installed plugins will be # used but only the uninstalled ones. # # This script assumes that the relevant modules are checked out one by one # under a given tree specified below in MYGST. # # Symlink this script in a directory in your path (for example $HOME/bin). You # must name the symlink gst-something, where something is the subdirectory # of MYGST that contains your gstreamer module checkouts. # # e.g.: # - mkdir $HOME/gst/head # - ln -sf gst-uninstalled $HOME/bin/gst-head # - checkout copies of gstreamer modules in $HOME/gst/head # - gst-head # This script is run -i so that PS1 doesn't get cleared # Change this variable to the location of your gstreamer git checkouts MYGST=$HOME/gst # # Everything below this line shouldn't be edited! # # extract version from $0 # if this script is called "gst-head" then version will be "head" VERSION=`echo $0 | sed s/.*gst-//g` # base path under which dirs are installed GST=$MYGST/$VERSION if test ! -e $GST; then echo "$GST does not exist !" exit fi # set up a bunch of paths PATH="\ $GST/gstreamer/tools:\ $GST/gst-plugins-base/tools:\ $GST/gst-player/src:\ $GST/gst-editor/src:\ $GST/gstreamer-sharp/tools:\ $GST/prefix/bin:\ $PATH" # /some/path: makes the dynamic linker look in . too, so avoid this LD_LIBRARY_PATH=$GST/prefix/lib${LD_LIBRARY_PATH:+:$LD_LIBRARY_PATH} DYLD_LIBRARY_PATH=$GST/prefix/lib${DYLD_LIBRARY_PATH:+:$DYLD_LIBRARY_PATH} # GStreamer rtsp server library LD_LIBRARY_PATH=$GST/gst-rtsp-server/gst/rtsp-server/.libs:$LD_LIBRARY_PATH DYLD_LIBRARY_PATH=$GST/gst-rtsp-server/gst/rtsp-server/.libs:$DYLD_LIBRARY_PATH # GStreamer ffmpeg libraries for path in libavformat libavutil libavcodec libpostproc libavdevice do LD_LIBRARY_PATH=$GST/gst-ffmpeg/gst-libs/ext/ffmpeg/$path:$LD_LIBRARY_PATH DYLD_LIBRARY_PATH=$GST/gst-ffmpeg/gst-libs/ext/ffmpeg/$path:$DYLD_LIBRARY_PATH done # GStreamer plugins base libraries for path in app audio cdda fft interfaces pbutils netbuffer riff rtp rtsp sdp tag utils video do LD_LIBRARY_PATH=$GST/gst-plugins-base/gst-libs/gst/$path/.libs:$LD_LIBRARY_PATH DYLD_LIBRARY_PATH=$GST/gst-plugins-base/gst-libs/gst/$path/.libs:$DYLD_LIBRARY_PATH done # GStreamer core libraries for path in base net check controller dataprotocol do LD_LIBRARY_PATH=$GST/gstreamer/libs/gst/$path/.libs:$LD_LIBRARY_PATH DYLD_LIBRARY_PATH=$GST/gstreamer/libs/gst/$path/.libs:$DYLD_LIBRARY_PATH done LD_LIBRARY_PATH=$GST/gstreamer/gst/.libs:$LD_LIBRARY_PATH DYLD_LIBRARY_PATH=$GST/gstreamer/gst/.libs:$DYLD_LIBRARY_PATH export LD_LIBRARY_PATH export DYLD_LIBRARY_PATH export PKG_CONFIG_PATH="\ $GST/prefix/lib/pkgconfig\ :$GST/gstreamer/pkgconfig\ :$GST/gst-plugins-base/pkgconfig\ :$GST/gst-plugins-good/pkgconfig\ :$GST/gst-plugins-ugly/pkgconfig\ :$GST/gst-plugins-bad/pkgconfig\ :$GST/gst-ffmpeg/pkgconfig\ :$GST/gst-python/pkgconfig\ :$GST/gst-rtsp-server/pkgconfig\ :$GST/gstreamer-sharp/pkgconfig\ ${PKG_CONFIG_PATH:+:$PKG_CONFIG_PATH}" export GST_PLUGIN_PATH="\ $GST/gstreamer/plugins\ :$GST/gst-plugins-base/ext\ :$GST/gst-plugins-base/gst\ :$GST/gst-plugins-base/sys\ :$GST/gst-plugins-good/ext\ :$GST/gst-plugins-good/gst\ :$GST/gst-plugins-good/sys\ :$GST/gst-plugins-ugly/ext\ :$GST/gst-plugins-ugly/gst\ :$GST/gst-plugins-ugly/sys\ :$GST/gst-plugins-bad/ext\ :$GST/gst-plugins-bad/gst\ :$GST/gst-plugins-bad/sys\ :$GST/gst-ffmpeg/ext\ :$GST/gnonlin/gnl\ :$GST/gst-openmax\ :$GST/gst-plugins-gl/gst\ :$GST/plugins\ ${GST_PLUGIN_PATH:+:$GST_PLUGIN_PATH}" # don't use any system-installed plug-ins at all export GST_PLUGIN_SYSTEM_PATH= # set our registry somewhere else so we don't mess up the registry generated # by an installed copy rm -f $GST/gstreamer/registry.xml 2>/dev/null export GST_REGISTRY=$GST/gstreamer/registry.dat # Point at the uninstalled plugin scanner export GST_PLUGIN_SCANNER=$GST/gstreamer/libs/gst/helpers/gst-plugin-scanner # once MANPATH is set, it needs at least an "empty"component to keep pulling # in the system-configured man paths from man.config # this still doesn't make it work for the uninstalled case, since man goes # look for a man directory "nearby" instead of the directory I'm telling it to export MANPATH=$GST/gstreamer/tools:$GST/prefix/share/man:$MANPATH pythonver=`python -c "import sys; print sys.version[:3]"` export PYTHONPATH=$GST/gst-python:$GST/prefix/lib/python$pythonver/site-packages${PYTHONPATH:+:$PYTHONPATH} # totem-pl-parser export PKG_CONFIG_PATH=$GST/totem-pl-parser:$PKG_CONFIG_PATH export LD_LIBRARY_PATH=$GST/totem-pl-parser/plparse/.libs:$LD_LIBRARY_PATH export DYLD_LIBRARY_PATH=$GST/totem-pl-parser/plparse/.libs:$DYLD_LIBRARY_PATH # totem export PATH=$GST/totem/src:$PATH # gstreamer-sharp export MONO_PATH=$GST/gstreamer-sharp/gstreamer-sharp:$MONO_PATH export LD_LIBRARY_PATH=$GST/gstreamer-sharp/gstreamer-sharp/glue/.libs:$LD_LIBRARY_PATH export DYLD_LIBRARY_PATH=$GST/gstreamer-sharp/gstreamer-sharp/glue/.libs:$DYLD_LIBRARY_PATH # gst-qa-system export PYTHONPATH=$GST/gst-qa-system:$PYTHONPATH export PATH=$GST/gst-qa-system/bin:$PATH # if we got a command, run it, else start a shell if test ! -z "$1"; then $@ exit $? fi # set up prompt to help us remember we're in a subshell, cd to # the gstreamer base dir and start $SHELL cd $GST shell=$SHELL if test "x$SHELL" == "x/bin/bash" then # debian/ubuntu resets our PS1. bastards. shell="$SHELL --noprofile" fi PS1="[gst-$VERSION] $PS1" $shell