/* GStreamer * Copyright (C) <1999> Erik Walthinsen * Copyright (C) <2004> Thomas Vander Stichele * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #include #include #include static GstPoll *set; static GList *fds = NULL; static GMutex *fdlock; static GTimer *timer; #define MAX_THREADS 100 static void mess_some_more (void) { GList *walk; gint random; gint removed = 0; g_mutex_lock (fdlock); for (walk = fds; walk;) { GstPollFD *fd = (GstPollFD *) walk->data; walk = g_list_next (walk); random = (gint) (10.0 * rand () / (RAND_MAX + 1.0)); switch (random) { case 0: { /* GstPollFD *newfd = g_new0 (GstPollFD, 1); gst_poll_add_fd (set, newfd); fds = g_list_prepend (fds, newfd); */ break; } case 1: if ((gint) (10.0 * rand () / (RAND_MAX + 1.0)) < 2) { gst_poll_remove_fd (set, fd); fds = g_list_remove (fds, fd); g_free (fd); removed++; } break; case 2: gst_poll_fd_ctl_write (set, fd, TRUE); break; case 3: gst_poll_fd_ctl_write (set, fd, FALSE); break; case 4: gst_poll_fd_ctl_read (set, fd, TRUE); break; case 5: gst_poll_fd_ctl_read (set, fd, FALSE); break; case 6: gst_poll_fd_has_closed (set, fd); break; case 7: gst_poll_fd_has_error (set, fd); break; case 8: gst_poll_fd_can_read (set, fd); break; case 9: gst_poll_fd_can_write (set, fd); break; default: g_assert_not_reached (); break; } } if (g_list_length (fds) < 900) { random = removed + (gint) (2.0 * rand () / (RAND_MAX + 1.0)); while (random) { GstPollFD *newfd = g_new0 (GstPollFD, 1); gst_poll_add_fd (set, newfd); fds = g_list_prepend (fds, newfd); random--; } } g_mutex_unlock (fdlock); } static void * run_test (void *threadid) { gint id = GPOINTER_TO_INT (threadid); while (TRUE) { if (id == 0) { gint res = gst_poll_wait (set, 10); if (res < 0) { g_print ("error %d %s\n", errno, g_strerror (errno)); } } else { mess_some_more (); if (g_timer_elapsed (timer, NULL) > 0.5) { g_mutex_lock (fdlock); g_print ("active fds :%d\n", g_list_length (fds)); g_timer_start (timer); g_mutex_unlock (fdlock); } g_usleep (1); } } return NULL; } gint main (gint argc, gchar * argv[]) { GThread *threads[MAX_THREADS]; gint num_threads; gint t; gst_init (&argc, &argv); fdlock = g_mutex_new (); timer = g_timer_new (); if (argc != 2) { g_print ("usage: %s \n", argv[0]); exit (-1); } num_threads = atoi (argv[1]); set = gst_poll_new (TRUE); for (t = 0; t < num_threads; t++) { GError *error = NULL; threads[t] = g_thread_create (run_test, GINT_TO_POINTER (t), TRUE, &error); if (error) { printf ("ERROR: g_thread_create() %s\n", error->message); exit (-1); } } printf ("main(): Created %d threads.\n", t); for (t = 0; t < num_threads; t++) { g_thread_join (threads[t]); } gst_poll_free (set); return 0; }