#include /* threadf.c * this tests if we can make a GThread and construct and interate a pipeline * inside it * used to fail because of cothread ctx key not being reset on context * destroy */ #define MAX_IDENTITIES 29 #define RUNS_PER_IDENTITY 5 gboolean running = FALSE; gboolean done = FALSE; static void construct_pipeline (GstElement *pipeline, gint identities) { GstElement *src, *sink; GstElement *identity = NULL; GstElement *from; int i; identity = NULL; src = gst_element_factory_make ("fakesrc", NULL); sink = gst_element_factory_make ("fakesink", NULL); g_assert (src); g_assert (sink); gst_bin_add_many (GST_BIN (pipeline), src, sink, NULL); from = src; for (i = 0; i < identities; ++i) { identity = gst_element_factory_make ("identity", NULL); g_assert (identity); gst_bin_add (GST_BIN (pipeline), identity); if (!(gst_element_link (from, identity))) g_print ("Warning: can't link identity with previous element\n"); from = identity; } gst_element_link (identity, sink); g_object_set (G_OBJECT (src), "num_buffers", 10, "sizetype", 3, NULL); } static void thread (void) { int runs = MAX_IDENTITIES * RUNS_PER_IDENTITY; int i; GstElement *pipeline; for (i = 30; i < runs; ++i) { pipeline = gst_pipeline_new ("main_pipeline"); g_assert (pipeline); g_print ("Run %d, using %d identities\n", i, i / RUNS_PER_IDENTITY + 1); construct_pipeline (pipeline, i / RUNS_PER_IDENTITY + 1); if (!gst_element_set_state (pipeline, GST_STATE_PLAYING)) g_print ("WARNING: can't set pipeline to play\n"); while (gst_bin_iterate (GST_BIN (pipeline))) g_print ("+"); g_print ("\n"); g_print ("Unreffing pipeline\n"); g_object_unref (G_OBJECT (pipeline)); } done = TRUE; } int main (gint argc, gchar *argv[]) { done = FALSE; g_thread_init (NULL); gst_init (&argc, &argv); g_thread_create ((GThreadFunc) thread, NULL, FALSE, NULL); g_print ("main: created GThread\n"); while (!done) g_usleep (G_USEC_PER_SEC); g_print ("main: done\n"); return 0; }