Building GStreamer on Windows ----------------------------- Running GStreamer on Windows is currently experimental, but improving. Building on MingW/MSys ---------------------- Should work out of the box from the toplevel directory using the standard Unix build system provided. This build type is fairly well supported. Building with Visual Studio 6 ----------------------------- The directory vs6/ contains the workspaces needed to build GStreamer from Visual Studio. This build type is fairly well supported. Building with Visual Studio 7 ----------------------------- vs7/ contains the files needed, but they haven't been updated since the 0.8 series. This build is currently unsupported. The common/ directory contains support files that can be shared between these two versions of Visual Studio.