/* config.h.in. Generated from configure.ac by autoheader. */ /* This copy of config.h.in is specifically for win32 Visual Studio builds */ /* Define to 1 if translation of program messages to the user's native language is requested. */ #undef ENABLE_NLS /* gettext package name */ #define GETTEXT_PACKAGE "gstreamer-0.10" /* PREFIX - specifically added for Windows for easier moving */ #define PREFIX "C:\\gstreamer" /* Location of registry */ #define GST_CACHE_DIR PREFIX "\\var\\cache" /* Define if pipeline parsing code is disabled */ /* #undef GST_DISABLE_PARSE */ /* macro to use to show function name */ #define GST_FUNCTION "(function)" /* Defined if gcov is enabled to force a rebuild due to config.h changing */ /* #undef GST_GCOV_ENABLED */ /* Default errorlevel to use */ #define GST_LEVEL_DEFAULT GST_LEVEL_ERROR /* GStreamer license */ #define GST_LICENSE "LGPL" /* library major.minor version */ #define GST_MAJORMINOR "0.10" /* package name in plugins */ #define GST_PACKAGE_NAME "GStreamer CVS/prerelease" /* package origin */ #define GST_PACKAGE_ORIGIN "Unknown package origin" /* Define if the host CPU is an Alpha */ #undef HAVE_CPU_ALPHA /* Define if the host CPU is an ARM */ #undef HAVE_CPU_ARM /* Define if the host CPU is a HPPA */ #undef HAVE_CPU_HPPA /* Define if the host CPU is an x86 */ #undef HAVE_CPU_I386 /* Define if the host CPU is a IA64 */ #undef HAVE_CPU_IA64 /* Define if the host CPU is a M68K */ #undef HAVE_CPU_M68K /* Define if the host CPU is a MIPS */ #undef HAVE_CPU_MIPS /* Define if the host CPU is a PowerPC */ #undef HAVE_CPU_PPC /* Define if the host CPU is a S390 */ #undef HAVE_CPU_S390 /* Define if the host CPU is a SPARC */ #undef HAVE_CPU_SPARC /* Define if the host CPU is a x86_64 */ #undef HAVE_CPU_X86_64 /* Define if the GNU dcgettext() function is already present or preinstalled. */ #undef HAVE_DCGETTEXT /* Defined if we have dladdr () */ #undef HAVE_DLADDR /* Define to 1 if you have the header file. */ #undef HAVE_DLFCN_H /* Define to 1 if you have the `fgetpos' function. */ #define HAVE_FGETPOS 1 /* Define to 1 if you have the `fork' function. */ #undef HAVE_FORK /* Define to 1 if fseeko (and presumably ftello) exists and is declared. */ #undef HAVE_FSEEKO /* Define to 1 if you have the `fsetpos' function. */ #define HAVE_FSETPOS 1 /* Define to 1 if you have the `ftello' function. */ #undef HAVE_FTELLO /* defined if the compiler implements __func__ */ #undef HAVE_FUNC /* defined if the compiler implements __FUNCTION__ */ #undef HAVE_FUNCTION /* Define to 1 if you have the `getpagesize' function. */ #undef HAVE_GETPAGESIZE /* Define if the GNU gettext() function is already present or preinstalled. */ #undef HAVE_GETTEXT /* Define if you have the iconv() function. */ #undef HAVE_ICONV /* Define to 1 if you have the header file. */ #undef HAVE_INTTYPES_H /* Define if libxml2 is available */ #define HAVE_LIBXML2 1 /* Define to 1 if you have the header file. */ #undef HAVE_MEMORY_H /* Define to 1 if you have a working `mmap' system call. */ #undef HAVE_MMAP /* defined if the compiler implements __PRETTY_FUNCTION__ */ #undef HAVE_PRETTY_FUNCTION /* Defined if we have register_printf_function () */ #undef HAVE_PRINTF_EXTENSION /* Define to 1 if you have the header file. */ #define HAVE_PROCESS_H 1 /* Define if RDTSC is available */ #undef HAVE_RDTSC /* Define to 1 if you have the `sigaction' function. */ #undef HAVE_SIGACTION /* Define to 1 if you have the header file. */ #undef HAVE_STDINT_H /* Define to 1 if you have the header file. */ #define HAVE_STDLIB_H 1 /* Define to 1 if you have the header file. */ #undef HAVE_STRINGS_H /* Define to 1 if you have the header file. */ #define HAVE_STRING_H 1 /* Define to 1 if you have the header file. */ #undef HAVE_SYS_SOCKET_H /* Define to 1 if you have the header file. */ #define HAVE_SYS_STAT_H 1 /* Define to 1 if you have the header file. */ #define HAVE_SYS_TYPES_H 1 /* Define to 1 if you have the header file. */ #undef HAVE_UCONTEXT_H /* defined if unaligned memory access works correctly */ #undef HAVE_UNALIGNED_ACCESS /* Define to 1 if you have the header file. */ #undef HAVE_UNISTD_H /* Define if valgrind should be used */ #undef HAVE_VALGRIND /* Defined if compiling for Windows */ #define HAVE_WIN32 1 /* Define host CPU */ #define HOST_CPU "i686" /* library dir */ #ifdef _DEBUG # define LIBDIR PREFIX "\\debug\\lib" #else # define LIBDIR PREFIX "\\lib" #endif /* gettext locale dir */ #define LOCALEDIR PREFIX "\\share\\locale" /* Name of package */ #define PACKAGE "gstreamer" /* Define to the address where bug reports for this package should be sent. */ #define PACKAGE_BUGREPORT "http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer" /* Define to the full name of this package. */ #define PACKAGE_NAME "GStreamer" /* Define to the full name and version of this package. */ #define PACKAGE_STRING "GStreamer 0.10.12.1" /* Define to the one symbol short name of this package. */ #define PACKAGE_TARNAME "gstreamer" /* Define to the version of this package. */ #define PACKAGE_VERSION "0.10.12.1" /* Define the plugin directory */ #ifdef _DEBUG # define PLUGINDIR PREFIX "\\debug\\lib\\gstreamer-0.10" #else # define PLUGINDIR PREFIX "\\lib\\gstreamer-0.10" #endif /* Define to 1 if you have the ANSI C header files. */ #undef STDC_HEADERS /* Define if we should poison deallocated memory */ #undef USE_POISONING /* Version number of package */ #define VERSION "0.10.12.1" /* Define to 1 if your processor stores words with the most significant byte first (like Motorola and SPARC, unlike Intel and VAX). */ #undef WORDS_BIGENDIAN /* Number of bits in a file offset, on hosts where this is settable. */ #undef _FILE_OFFSET_BITS /* Define to 1 to make fseeko visible on some hosts (e.g. glibc 2.2). */ #undef _LARGEFILE_SOURCE /* Define for large files, on AIX-style hosts. */ #undef _LARGE_FILES /* Define to `__inline__' or `__inline' if that's what the C compiler calls it, or to nothing if 'inline' is not supported under any name. */ /* #undef inline */