diff --git a/ChangeLog b/ChangeLog
index 53b6a11cdb700d67e48e339b1ff9528c7000f652..b0577f33a3e3da1915259c8d3ce20214015c9763 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * libs/gst/dataprotocol/dataprotocol.c:
+ (gst_dp_header_from_buffer), (gst_dp_packet_from_caps),
+ (gst_dp_packet_from_event):
+ * libs/gst/dataprotocol/dataprotocol.h:
+ * libs/gst/dataprotocol/dp-private.h:
+ It's about time we bump the version number.
+ Since event types don't fit in the guint8 anymore describing
+ the payload type, make payload type 16 bits wide.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * docs/design/part-TODO.txt:
+ * docs/design/part-clocks.txt:
+ * docs/design/part-events.txt:
+ * docs/design/part-gstbin.txt:
+ * docs/design/part-gstelement.txt:
+ * docs/design/part-gstpipeline.txt:
+ * docs/design/part-live-source.txt:
+ * docs/design/part-messages.txt:
+ * docs/design/part-overview.txt:
+ * docs/design/part-states.txt:
+ Many doc updates.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * gst/gstevent.c:
+ * gst/gstevent.h:
+ Fix event quark registration.
+ Add some space between events so we can insert them in the
+ right groups.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * gst/base/gstbasesink.c: (gst_base_sink_handle_object),
+ (gst_base_sink_handle_buffer):
+ Better log message.
+
+ * gst/gstbus.h:
+ * gst/gstelement.h:
+ More docs.
+
+ * gst/gstqueue.c: (gst_queue_class_init), (gst_queue_init),
+ (gst_queue_set_property), (gst_queue_get_property):
+ * gst/gstqueue.h:
+ Remove old unused properties.
+
+2005-10-08 Stefan Kost <ensonic@users.sf.net>
+ * docs/gst/gstreamer-sections.txt:
+ * gst/gstmessage.c:
+ * gst/gstmessage.h:
+ * gst/gstminiobject.c:
+ * gst/gstminiobject.h:
+ * gst/gstobject.h:
+ * gst/gstpad.h:
+ * gst/gstutils.h:
+ lots of new docs and doc fixes
+
+2005-10-08 Thomas Vander Stichele <thomas at apestaart dot org>
+
+ * gst/gstplugin.c: (gst_plugin_finalize), (gst_plugin_load_file):
+ * gst/gstplugin.h:
+ * gst/gstregistry.c: (gst_registry_lookup_locked),
+ (gst_registry_scan_path_level):
+ * gst/gstregistryxml.c: (load_plugin):
+ Only ever load one plugin for a given plugin basename.
+ This ensures correct overriding of GST_PLUGIN_PATH over
+ GST_PLUGIN_SYSTEM_PATH and of home dir plugins over
+ system installed plugins.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * gst/base/gstbasesink.c: (gst_base_sink_handle_object),
+ (gst_base_sink_do_sync), (gst_base_sink_handle_buffer):
+ Prepare for doing QOS.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * check/gst/gstbin.c: (GST_START_TEST):
+ * check/pipelines/cleanup.c: (GST_START_TEST):
+ * check/pipelines/simple_launch_lines.c: (GST_START_TEST):
+ Allow new clock message too.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * gst/gstmessage.c: (gst_message_new_error),
+ (gst_message_new_warning), (gst_message_new_tag),
+ (gst_message_new_state_changed), (gst_message_new_clock_provide),
+ (gst_message_new_clock_lost), (gst_message_new_new_clock),
+ (gst_message_new_segment_start), (gst_message_new_segment_done),
+ (gst_message_parse_state_changed),
+ (gst_message_parse_clock_provide), (gst_message_parse_clock_lost),
+ (gst_message_parse_new_clock):
+ * gst/gstmessage.h:
+ Also carry the clock in question.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * gst/gstmessage.c: (gst_message_new_custom),
+ (gst_message_new_eos), (gst_message_new_error),
+ (gst_message_new_warning), (gst_message_new_tag),
+ (gst_message_new_state_changed), (gst_message_new_clock_provide),
+ (gst_message_new_new_clock), (gst_message_new_segment_start),
+ (gst_message_new_segment_done), (gst_message_parse_state_changed),
+ (gst_message_parse_clock_provide), (gst_message_parse_new_clock):
+ * gst/gstmessage.h:
+ Clean up.
+ Added clock related messages.
+
+ * gst/gstpipeline.c: (gst_pipeline_change_state):
+ Post message when the clock changed.
+
+ * tools/gst-launch.c: (event_loop):
+ Print new clock.
+
+2005-10-08 Tim-Philipp Müller <tim at centricular dot net>
+
+ * tools/gst-inspect.c: (print_element_properties_info):
+ Can't pass NULL strings to g_print() on windows.
+
+2005-10-08 Thomas Vander Stichele <thomas at apestaart dot org>
+
+ * docs/Makefile.am:
+ * docs/gst/Makefile.am:
+ * docs/gst/gstreamer-docs.sgml:
+ * docs/gst/running.xml:
+ * docs/version.entities.in:
+ add a chapter on running GStreamer.
+ document GST_DEBUG and GST_PLUGIN* env vars
+
+2005-10-08 Thomas Vander Stichele <thomas at apestaart dot org>
+
+ * Makefile.am:
+ remove include dir
+ * configure.ac:
+ remove PLUGINS_BUILDDIR stuff
+ * gst/gst.c: (init_post):
+ reorder parsing of GST_PLUGIN_PATH and GST_PLUGIN_SYSTEM_PATH
+ * idiottest.mak:
+ remove, it was condescending and not needed
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * gst/base/gstbasesink.c: (gst_base_sink_preroll_queue_flush),
+ (gst_base_sink_handle_object), (gst_base_sink_event),
+ (gst_base_sink_wait), (gst_base_sink_handle_event),
+ (gst_base_sink_change_state):
+ * gst/base/gstbasesink.h:
+ Repost EOS message while going to PLAYING if still EOS.
+ Make sure that when receiving a FLUSH_START we don't attempt
+ to sync on the clock anymore.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * tools/gst-launch.c: (event_loop):
+ Better message printout.
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * gst/gstbin.c: (gst_bin_child_proxy_get_child_by_index),
+ (gst_bin_child_proxy_get_children_count):
+ * gst/gstchildproxy.c: (gst_child_proxy_get_child_by_name),
+ (gst_child_proxy_lookup), (gst_child_proxy_get_property),
+ (gst_child_proxy_get_valist), (gst_child_proxy_set_property),
+ (gst_child_proxy_set_valist):
+ * gst/parse/grammar.y:
+ Make ChildProxy threadsafe and fix mem leaks.
+
+2005-10-08 Thomas Vander Stichele <thomas at apestaart dot org>
+
+ * gst/gst.c: (init_post):
+ debug the GST_PLUGIN_ env vars
+
+2005-10-08 Wim Taymans <wim@fluendo.com>
+
+ * check/gst/gstbin.c: (GST_START_TEST):
+ * check/gst/gstmessage.c: (GST_START_TEST):
+ * check/gst/gstpipeline.c: (GST_START_TEST), (message_received):
+ * gst/gstelement.c: (gst_element_commit_state),
+ (gst_element_lost_state):
+ * gst/gstmessage.c: (gst_message_new_state_changed),
+ (gst_message_parse_state_changed):
+ * gst/gstmessage.h:
+ * tools/gst-launch.c: (event_loop):
+ Added extra field to STATE_CHANGE message with the pending
+ state, which will be different from the new state soon.
+
2005-10-08 Wim Taymans <wim@fluendo.com>
* gst/gstbus.c: (gst_bus_pop):