index 1c40a3723fd7be225eb7fb31f489017c235cb919..1149ebbc80a86114a19988a15200154fcc9e475c 100644 (file)
--- a/NEWS
+++ b/NEWS
-This is GStreamer 0.10.32 "Take Me to the Bonus Level"
+This is GStreamer 0.10.35 "Nuclear Fission"
+
+Changes since 0.10.34:
+
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
+
+Bugs fixed since 0.10.34:
+
+ * 652211 : Use const instead G_CONST_RETURN
+
+Changes since 0.10.33:
+
+ * Fix multiqueue thread-safety regression
+ * Don't set artificial 0-timestamp on first packet for TIME-based live sources
+ * Otherwise identical to the previous release (0.10.33)
+
+Bugs fixed since 0.10.33:
+
+ * 649369 : basesrc: do not set first buffer timestamp to 0 for live sources
+ * 649878 : multiqueue regression: gst_single_queue_new not MT-safe
+
+Changes since 0.10.32:
+
+ * atomicqueue: add an atomic/lock-free queue structure based
+ * bufferlist: improve _add*() performance
+ * bus: in _add_watch() honour any per-thread default main context set via g_main_thread_push_thread_default()
+ * caps: new gst_caps_intersect_full() to intersect in different modes
+ * clock: add functions to re-init existing periodic GstClockIDs
+ * event: add QoS type (overflow, underflow, throttle) for QoS events
+ * ghostpad: The internally linked pad of the proxypad is the ghostpad
+ * gstpoll: retry reading the control socket to release properly all wakeups
+ * message: new progress message API for asynchronous operations
+ * pad: unlock before freeing the pad cache to avoid deadlock
+ * pad: better handling for when parent goes away during data/query/event flow
+ * parse-launch: allow element names to begin with digits
+ * pluginloader: call gst-plugin-scanner with the right arch on OSX, fixing hangs with firefox
+ * registry: fixes elements (features) disappearing if a plugin or plugin file is renamed
+ * structure: Add "(date)" as a type abbreviation of GDate
+ * structure: Don't allow invalid GDates in all structures and don't allow NULL GDates in taglists
+ * taglist: add a new "encoded-by" tag
+ * uri: add gst_filename_to_uri() that takes relative filenames
+ * utils: add gst_element_factory_can_{src|sink}_{any|all}_caps() to replace can_{sink,src}_caps()
+ * baseparse: new GstBaseParse class for parsers
+ * basesink: improve rate, duration, and average duration calculation
+ * basesink: use new QoS types and add add "throttle-time" property
+ * basesrc: Handle tag and custom downstream events the same
+ * basesrc: keep downstream caps order when fixating, to honour downstream preferences when negotiating
+ * basesrc: Return FALSE if we don't handle an event
+ * basesrc: Send synchronized custom downstream/both events downstream from the streaming thread
+ * basetransform: Be smarter with pad allocs
+ * basetransform: Check for pad alloc caps when suggestion is not fixed
+ * basetransform: Retain caps order when getting caps, to honour downstream preferences when negotiating
+ * funnel: new N-to-1 pipe fitting element imported from farsight
+ * fakesink: print buffer flags
+ * filesink: Fix escaping of URIs
+ * file{sink,src}: Check if non-URI characters are escaped, but only for the URI not the location property
+ * filesrc, filesink: fix URI creation regression for non-absolute locations
+ * filesrc: Fix escaping of file uris
+ * inputselector: Hold the selector lock while reading properties of the active pad
+ * inputselector: Make sure that EOS is always sent downstream for the active pad
+ * inputselector: Return GST_FLOW_OK until the selected pad pushed something downstream
+ * inputselector: Stop waiting for a pad switch when the pad is flushing
+ * multiqueue: fix some potential corner-case deadlocks and some leaks
+ * multiqueue: handle arbitrary sink + source pad naming
+ * queue2: don't read beyond the end of file upstream in pull mode; leak fixes
+ * plugins: make query and event functions more thread-safe, protect against parent-pad disappearing
+ * gst-launch: add GstIndex support
+
+Bugs fixed since 0.10.32:
+
+ * 642356 : [Index] review api and add an example
+ * 402141 : gst_element_factory_can_{sink,src}_caps seems to be broken
+ * 518857 : [API] GstBaseParse: new base class for parsers
+ * 604094 : registry: do not remove features when removing a cached plugin that no longer is present
+ * 615357 : [macosx] Handle multi-arch plugin-scanner
+ * 617045 : [caps] New method for intersecting caps while retaining order
+ * 639674 : parse-launch: improve parsing resilience (for escapes at end of string)
+ * 639962 : design docs: Fix a few typos and a think
+ * 640071 : pluginloader: do not leak the description string of blacklisted plugin
+ * 640437 : design docs: fix 2 typos in part-MT-refcounting
+ * 640502 : fix a few typos
+ * 640622 : gst_element_link_pads_full function return wrong error information
+ * 640675 : high cpu-load with 0.10.32 release
+ * 640850 : GstElement: Fix warning with GCC 4.6
+ * 641212 : gst-uninstalled: use $GST_PREFIX variable
+ * 641928 : gst_pad_push fast path races with pad deactivation
+ * 642071 : Incorrect comparing of number of source and sink links when parsing a launch string
+ * 642130 : [basetransform] Check for pad alloc caps when suggestion is not fixed
+ * 642271 : crash in gst_caps_structure_intersect, encoder_match_media_type
+ * 642373 : [basetransform] Avoid too may pad allocs
+ * 642393 : [filesrc] Fails setting the same uri it's setting in the uri queries.
+ * 642504 : [mingw/cygwin build] correctly export plugin description
+ * 642522 : gstvalue.c does not include a deserialize function for uchar
+ * 642869 : gst_index_new: documentation typo
+ * 643301 : Adding a buffer to a buffer list iterates the list
+ * 643455 : [regression] Lots of dropouts in Empathy voip calls
+ * 644935 : [inputselector] During switching of streams it can happen that all pads returned not-linked last
+ * 645022 : GstTask: typo in GST_TASK_BROADCAST - g_cond_breadcast should probably be g_cond_broadcast
+ * 645267 : build: fix build with -Werror with GCC 4.6.0
+ * 645595 : bytereader, bytewriter: fix warnings when using inline functions with g++
+ * 645746 : [gstpoll] Regression causes 100% cpu usage in multifdsink
+ * 645877 : commit 14d7db1 causes cpu spinning and other bus weirdness
+ * 645931 : [gstmultiqueue] fix arbitrary sink + source pad naming
+ * 646118 : [gstmultiqueue] if arbitrary sink number is specified by caller, use this as single queue id
+ * 646341 : [baseparse] Add a queued flow return so parsers can keep frames in a queue
+ * 646531 : GST_BOILERPLATE: don't use " type " as both a variable name and a macro argument
+ * 646566 : Protect against Pad-Parent disappearing
+ * 646569 : poll: don't call WSAWaitForMultipleEvents with no events
+ * 646624 : GstBin: regression: creating too many bins fails, exhausting allowed file descriptor limit
+ * 646811 : baseparse: deadlock in gst_base_parse_set_index
+ * 646971 : iterator: resync to avoid infinite loop
+ * 647005 : GstBus: Only create the socketpair for async message delivery if required
+ * 647131 : recent multiqueue changes break DVD playback (again)
+ * 647293 : Fix pad callbacks so they handle when parent goes away
+ * 647763 : [bus] Bus is leaked if a watch is installed in the default main context
+ * 647844 : baseparse: Remove unused but set variable
+ * 647922 : [introspection] Needs to call gst_init() before anything else
+ * 648199 : pad: potential deadlock / crash when freeing cache
+ * 648215 : basetransform: unref in wrong place
+ * 648220 : Regression: videoscale fails to negotiate for PAR transformation
+ * 648297 : [bus] regression: critical assertion failure
+ * 649195 : [miniobject] Fix dup_mini_object function to handle NULL gvalues
+ * 635718 : [basesrc] custom, non-OOB events aren't pushed downstream
+ * 625396 : gst_debug_remove_log_function doesn't remove default log handler
+ * 640771 : amarok doesn't start with new phonon gstreamer
+ * 646972 : queue2: Fixes memory leak on out_flushing error in gst_queue2_create_read
+ * 640665 : basesink: drops too many buffers when there's no duration
+
+API additions since 0.10.32:
+
+ * gst_atomic_queue_length()
+ * gst_atomic_queue_new()
+ * gst_atomic_queue_peek()
+ * gst_atomic_queue_pop()
+ * gst_atomic_queue_push()
+ * gst_atomic_queue_ref()
+ * gst_atomic_queue_unref()
+ * gst_buffer_list_iterator_get_type()
+ * gst_caps_intersect_full()
+ * gst_caps_intersect_mode_get_type()
+ * gst_clock_periodic_id_reinit()
+ * gst_element_factory_can_sink_all_caps()
+ * gst_element_factory_can_sink_any_caps()
+ * gst_element_factory_can_src_all_caps()
+ * gst_element_factory_can_src_any_caps()
+ * gst_event_new_qos_full()
+ * gst_event_parse_qos_full()
+ * gst_filename_to_uri()
+ * gst_message_new_progress()
+ * gst_message_parse_progress()
+ * gst_parse_context_get_type()
+ * gst_progress_type_get_type()
+ * gst_qos_type_get_type()
+ * GST_TAG_ENCODED_BY
+ * gst_base_parse_add_index_entry()
+ * gst_base_parse_convert_default()
+ * gst_base_parse_frame_free()
+ * gst_base_parse_frame_get_type()
+ * gst_base_parse_frame_init()
+ * gst_base_parse_frame_new()
+ * gst_base_parse_get_type()
+ * gst_base_parse_push_frame()
+ * gst_base_parse_set_average_bitrate()
+ * gst_base_parse_set_duration()
+ * gst_base_parse_set_frame_rate()
+ * gst_base_parse_set_has_timing_info()
+ * gst_base_parse_set_min_frame_size()
+ * gst_base_parse_set_passthrough()
+ * gst_base_parse_set_syncable()
+ * gst_base_sink_get_throttle_time()
+ * gst_base_sink_set_throttle_time()
+
+API deprecated since 0.10.32:
+
+ * gst_element_factory_can_src_caps()
+ * gst_element_factory_can_sink_caps()
Changes since 0.10.31: