index 326b2db3f96254eee9e0e18705f21617cd909542..1149ebbc80a86114a19988a15200154fcc9e475c 100644 (file)
--- a/NEWS
+++ b/NEWS
-This is GStreamer 0.10.28 "Same Old, Same Old"
+This is GStreamer 0.10.35 "Nuclear Fission"
+
+Changes since 0.10.34:
+
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
+
+Bugs fixed since 0.10.34:
+
+ * 652211 : Use const instead G_CONST_RETURN
+
+Changes since 0.10.33:
+
+ * Fix multiqueue thread-safety regression
+ * Don't set artificial 0-timestamp on first packet for TIME-based live sources
+ * Otherwise identical to the previous release (0.10.33)
+
+Bugs fixed since 0.10.33:
+
+ * 649369 : basesrc: do not set first buffer timestamp to 0 for live sources
+ * 649878 : multiqueue regression: gst_single_queue_new not MT-safe
+
+Changes since 0.10.32:
+
+ * atomicqueue: add an atomic/lock-free queue structure based
+ * bufferlist: improve _add*() performance
+ * bus: in _add_watch() honour any per-thread default main context set via g_main_thread_push_thread_default()
+ * caps: new gst_caps_intersect_full() to intersect in different modes
+ * clock: add functions to re-init existing periodic GstClockIDs
+ * event: add QoS type (overflow, underflow, throttle) for QoS events
+ * ghostpad: The internally linked pad of the proxypad is the ghostpad
+ * gstpoll: retry reading the control socket to release properly all wakeups
+ * message: new progress message API for asynchronous operations
+ * pad: unlock before freeing the pad cache to avoid deadlock
+ * pad: better handling for when parent goes away during data/query/event flow
+ * parse-launch: allow element names to begin with digits
+ * pluginloader: call gst-plugin-scanner with the right arch on OSX, fixing hangs with firefox
+ * registry: fixes elements (features) disappearing if a plugin or plugin file is renamed
+ * structure: Add "(date)" as a type abbreviation of GDate
+ * structure: Don't allow invalid GDates in all structures and don't allow NULL GDates in taglists
+ * taglist: add a new "encoded-by" tag
+ * uri: add gst_filename_to_uri() that takes relative filenames
+ * utils: add gst_element_factory_can_{src|sink}_{any|all}_caps() to replace can_{sink,src}_caps()
+ * baseparse: new GstBaseParse class for parsers
+ * basesink: improve rate, duration, and average duration calculation
+ * basesink: use new QoS types and add add "throttle-time" property
+ * basesrc: Handle tag and custom downstream events the same
+ * basesrc: keep downstream caps order when fixating, to honour downstream preferences when negotiating
+ * basesrc: Return FALSE if we don't handle an event
+ * basesrc: Send synchronized custom downstream/both events downstream from the streaming thread
+ * basetransform: Be smarter with pad allocs
+ * basetransform: Check for pad alloc caps when suggestion is not fixed
+ * basetransform: Retain caps order when getting caps, to honour downstream preferences when negotiating
+ * funnel: new N-to-1 pipe fitting element imported from farsight
+ * fakesink: print buffer flags
+ * filesink: Fix escaping of URIs
+ * file{sink,src}: Check if non-URI characters are escaped, but only for the URI not the location property
+ * filesrc, filesink: fix URI creation regression for non-absolute locations
+ * filesrc: Fix escaping of file uris
+ * inputselector: Hold the selector lock while reading properties of the active pad
+ * inputselector: Make sure that EOS is always sent downstream for the active pad
+ * inputselector: Return GST_FLOW_OK until the selected pad pushed something downstream
+ * inputselector: Stop waiting for a pad switch when the pad is flushing
+ * multiqueue: fix some potential corner-case deadlocks and some leaks
+ * multiqueue: handle arbitrary sink + source pad naming
+ * queue2: don't read beyond the end of file upstream in pull mode; leak fixes
+ * plugins: make query and event functions more thread-safe, protect against parent-pad disappearing
+ * gst-launch: add GstIndex support
+
+Bugs fixed since 0.10.32:
+
+ * 642356 : [Index] review api and add an example
+ * 402141 : gst_element_factory_can_{sink,src}_caps seems to be broken
+ * 518857 : [API] GstBaseParse: new base class for parsers
+ * 604094 : registry: do not remove features when removing a cached plugin that no longer is present
+ * 615357 : [macosx] Handle multi-arch plugin-scanner
+ * 617045 : [caps] New method for intersecting caps while retaining order
+ * 639674 : parse-launch: improve parsing resilience (for escapes at end of string)
+ * 639962 : design docs: Fix a few typos and a think
+ * 640071 : pluginloader: do not leak the description string of blacklisted plugin
+ * 640437 : design docs: fix 2 typos in part-MT-refcounting
+ * 640502 : fix a few typos
+ * 640622 : gst_element_link_pads_full function return wrong error information
+ * 640675 : high cpu-load with 0.10.32 release
+ * 640850 : GstElement: Fix warning with GCC 4.6
+ * 641212 : gst-uninstalled: use $GST_PREFIX variable
+ * 641928 : gst_pad_push fast path races with pad deactivation
+ * 642071 : Incorrect comparing of number of source and sink links when parsing a launch string
+ * 642130 : [basetransform] Check for pad alloc caps when suggestion is not fixed
+ * 642271 : crash in gst_caps_structure_intersect, encoder_match_media_type
+ * 642373 : [basetransform] Avoid too may pad allocs
+ * 642393 : [filesrc] Fails setting the same uri it's setting in the uri queries.
+ * 642504 : [mingw/cygwin build] correctly export plugin description
+ * 642522 : gstvalue.c does not include a deserialize function for uchar
+ * 642869 : gst_index_new: documentation typo
+ * 643301 : Adding a buffer to a buffer list iterates the list
+ * 643455 : [regression] Lots of dropouts in Empathy voip calls
+ * 644935 : [inputselector] During switching of streams it can happen that all pads returned not-linked last
+ * 645022 : GstTask: typo in GST_TASK_BROADCAST - g_cond_breadcast should probably be g_cond_broadcast
+ * 645267 : build: fix build with -Werror with GCC 4.6.0
+ * 645595 : bytereader, bytewriter: fix warnings when using inline functions with g++
+ * 645746 : [gstpoll] Regression causes 100% cpu usage in multifdsink
+ * 645877 : commit 14d7db1 causes cpu spinning and other bus weirdness
+ * 645931 : [gstmultiqueue] fix arbitrary sink + source pad naming
+ * 646118 : [gstmultiqueue] if arbitrary sink number is specified by caller, use this as single queue id
+ * 646341 : [baseparse] Add a queued flow return so parsers can keep frames in a queue
+ * 646531 : GST_BOILERPLATE: don't use " type " as both a variable name and a macro argument
+ * 646566 : Protect against Pad-Parent disappearing
+ * 646569 : poll: don't call WSAWaitForMultipleEvents with no events
+ * 646624 : GstBin: regression: creating too many bins fails, exhausting allowed file descriptor limit
+ * 646811 : baseparse: deadlock in gst_base_parse_set_index
+ * 646971 : iterator: resync to avoid infinite loop
+ * 647005 : GstBus: Only create the socketpair for async message delivery if required
+ * 647131 : recent multiqueue changes break DVD playback (again)
+ * 647293 : Fix pad callbacks so they handle when parent goes away
+ * 647763 : [bus] Bus is leaked if a watch is installed in the default main context
+ * 647844 : baseparse: Remove unused but set variable
+ * 647922 : [introspection] Needs to call gst_init() before anything else
+ * 648199 : pad: potential deadlock / crash when freeing cache
+ * 648215 : basetransform: unref in wrong place
+ * 648220 : Regression: videoscale fails to negotiate for PAR transformation
+ * 648297 : [bus] regression: critical assertion failure
+ * 649195 : [miniobject] Fix dup_mini_object function to handle NULL gvalues
+ * 635718 : [basesrc] custom, non-OOB events aren't pushed downstream
+ * 625396 : gst_debug_remove_log_function doesn't remove default log handler
+ * 640771 : amarok doesn't start with new phonon gstreamer
+ * 646972 : queue2: Fixes memory leak on out_flushing error in gst_queue2_create_read
+ * 640665 : basesink: drops too many buffers when there's no duration
+
+API additions since 0.10.32:
+
+ * gst_atomic_queue_length()
+ * gst_atomic_queue_new()
+ * gst_atomic_queue_peek()
+ * gst_atomic_queue_pop()
+ * gst_atomic_queue_push()
+ * gst_atomic_queue_ref()
+ * gst_atomic_queue_unref()
+ * gst_buffer_list_iterator_get_type()
+ * gst_caps_intersect_full()
+ * gst_caps_intersect_mode_get_type()
+ * gst_clock_periodic_id_reinit()
+ * gst_element_factory_can_sink_all_caps()
+ * gst_element_factory_can_sink_any_caps()
+ * gst_element_factory_can_src_all_caps()
+ * gst_element_factory_can_src_any_caps()
+ * gst_event_new_qos_full()
+ * gst_event_parse_qos_full()
+ * gst_filename_to_uri()
+ * gst_message_new_progress()
+ * gst_message_parse_progress()
+ * gst_parse_context_get_type()
+ * gst_progress_type_get_type()
+ * gst_qos_type_get_type()
+ * GST_TAG_ENCODED_BY
+ * gst_base_parse_add_index_entry()
+ * gst_base_parse_convert_default()
+ * gst_base_parse_frame_free()
+ * gst_base_parse_frame_get_type()
+ * gst_base_parse_frame_init()
+ * gst_base_parse_frame_new()
+ * gst_base_parse_get_type()
+ * gst_base_parse_push_frame()
+ * gst_base_parse_set_average_bitrate()
+ * gst_base_parse_set_duration()
+ * gst_base_parse_set_frame_rate()
+ * gst_base_parse_set_has_timing_info()
+ * gst_base_parse_set_min_frame_size()
+ * gst_base_parse_set_passthrough()
+ * gst_base_parse_set_syncable()
+ * gst_base_sink_get_throttle_time()
+ * gst_base_sink_set_throttle_time()
+
+API deprecated since 0.10.32:
+
+ * gst_element_factory_can_src_caps()
+ * gst_element_factory_can_sink_caps()
+
+Changes since 0.10.31:
+
+ * GLib requirement is now >= 2.22
+ * New core element: valve (moved from -bad)
+ * New core element: input-selector (N.B. without "select-all" property,
+ use fsfunnel instead) (moved from -bad)
+ * New core element: output-selector (N.B. with different negotiation
+ behaviour by default, set pad-negotiation-mode=active for previous
+ behaviour) (moved from -bad)
+ * Performance improvements for many heavily-used code paths: GstPad,
+ GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue
+ * gobject-introspection: add annotations for most core API
+ * clock: make sync clock wait lockfree
+ * fdsrc/fdsink: reenable on MSVC
+ * registry: fix GStatBuf definition for win32 when building against older
+ glib (fixes unnecessary rescanning of plugins at start-up)
+ * element: add a more flexible way to get request pads from elements
+ * multiqueue: return upon input when already eos
+ * object: fix creation of default name (when creating more than 100000 elements)
+ * pluginloader: fix hangs on OSX
+ * poll: fixes for (p)select backend (used e.g. on OSX)
+ * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
+ * registry: don't replace valid existing plugins by blacklisted ones
+ * tags: don't produce duplicated entries when merging same value twice
+ * basesink: preroll fixes for async=false case
+ * basesink: rework position reporting code
+ * basetransform: handle downstream giving a buffer with new caps but invalid size
+
+Bugs fixed since 0.10.31:
+
+ * 635785 : basesrc: fix deadlock
+ * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
+ * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
+ * 564056 : Protect against umask(0177)
+ * 607513 : input-selector segfaults in g_object_notify()
+ * 632168 : [gsttask] MSVC thread names for task debugging
+ * 632447 : reduce static memory allocated by the registry
+ * 632557 : [macros] Define restrict keyword if not available
+ * 632778 : Optimisations to GstBaseSink
+ * 632779 : gstdataqueue: Only emit g_cond_signal when needed
+ * 632780 : queue: Remove useless checks from e406f7
+ * 633918 : [fakesink] [PATCH] print sink-message events like a message and its structure
+ * 634965 : sinks render buffers in state PAUSED when async is FALSE
+ * 635001 : basesink: fix position reporting in PAUSED
+ * 636268 : configure test fails on FreeBSD
+ * 636455 : basesrc: Avoid taking object locks for just checking tag presence
+ * 637057 : [plugin-scanner] gstpoll fails with select backend
+ * 637300 : [API] request pad based on caps
+ * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
+ * 637776 : merging the same tag values again produces lists containing duplicates
+ * 638381 : {input,output}-selector: double-check API before release
+ * 638399 : a few typos in GStreamer
+ * 638900 : [GstPoll] Doesn't compile with MinGW
+ * 638941 : registry scan/loading race and inconsistency
+
+API additions since 0.10.31:
+
+ * gst_clock_single_shot_id_reinit()
+ * gst_element_request_pad()
+ * GstElementClass::request_new_pad_full()
+ * gst_poll_get_read_gpollfd()
+ * gst_value_list_merge()
+ * GST_CLOCK_DONE
+
+Changes since 0.10.30:
+
+ * bin: add "message-forward" property to force forwarding of messages that would usually be filtered such as ASYNC_DONE or EOS
+ * bin: improve tracking of source elements for more efficient event dispatch
+ * bufferlist: add function to add a list of buffers
+ * clock: fix racy shutdown clock id leak
+ * element: add support for arbitrary element class / factory details
+ * element: link_many should activate pads if needed
+ * gst: add math-compat.h header
+ * datetime: add GstDateTime API
+ * elementfactory: add utility functions to filter features by type
+ * plugin: load the gst-python plugin loader with G_MODULE_BIND_LAZY
+ * query: add buffering ranges API to retrieve informations about the areas of the stream currently buffered
+ * value: add int64 range type
+ * info: write debugging output to file if GST_DEBUG_FILE environment variable is set
+ * pad: use more efficient g_object_notify_by_pspec() for caps notifies if compiling against new-enough GLib
+ * pipeline: If the currently used clock gets lost update it the next time when going from PAUSED to playing
+ * plugin: add release datetime field to GstPluginDesc and set it if GST_PACKAGE_RELEASE_DATETIME is defined
+ * utils: speed up pad linking utility functions by not trying pads that will never work
+ * adapter: add function to get a list of buffers; support 0-sized buffers
+ * adapter: optimize gst_adapter_take() and gst_adapter_peek() a little
+ * basesink: only answer the SEGMENT query in pull mode
+ * basesrc: return values in stream time for the POSITION query
+ * basetransform: allow the subclass to add new fields to caps when getting new caps from downstream
+ * basetransform: avoid useless memcpy
+ * basetransform: upstream caps-renegotiation fixes
+ * bitreader: add inlined and unchecked versions of the most important functions
+ * bytewriter: add inline and unchecked variants of all important functions
+ * bytewriter: fix possible infinite loop caused by an overflow
+ * queue: add "silent" property to suppress signal emission (for better performance)
+ * queue: avoid unnecessary g_cond_signal() (for better performance)
+ * queue: push newsegment event when linking in PLAYING
+ * queue2: extend ring buffer to support RAM mode
+ * queue2: in download mode, prevent range corruption due to race
+ * queue2: don't send seeks beyond the end of the file upstream in pull mode (fixes apple trailers and youtube/html5 playback in webkit)
+ * multiqueue: flush the data queue if downstream return WRONG_STATE too
+ * gst-inspect: print GST_PARAM_MUTABLE_* property flags
+
+Bugs fixed since 0.10.30:
+
+ * 396774 : Make GstElementDetails extensible
+ * 482147 : [queue] Issue with current time level if source task is not started
+ * 579127 : gst-launch: disable CLOCK_LOST message handling
+ * 594504 : Need a GType of " Date AND Time AND Timezone "
+ * 600004 : underrun signal emits when i tested queue overrun test case from file /gstreamerXXXX/tests/check/element/queue.c
+ * 610366 : [gstcollectpads][doc] Add a reminder for 'data' doc
+ * 611918 : leaky queue might not push newsegment event
+ * 618919 : Registry/Plugin Loading Memory Leak
+ * 619522 : basetransform fix for upstream caps-renegotiation
+ * 621299 : make simple queues faster
+ * 621332 : BaseTransform should disable proxy alloc if downstream changes caps
+ * 622740 : GstPad: Do not call gst_pad_accept_caps() when caps change
+ * 623040 : Add release_datetime field to GstPluginDesc
+ * 623121 : [queue2] downloaded areas of the media are not exposed
+ * 623491 : make *_get_type() thread safe
+ * 623541 : [basetransform] Implement POSITION query
+ * 623622 : [basesink/basesrc] Should return values in stream time for POSITION query
+ * 623806 : [pipeline] Doesn't update the clock if the currently used one gets lost and the start time did not change
+ * 623875 : gstregistrybinary.c compatibility with glib > = 2.25.0
+ * 624203 : gstutils: Make gst_pad_proxy_getcaps() return empty caps if it's what the other side has
+ * 625239 : FTBFS: ./gstreamer-decl.txt:9461: warning: GstTagList has multiple definitions.
+ * 625295 : [info] regression: doesn't flush output stream after every debug print any longer
+ * 625368 : gstdatetime.c doesn't compile in VS 2008
+ * 625862 : [docs] unused symbol GST_CAT_LEVEL_LOG_valist breaks the build
+ * 626027 : [tag] Add GST_TAG_APPLICATION_NAME
+ * 626181 : GstElementFactory: add listing/filtering API
+ * 626651 : [tag] Photography/capture settings tags
+ * 626784 : element: link_many might assert elements are in paused or playing
+ * 627438 : gst: Add a gst_is_initialized() API
+ * 627826 : GstInt64Range type
+ * 627910 : Warnings emitted when -Wcast-qual used
+ * 627959 : [queue2] on-disk buffering failing for AVI container
+ * 628014 : Deprecate GST_FLOW_IS_FATAL/GST_FLOW_IS_SUCCESS
+ * 628174 : New gstvalue checks cause trouble in thoggen
+ * 628176 : [basetransform] Problems with buffer handling in inplace mode
+ * 628408 : Use GDateTime that has been released
+ * 629241 : Build broken with introspection using gobject-introspection from master
+ * 629410 : GstBaseTransform: position query refers to sink pad, not source pad
+ * 629494 : Latest gst-launch.c doesn't build in Visual Studio 2008
+ * 629553 : GstAdapter: timestamp not updated when empty buffer is pushed
+ * 629831 : [API] add gst_structure_take_value() and gst_structure_id_take_value()
+ * 629946 : Enumerations have incorrect names of enum values (GEnumValue.value_name)
+ * 630257 : GST_DEBUG_DUMP_DOT_DIR not working anymore
+ * 630436 : basesink: renderdelay needs to be subtracted in adjust_time()
+ * 630437 : basetransform: Make a WARNING into a DEBUG statement
+ * 630439 : clock: fix racy shutdown clock id leak
+ * 631755 : Fix build with glib 2.21.3
+ * 631853 : [queue2] deadlock when using temp-location and dispatch-properties
+ * 632236 : [gst-inspect] unhelpful uri handler output
+ * 632433 : [basesink] hangs/drops going to PLAYING following flushing step in PAUSED
+ * 632977 : [queue2] qtdemux causes soup to request seeks past the end of the range
+ * 633147 : Simple reverse negotiation pipeline is broken.
+ * 633886 : Visual Studio emits warnings about double defined _USE_MATH_DEFINES
+ * 635031 : [datetime] Fix unix epoch handling
+ * 635389 : Include information on exported packages in GIRs
+ * 635869 : GST_BOILERPLATE_FULL causes warnings in user C++ code
+ * 633176 : recent multiqueue changes break DVD playback
+
+API additions since 0.10.30:
+
+ * gst_is_initialized
+ * gst_buffer_list_iterator_add_list
+ * GstBin:message-forward
+ * GST_TYPE_DATE_TIME
+ * gst_date_time_get_day
+ * gst_date_time_get_hour
+ * gst_date_time_get_microsecond
+ * gst_date_time_get_minute
+ * gst_date_time_get_month
+ * gst_date_time_get_second
+ * gst_date_time_get_time_zone_offset
+ * gst_date_time_get_type
+ * gst_date_time_get_year
+ * gst_date_time_new
+ * gst_date_time_new_from_unix_epoch_local_time
+ * gst_date_time_new_from_unix_epoch_utc
+ * gst_date_time_new_local_time
+ * gst_date_time_new_now_local_time
+ * gst_date_time_new_now_utc
+ * gst_date_time_ref
+ * gst_date_time_unref
+ * gst_tag_list_get_date_time
+ * gst_tag_list_get_date_time_index
+ * GST_TAG_GEO_LOCATION_HORIZONTAL_ERROR
+ * GST_TAG_APPLICATION_DATA
+ * GST_TAG_APPLICATION_NAME
+ * GST_TAG_DATE_TIME
+ * GST_ELEMENT_IS_SOURCE
+ * gst_element_class_set_documentation_uri
+ * gst_element_class_set_icon_name
+ * gst_element_factory_get_documentation_uri
+ * gst_element_factory_get_icon_name
+ * gst_element_factory_list_filter
+ * gst_element_factory_list_get_elements
+ * gst_element_factory_list_is_type
+ * GstElementFactoryListType
+ * GST_ELEMENT_FACTORY_TYPE_ANY
+ * GST_ELEMENT_FACTORY_TYPE_AUDIOVIDEO_SINKS
+ * GST_ELEMENT_FACTORY_TYPE_AUDIO_ENCODER
+ * GST_ELEMENT_FACTORY_TYPE_DECODABLE
+ * GST_ELEMENT_FACTORY_TYPE_DECODER
+ * GST_ELEMENT_FACTORY_TYPE_DEMUXER
+ * GST_ELEMENT_FACTORY_TYPE_DEPAYLOADER
+ * GST_ELEMENT_FACTORY_TYPE_ENCODER
+ * GST_ELEMENT_FACTORY_TYPE_FORMATTER
+ * GST_ELEMENT_FACTORY_TYPE_MAX_ELEMENTS
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_AUDIO
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_IMAGE
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_METADATA
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_SUBTITLE
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_VIDEO
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_ANY
+ * GST_ELEMENT_FACTORY_TYPE_MUXER
+ * GST_ELEMENT_FACTORY_TYPE_PARSER
+ * GST_ELEMENT_FACTORY_TYPE_PAYLOADER
+ * GST_ELEMENT_FACTORY_TYPE_SINK
+ * GST_ELEMENT_FACTORY_TYPE_SRC
+ * GST_ELEMENT_FACTORY_TYPE_VIDEO_ENCODER
+ * GST_ELEMENT_FACTORY_KLASS_DECODER
+ * GST_ELEMENT_FACTORY_KLASS_ENCODER
+ * GST_ELEMENT_FACTORY_KLASS_SINK
+ * GST_ELEMENT_FACTORY_KLASS_SRC
+ * GST_ELEMENT_FACTORY_KLASS_MUXER
+ * GST_ELEMENT_FACTORY_KLASS_DEMUXER
+ * GST_ELEMENT_FACTORY_KLASS_PARSER
+ * GST_ELEMENT_FACTORY_KLASS_PAYLOADER
+ * GST_ELEMENT_FACTORY_KLASS_DEPAYLOADER
+ * GST_ELEMENT_FACTORY_KLASS_FORMATTER
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_VIDEO
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_AUDIO
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_IMAGE
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_SUBTITLE
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_METADATA
+ * gst_plugin_feature_list_debug
+ * gst_plugin_feature_rank_compare_func
+ * gst_query_add_buffering_range
+ * gst_query_get_n_buffering_ranges
+ * gst_query_parse_nth_buffering_range
+ * gst_structure_get_date_time
+ * gst_structure_id_take_value
+ * gst_structure_take_value
+ * GST_TYPE_INT64_RANGE
+ * gst_int64_range_get_type
+ * gst_util_fraction_compare
+ * gst_value_get_int64_range_max
+ * gst_value_get_int64_range_min
+ * gst_value_set_int64_range
+ * GST_VALUE_HOLDS_DATE_TIME
+ * gst_adapter_take_list
+ * gst_bit_reader_skip_unchecked
+ * gst_bit_reader_skip_to_byte_unchecked
+ * gst_bit_reader_get_bits_uint16_unchecked
+ * gst_bit_reader_get_bits_uint32_unchecked
+ * gst_bit_reader_get_bits_uint64_unchecked
+ * gst_bit_reader_get_bits_uint8_unchecked
+ * gst_bit_reader_peek_bits_uint16_unchecked
+ * gst_bit_reader_peek_bits_uint32_unchecked
+ * gst_bit_reader_peek_bits_uint64_unchecked
+ * gst_bit_reader_peek_bits_uint8_unchecked
+ * gst_byte_writer_put_int8_unchecked
+ * gst_byte_writer_put_int16_be_unchecked
+ * gst_byte_writer_put_int16_le_unchecked
+ * gst_byte_writer_put_int24_be_unchecked
+ * gst_byte_writer_put_int32_be_unchecked
+ * gst_byte_writer_put_int32_le_unchecked
+ * gst_byte_writer_put_int64_be_unchecked
+ * gst_byte_writer_put_int64_le_unchecked
+ * gst_byte_writer_put_uint8_unchecked
+ * gst_byte_writer_put_uint16_be_unchecked
+ * gst_byte_writer_put_uint16_le_unchecked
+ * gst_byte_writer_put_uint24_be_unchecked
+ * gst_byte_writer_put_uint24_le_unchecked
+ * gst_byte_writer_put_uint32_be_unchecked
+ * gst_byte_writer_put_uint32_le_unchecked
+ * gst_byte_writer_put_uint64_be_unchecked
+ * gst_byte_writer_put_uint64_le_unchecked
+ * gst_byte_writer_put_float32_be_unchecked
+ * gst_byte_writer_put_float32_le_unchecked
+ * gst_byte_writer_put_float64_be_unchecked
+ * gst_byte_writer_put_float64_le_unchecked
+ * gst_byte_writer_put_data_unchecked
+ * gst_byte_writer_fill_unchecked
+
+API deprecated since 0.10.30:
+
+ * GST_FLOW_IS_FATAL
+ * GST_FLOW_IS_SUCCESS
+
+Changes since 0.10.29:
+
+ * GLib requirement was bumped to 2.20, automake requirement to 1.10
+ * bin: unlock gst_element_get_state() on error, instead of hanging forever if no timeout is given
+ * clock: fix refcounting bug in gst_clock_set_master
+ * caps: make sure _normalize() is applied on all structures
+ * info: add new TRACE log level and move refcounting there from LOG level
+ * pad: don't check twice for changed caps per push
+ * pad: fix iterator aggregation of all pads in the internal links fallback
+ * tagsetter: protect tagsetter operations with a lock
+ * value: support short fourccs (esp. serialisation/deserialisation)
+ * adapter: fix _try_to_merge_up(); optimize progressive masked scans
+ * basesink: implement percentage position and duration queries
+ * basesink: fix segment query return value
+ * basetransform: add accept_caps vmethod
+ * basetransform: re-evaluate proxy_alloc when reconfigured
+ * basetransform: assume in_size equals out_size if there's no transform_size/get_unit_size vfunc
+ * fdsink, filesink: make sync property work correctly
+ * typefind: make sure buffers' metadata is writable before setting caps on them
+ * queue2: fix merging of ranges
+ * queue2: don't wait for data when EOS
+ * queue2: don't ignore failure to open the temporary file location
+ * tools: make gst-launch print things correctly to stderr/stdout and make --quiet work correctly
+ * introspection: add many more gobject-introspection annotations
+ * xml: serialisation/deserialisation to/from XML has been deprecated, since it's always been broken
+ for all but the most trivial pipelines, and will likely never be fixed
+
+Bugs fixed since 0.10.29:
+
+ * 623586 : gst/tagsetter check fails
+ * 463435 : Skip #include < libxml/parser.h > in gstconfig.h.in when not needed
+ * 505770 : gst_element_get_state() should unblock if element posts an error
+ * 615820 : implement percentage position and duration queries
+ * 615941 : [tags] Add GST_TAG_DEVICE_MANUFACTURER and GST_TAG_DEVICE_MODEL
+ * 616586 : Use GObject's boxed type for GError
+ * 617223 : [tags] Add tags for direction of capture and movement
+ * 617625 : Commandline utility wrappers (gst-run) don't work on Windows
+ * 618644 : gst_pad_get_caps() Return pad template if parent element is in GST_STATE_NULL
+ * 619508 : [tag] Add image orientation tag
+ * 619815 : GST_PLUGIN_LOADING_WHITELIST env var for unit tests
+ * 619828 : [API] adapter: add masked_scan_uint32_peek
+ * 620460 : info: add new TRACE log level and move refcounting there from LOG level
+ * 620490 : [basesink] segment query unconditionally returns FALSE
+ * 621006 : Deprecate unused gst_object_{get|set}_name_prefix()
+ * 621282 : Display of short fourccs is in hex instead of text
+ * 621332 : BaseTransform should disable proxy alloc if downstream changes caps
+ * 621334 : GstBaseTransform should not require a transform_size function
+ * 621505 : Disable memory poisoning by default for releases
+ * 621527 : gstcaps: New gst_caps_steal_structure() method
+ * 621530 : filesink ignores sync=true
+ * 621595 : --quiet doesnt make gst-launch be completely quiet, also messages should not go to stdout
+ * 621773 : Add introspection annotations
+ * 621867 : gst-launch: rename new --no-play command line option
+ * 621896 : [API][taglist] Add gst_tag_list_peek_string_index
+ * 622504 : [GstPad] Provide more fine-grained linking methods
+ * 622546 : distcheck fails in docs/plugins/
+ * 622685 : [GstXml] Deprecate GstXml
+ * 622967 : [queue2] Problems with progressive downloading
+ * 623301 : gst_caps_normalize : doesn't normalize completely
+ * 623589 : Fix races/refcounting bugs with slave clocks
+ * 624113 : [tags] wrong behaviour in merge function for strings
+ * 622025 : Can't build gstreamer due to Gst-0.10.gir: error: Can't resolve type 'PadIntLinkFunction' for field Gst.Pad.intlinkfunc
+
+API additions since 0.10.29:
+
+ * gst_caps_steal_structure()
+ * gst_clock_id_wait_async_full()
+ * gst_element_link_pads_full()
+ * GstPadLinkCheck
+ * gst_pad_link_check_get_type()
+ * gst_pad_link_full()
+ * gst_structure_fixate_field_string()
+ * GST_TAG_DEVICE_MANUFACTURER
+ * GST_TAG_DEVICE_MODEL
+ * GST_TAG_IMAGE_ORIENTATION
+ * GST_TAG_GEO_LOCATION_CAPTURE_DIRECTION
+ * GST_TAG_GEO_LOCATION_MOVEMENT_DIRECTION
+ * GST_TAG_GEO_LOCATION_MOVEMENT_SPEED
+ * gst_tag_list_peek_string_index()
+ * GST_TRACE
+ * GST_TRACE_OBJECT
+ * GST_CAT_TRACE
+ * GST_CAT_TRACE_OBJECT
+ * GST_LEVEL_TRACE
+ * gst_adapter_masked_scan_uint32_peek
+ * GstBaseSink::enable-last-buffer
+ * gst_base_sink_is_last_buffer_enabled()
+ * gst_base_sink_set_last_buffer_enabled()
+ * GstBaseTransform::accept_caps()
+
+API deprecated since 0.10.29:
+
+ * gst_object_get_name_prefix()
+ * gst_object_set_name_prefix()
+ * gst_caps_load_thyself()
+ * gst_caps_save_thyself()
+ * gst_class_signal_emit_by_name()
+ * gst_object_save_thyself()
+ * gst_object_restore_thyself()
+ * gst_pad_load_and_link()
+ * gst_xml_get_element()
+ * gst_xml_get_topelements()
+ * gst_xml_get_type()
+ * gst_xml_make_element()
+ * gst_xml_new()
+ * gst_xml_parse_doc()
+ * gst_xml_parse_file()
+ * gst_xml_parse_memory()
+ * gst_xml_write()
+ * gst_xml_write_file()
+
+Changes since 0.10.28:
+
+ * improve plugin loading robustness: do not ever unload a plugin after
+ calling into it: should fix mystery crashers during registry loading
+ when a plugin init function returns FALSE (e.g. when some supporting
+ library fails to initialise or a wrapper plugin found no features to
+ wrap and wrongly returned FALSE)
+ * configurable memory alignment for GstBuffers
+ * add QoS message to inform apps of lost data, dropped frames etc.
+ * basesink, basetransform: add support for new QoS message
+ * basetransform: accept non-fixed caps suggestions
+ * basesrc: fix gst_base_src_new_seamless_segment()
+ * GstController fixes and optimisations
+ * set thread name for pad tasks on Linux
+ * pipeline, bin: fix refcount issue when removing elements during a state change
+ * queue2: implement seeking in download mode
+ * queue2: implement flushing in download buffering
+ * queue2: improve buffer level measurement in download mode
+ * fdsrc: allow specifying the size in bytes on the uri
+ * build fixes: better checks for uint128_t, inline assembly on OSX, compilation
+ if HAVE_REGISTER_PRINTF_SPECIFIER is undefined, gobject-introspection
+ * two symbols were removed that had been exported but never been used or been
+ declared in any header file: gst_element_default_error and gst_element_request_compatible_pad
+
+Bugs fixed since 0.10.28:
+
+ * 576234 : [basetransform] Suggesting non-fixed caps or no size doesn't work for upstream negotiation
+ * 520697 : [API] Add GST_TAG_USER_RATING
+ * 590718 : docs build failures with -jN: cp: cannot create regular file `build/image.entities': File exists
+ * 595958 : Position not updated after a backwards gst_event_new_step()
+ * 596832 : configurable buffer alignment
+ * 600718 : autoconf fails with gobject-introspection
+ * 600877 : [uridecodebin] Needs to disable download buffering for non-fast-start files
+ * 603710 : Can't compile with introspection support
+ * 603831 : build with libtool 1.x.y only works if --disable-shave is used
+ * 609046 : basetransform now ignores suggestions from capsfilter
+ * 609170 : basesrc pushes two newsegment
+ * 610256 : Use G_VALUE_COLLECT_INIT if available
+ * 611075 : Typo in debug_dump_pad function
+ * 611911 : Set thread names on pipeline threads
+ * 612370 : gstutils.c inline asm typo, compilation fails
+ * 612410 : [API][tags] add new geo tags
+ * 612733 : Build fails because HAVE_REGISTER_PRINTF_SPECIFIER is undefined
+ * 612881 : [utils] gst_pad_proxy_setcaps() doesn't handler iterator resyncs
+ * 613215 : delayed set in gst-launch are not recursive
+ * 613593 : git-update.sh script does not work on fresh git repository clones
+ * 614167 : gstinfo: no previous prototype for 'xxx' when buildign with --disable-gst-debug
+ * 614629 : utils: Use G_GNUC_CONST instead of G_GNUC_PURE for conversion functions
+ * 614767 : libgstreamer build failure on OS X x86_64
+ * 614833 : out of srcdir build fails for libs/gst/check
+ * 615698 : " warning: cast increases required alignment of target type " with gcc 4.2.1 on arm
+ * 615756 : [bin] refcount issue when removing element in error
+ * 615880 : Add some more custom flow returns
+ * 615881 : [LFOControlSource] Use correct setter for double GValues
+ * 616846 : Crash in gst_interpolation_control_source_find_control_point_iter
+
+API additions since 0.10.28:
+
+ * GST_MESSAGE_QOS
+ * gst_message_new_qos()
+ * gst_message_parse_qos()
+ * gst_message_parse_qos_stats()
+ * gst_message_parse_qos_values()
+ * gst_message_set_qos_stats()
+ * gst_message_set_qos_values()
+ * GST_FLOW_CUSTOM_SUCCESS_1
+ * GST_FLOW_CUSTOM_SUCCESS_2
+ * GST_FLOW_CUSTOM_ERROR_1
+ * GST_FLOW_CUSTOM_ERROR_2
+ * GST_TAG_USER_RATING
+ * GST_TAG_GEO_LOCATION_COUNTRY
+ * GST_TAG_GEO_LOCATION_CITY
+ * GST_TAG_GEO_LOCATION_SUBLOCATION
+
+API deprecated since 0.10.28:
+
+ * gst_element_class_set_details()
Changes since 0.10.27: