index 65bcb011e96fa0e256fb514da7c265f9b1769309..1c40a3723fd7be225eb7fb31f489017c235cb919 100644 (file)
--- a/NEWS
+++ b/NEWS
-This is GStreamer 0.10.20 "You Crazy Diamond"
+This is GStreamer 0.10.32 "Take Me to the Bonus Level"
+
+Changes since 0.10.31:
+
+ * GLib requirement is now >= 2.22
+ * New core element: valve (moved from -bad)
+ * New core element: input-selector (N.B. without "select-all" property,
+ use fsfunnel instead) (moved from -bad)
+ * New core element: output-selector (N.B. with different negotiation
+ behaviour by default, set pad-negotiation-mode=active for previous
+ behaviour) (moved from -bad)
+ * Performance improvements for many heavily-used code paths: GstPad,
+ GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue
+ * gobject-introspection: add annotations for most core API
+ * clock: make sync clock wait lockfree
+ * fdsrc/fdsink: reenable on MSVC
+ * registry: fix GStatBuf definition for win32 when building against older
+ glib (fixes unnecessary rescanning of plugins at start-up)
+ * element: add a more flexible way to get request pads from elements
+ * multiqueue: return upon input when already eos
+ * object: fix creation of default name (when creating more than 100000 elements)
+ * pluginloader: fix hangs on OSX
+ * poll: fixes for (p)select backend (used e.g. on OSX)
+ * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
+ * registry: don't replace valid existing plugins by blacklisted ones
+ * tags: don't produce duplicated entries when merging same value twice
+ * basesink: preroll fixes for async=false case
+ * basesink: rework position reporting code
+ * basetransform: handle downstream giving a buffer with new caps but invalid size
+
+Bugs fixed since 0.10.31:
+
+ * 635785 : basesrc: fix deadlock
+ * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
+ * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
+ * 564056 : Protect against umask(0177)
+ * 607513 : input-selector segfaults in g_object_notify()
+ * 632168 : [gsttask] MSVC thread names for task debugging
+ * 632447 : reduce static memory allocated by the registry
+ * 632557 : [macros] Define restrict keyword if not available
+ * 632778 : Optimisations to GstBaseSink
+ * 632779 : gstdataqueue: Only emit g_cond_signal when needed
+ * 632780 : queue: Remove useless checks from e406f7
+ * 633918 : [fakesink] [PATCH] print sink-message events like a message and its structure
+ * 634965 : sinks render buffers in state PAUSED when async is FALSE
+ * 635001 : basesink: fix position reporting in PAUSED
+ * 636268 : configure test fails on FreeBSD
+ * 636455 : basesrc: Avoid taking object locks for just checking tag presence
+ * 637057 : [plugin-scanner] gstpoll fails with select backend
+ * 637300 : [API] request pad based on caps
+ * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
+ * 637776 : merging the same tag values again produces lists containing duplicates
+ * 638381 : {input,output}-selector: double-check API before release
+ * 638399 : a few typos in GStreamer
+ * 638900 : [GstPoll] Doesn't compile with MinGW
+ * 638941 : registry scan/loading race and inconsistency
+
+API additions since 0.10.31:
+
+ * gst_clock_single_shot_id_reinit()
+ * gst_element_request_pad()
+ * GstElementClass::request_new_pad_full()
+ * gst_poll_get_read_gpollfd()
+ * gst_value_list_merge()
+ * GST_CLOCK_DONE
+
+Changes since 0.10.30:
+
+ * bin: add "message-forward" property to force forwarding of messages that would usually be filtered such as ASYNC_DONE or EOS
+ * bin: improve tracking of source elements for more efficient event dispatch
+ * bufferlist: add function to add a list of buffers
+ * clock: fix racy shutdown clock id leak
+ * element: add support for arbitrary element class / factory details
+ * element: link_many should activate pads if needed
+ * gst: add math-compat.h header
+ * datetime: add GstDateTime API
+ * elementfactory: add utility functions to filter features by type
+ * plugin: load the gst-python plugin loader with G_MODULE_BIND_LAZY
+ * query: add buffering ranges API to retrieve informations about the areas of the stream currently buffered
+ * value: add int64 range type
+ * info: write debugging output to file if GST_DEBUG_FILE environment variable is set
+ * pad: use more efficient g_object_notify_by_pspec() for caps notifies if compiling against new-enough GLib
+ * pipeline: If the currently used clock gets lost update it the next time when going from PAUSED to playing
+ * plugin: add release datetime field to GstPluginDesc and set it if GST_PACKAGE_RELEASE_DATETIME is defined
+ * utils: speed up pad linking utility functions by not trying pads that will never work
+ * adapter: add function to get a list of buffers; support 0-sized buffers
+ * adapter: optimize gst_adapter_take() and gst_adapter_peek() a little
+ * basesink: only answer the SEGMENT query in pull mode
+ * basesrc: return values in stream time for the POSITION query
+ * basetransform: allow the subclass to add new fields to caps when getting new caps from downstream
+ * basetransform: avoid useless memcpy
+ * basetransform: upstream caps-renegotiation fixes
+ * bitreader: add inlined and unchecked versions of the most important functions
+ * bytewriter: add inline and unchecked variants of all important functions
+ * bytewriter: fix possible infinite loop caused by an overflow
+ * queue: add "silent" property to suppress signal emission (for better performance)
+ * queue: avoid unnecessary g_cond_signal() (for better performance)
+ * queue: push newsegment event when linking in PLAYING
+ * queue2: extend ring buffer to support RAM mode
+ * queue2: in download mode, prevent range corruption due to race
+ * queue2: don't send seeks beyond the end of the file upstream in pull mode (fixes apple trailers and youtube/html5 playback in webkit)
+ * multiqueue: flush the data queue if downstream return WRONG_STATE too
+ * gst-inspect: print GST_PARAM_MUTABLE_* property flags
+
+Bugs fixed since 0.10.30:
+
+ * 396774 : Make GstElementDetails extensible
+ * 482147 : [queue] Issue with current time level if source task is not started
+ * 579127 : gst-launch: disable CLOCK_LOST message handling
+ * 594504 : Need a GType of " Date AND Time AND Timezone "
+ * 600004 : underrun signal emits when i tested queue overrun test case from file /gstreamerXXXX/tests/check/element/queue.c
+ * 610366 : [gstcollectpads][doc] Add a reminder for 'data' doc
+ * 611918 : leaky queue might not push newsegment event
+ * 618919 : Registry/Plugin Loading Memory Leak
+ * 619522 : basetransform fix for upstream caps-renegotiation
+ * 621299 : make simple queues faster
+ * 621332 : BaseTransform should disable proxy alloc if downstream changes caps
+ * 622740 : GstPad: Do not call gst_pad_accept_caps() when caps change
+ * 623040 : Add release_datetime field to GstPluginDesc
+ * 623121 : [queue2] downloaded areas of the media are not exposed
+ * 623491 : make *_get_type() thread safe
+ * 623541 : [basetransform] Implement POSITION query
+ * 623622 : [basesink/basesrc] Should return values in stream time for POSITION query
+ * 623806 : [pipeline] Doesn't update the clock if the currently used one gets lost and the start time did not change
+ * 623875 : gstregistrybinary.c compatibility with glib > = 2.25.0
+ * 624203 : gstutils: Make gst_pad_proxy_getcaps() return empty caps if it's what the other side has
+ * 625239 : FTBFS: ./gstreamer-decl.txt:9461: warning: GstTagList has multiple definitions.
+ * 625295 : [info] regression: doesn't flush output stream after every debug print any longer
+ * 625368 : gstdatetime.c doesn't compile in VS 2008
+ * 625862 : [docs] unused symbol GST_CAT_LEVEL_LOG_valist breaks the build
+ * 626027 : [tag] Add GST_TAG_APPLICATION_NAME
+ * 626181 : GstElementFactory: add listing/filtering API
+ * 626651 : [tag] Photography/capture settings tags
+ * 626784 : element: link_many might assert elements are in paused or playing
+ * 627438 : gst: Add a gst_is_initialized() API
+ * 627826 : GstInt64Range type
+ * 627910 : Warnings emitted when -Wcast-qual used
+ * 627959 : [queue2] on-disk buffering failing for AVI container
+ * 628014 : Deprecate GST_FLOW_IS_FATAL/GST_FLOW_IS_SUCCESS
+ * 628174 : New gstvalue checks cause trouble in thoggen
+ * 628176 : [basetransform] Problems with buffer handling in inplace mode
+ * 628408 : Use GDateTime that has been released
+ * 629241 : Build broken with introspection using gobject-introspection from master
+ * 629410 : GstBaseTransform: position query refers to sink pad, not source pad
+ * 629494 : Latest gst-launch.c doesn't build in Visual Studio 2008
+ * 629553 : GstAdapter: timestamp not updated when empty buffer is pushed
+ * 629831 : [API] add gst_structure_take_value() and gst_structure_id_take_value()
+ * 629946 : Enumerations have incorrect names of enum values (GEnumValue.value_name)
+ * 630257 : GST_DEBUG_DUMP_DOT_DIR not working anymore
+ * 630436 : basesink: renderdelay needs to be subtracted in adjust_time()
+ * 630437 : basetransform: Make a WARNING into a DEBUG statement
+ * 630439 : clock: fix racy shutdown clock id leak
+ * 631755 : Fix build with glib 2.21.3
+ * 631853 : [queue2] deadlock when using temp-location and dispatch-properties
+ * 632236 : [gst-inspect] unhelpful uri handler output
+ * 632433 : [basesink] hangs/drops going to PLAYING following flushing step in PAUSED
+ * 632977 : [queue2] qtdemux causes soup to request seeks past the end of the range
+ * 633147 : Simple reverse negotiation pipeline is broken.
+ * 633886 : Visual Studio emits warnings about double defined _USE_MATH_DEFINES
+ * 635031 : [datetime] Fix unix epoch handling
+ * 635389 : Include information on exported packages in GIRs
+ * 635869 : GST_BOILERPLATE_FULL causes warnings in user C++ code
+ * 633176 : recent multiqueue changes break DVD playback
+
+API additions since 0.10.30:
+
+ * gst_is_initialized
+ * gst_buffer_list_iterator_add_list
+ * GstBin:message-forward
+ * GST_TYPE_DATE_TIME
+ * gst_date_time_get_day
+ * gst_date_time_get_hour
+ * gst_date_time_get_microsecond
+ * gst_date_time_get_minute
+ * gst_date_time_get_month
+ * gst_date_time_get_second
+ * gst_date_time_get_time_zone_offset
+ * gst_date_time_get_type
+ * gst_date_time_get_year
+ * gst_date_time_new
+ * gst_date_time_new_from_unix_epoch_local_time
+ * gst_date_time_new_from_unix_epoch_utc
+ * gst_date_time_new_local_time
+ * gst_date_time_new_now_local_time
+ * gst_date_time_new_now_utc
+ * gst_date_time_ref
+ * gst_date_time_unref
+ * gst_tag_list_get_date_time
+ * gst_tag_list_get_date_time_index
+ * GST_TAG_GEO_LOCATION_HORIZONTAL_ERROR
+ * GST_TAG_APPLICATION_DATA
+ * GST_TAG_APPLICATION_NAME
+ * GST_TAG_DATE_TIME
+ * GST_ELEMENT_IS_SOURCE
+ * gst_element_class_set_documentation_uri
+ * gst_element_class_set_icon_name
+ * gst_element_factory_get_documentation_uri
+ * gst_element_factory_get_icon_name
+ * gst_element_factory_list_filter
+ * gst_element_factory_list_get_elements
+ * gst_element_factory_list_is_type
+ * GstElementFactoryListType
+ * GST_ELEMENT_FACTORY_TYPE_ANY
+ * GST_ELEMENT_FACTORY_TYPE_AUDIOVIDEO_SINKS
+ * GST_ELEMENT_FACTORY_TYPE_AUDIO_ENCODER
+ * GST_ELEMENT_FACTORY_TYPE_DECODABLE
+ * GST_ELEMENT_FACTORY_TYPE_DECODER
+ * GST_ELEMENT_FACTORY_TYPE_DEMUXER
+ * GST_ELEMENT_FACTORY_TYPE_DEPAYLOADER
+ * GST_ELEMENT_FACTORY_TYPE_ENCODER
+ * GST_ELEMENT_FACTORY_TYPE_FORMATTER
+ * GST_ELEMENT_FACTORY_TYPE_MAX_ELEMENTS
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_AUDIO
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_IMAGE
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_METADATA
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_SUBTITLE
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_VIDEO
+ * GST_ELEMENT_FACTORY_TYPE_MEDIA_ANY
+ * GST_ELEMENT_FACTORY_TYPE_MUXER
+ * GST_ELEMENT_FACTORY_TYPE_PARSER
+ * GST_ELEMENT_FACTORY_TYPE_PAYLOADER
+ * GST_ELEMENT_FACTORY_TYPE_SINK
+ * GST_ELEMENT_FACTORY_TYPE_SRC
+ * GST_ELEMENT_FACTORY_TYPE_VIDEO_ENCODER
+ * GST_ELEMENT_FACTORY_KLASS_DECODER
+ * GST_ELEMENT_FACTORY_KLASS_ENCODER
+ * GST_ELEMENT_FACTORY_KLASS_SINK
+ * GST_ELEMENT_FACTORY_KLASS_SRC
+ * GST_ELEMENT_FACTORY_KLASS_MUXER
+ * GST_ELEMENT_FACTORY_KLASS_DEMUXER
+ * GST_ELEMENT_FACTORY_KLASS_PARSER
+ * GST_ELEMENT_FACTORY_KLASS_PAYLOADER
+ * GST_ELEMENT_FACTORY_KLASS_DEPAYLOADER
+ * GST_ELEMENT_FACTORY_KLASS_FORMATTER
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_VIDEO
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_AUDIO
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_IMAGE
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_SUBTITLE
+ * GST_ELEMENT_FACTORY_KLASS_MEDIA_METADATA
+ * gst_plugin_feature_list_debug
+ * gst_plugin_feature_rank_compare_func
+ * gst_query_add_buffering_range
+ * gst_query_get_n_buffering_ranges
+ * gst_query_parse_nth_buffering_range
+ * gst_structure_get_date_time
+ * gst_structure_id_take_value
+ * gst_structure_take_value
+ * GST_TYPE_INT64_RANGE
+ * gst_int64_range_get_type
+ * gst_util_fraction_compare
+ * gst_value_get_int64_range_max
+ * gst_value_get_int64_range_min
+ * gst_value_set_int64_range
+ * GST_VALUE_HOLDS_DATE_TIME
+ * gst_adapter_take_list
+ * gst_bit_reader_skip_unchecked
+ * gst_bit_reader_skip_to_byte_unchecked
+ * gst_bit_reader_get_bits_uint16_unchecked
+ * gst_bit_reader_get_bits_uint32_unchecked
+ * gst_bit_reader_get_bits_uint64_unchecked
+ * gst_bit_reader_get_bits_uint8_unchecked
+ * gst_bit_reader_peek_bits_uint16_unchecked
+ * gst_bit_reader_peek_bits_uint32_unchecked
+ * gst_bit_reader_peek_bits_uint64_unchecked
+ * gst_bit_reader_peek_bits_uint8_unchecked
+ * gst_byte_writer_put_int8_unchecked
+ * gst_byte_writer_put_int16_be_unchecked
+ * gst_byte_writer_put_int16_le_unchecked
+ * gst_byte_writer_put_int24_be_unchecked
+ * gst_byte_writer_put_int32_be_unchecked
+ * gst_byte_writer_put_int32_le_unchecked
+ * gst_byte_writer_put_int64_be_unchecked
+ * gst_byte_writer_put_int64_le_unchecked
+ * gst_byte_writer_put_uint8_unchecked
+ * gst_byte_writer_put_uint16_be_unchecked
+ * gst_byte_writer_put_uint16_le_unchecked
+ * gst_byte_writer_put_uint24_be_unchecked
+ * gst_byte_writer_put_uint24_le_unchecked
+ * gst_byte_writer_put_uint32_be_unchecked
+ * gst_byte_writer_put_uint32_le_unchecked
+ * gst_byte_writer_put_uint64_be_unchecked
+ * gst_byte_writer_put_uint64_le_unchecked
+ * gst_byte_writer_put_float32_be_unchecked
+ * gst_byte_writer_put_float32_le_unchecked
+ * gst_byte_writer_put_float64_be_unchecked
+ * gst_byte_writer_put_float64_le_unchecked
+ * gst_byte_writer_put_data_unchecked
+ * gst_byte_writer_fill_unchecked
+
+API deprecated since 0.10.30:
+
+ * GST_FLOW_IS_FATAL
+ * GST_FLOW_IS_SUCCESS
+
+Changes since 0.10.29:
+
+ * GLib requirement was bumped to 2.20, automake requirement to 1.10
+ * bin: unlock gst_element_get_state() on error, instead of hanging forever if no timeout is given
+ * clock: fix refcounting bug in gst_clock_set_master
+ * caps: make sure _normalize() is applied on all structures
+ * info: add new TRACE log level and move refcounting there from LOG level
+ * pad: don't check twice for changed caps per push
+ * pad: fix iterator aggregation of all pads in the internal links fallback
+ * tagsetter: protect tagsetter operations with a lock
+ * value: support short fourccs (esp. serialisation/deserialisation)
+ * adapter: fix _try_to_merge_up(); optimize progressive masked scans
+ * basesink: implement percentage position and duration queries
+ * basesink: fix segment query return value
+ * basetransform: add accept_caps vmethod
+ * basetransform: re-evaluate proxy_alloc when reconfigured
+ * basetransform: assume in_size equals out_size if there's no transform_size/get_unit_size vfunc
+ * fdsink, filesink: make sync property work correctly
+ * typefind: make sure buffers' metadata is writable before setting caps on them
+ * queue2: fix merging of ranges
+ * queue2: don't wait for data when EOS
+ * queue2: don't ignore failure to open the temporary file location
+ * tools: make gst-launch print things correctly to stderr/stdout and make --quiet work correctly
+ * introspection: add many more gobject-introspection annotations
+ * xml: serialisation/deserialisation to/from XML has been deprecated, since it's always been broken
+ for all but the most trivial pipelines, and will likely never be fixed
+
+Bugs fixed since 0.10.29:
+
+ * 623586 : gst/tagsetter check fails
+ * 463435 : Skip #include < libxml/parser.h > in gstconfig.h.in when not needed
+ * 505770 : gst_element_get_state() should unblock if element posts an error
+ * 615820 : implement percentage position and duration queries
+ * 615941 : [tags] Add GST_TAG_DEVICE_MANUFACTURER and GST_TAG_DEVICE_MODEL
+ * 616586 : Use GObject's boxed type for GError
+ * 617223 : [tags] Add tags for direction of capture and movement
+ * 617625 : Commandline utility wrappers (gst-run) don't work on Windows
+ * 618644 : gst_pad_get_caps() Return pad template if parent element is in GST_STATE_NULL
+ * 619508 : [tag] Add image orientation tag
+ * 619815 : GST_PLUGIN_LOADING_WHITELIST env var for unit tests
+ * 619828 : [API] adapter: add masked_scan_uint32_peek
+ * 620460 : info: add new TRACE log level and move refcounting there from LOG level
+ * 620490 : [basesink] segment query unconditionally returns FALSE
+ * 621006 : Deprecate unused gst_object_{get|set}_name_prefix()
+ * 621282 : Display of short fourccs is in hex instead of text
+ * 621332 : BaseTransform should disable proxy alloc if downstream changes caps
+ * 621334 : GstBaseTransform should not require a transform_size function
+ * 621505 : Disable memory poisoning by default for releases
+ * 621527 : gstcaps: New gst_caps_steal_structure() method
+ * 621530 : filesink ignores sync=true
+ * 621595 : --quiet doesnt make gst-launch be completely quiet, also messages should not go to stdout
+ * 621773 : Add introspection annotations
+ * 621867 : gst-launch: rename new --no-play command line option
+ * 621896 : [API][taglist] Add gst_tag_list_peek_string_index
+ * 622504 : [GstPad] Provide more fine-grained linking methods
+ * 622546 : distcheck fails in docs/plugins/
+ * 622685 : [GstXml] Deprecate GstXml
+ * 622967 : [queue2] Problems with progressive downloading
+ * 623301 : gst_caps_normalize : doesn't normalize completely
+ * 623589 : Fix races/refcounting bugs with slave clocks
+ * 624113 : [tags] wrong behaviour in merge function for strings
+ * 622025 : Can't build gstreamer due to Gst-0.10.gir: error: Can't resolve type 'PadIntLinkFunction' for field Gst.Pad.intlinkfunc
+
+API additions since 0.10.29:
+
+ * gst_caps_steal_structure()
+ * gst_clock_id_wait_async_full()
+ * gst_element_link_pads_full()
+ * GstPadLinkCheck
+ * gst_pad_link_check_get_type()
+ * gst_pad_link_full()
+ * gst_structure_fixate_field_string()
+ * GST_TAG_DEVICE_MANUFACTURER
+ * GST_TAG_DEVICE_MODEL
+ * GST_TAG_IMAGE_ORIENTATION
+ * GST_TAG_GEO_LOCATION_CAPTURE_DIRECTION
+ * GST_TAG_GEO_LOCATION_MOVEMENT_DIRECTION
+ * GST_TAG_GEO_LOCATION_MOVEMENT_SPEED
+ * gst_tag_list_peek_string_index()
+ * GST_TRACE
+ * GST_TRACE_OBJECT
+ * GST_CAT_TRACE
+ * GST_CAT_TRACE_OBJECT
+ * GST_LEVEL_TRACE
+ * gst_adapter_masked_scan_uint32_peek
+ * GstBaseSink::enable-last-buffer
+ * gst_base_sink_is_last_buffer_enabled()
+ * gst_base_sink_set_last_buffer_enabled()
+ * GstBaseTransform::accept_caps()
+
+API deprecated since 0.10.29:
+
+ * gst_object_get_name_prefix()
+ * gst_object_set_name_prefix()
+ * gst_caps_load_thyself()
+ * gst_caps_save_thyself()
+ * gst_class_signal_emit_by_name()
+ * gst_object_save_thyself()
+ * gst_object_restore_thyself()
+ * gst_pad_load_and_link()
+ * gst_xml_get_element()
+ * gst_xml_get_topelements()
+ * gst_xml_get_type()
+ * gst_xml_make_element()
+ * gst_xml_new()
+ * gst_xml_parse_doc()
+ * gst_xml_parse_file()
+ * gst_xml_parse_memory()
+ * gst_xml_write()
+ * gst_xml_write_file()
+
+Changes since 0.10.28:
+
+ * improve plugin loading robustness: do not ever unload a plugin after
+ calling into it: should fix mystery crashers during registry loading
+ when a plugin init function returns FALSE (e.g. when some supporting
+ library fails to initialise or a wrapper plugin found no features to
+ wrap and wrongly returned FALSE)
+ * configurable memory alignment for GstBuffers
+ * add QoS message to inform apps of lost data, dropped frames etc.
+ * basesink, basetransform: add support for new QoS message
+ * basetransform: accept non-fixed caps suggestions
+ * basesrc: fix gst_base_src_new_seamless_segment()
+ * GstController fixes and optimisations
+ * set thread name for pad tasks on Linux
+ * pipeline, bin: fix refcount issue when removing elements during a state change
+ * queue2: implement seeking in download mode
+ * queue2: implement flushing in download buffering
+ * queue2: improve buffer level measurement in download mode
+ * fdsrc: allow specifying the size in bytes on the uri
+ * build fixes: better checks for uint128_t, inline assembly on OSX, compilation
+ if HAVE_REGISTER_PRINTF_SPECIFIER is undefined, gobject-introspection
+ * two symbols were removed that had been exported but never been used or been
+ declared in any header file: gst_element_default_error and gst_element_request_compatible_pad
+
+Bugs fixed since 0.10.28:
+
+ * 576234 : [basetransform] Suggesting non-fixed caps or no size doesn't work for upstream negotiation
+ * 520697 : [API] Add GST_TAG_USER_RATING
+ * 590718 : docs build failures with -jN: cp: cannot create regular file `build/image.entities': File exists
+ * 595958 : Position not updated after a backwards gst_event_new_step()
+ * 596832 : configurable buffer alignment
+ * 600718 : autoconf fails with gobject-introspection
+ * 600877 : [uridecodebin] Needs to disable download buffering for non-fast-start files
+ * 603710 : Can't compile with introspection support
+ * 603831 : build with libtool 1.x.y only works if --disable-shave is used
+ * 609046 : basetransform now ignores suggestions from capsfilter
+ * 609170 : basesrc pushes two newsegment
+ * 610256 : Use G_VALUE_COLLECT_INIT if available
+ * 611075 : Typo in debug_dump_pad function
+ * 611911 : Set thread names on pipeline threads
+ * 612370 : gstutils.c inline asm typo, compilation fails
+ * 612410 : [API][tags] add new geo tags
+ * 612733 : Build fails because HAVE_REGISTER_PRINTF_SPECIFIER is undefined
+ * 612881 : [utils] gst_pad_proxy_setcaps() doesn't handler iterator resyncs
+ * 613215 : delayed set in gst-launch are not recursive
+ * 613593 : git-update.sh script does not work on fresh git repository clones
+ * 614167 : gstinfo: no previous prototype for 'xxx' when buildign with --disable-gst-debug
+ * 614629 : utils: Use G_GNUC_CONST instead of G_GNUC_PURE for conversion functions
+ * 614767 : libgstreamer build failure on OS X x86_64
+ * 614833 : out of srcdir build fails for libs/gst/check
+ * 615698 : " warning: cast increases required alignment of target type " with gcc 4.2.1 on arm
+ * 615756 : [bin] refcount issue when removing element in error
+ * 615880 : Add some more custom flow returns
+ * 615881 : [LFOControlSource] Use correct setter for double GValues
+ * 616846 : Crash in gst_interpolation_control_source_find_control_point_iter
+
+API additions since 0.10.28:
+
+ * GST_MESSAGE_QOS
+ * gst_message_new_qos()
+ * gst_message_parse_qos()
+ * gst_message_parse_qos_stats()
+ * gst_message_parse_qos_values()
+ * gst_message_set_qos_stats()
+ * gst_message_set_qos_values()
+ * GST_FLOW_CUSTOM_SUCCESS_1
+ * GST_FLOW_CUSTOM_SUCCESS_2
+ * GST_FLOW_CUSTOM_ERROR_1
+ * GST_FLOW_CUSTOM_ERROR_2
+ * GST_TAG_USER_RATING
+ * GST_TAG_GEO_LOCATION_COUNTRY
+ * GST_TAG_GEO_LOCATION_CITY
+ * GST_TAG_GEO_LOCATION_SUBLOCATION
+
+API deprecated since 0.10.28:
+
+ * gst_element_class_set_details()
+
+Changes since 0.10.27:
+
+ * parse "1/MAX" fraction strings
+ * no material changes compared to 0.10.27, this release is mostly to
+ keep core/base version numbers in sync
+
+Changes since 0.10.26:
+
+ * basesrc: protect segment values from concurrent access from different threads
+ * typefind: protect internal fields from concurrent changes from different threads
+ * typefind: fix pad activation corner-case with have-type already having been emitted
+ * typefind: reset the working mode when going to READY/NULL, fixes re-use from
+ READY state as with decodebin2
+ * gstpoll: fix crash when logging is enabled for GST_POLL
+ * bytewriter: expose gst_byte_writer_put_{float32|float64}_*() properly in header
+ * basesink: fix emergency rendering timestamp tracking
+ * fdsink, fdsrc: fix compilation with MSVC
+ * memindex: avoid busy loop when doing EXACT lookup
+
+Bugs fixed since 0.10.26:
+
+ * 610366 : [gstcollectpads][doc] Add a reminder for 'data' doc
+ * 605189 : gst_element_get_state has wrong introspection
+ * 607771 : [API] Add gst_byte_writer_fill
+ * 608036 : [typefind] deadlock when upstream puts caps on buffers on pull mode
+ * 608877 : [typefind] Access to internal fields not threadsafe
+ * 609941 : GStreamer-WARNING **: External plugin loader failed.
+ * 610210 : [PATCH] Fix compilation of fdsink and fdsrc with MSVC
+ * 610246 : [optimization] Speed up _get_range()
+ * 610367 : [memindex] might busy loop upon EXACT lookup
+ * 610444 : [controller] Interpolation control source passes NULL pointers to GSequence API
+ * 611087 : [basesink] emergency rendering of late buffers fails after resuming from PAUSE
+ * 611719 : GST_DEBUG_OBJECT macros not fed with GObject* in gstpoll.c
+
+API additions since 0.10.26:
+
+ * gst_byte_writer_fill()
+
+Changes since 0.10.25:
+
+ * registry: do plugin scanning (on *nix) using an external helper binary
+ * lots of performance improvements all over the place (ghostpads,
+ multiqueue, pad construction, superfluous type checks, registry loading)
+ * add GstByteWriter, a simple generic byte writer
+ * filesink: Use _wfopen on win32 to open files with non-ascii filenames correctly.
+ * queue2: add option to remove the temp-file (enabled by default)
+ * it is now allowed to use gst_caps_set_simple() on non-simple caps
+ * queue2: move from gst-plugins-base into the coreelements plugin in core
+ (this means you may need to remove libgstqueue2.so manually if you
+ installed from source and don't do make uninstall before upgrading, or
+ combine an older -base with a newer core)
+ * multiqueue: add support for buffering mode where we post BUFFERING
+ messages based on the level of the queues
+ * typefind: speed up typefinding a lot by first trying the typefinder for
+ the file's extension
+ * buffer: remove private/internal subbuffer subclass and keep track of
+ the parent buffer directly in the GstBuffer structure (this removes
+ quite a bit of special-casing and will allow for future improvements/
+ extensions that are harder to do if there's a separate subbuffer class.
+ * collectpads: add ability to install clipping functions
+ * new tags for TV/Radio shows/episodes, lyrics, composer sortname and
+ grouping
+ * miniobject: avoid race when recycling buffers
+ * basesrc: fix race in PLAYING->PAUSED->PLAYING
+
+Bugs fixed since 0.10.25:
+
+ * 476514 : [multiqueue] Doesn't forward EOS event in all cases
+ * 590941 : API: add gst_pad_get_caps() variant that avoids unneeded caps copies
+ * 595602 : g_child_proxy_get_valist doesn't initialize GValue correctly
+ * 535069 : basesrc no longer support non-flushing seeks on itself
+ * 560442 : GNOME Goal: Remove deprecated GLib symbols
+ * 595511 : Annotations for gst_element_query_{position,duration}
+ * 595886 : gst_pad_fixate_caps() does not return fixed caps in case of multiple structures
+ * 595964 : [multiqueue] can hang pipeline during startup
+ * 596366 : proxy_getcaps reverses direction of getcaps
+ * 597407 : GstPipeline calculates base_time incorrectly when a new clock appears during PAUSED state
+ * 597550 : basesrc: sometimes no buffers produced after PLAYING - PAUSED - PLAYING
+ * 597690 : Improve caps setters API
+ * 598297 : make check fails when any --disable option which changes the API has been used
+ * 598526 : bytewriter: fails to compile with gcc 4.2.4 on Ubuntu Hardy 64 bits
+ * 598700 : scripts: Parallelise git-update.sh build script
+ * 598895 : [GstRegistry] Use hash table for feature lookups
+ * 598896 : [GstRegistry] Cache lists of ElementFactory and TypeFindFactory
+ * 599147 : typefind : Avoid having to re-sort the typefind factory list
+ * 599759 : [qtdemux] Add support for more tags
+ * 600313 : Visualisations stop updating after seek
+ * 600922 : gst-launch: wake up less often to check for Ctrl-C
+ * 601587 : MiniObject race condition
+ * 601668 : [gstregistry] gstregistry.c uses a variable from gst.c
+ * 601669 : [tests] tests/examples/manual depends on libgstcheck
+ * 602093 : libgstcheck fails to export some symbols when built under et_EE locale
+ * 602275 : [API] Add new sink-message event
+ * 602419 : [basesink] Regression with position reporting
+ * 603059 : Totem crashes when DVD is encrypted but libdvdcss isn't available
+ * 603787 : [registry] Doesn't use GMappedFile
+ * 604091 : tee: cleanup requestpads in dispose
+ * 604093 : gst-inspect/launch: move gst_tools_print_version to avoid glib warning
+ * 605251 : tee causes segfault if there is no source pad
+ * 605930 : [shave] common/shave not existing yet when configure checks need it
+ * 606435 : gsttee not threadsafe
+ * 607283 : segfaults and/or miniobject warnings with GLib > = 2.23.2
+ * 607317 : [PATCH] fix unaligned detection for x86-64 when cross compiling
+ * 607431 : update common modules before freeze
+ * 607481 : Should define G_THREADS_MANDATORY everywhere
+ * 607739 : [queue2] Temporary file is removed although code claims the opposite
+ * 607842 : Audio comes out with short breaks after resume pipeline (paused- > playing)
+ * 608136 : multiqueue handles UNEXPECTED flowreturn wrongly
+ * 608398 : Initializing the glib thread system seems not to work
+ * 608442 : [filesrc] typo in warning message
+ * 608726 : bytewriter: mistake in .h/.c function naming
+ * 609166 : Buffer list docs ascii art
+ * 590669 : [API] need GstByteWriter or GstChunkWriter
+ * 601698 : Rename new plugin-scanner helper executable before release
+ * 604565 : [gstcheck] Update check to 0.9.8
+ * 596877 : New internal libcheck breaks the Solaris build
+
+API additions since 0.10.25:
+
+ * GST_DEBUG_REGISTER_FUNCPTR()
+ * gst_base_src_new_seamless_segment()
+ * gst_event_new_sink_message()
+ * gst_event_parse_sink_message()
+ * gst_util_fraction_add()
+ * gst_util_fraction_multiply()
+ * gst_util_greatest_common_divisor()
+ * gst_util_double_to_fraction()
+ * gst_util_fraction_to_double()
+ * gst_registry_get_feature_list_cookie()
+ * gst_default_registry_get_feature_list_cookie()
+ * gst_pad_get_caps_reffed()
+ * gst_pad_peer_get_caps_reffed()
+ * gst_structure_id_has_field()
+ * gst_structure_id_has_field_typed()
+ * gst_plugin_feature_list_copy()
+ * gst_caps_set_value()
+ * gst_byte_writer_ensure_free_space()
+ * gst_byte_writer_free()
+ * gst_byte_writer_free_and_get_buffer()
+ * gst_byte_writer_free_and_get_data()
+ * gst_byte_writer_get_remaining()
+ * gst_byte_writer_init()
+ * gst_byte_writer_init_with_buffer()
+ * gst_byte_writer_init_with_data()
+ * gst_byte_writer_init_with_size()
+ * gst_byte_writer_new()
+ * gst_byte_writer_new_with_buffer()
+ * gst_byte_writer_new_with_data()
+ * gst_byte_writer_new_with_size()
+ * gst_byte_writer_put_data()
+ * gst_byte_writer_put_float32_be()
+ * gst_byte_writer_put_float32_le()
+ * gst_byte_writer_put_float64_be()
+ * gst_byte_writer_put_float64_le()
+ * gst_byte_writer_put_int16_be()
+ * gst_byte_writer_put_int16_le()
+ * gst_byte_writer_put_int24_be()
+ * gst_byte_writer_put_int24_le()
+ * gst_byte_writer_put_int32_be()
+ * gst_byte_writer_put_int32_le()
+ * gst_byte_writer_put_int64_be()
+ * gst_byte_writer_put_int64_le()
+ * gst_byte_writer_put_int8()
+ * gst_byte_writer_put_string_utf16()
+ * gst_byte_writer_put_string_utf32()
+ * gst_byte_writer_put_string_utf8()
+ * gst_byte_writer_put_uint16_be()
+ * gst_byte_writer_put_uint16_le()
+ * gst_byte_writer_put_uint24_be()
+ * gst_byte_writer_put_uint24_le()
+ * gst_byte_writer_put_uint32_be()
+ * gst_byte_writer_put_uint32_le()
+ * gst_byte_writer_put_uint64_be()
+ * gst_byte_writer_put_uint64_le()
+ * gst_byte_writer_put_uint8()
+ * gst_byte_writer_reset()
+ * gst_byte_writer_reset_and_get_buffer()
+ * gst_byte_writer_reset_and_get_data()
+ * gst_bit_reader_get_size()
+ * gst_byte_reader_get_size()
+ * gst_data_queue_new_full()
+ * gst_collect_pads_set_clip_function()
+ * gst_type_find_helper_get_range_ext()
+
+Changes since 0.10.24:
+
+ * Improve the byte-reader API
+ * GObject introspection support
+ * Improve clock accuracy on win32
+ * Optimisations in capabilities checking
+ * Optimisations and fixes in the basetransform base class
+ * new 64-bit scaling utility function variants
+ * Various bug-fixes and improvements (see ChangeLog and bugs list below)
+
+Bugs fixed since 0.10.24:
+
+ * 583999 : [basetransform] caps refcounting problem causing GST_IS_CAPS assertion failures
+ * 566881 : [GstIndex] support/caching in GstBin
+ * 588472 : [basetransform] problems in reverse-negotiating
+ * 589173 : macros cause spurious semicolon warnings
+ * 589314 : [basetransform] clears GAP flag in passthrough mode
+ * 589524 : gst_base_transform_acceptcaps() could provide more verbose debugging output
+ * 589849 : [segment] Clipping fails to handle start=stop < segment_start correctly
+ * 589991 : [queue] limited error handling might cause pipeline appearing to hang
+ * 590045 : Query position fails when pipeline is paused and format is not time
+ * 590430 : Add support for " album artist " tags
+ * 590841 : configure script check for libxml2 is incorrect
+ * 590919 : gst_util_uint64_scale_int() and friends don't round
+ * 591045 : [basesrc] Leaking GstTask instances
+ * 591318 : ghostpad : core dump : on_src_target_notify called with an invalid ghostpad
+ * 591441 : append mode for filesink
+ * 592209 : [GstPad] Deprecated markers missing in the header for internal links function related things
+ * 592314 : core/tests/examples/streams/ does not link to pthread
+ * 593460 : Broken win32-specific systemclock code
+ * 593719 : regression: segfault when using gstrtpbin and certain video codecs
+ * 594107 : [gstbin] : use of freed message : valgrind Invalid read
+ * 594225 : [API] [bytereader] add _unchecked() variants and inline most common functions
+ * 594990 : [introspection] pkg-config file madness and another bug
+ * 595130 : checks fail
+ * 595133 : gst/gstutils check fails
+ * 595209 : Fix out-of-tree build
+ * 368536 : bin_change_state makes children go through unnecessary state changes
+
+API additions since 0.10.24:
+
+ * gst_caps_can_intersect()
+ * gst_util_uint64_scale_int_round()
+ * gst_util_uint64_scale_int_ceil()
+ * gst_util_uint64_scale_round()
+ * gst_util_uint64_scale_ceil()
+ * gst_iterator_new_single()
+ * gst_byte_reader_skip_unchecked()
+ * gst_byte_reader_peek_*_unchecked()
+ * gst_byte_reader_get_*_unchecked()
+ * gst_byte_reader_{peek,get,dup}_data_unchecked()
+ * gst_byte_reader_get_float*_unchecked()
+
+Changes since 0.10.23:
+
+ * Fully support nested structures in caps
+ * Support frame-by-frame stepping in sinks
+ * Add support for buffer-lists to pass around groups of buffers
+ * Use TaskPools for managing worker threads
+ * New stream-status API for finer thread control
+ * Code optimisations
+ * Many other bug-fixes and enhancements
+
+Bugs fixed since 0.10.23:
+
+ * 580579 : crash in Volume Control: aucunes idées désolé.
+ * 527488 : [GstXML] can't load elements with request pads from XML
+ * 570233 : allow plugins caching data in the registry
+ * 584389 : don't recreate plugin feature and element factories on fi...
+ * 534208 : [API] add gst_structure_get()
+ * 545787 : [API] add gst_plugin_register_static_full() for bindings
+ * 554460 : thumbnailer crash in gst_fake_sink_event() on FLUSH_START...
+ * 559643 : Don't allow empty or NULL strings in taglists
+ * 560345 : gst_tag_list_get_string() may return NULL or empty string
+ * 560442 : GNOME Goal: Remove deprecated GLib symbols
+ * 572285 : Buffer Lists
+ * 577926 : Remove old xml registry
+ * 578908 : [fdsink] implement seeking on seekable fds
+ * 580177 : glibc 2.10 deprecates register_printf_function
+ * 580716 : race condition in gst_element_lost_state
+ * 581198 : [tags] Add gst_tag_setter_add_tag_value() and gst_tag_lis...
+ * 581281 : [GstURIHandler] Doesn't use get_type_full() at all
+ * 582010 : audiotestsrc is-live=1 ! pulsesink unreliable
+ * 582564 : [controller] Use ordered GSequence instead of GList in th...
+ * 582588 : [API] Add a way to get the pad corresponding to a taglist
+ * 582878 : [GstClock] ABI breakage in GIT on x86
+ * 583187 : [API] add gst_adapter_masked_scan_uint32() and gst_adapte...
+ * 583419 : Bad translatable string in gst-launch.c
+ * 583456 : framestep functionality
+ * 583554 : Slow down or lock if date time is changed to the past
+ * 584835 : MSVC compiler fails with 'static inline' function
+ * 584838 : basesrc: confusing QUERY_SEEKING handling
+ * 585039 : rtpool-test can't find pthreads
+ * 585075 : Compilation with MSVC fails for files including config.h ...
+ * 585137 : gst_xml_write_file() fails serialising GstStructure property
+ * 585592 : [API] add gst_byte_reader_masked_scan_uint32()
+ * 585733 : Wrong #include order in gstsegment.c
+ * 585748 : [API] add gst_tag_list_new_full() to create taglist with ...
+ * 586566 : Add GAP Flag support to gstcapsfilter
+ * 586568 : [bytereader] add misc. string functions and gst_byte_read...
+ * 587973 : use G_DIR_SEPARATOR_S instead of " /' "
+ * 587976 : Fix for gst-inspect and gst-launch when option parsing is...
+ * 588744 : [check] Stream consistency checker utility
+ * 588745 : [basesrc] Serialize tags in the dataflow
+ * 589127 : gsttask leaks the pool
+ * 590056 : [collectpads] race resulting in double flush-stop being o...
+ * 590622 : [bytereader] buffer size checks subject to wrap-around ov...
+ * 579177 : GstInfo: maintain ABI compatibility
+ * 581321 : typefind element leaks force-caps property
+ * 584118 : [gstadapter][doc] Improve documentation of gst_adapter_ma...
+ * 585433 : [queue] Can lock down if min-threshold conflicts with max...
+ * 585569 : rtsp/rtp streaming fails when skipping explicit PAUSED st...
+ * 585834 : Support for GstBufferList in ghostpads
+ * 585960 : Support for GstBufferList in gstbasesink
+ * 587052 : [filesink.c] Support for files > 4GB on windows makes file...
+
+API added since 0.10.23:
+
+ * GST_DEBUG_CATEGORY_GET() macro
+ * gst_byte_reader_dup_data
+ * gst_byte_reader_dup_string
+ * gst_byte_reader_dup_string_utf8
+ * gst_byte_reader_dup_string_utf16
+ * gst_byte_reader_dup_string_utf32
+ * gst_byte_reader_skip_string
+ * gst_byte_reader_skip_string_utf8
+ * gst_byte_reader_skip_string_utf16
+ * gst_byte_reader_skip_string_utf32
+ * gst_byte_reader_peek_string
+ * gst_byte_reader_peek_string_utf8
+ * gst_byte_reader_get_string
+ * gst_byte_reader_get_string_utf8
+ * add gst_tag_list_new_full()
+ * add gst_tag_list_new_full_valist()
+ * add gst_byte_reader_masked_scan_uint32()
+ * add gst_plugin_get_cache_data, gst_plugin_set_cache_data
+ * gst_structure_get()
+ * gst_structure_id_get()
+ * gst_structure_get_valist()
+ * gst_structure_id_get_valist()
+ * GstSegment::gst_segment_set_running_time()
+ * Add GST_MESSAGE_SRC_NAME() macro
+ * GstSegment::gst_segment_to_position()
+ * GstEvent::gst_event_new_step()
+ * GstEvent::gst_event_parse_step()
+ * GstMessage::gst_message_new_step_done()
+ * GstMessage::gst_message_parse_step_done()
+ * gst_structure_id_new()
+ * Add gst_message_{new,parse}_tag_full() to get/set the source pad
+ * GstAdapter::gst_adapter_masked_scan_uint32()
+ * GstElement::gst_element_lost_state_full()
+ * GstAdapter::gst_adapter_prev_timestamp()
+ * gst_plugin_register_static_full()
+ * gst_tag_list_add_value()
+ * gst_tag_setter_add_tag_value()
+ * add GST_TAG_CONTAINER_FORMAT tag
+ * GstTask::gst_task_set_state()
+ * GstObject::gst_object_ref_sink()
+
+Changes since 0.10.22:
+ * Support files > 4GB on Windows
+ * Controller interpolation fixes
+ * Add timer support to GstPoll and use it for clocking
+ * Attempt to typefind contents from the file extension if all else fails
+ * GStreamer revision control switched to Git
+ * Many other bug fixes and improvements
+
+Bugs fixed since 0.10.22:
+
+ * 579177 : GstInfo: maintain ABI compatibility
+ * 163577 : [RFC] Interlaced/progressive media support in GStreamer.
+ * 574160 : collectpads does not reliably eos when last pad is removed
+ * 575598 : hierarchical pipelines accumulate segment-done wrongly
+ * 575922 : disabling subsystems cause API break
+ * 576842 : loading a broken registry file can crash
+ * 555978 : [ladspa] no elements exposed/found on Cygwin
+ * 565607 : Broken macros in gsturi.h and gstinterface.h
+ * 566936 : [ghostpads] unlink function wrongly called on target
+ * 567692 : gstinfo.h header not compatible with C++
+ * 567725 : [qtdemux] stopping at a time sometimes shows a different ...
+ * 568289 : gst_pad_template_new() leaks caps it's supposed to take o...
+ * 568438 : gst_poll_wait calling read() on control socket
+ * 568481 : GStreamer linking failures.
+ * 568632 : __MSVCRT_VERSION__ not defined with mingw, causing " stora...
+ * 568678 : filesrc doesn't logs offsets
+ * 570910 : Removing the target of a ghostpad does not re-target the ...
+ * 571227 : Add home page tag
+ * 571559 : [API] add GST_PARAM_MUTABLE_PLAYING etc. to indicate vali...
+ * 572480 : unref and copy functions should not be macros
+ * 573623 : [API] Array binary search utility function
+ * 574024 : [GstAdapter] gst_adapter_push should not accept empty buf...
+ * 574211 : gst_poll_*_control always returns FALSE on Windows
+ * 574213 : [gstcheck] fix for libcheck > 0.9.6
+ * 574241 : gst_tag_list_add and gst_tag_list_add_values behave incon...
+ * 574484 : [patch] Make caps in DOT debug graphs more readable
+ * 574623 : [dot_file_with_ts] ':' not a valid character for a filename
+ * 574805 : [capsfilter] Doesn't reset the internal suggestion with A...
+ * 575695 : build fails on OpenSolaris due to incorrect header file i...
+ * 575814 : flag for EOS on gst-launch when exiting with ctrl-c
+ * 576381 : [basesink] QoS: emergency rendering not always done
+ * 576563 : pidgin crashes on exit in gst_plugin_ext_dep_free()
+ * 576582 : A patch to enable the use of 'name' in Enum parameters
+ * 577887 : Missing GST_DISABLE_GST_DEBUG in gstregistrybinary.c
+ * 577891 : add alloc-pad property on tee
+ * 578114 : API: add two new log levels: FIXME and MEMDUMP
+ * 578201 : _gst_plugin_fault_handler_is_setup undefined under HAVE_W...
+ * 579127 : gst-launch: disable CLOCK_LOST message handling
+ * 580121 : race condition in GStreamer state changes causes problems...
+ * 361155 : Add monotonic clock
+ * 517231 : threadsafe/colored windows logging
+ * 572591 : Another batch of " differs in signedness " warnings
+ * 573823 : pad block callback if it is re-blocked while the previous...
+ * 574163 : Fix gst_pad_activate_pull deactivation with unlinked element
+ * 575682 : Add gst_pad_is_compatible()
+ * 575988 : On Windows filesink can't write files longer than 2-4 GiB...
+
+API additions since 0.10.22:
+
+ * New FIXME and MEMDUMP debug levels
+ * gst_tag_list_get_buffer() and gst_tag_list_get_buffer_index()
+ * New tags: GST_TAG_SUBTITLE_CODEC, GST_TAG_HOMEPAGE
+ * gst_util_array_binary_search()
+ * gst_message_new_request_state(), gst_message_parse_request_state(), GST_MESSAGE_REQUEST_STATE
+ * GstPoll::gst_poll_new_timer()
+ * GstPoll::gst_poll_write_control()
+ * GstPoll::gst_poll_read_control()
+
+Changes since 0.10.21:
+
+ * GstController improvements
+ * Extensions to the latency setting behaviours
+ * Ability for plugins to register dependencies to trigger re-scanning
+ * Optimisations in some common operations on caps and values and elsewhere
+ * Add sequence numbers to events so dependent events can be associated with
+ the event that caused them
+ * New macros for reading and writing float values
+ * Many improvements in the basesink base class
+ * Support non-default main contexts for GstBus watches
+ * Improvements in pull-mode scheduling of sinks
+ * Fixes for alignment issues on sparc
+ * Ghost pad fixes
+ * New bit-reader assistance API
+ * Many other bug fixes and improvements
+
+Bugs fixed since 0.10.21:
+
+ * 567002 : --gst-disable-registry-update also skips registry creation
+ * 350477 : [Registry] Provide a way for plugins to delegate the 'cha...
+ * 510354 : post GST_MESSAGE_STRUCTURE_CHANGE when linking and unlink...
+ * 526044 : Crash if there is more than one watcher for a GstBus
+ * 539108 : gst_ghost_pad_new() does more than call g_object_new()
+ * 544003 : [parse] Links to wrong pad if no padtemplate name is given
+ * 544293 : rtspsrc / gstpoll regression
+ * 545714 : GST_READ_UINT_* and GST_WRITE_UINT_* are not always safe ...
+ * 548786 : [win32] search for plugins based on location of DLL
+ * 551676 : Small Memleak fix in gst_pad_link_check_compatible_unlocked
+ * 552778 : add free_func in gstbuffer instances
+ * 553554 : [base] Add a generic bit reader
+ * 553874 : query_position broken during seek
+ * 555196 : Move floating point endian conversion macros into core
+ * 555307 : Need to push latency event into the pipeline
+ * 555631 : Banshee crashes; gstreamer GST_CAPS GST_IS_CAPS warnings
+ * 556091 : libtool-2.2 and old gettext don't mix
+ * 556900 : a copy & paste bug in helloworld example
+ * 557154 : Allow totem to run without write-access to home directory
+ * 557300 : libgstnet needs to link against $(WIN32_LIBS)
+ * 557438 : Gstreamer crashes when Banshee supposed to change track
+ * 557649 : GstBaseTransform can cause ivalid memory references
+ * 559250 : segments need identifiers.
+ * 560301 : Add --plugin to gst-inspect
+ * 560360 : Excessive statting when reading binary cache
+ * 560399 : Unnecessary CRC checksum for binary registry cache
+ * 560442 : GNOME Goal: Remove deprecated GLib symbols
+ * 561501 : g_type_class_ref without unref
+ * 562170 : GstBus watch doesn't work with non-default main context
+ * 562949 : [API] Add an URI query type for querying the source/sink URI
+ * 564863 : Caps are not propagated from a ghostpad's target to the g...
+ * 567225 : volatile gonce_data in BOILERPLATE not initialized to 0
+ * 566393 : [deadlock] Setting index on a pipeline
+
+API added since 0.10.21:
+
+ * Add bit reader and byte reader classes.
+ * gst_message_new_structure_change()
+ * gst_message_parse_structure_change()
+ * GST_BUFFER_FREE_FUNC()
+ * Add GST_READ_UINT24_(LE|BE) and GST_WRITE_UINT24_(LE|BE).
+ * GstBaseSrc::gst_base_src_set_blocksize()
+ * GstBaseSrc::gst_base_src_get_blocksize()
+ * GstBaseSink::gst_base_sink_set_blocksize()
+ * GstBaseSink::gst_base_sink_get_blocksize()
+ * GstBaseSink::blocksize
+ * GstBaseSink::gst_base_sink_do_preroll()
+ * Add gst_byte_reader_get_data and gst_byte_reader_peek_data
+ * Move float endianness conversion macros from libgstfloatcast to core
+ * gst_util_seqnum_next, gst_util_seqnum_compare
+ * gst_event_get_seqnum, gst_event_set_seqnum
+ * gst_message_get_seqnum, gst_message_set_seqnum
+ * GstSeekFlags::GST_SEEK_FLAG_SKIP
+ * gst_bin_recalculate_latency()
+ * GstBin::do-latency
+ * gst_tag_setter_reset_tags()
+ * gst_query_new_uri, gst_query_set_uri, gst_query_parse_uri
+ * add gst_plugin_add_dependency()
+ * add gst_plugin_add_dependency_simple()
+
+
+Changes since 0.10.20:
+
+ * Basetransform rework
+ * Basesink synchronisation extensions
+ * New documentation
+ * Many bug fixes, enhancements and optimisations
+
+Bugs fixed since 0.10.20:
+
+ * 481169 : [tag] add support for geo tags (gps location etc.)
+ * 520694 : adding GST_TAG_KEYWORDS
+ * 538201 : deleting the control point at ts=0 does not lower the con...
+ * 544855 : fakesrc and fakesink should call super::event()
+ * 339795 : [GstBaseTransform] Reverse negotiation issues in passthro...
+ * 348114 : [PPC64?] [gcc-4.1.2?] GST_BUFFER_IN_CAPS flag should have...
+ * 361718 : [basetransform] needs API to force renegotiation
+ * 533856 : gst_buffer_join() documentation is unclear
+ * 536978 : GTKDOC_CFLAGS should include CFLAGS
+ * 537804 : [multiqueue] wrongly reporting that the queue is full.
+ * 537812 : [check] add api to setup a pad by name
+ * 538568 : Add GST_TAG_ATTACHMENT
+ * 539772 : gst_pad_template_new() does more than call g_object_new()
+ * 542175 : gst-inspect --gst-plugins-path fails with multiple direct...
+ * 543444 : gst_base_sink_get_position can return 0 unexpectedly
+ * 543853 : Bison version check failure on OSX 10.4 Tiger
+ * 544174 : [basesrc] allow dynamic value of the seekable value.
+ * 544776 : [win32] binary registry may fail if glib is using a diffe...
+ * 545352 : gsturi is too restrictive
+ * 545603 : gst-inspect: don't print uri handler when compiled withou...
+ * 545605 : gstelementfactory: don't use uri handler code without uri...
+ * 545607 : gst: include gstconfig when using macros defined therein
+ * 545853 : [basetransform] rewrite
+ * 546328 : fractions with G_MAXINT cause failure for fixation
+ * 546822 : gstreamer doesn't tell gettext to output its translations...
+ * 547277 : filesrc detect if a file is seekable using SEEK_SET and n...
+ * 547728 : [basetransform] fail on buffer_alloc
+ * 548394 : basesink should ignore EOS during flushing
+ * 548652 : [Inconsistency] GST_TAG_LOCATION is used for different me...
+ * 549504 : Thread-safe version of gst_pad_get_internal_links()
+ * 551952 : Need 'check' package when compile
+ * 551978 : Memleak in gst_element_sync_state_with_paren
+ * 547835 : tee release_request_pad while buffer_alloc racyness
+ * 538628 : Patch: added a timeout property to fdsrc used in gst_poll...
+ * 546883 : [basetransform] ximagesink fails when resizing video window
+ * 551509 : gst_base_transform_prepare_output_buffer: assertion faile...
+
+API added since 0.10.20:
+
+ * Add GST_TAG_ATTACHMENT for generic file attachments to streams.
+ * Add gst_base_sink_set_render_delay()
+ * Add gst_base_sink_get_render_delay()
+ * Add gst_check_setup_src_pad_by_name
+ * Add gst_check_setup_sink_pad_by_name
+ * Add gst_check_teardown_pad_by_name
+ * Add GstBaseTransform::gst_base_transform_suggest()
+ * GstBaseTransform::gst_base_transform_reconfigure()
+ * GstPad::gst_pad_set_iterate_internal_links_function()
+ * GstPad::GstPadIterIntLinkFunction
+ * GstPad::gst_pad_iterate_internal_links()
+ * GstPad::gst_pad_iterate_internal_links_default()
+
+API deprecated since 0.10.20:
+
+ * gst_pad_get_internal_links()
+ * gst_pad_set_internal_link_function()
+ * gst_pad_get_internal_links_default()
Changes since 0.10.19: