]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blobdiff - NEWS
Release 0.10.32
[glsdk/gstreamer0-10.git] / NEWS
diff --git a/NEWS b/NEWS
index b408b3e771e29fa73d25b007a325173cf7654318..1c40a3723fd7be225eb7fb31f489017c235cb919 100644 (file)
--- a/NEWS
+++ b/NEWS
-This is GStreamer 0.10.16 "Special Dispensation"
+This is GStreamer 0.10.32 "Take Me to the Bonus Level"
+
+Changes since 0.10.31:
+
+      * GLib requirement is now >= 2.22
+      * New core element: valve (moved from -bad)
+      * New core element: input-selector (N.B. without "select-all" property,
+        use fsfunnel instead) (moved from -bad)
+      * New core element: output-selector (N.B. with different negotiation
+        behaviour by default, set pad-negotiation-mode=active for previous
+        behaviour) (moved from -bad)
+      * Performance improvements for many heavily-used code paths: GstPad,
+        GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue
+      * gobject-introspection: add annotations for most core API
+      * clock: make sync clock wait lockfree
+      * fdsrc/fdsink: reenable on MSVC
+      * registry: fix GStatBuf definition for win32 when building against older
+        glib (fixes unnecessary rescanning of plugins at start-up)
+      * element: add a more flexible way to get request pads from elements
+      * multiqueue: return upon input when already eos
+      * object: fix creation of default name (when creating more than 100000 elements)
+      * pluginloader: fix hangs on OSX
+      * poll: fixes for (p)select backend (used e.g. on OSX)
+      * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
+      * registry: don't replace valid existing plugins by blacklisted ones
+      * tags: don't produce duplicated entries when merging same value twice
+      * basesink: preroll fixes for async=false case
+      * basesink: rework position reporting code
+      * basetransform: handle downstream giving a buffer with new caps but invalid size
+
+Bugs fixed since 0.10.31:
+
+      * 635785 : basesrc: fix deadlock
+      * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
+      * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
+      * 564056 : Protect against umask(0177)
+      * 607513 : input-selector segfaults in g_object_notify()
+      * 632168 : [gsttask] MSVC thread names for task debugging
+      * 632447 : reduce static memory allocated by the registry
+      * 632557 : [macros] Define restrict keyword if not available
+      * 632778 : Optimisations to GstBaseSink
+      * 632779 : gstdataqueue: Only emit g_cond_signal when needed
+      * 632780 : queue: Remove useless checks from e406f7
+      * 633918 : [fakesink] [PATCH] print sink-message events like a  message and its structure
+      * 634965 : sinks render buffers in state PAUSED when async is FALSE
+      * 635001 : basesink: fix position reporting in PAUSED
+      * 636268 : configure test fails on FreeBSD
+      * 636455 : basesrc: Avoid taking object locks for just checking tag presence
+      * 637057 : [plugin-scanner] gstpoll fails with select backend
+      * 637300 : [API] request pad based on caps
+      * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
+      * 637776 : merging the same tag values again produces lists containing duplicates
+      * 638381 : {input,output}-selector: double-check API before release
+      * 638399 : a few typos in GStreamer
+      * 638900 : [GstPoll] Doesn't compile with MinGW
+      * 638941 : registry scan/loading race and inconsistency
+
+API additions since 0.10.31:
+
+      * gst_clock_single_shot_id_reinit()
+      * gst_element_request_pad()
+      * GstElementClass::request_new_pad_full()
+      * gst_poll_get_read_gpollfd()
+      * gst_value_list_merge()
+      * GST_CLOCK_DONE
+
+Changes since 0.10.30:
+
+      * bin: add "message-forward" property to force forwarding of messages that would usually be filtered such as ASYNC_DONE or EOS
+      * bin: improve tracking of source elements for more efficient event dispatch
+      * bufferlist: add function to add a list of buffers
+      * clock: fix racy shutdown clock id leak
+      * element: add support for arbitrary element class / factory details
+      * element: link_many should activate pads if needed
+      * gst: add math-compat.h header
+      * datetime: add GstDateTime API
+      * elementfactory: add utility functions to filter features by type
+      * plugin: load the gst-python plugin loader with G_MODULE_BIND_LAZY
+      * query: add buffering ranges API to retrieve informations about the areas of the stream currently buffered
+      * value: add int64 range type
+      * info: write debugging output to file if GST_DEBUG_FILE environment variable is set
+      * pad: use more efficient g_object_notify_by_pspec() for caps notifies if compiling against new-enough GLib
+      * pipeline: If the currently used clock gets lost update it the next time when going from PAUSED to playing
+      * plugin: add release datetime field to GstPluginDesc and set it if GST_PACKAGE_RELEASE_DATETIME is defined
+      * utils: speed up pad linking utility functions by not trying pads that will never work
+      * adapter: add function to get a list of buffers; support 0-sized buffers
+      * adapter: optimize gst_adapter_take() and gst_adapter_peek() a little
+      * basesink: only answer the SEGMENT query in pull mode
+      * basesrc: return values in stream time for the POSITION query
+      * basetransform: allow the subclass to add new fields to caps when getting new caps from downstream
+      * basetransform: avoid useless memcpy
+      * basetransform: upstream caps-renegotiation fixes
+      * bitreader: add inlined and unchecked versions of the most important functions
+      * bytewriter: add inline and unchecked variants of all important functions
+      * bytewriter: fix possible infinite loop caused by an overflow
+      * queue: add "silent" property to suppress signal emission (for better performance)
+      * queue: avoid unnecessary g_cond_signal() (for better performance)
+      * queue: push newsegment event when linking in PLAYING
+      * queue2: extend ring buffer to support RAM mode
+      * queue2: in download mode, prevent range corruption due to race
+      * queue2: don't send seeks beyond the end of the file upstream in pull mode (fixes apple trailers and youtube/html5 playback in webkit)
+      * multiqueue: flush the data queue if downstream return WRONG_STATE too
+      * gst-inspect: print GST_PARAM_MUTABLE_* property flags
+
+Bugs fixed since 0.10.30:
+
+      * 396774 : Make GstElementDetails extensible
+      * 482147 : [queue] Issue with current time level if source task is not started
+      * 579127 : gst-launch: disable CLOCK_LOST message handling
+      * 594504 : Need a GType of " Date AND Time AND Timezone "
+      * 600004 : underrun signal emits when i tested queue overrun test case from file /gstreamerXXXX/tests/check/element/queue.c
+      * 610366 : [gstcollectpads][doc] Add a reminder for 'data' doc
+      * 611918 : leaky queue might not push newsegment event
+      * 618919 : Registry/Plugin Loading Memory Leak
+      * 619522 : basetransform fix for upstream caps-renegotiation
+      * 621299 : make simple queues faster
+      * 621332 : BaseTransform should disable proxy alloc if downstream changes caps
+      * 622740 : GstPad: Do not call gst_pad_accept_caps() when caps change
+      * 623040 : Add release_datetime field to GstPluginDesc
+      * 623121 : [queue2] downloaded areas of the media are not exposed
+      * 623491 : make *_get_type() thread safe
+      * 623541 : [basetransform] Implement POSITION query
+      * 623622 : [basesink/basesrc] Should return values in stream time for POSITION query
+      * 623806 : [pipeline] Doesn't update the clock if the currently used one gets lost and the start time did not change
+      * 623875 : gstregistrybinary.c compatibility with glib > = 2.25.0
+      * 624203 : gstutils: Make gst_pad_proxy_getcaps() return empty caps if it's what the other side has
+      * 625239 : FTBFS: ./gstreamer-decl.txt:9461: warning: GstTagList has multiple definitions.
+      * 625295 : [info] regression: doesn't flush output stream after every debug print any longer
+      * 625368 : gstdatetime.c doesn't compile in VS 2008
+      * 625862 : [docs] unused symbol GST_CAT_LEVEL_LOG_valist breaks the build
+      * 626027 : [tag] Add GST_TAG_APPLICATION_NAME
+      * 626181 : GstElementFactory: add listing/filtering API
+      * 626651 : [tag] Photography/capture settings tags
+      * 626784 : element: link_many might assert elements are in paused or playing
+      * 627438 : gst: Add a gst_is_initialized() API
+      * 627826 : GstInt64Range type
+      * 627910 : Warnings emitted when -Wcast-qual used
+      * 627959 : [queue2] on-disk buffering failing for AVI container
+      * 628014 : Deprecate GST_FLOW_IS_FATAL/GST_FLOW_IS_SUCCESS
+      * 628174 : New gstvalue checks cause trouble in thoggen
+      * 628176 : [basetransform] Problems with buffer handling in inplace mode
+      * 628408 : Use GDateTime that has been released
+      * 629241 : Build broken with introspection using gobject-introspection from master
+      * 629410 : GstBaseTransform: position query refers to sink pad, not source pad
+      * 629494 : Latest gst-launch.c doesn't build in Visual Studio 2008
+      * 629553 : GstAdapter: timestamp not updated when empty buffer is pushed
+      * 629831 : [API] add gst_structure_take_value() and gst_structure_id_take_value()
+      * 629946 : Enumerations have incorrect names of enum values (GEnumValue.value_name)
+      * 630257 : GST_DEBUG_DUMP_DOT_DIR not working anymore
+      * 630436 : basesink: renderdelay needs to be subtracted in adjust_time()
+      * 630437 : basetransform: Make a WARNING into a DEBUG statement
+      * 630439 : clock: fix racy shutdown clock id leak
+      * 631755 : Fix build with glib 2.21.3
+      * 631853 : [queue2] deadlock when using temp-location and dispatch-properties
+      * 632236 : [gst-inspect] unhelpful uri handler output
+      * 632433 : [basesink] hangs/drops going to PLAYING following flushing step in PAUSED
+      * 632977 : [queue2] qtdemux causes soup to request seeks past the end of the range
+      * 633147 : Simple reverse negotiation pipeline is broken.
+      * 633886 : Visual Studio emits warnings about double defined _USE_MATH_DEFINES
+      * 635031 : [datetime] Fix unix epoch handling
+      * 635389 : Include information on exported packages in GIRs
+      * 635869 : GST_BOILERPLATE_FULL causes warnings in user C++ code
+      * 633176 : recent multiqueue changes break DVD playback
+
+API additions since 0.10.30:
+
+      * gst_is_initialized
+      * gst_buffer_list_iterator_add_list
+      * GstBin:message-forward
+      * GST_TYPE_DATE_TIME
+      * gst_date_time_get_day
+      * gst_date_time_get_hour
+      * gst_date_time_get_microsecond
+      * gst_date_time_get_minute
+      * gst_date_time_get_month
+      * gst_date_time_get_second
+      * gst_date_time_get_time_zone_offset
+      * gst_date_time_get_type
+      * gst_date_time_get_year
+      * gst_date_time_new
+      * gst_date_time_new_from_unix_epoch_local_time
+      * gst_date_time_new_from_unix_epoch_utc
+      * gst_date_time_new_local_time
+      * gst_date_time_new_now_local_time
+      * gst_date_time_new_now_utc
+      * gst_date_time_ref
+      * gst_date_time_unref
+      * gst_tag_list_get_date_time
+      * gst_tag_list_get_date_time_index
+      * GST_TAG_GEO_LOCATION_HORIZONTAL_ERROR
+      * GST_TAG_APPLICATION_DATA
+      * GST_TAG_APPLICATION_NAME
+      * GST_TAG_DATE_TIME
+      * GST_ELEMENT_IS_SOURCE
+      * gst_element_class_set_documentation_uri
+      * gst_element_class_set_icon_name
+      * gst_element_factory_get_documentation_uri
+      * gst_element_factory_get_icon_name
+      * gst_element_factory_list_filter
+      * gst_element_factory_list_get_elements
+      * gst_element_factory_list_is_type
+      * GstElementFactoryListType
+      * GST_ELEMENT_FACTORY_TYPE_ANY
+      * GST_ELEMENT_FACTORY_TYPE_AUDIOVIDEO_SINKS
+      * GST_ELEMENT_FACTORY_TYPE_AUDIO_ENCODER
+      * GST_ELEMENT_FACTORY_TYPE_DECODABLE
+      * GST_ELEMENT_FACTORY_TYPE_DECODER
+      * GST_ELEMENT_FACTORY_TYPE_DEMUXER
+      * GST_ELEMENT_FACTORY_TYPE_DEPAYLOADER
+      * GST_ELEMENT_FACTORY_TYPE_ENCODER
+      * GST_ELEMENT_FACTORY_TYPE_FORMATTER
+      * GST_ELEMENT_FACTORY_TYPE_MAX_ELEMENTS
+      * GST_ELEMENT_FACTORY_TYPE_MEDIA_AUDIO
+      * GST_ELEMENT_FACTORY_TYPE_MEDIA_IMAGE
+      * GST_ELEMENT_FACTORY_TYPE_MEDIA_METADATA
+      * GST_ELEMENT_FACTORY_TYPE_MEDIA_SUBTITLE
+      * GST_ELEMENT_FACTORY_TYPE_MEDIA_VIDEO
+      * GST_ELEMENT_FACTORY_TYPE_MEDIA_ANY
+      * GST_ELEMENT_FACTORY_TYPE_MUXER
+      * GST_ELEMENT_FACTORY_TYPE_PARSER
+      * GST_ELEMENT_FACTORY_TYPE_PAYLOADER
+      * GST_ELEMENT_FACTORY_TYPE_SINK
+      * GST_ELEMENT_FACTORY_TYPE_SRC
+      * GST_ELEMENT_FACTORY_TYPE_VIDEO_ENCODER
+      * GST_ELEMENT_FACTORY_KLASS_DECODER
+      * GST_ELEMENT_FACTORY_KLASS_ENCODER
+      * GST_ELEMENT_FACTORY_KLASS_SINK
+      * GST_ELEMENT_FACTORY_KLASS_SRC
+      * GST_ELEMENT_FACTORY_KLASS_MUXER
+      * GST_ELEMENT_FACTORY_KLASS_DEMUXER
+      * GST_ELEMENT_FACTORY_KLASS_PARSER
+      * GST_ELEMENT_FACTORY_KLASS_PAYLOADER
+      * GST_ELEMENT_FACTORY_KLASS_DEPAYLOADER
+      * GST_ELEMENT_FACTORY_KLASS_FORMATTER
+      * GST_ELEMENT_FACTORY_KLASS_MEDIA_VIDEO
+      * GST_ELEMENT_FACTORY_KLASS_MEDIA_AUDIO
+      * GST_ELEMENT_FACTORY_KLASS_MEDIA_IMAGE
+      * GST_ELEMENT_FACTORY_KLASS_MEDIA_SUBTITLE
+      * GST_ELEMENT_FACTORY_KLASS_MEDIA_METADATA
+      * gst_plugin_feature_list_debug
+      * gst_plugin_feature_rank_compare_func
+      * gst_query_add_buffering_range
+      * gst_query_get_n_buffering_ranges
+      * gst_query_parse_nth_buffering_range
+      * gst_structure_get_date_time
+      * gst_structure_id_take_value
+      * gst_structure_take_value
+      * GST_TYPE_INT64_RANGE
+      * gst_int64_range_get_type
+      * gst_util_fraction_compare
+      * gst_value_get_int64_range_max
+      * gst_value_get_int64_range_min
+      * gst_value_set_int64_range
+      * GST_VALUE_HOLDS_DATE_TIME
+      * gst_adapter_take_list
+      * gst_bit_reader_skip_unchecked
+      * gst_bit_reader_skip_to_byte_unchecked
+      * gst_bit_reader_get_bits_uint16_unchecked
+      * gst_bit_reader_get_bits_uint32_unchecked
+      * gst_bit_reader_get_bits_uint64_unchecked
+      * gst_bit_reader_get_bits_uint8_unchecked
+      * gst_bit_reader_peek_bits_uint16_unchecked
+      * gst_bit_reader_peek_bits_uint32_unchecked
+      * gst_bit_reader_peek_bits_uint64_unchecked
+      * gst_bit_reader_peek_bits_uint8_unchecked
+      * gst_byte_writer_put_int8_unchecked
+      * gst_byte_writer_put_int16_be_unchecked
+      * gst_byte_writer_put_int16_le_unchecked
+      * gst_byte_writer_put_int24_be_unchecked
+      * gst_byte_writer_put_int32_be_unchecked
+      * gst_byte_writer_put_int32_le_unchecked
+      * gst_byte_writer_put_int64_be_unchecked
+      * gst_byte_writer_put_int64_le_unchecked
+      * gst_byte_writer_put_uint8_unchecked
+      * gst_byte_writer_put_uint16_be_unchecked
+      * gst_byte_writer_put_uint16_le_unchecked
+      * gst_byte_writer_put_uint24_be_unchecked
+      * gst_byte_writer_put_uint24_le_unchecked
+      * gst_byte_writer_put_uint32_be_unchecked
+      * gst_byte_writer_put_uint32_le_unchecked
+      * gst_byte_writer_put_uint64_be_unchecked
+      * gst_byte_writer_put_uint64_le_unchecked
+      * gst_byte_writer_put_float32_be_unchecked
+      * gst_byte_writer_put_float32_le_unchecked
+      * gst_byte_writer_put_float64_be_unchecked
+      * gst_byte_writer_put_float64_le_unchecked
+      * gst_byte_writer_put_data_unchecked
+      * gst_byte_writer_fill_unchecked
+
+API deprecated since 0.10.30:
+
+      * GST_FLOW_IS_FATAL
+      * GST_FLOW_IS_SUCCESS
+
+Changes since 0.10.29:
+
+      * GLib requirement was bumped to 2.20, automake requirement to 1.10
+      * bin: unlock gst_element_get_state() on error, instead of hanging forever if no timeout is given
+      * clock: fix refcounting bug in gst_clock_set_master
+      * caps: make sure _normalize() is applied on all structures
+      * info: add new TRACE log level and move refcounting there from LOG level
+      * pad: don't check twice for changed caps per push
+      * pad: fix iterator aggregation of all pads in the internal links fallback
+      * tagsetter: protect tagsetter operations with a lock
+      * value: support short fourccs (esp. serialisation/deserialisation)
+      * adapter: fix _try_to_merge_up(); optimize progressive masked scans
+      * basesink: implement percentage position and duration queries
+      * basesink: fix segment query return value
+      * basetransform: add accept_caps vmethod
+      * basetransform: re-evaluate proxy_alloc when reconfigured
+      * basetransform: assume in_size equals out_size if there's no transform_size/get_unit_size vfunc
+      * fdsink, filesink: make sync property work correctly
+      * typefind: make sure buffers' metadata is writable before setting caps on them
+      * queue2: fix merging of ranges
+      * queue2: don't wait for data when EOS
+      * queue2: don't ignore failure to open the temporary file location
+      * tools: make gst-launch print things correctly to stderr/stdout and make --quiet work correctly
+      * introspection: add many more gobject-introspection annotations
+      * xml: serialisation/deserialisation to/from XML has been deprecated, since it's always been broken
+        for all but the most trivial pipelines, and will likely never be fixed
+
+Bugs fixed since 0.10.29:
+
+      * 623586 : gst/tagsetter check fails
+      * 463435 : Skip #include < libxml/parser.h > in gstconfig.h.in when  not needed
+      * 505770 : gst_element_get_state() should unblock if element posts an error
+      * 615820 : implement percentage position and duration queries
+      * 615941 : [tags] Add GST_TAG_DEVICE_MANUFACTURER and GST_TAG_DEVICE_MODEL
+      * 616586 : Use GObject's boxed type for GError
+      * 617223 : [tags] Add tags for direction of capture and movement
+      * 617625 : Commandline utility wrappers (gst-run) don't work on Windows
+      * 618644 : gst_pad_get_caps() Return pad template if parent element is in GST_STATE_NULL
+      * 619508 : [tag] Add image orientation tag
+      * 619815 : GST_PLUGIN_LOADING_WHITELIST env var for unit tests
+      * 619828 : [API] adapter: add masked_scan_uint32_peek
+      * 620460 : info: add new TRACE log level and move refcounting there from LOG level
+      * 620490 : [basesink] segment query unconditionally returns FALSE
+      * 621006 : Deprecate unused gst_object_{get|set}_name_prefix()
+      * 621282 : Display of short fourccs is in hex instead of text
+      * 621332 : BaseTransform should disable proxy alloc if downstream changes caps
+      * 621334 : GstBaseTransform should not require a transform_size function
+      * 621505 : Disable memory poisoning by default for releases
+      * 621527 : gstcaps: New gst_caps_steal_structure() method
+      * 621530 : filesink ignores sync=true
+      * 621595 : --quiet doesnt make gst-launch be completely quiet, also messages should not go to stdout
+      * 621773 : Add introspection annotations
+      * 621867 : gst-launch: rename new --no-play command line option
+      * 621896 : [API][taglist] Add gst_tag_list_peek_string_index
+      * 622504 : [GstPad] Provide more fine-grained linking methods
+      * 622546 : distcheck fails in docs/plugins/
+      * 622685 : [GstXml] Deprecate GstXml
+      * 622967 : [queue2] Problems with progressive downloading
+      * 623301 : gst_caps_normalize : doesn't normalize completely
+      * 623589 : Fix races/refcounting bugs with slave clocks
+      * 624113 : [tags] wrong behaviour in merge function for strings
+      * 622025 : Can't build gstreamer due to Gst-0.10.gir: error: Can't resolve type 'PadIntLinkFunction' for field Gst.Pad.intlinkfunc
+
+API additions since 0.10.29:
+
+      * gst_caps_steal_structure()
+      * gst_clock_id_wait_async_full()
+      * gst_element_link_pads_full()
+      * GstPadLinkCheck
+      * gst_pad_link_check_get_type()
+      * gst_pad_link_full()
+      * gst_structure_fixate_field_string()
+      * GST_TAG_DEVICE_MANUFACTURER
+      * GST_TAG_DEVICE_MODEL
+      * GST_TAG_IMAGE_ORIENTATION
+      * GST_TAG_GEO_LOCATION_CAPTURE_DIRECTION
+      * GST_TAG_GEO_LOCATION_MOVEMENT_DIRECTION
+      * GST_TAG_GEO_LOCATION_MOVEMENT_SPEED
+      * gst_tag_list_peek_string_index()
+      * GST_TRACE
+      * GST_TRACE_OBJECT
+      * GST_CAT_TRACE
+      * GST_CAT_TRACE_OBJECT
+      * GST_LEVEL_TRACE
+      * gst_adapter_masked_scan_uint32_peek
+      * GstBaseSink::enable-last-buffer
+      * gst_base_sink_is_last_buffer_enabled()
+      * gst_base_sink_set_last_buffer_enabled()
+      * GstBaseTransform::accept_caps()
+
+API deprecated since 0.10.29:
+
+      * gst_object_get_name_prefix()
+      * gst_object_set_name_prefix()
+      * gst_caps_load_thyself()
+      * gst_caps_save_thyself()
+      * gst_class_signal_emit_by_name()
+      * gst_object_save_thyself()
+      * gst_object_restore_thyself()
+      * gst_pad_load_and_link()
+      * gst_xml_get_element()
+      * gst_xml_get_topelements()
+      * gst_xml_get_type()
+      * gst_xml_make_element()
+      * gst_xml_new()
+      * gst_xml_parse_doc()
+      * gst_xml_parse_file()
+      * gst_xml_parse_memory()
+      * gst_xml_write()
+      * gst_xml_write_file()
+
+Changes since 0.10.28:
+
+      * improve plugin loading robustness: do not ever unload a plugin after
+        calling into it: should fix mystery crashers during registry loading
+        when a plugin init function returns FALSE (e.g. when some supporting
+        library fails to initialise or a wrapper plugin found no features to
+        wrap and wrongly returned FALSE)
+      * configurable memory alignment for GstBuffers
+      * add QoS message to inform apps of lost data, dropped frames etc.
+      * basesink, basetransform: add support for new QoS message
+      * basetransform: accept non-fixed caps suggestions
+      * basesrc: fix gst_base_src_new_seamless_segment()
+      * GstController fixes and optimisations
+      * set thread name for pad tasks on Linux
+      * pipeline, bin: fix refcount issue when removing elements during a state change
+      * queue2: implement seeking in download mode
+      * queue2: implement flushing in download buffering
+      * queue2: improve buffer level measurement in download mode
+      * fdsrc: allow specifying the size in bytes on the uri
+      * build fixes: better checks for uint128_t, inline assembly on OSX, compilation
+        if HAVE_REGISTER_PRINTF_SPECIFIER is undefined, gobject-introspection
+      * two symbols were removed that had been exported but never been used or been
+        declared in any header file: gst_element_default_error and gst_element_request_compatible_pad
+
+Bugs fixed since 0.10.28:
+
+      * 576234 : [basetransform] Suggesting non-fixed caps or no size doesn't work for upstream negotiation
+      * 520697 : [API] Add GST_TAG_USER_RATING
+      * 590718 : docs build failures with -jN: cp: cannot create regular file `build/image.entities': File exists
+      * 595958 : Position not updated after a backwards gst_event_new_step()
+      * 596832 : configurable buffer alignment
+      * 600718 : autoconf fails with gobject-introspection
+      * 600877 : [uridecodebin] Needs to disable download buffering for non-fast-start files
+      * 603710 : Can't compile with introspection support
+      * 603831 : build with libtool 1.x.y only works if --disable-shave is used
+      * 609046 : basetransform now ignores suggestions from capsfilter
+      * 609170 : basesrc pushes two newsegment
+      * 610256 : Use G_VALUE_COLLECT_INIT if available
+      * 611075 : Typo in debug_dump_pad function
+      * 611911 : Set thread names on pipeline threads
+      * 612370 : gstutils.c inline asm typo, compilation fails
+      * 612410 : [API][tags] add new geo tags
+      * 612733 : Build fails because HAVE_REGISTER_PRINTF_SPECIFIER is undefined
+      * 612881 : [utils] gst_pad_proxy_setcaps() doesn't handler iterator resyncs
+      * 613215 : delayed set in gst-launch are not recursive
+      * 613593 : git-update.sh script does not work on fresh git repository clones
+      * 614167 : gstinfo: no previous prototype for 'xxx' when buildign with --disable-gst-debug
+      * 614629 : utils: Use G_GNUC_CONST instead of G_GNUC_PURE for conversion functions
+      * 614767 : libgstreamer build failure on OS X x86_64
+      * 614833 : out of srcdir build fails for libs/gst/check
+      * 615698 :  " warning: cast increases required alignment of target type " with gcc 4.2.1 on arm
+      * 615756 : [bin] refcount issue when removing element in error
+      * 615880 : Add some more custom flow returns
+      * 615881 : [LFOControlSource] Use correct setter for double GValues
+      * 616846 : Crash in gst_interpolation_control_source_find_control_point_iter
+
+API additions since 0.10.28:
+
+      * GST_MESSAGE_QOS
+      * gst_message_new_qos()
+      * gst_message_parse_qos()
+      * gst_message_parse_qos_stats()
+      * gst_message_parse_qos_values()
+      * gst_message_set_qos_stats()
+      * gst_message_set_qos_values()
+      * GST_FLOW_CUSTOM_SUCCESS_1
+      * GST_FLOW_CUSTOM_SUCCESS_2
+      * GST_FLOW_CUSTOM_ERROR_1
+      * GST_FLOW_CUSTOM_ERROR_2
+      * GST_TAG_USER_RATING
+      * GST_TAG_GEO_LOCATION_COUNTRY
+      * GST_TAG_GEO_LOCATION_CITY
+      * GST_TAG_GEO_LOCATION_SUBLOCATION
+
+API deprecated since 0.10.28:
+
+      * gst_element_class_set_details()
+
+Changes since 0.10.27:
+
+     * parse "1/MAX" fraction strings
+     * no material changes compared to 0.10.27, this release is mostly to
+       keep core/base version numbers in sync
+
+Changes since 0.10.26:
+
+      * basesrc: protect segment values from concurrent access from different threads
+      * typefind: protect internal fields from concurrent changes from different threads
+      * typefind: fix pad activation corner-case with have-type already having been emitted
+      * typefind: reset the working mode when going to READY/NULL, fixes re-use from
+        READY state as with decodebin2
+      * gstpoll: fix crash when logging is enabled for GST_POLL
+      * bytewriter: expose gst_byte_writer_put_{float32|float64}_*() properly in header
+      * basesink: fix emergency rendering timestamp tracking
+      * fdsink, fdsrc: fix compilation with MSVC
+      * memindex: avoid busy loop when doing EXACT lookup
+
+Bugs fixed since 0.10.26:
+
+      * 610366 : [gstcollectpads][doc] Add a reminder for 'data' doc
+      * 605189 : gst_element_get_state has wrong introspection
+      * 607771 : [API] Add gst_byte_writer_fill
+      * 608036 : [typefind] deadlock when upstream puts caps on buffers on pull mode
+      * 608877 : [typefind] Access to internal fields not threadsafe
+      * 609941 : GStreamer-WARNING **: External plugin loader failed.
+      * 610210 : [PATCH] Fix compilation of fdsink and fdsrc with MSVC
+      * 610246 : [optimization] Speed up _get_range()
+      * 610367 : [memindex] might busy loop upon EXACT lookup
+      * 610444 : [controller] Interpolation control source passes NULL pointers to GSequence API
+      * 611087 : [basesink] emergency rendering of late buffers fails after resuming from PAUSE
+      * 611719 : GST_DEBUG_OBJECT macros not fed with GObject* in gstpoll.c
+
+API additions since 0.10.26:
+
+      * gst_byte_writer_fill()
+
+Changes since 0.10.25:
+
+      * registry: do plugin scanning (on *nix) using an external helper binary
+      * lots of performance improvements all over the place (ghostpads,
+        multiqueue, pad construction, superfluous type checks, registry loading)
+      * add GstByteWriter, a simple generic byte writer
+      * filesink: Use _wfopen on win32 to open files with non-ascii filenames correctly.
+      * queue2: add option to remove the temp-file (enabled by default)
+      * it is now allowed to use gst_caps_set_simple() on non-simple caps
+      * queue2: move from gst-plugins-base into the coreelements plugin in core
+        (this means you may need to remove libgstqueue2.so manually if you
+        installed from source and don't do make uninstall before upgrading, or
+        combine an older -base with a newer core)
+      * multiqueue: add support for buffering mode where we post BUFFERING
+        messages based on the level of the queues
+      * typefind: speed up typefinding a lot by first trying the typefinder for
+        the file's extension
+      * buffer: remove private/internal subbuffer subclass and keep track of
+        the parent buffer directly in the GstBuffer structure (this removes
+        quite a bit of special-casing and will allow for future improvements/
+        extensions that are harder to do if there's a separate subbuffer class.
+      * collectpads: add ability to install clipping functions
+      * new tags for TV/Radio shows/episodes, lyrics, composer sortname and
+        grouping
+      * miniobject: avoid race when recycling buffers
+      * basesrc: fix race in PLAYING->PAUSED->PLAYING
+
+Bugs fixed since 0.10.25:
+
+      * 476514 : [multiqueue] Doesn't forward EOS event in all cases
+      * 590941 : API: add gst_pad_get_caps() variant that avoids unneeded caps copies
+      * 595602 : g_child_proxy_get_valist doesn't initialize GValue correctly
+      * 535069 : basesrc no longer support non-flushing seeks on itself
+      * 560442 : GNOME Goal: Remove deprecated GLib symbols
+      * 595511 : Annotations for gst_element_query_{position,duration}
+      * 595886 : gst_pad_fixate_caps() does not return fixed caps in case of multiple structures
+      * 595964 : [multiqueue] can hang pipeline during startup
+      * 596366 : proxy_getcaps reverses direction of getcaps
+      * 597407 : GstPipeline calculates base_time incorrectly when a new clock appears during PAUSED state
+      * 597550 : basesrc: sometimes no buffers produced after PLAYING - PAUSED - PLAYING
+      * 597690 : Improve caps setters API
+      * 598297 : make check fails when any --disable option which changes the API has been used
+      * 598526 : bytewriter: fails to compile with gcc 4.2.4 on Ubuntu Hardy 64 bits
+      * 598700 : scripts: Parallelise git-update.sh build script
+      * 598895 : [GstRegistry] Use hash table for feature lookups
+      * 598896 : [GstRegistry] Cache lists of ElementFactory and TypeFindFactory
+      * 599147 : typefind : Avoid having to re-sort the typefind factory list
+      * 599759 : [qtdemux] Add support for more tags
+      * 600313 : Visualisations stop updating after seek
+      * 600922 : gst-launch: wake up less often to check for Ctrl-C
+      * 601587 : MiniObject race condition
+      * 601668 : [gstregistry] gstregistry.c uses a variable from gst.c
+      * 601669 : [tests] tests/examples/manual depends on libgstcheck
+      * 602093 : libgstcheck fails to export some symbols when built under et_EE locale
+      * 602275 : [API] Add new sink-message event
+      * 602419 : [basesink] Regression with position reporting
+      * 603059 : Totem crashes when DVD is encrypted but libdvdcss isn't available
+      * 603787 : [registry] Doesn't use GMappedFile
+      * 604091 : tee: cleanup requestpads in dispose
+      * 604093 : gst-inspect/launch: move gst_tools_print_version to avoid glib warning
+      * 605251 : tee causes segfault if there is no source pad
+      * 605930 : [shave] common/shave not existing yet when configure checks need it
+      * 606435 : gsttee not threadsafe
+      * 607283 : segfaults and/or miniobject warnings with GLib > = 2.23.2
+      * 607317 : [PATCH] fix unaligned detection for x86-64 when cross compiling
+      * 607431 : update common modules before freeze
+      * 607481 : Should define G_THREADS_MANDATORY everywhere
+      * 607739 : [queue2] Temporary file is removed although code claims the opposite
+      * 607842 : Audio comes out with short breaks after resume pipeline (paused- > playing)
+      * 608136 : multiqueue handles UNEXPECTED flowreturn wrongly
+      * 608398 : Initializing the glib thread system seems not to work
+      * 608442 : [filesrc] typo in warning message
+      * 608726 : bytewriter: mistake in .h/.c function naming
+      * 609166 : Buffer list docs ascii art
+      * 590669 : [API] need GstByteWriter or GstChunkWriter
+      * 601698 : Rename new plugin-scanner helper executable before release
+      * 604565 : [gstcheck] Update check to 0.9.8
+      * 596877 : New internal libcheck breaks the Solaris build
+
+API additions since 0.10.25:
+
+      * GST_DEBUG_REGISTER_FUNCPTR()
+      * gst_base_src_new_seamless_segment()
+      * gst_event_new_sink_message()
+      * gst_event_parse_sink_message()
+      * gst_util_fraction_add()
+      * gst_util_fraction_multiply()
+      * gst_util_greatest_common_divisor()
+      * gst_util_double_to_fraction()
+      * gst_util_fraction_to_double()
+      * gst_registry_get_feature_list_cookie()
+      * gst_default_registry_get_feature_list_cookie()
+      * gst_pad_get_caps_reffed()
+      * gst_pad_peer_get_caps_reffed()
+      * gst_structure_id_has_field()
+      * gst_structure_id_has_field_typed()
+      * gst_plugin_feature_list_copy()
+      * gst_caps_set_value()
+      * gst_byte_writer_ensure_free_space()
+      * gst_byte_writer_free()
+      * gst_byte_writer_free_and_get_buffer()
+      * gst_byte_writer_free_and_get_data()
+      * gst_byte_writer_get_remaining()
+      * gst_byte_writer_init()
+      * gst_byte_writer_init_with_buffer()
+      * gst_byte_writer_init_with_data()
+      * gst_byte_writer_init_with_size()
+      * gst_byte_writer_new()
+      * gst_byte_writer_new_with_buffer()
+      * gst_byte_writer_new_with_data()
+      * gst_byte_writer_new_with_size()
+      * gst_byte_writer_put_data()
+      * gst_byte_writer_put_float32_be()
+      * gst_byte_writer_put_float32_le()
+      * gst_byte_writer_put_float64_be()
+      * gst_byte_writer_put_float64_le()
+      * gst_byte_writer_put_int16_be()
+      * gst_byte_writer_put_int16_le()
+      * gst_byte_writer_put_int24_be()
+      * gst_byte_writer_put_int24_le()
+      * gst_byte_writer_put_int32_be()
+      * gst_byte_writer_put_int32_le()
+      * gst_byte_writer_put_int64_be()
+      * gst_byte_writer_put_int64_le()
+      * gst_byte_writer_put_int8()
+      * gst_byte_writer_put_string_utf16()
+      * gst_byte_writer_put_string_utf32()
+      * gst_byte_writer_put_string_utf8()
+      * gst_byte_writer_put_uint16_be()
+      * gst_byte_writer_put_uint16_le()
+      * gst_byte_writer_put_uint24_be()
+      * gst_byte_writer_put_uint24_le()
+      * gst_byte_writer_put_uint32_be()
+      * gst_byte_writer_put_uint32_le()
+      * gst_byte_writer_put_uint64_be()
+      * gst_byte_writer_put_uint64_le()
+      * gst_byte_writer_put_uint8()
+      * gst_byte_writer_reset()
+      * gst_byte_writer_reset_and_get_buffer()
+      * gst_byte_writer_reset_and_get_data()
+      * gst_bit_reader_get_size()
+      * gst_byte_reader_get_size()
+      * gst_data_queue_new_full()
+      * gst_collect_pads_set_clip_function()
+      * gst_type_find_helper_get_range_ext()
+
+Changes since 0.10.24:
+    
+      * Improve the byte-reader API
+      * GObject introspection support
+      * Improve clock accuracy on win32
+      * Optimisations in capabilities checking
+      * Optimisations and fixes in the basetransform base class
+      * new 64-bit scaling utility function variants
+      * Various bug-fixes and improvements (see ChangeLog and bugs list below)
+
+Bugs fixed since 0.10.24:
+     
+      * 583999 : [basetransform] caps refcounting problem causing GST_IS_CAPS assertion failures
+      * 566881 : [GstIndex] support/caching in GstBin
+      * 588472 : [basetransform] problems in reverse-negotiating
+      * 589173 : macros cause spurious semicolon warnings
+      * 589314 : [basetransform] clears GAP flag in passthrough mode
+      * 589524 : gst_base_transform_acceptcaps() could provide more verbose debugging output
+      * 589849 : [segment] Clipping fails to handle start=stop < segment_start correctly
+      * 589991 : [queue] limited error handling might cause pipeline appearing to hang
+      * 590045 : Query position fails when pipeline is paused and format is not time
+      * 590430 : Add support for " album artist " tags
+      * 590841 : configure script check for libxml2 is incorrect
+      * 590919 : gst_util_uint64_scale_int() and friends don't round
+      * 591045 : [basesrc] Leaking GstTask instances
+      * 591318 : ghostpad : core dump : on_src_target_notify called with an invalid ghostpad
+      * 591441 : append mode for filesink
+      * 592209 : [GstPad] Deprecated markers missing in the header for internal links function related things
+      * 592314 : core/tests/examples/streams/ does not link to pthread
+      * 593460 : Broken win32-specific systemclock code
+      * 593719 : regression: segfault when using gstrtpbin and certain video codecs
+      * 594107 : [gstbin] : use of freed message : valgrind Invalid read
+      * 594225 : [API] [bytereader] add _unchecked() variants and inline most common functions
+      * 594990 : [introspection] pkg-config file madness and another bug
+      * 595130 : checks fail
+      * 595133 : gst/gstutils check fails
+      * 595209 : Fix out-of-tree build
+      * 368536 : bin_change_state makes children go through unnecessary state changes
+
+API additions since 0.10.24:
+    
+      * gst_caps_can_intersect()
+      * gst_util_uint64_scale_int_round()
+      * gst_util_uint64_scale_int_ceil()
+      * gst_util_uint64_scale_round()
+      * gst_util_uint64_scale_ceil()
+      * gst_iterator_new_single()
+      * gst_byte_reader_skip_unchecked()
+      * gst_byte_reader_peek_*_unchecked()
+      * gst_byte_reader_get_*_unchecked()
+      * gst_byte_reader_{peek,get,dup}_data_unchecked()
+      * gst_byte_reader_get_float*_unchecked()
+
+Changes since 0.10.23:
+    
+      * Fully support nested structures in caps
+      * Support frame-by-frame stepping in sinks
+      * Add support for buffer-lists to pass around groups of buffers
+      * Use TaskPools for managing worker threads
+      * New stream-status API for finer thread control
+      * Code optimisations
+      * Many other bug-fixes and enhancements
+
+Bugs fixed since 0.10.23:
+     
+      * 580579 : crash in Volume Control: aucunes idées désolé.
+      * 527488 : [GstXML] can't load elements with request pads from XML
+      * 570233 : allow plugins caching data in the registry
+      * 584389 : don't recreate plugin feature and element factories on fi...
+      * 534208 : [API] add gst_structure_get()
+      * 545787 : [API] add gst_plugin_register_static_full() for bindings
+      * 554460 : thumbnailer crash in gst_fake_sink_event() on FLUSH_START...
+      * 559643 : Don't allow empty or NULL strings in taglists
+      * 560345 : gst_tag_list_get_string() may return NULL or empty string
+      * 560442 : GNOME Goal: Remove deprecated GLib symbols
+      * 572285 : Buffer Lists
+      * 577926 : Remove old xml registry
+      * 578908 : [fdsink] implement seeking on seekable fds
+      * 580177 : glibc 2.10 deprecates register_printf_function
+      * 580716 : race condition in gst_element_lost_state
+      * 581198 : [tags] Add gst_tag_setter_add_tag_value() and gst_tag_lis...
+      * 581281 : [GstURIHandler] Doesn't use get_type_full() at all
+      * 582010 : audiotestsrc is-live=1 ! pulsesink unreliable
+      * 582564 : [controller] Use ordered GSequence instead of GList in th...
+      * 582588 : [API] Add a way to get the pad corresponding to a taglist
+      * 582878 : [GstClock] ABI breakage in GIT on x86
+      * 583187 : [API] add gst_adapter_masked_scan_uint32() and gst_adapte...
+      * 583419 : Bad translatable string in gst-launch.c
+      * 583456 : framestep functionality
+      * 583554 : Slow down or lock if date time is changed to the past
+      * 584835 : MSVC compiler fails with 'static inline' function
+      * 584838 : basesrc: confusing QUERY_SEEKING handling
+      * 585039 : rtpool-test can't find pthreads
+      * 585075 : Compilation with MSVC fails for files including config.h ...
+      * 585137 : gst_xml_write_file() fails serialising GstStructure property
+      * 585592 : [API] add gst_byte_reader_masked_scan_uint32()
+      * 585733 : Wrong #include order in gstsegment.c
+      * 585748 : [API] add gst_tag_list_new_full() to create taglist with ...
+      * 586566 : Add GAP Flag support to gstcapsfilter
+      * 586568 : [bytereader] add misc. string functions and gst_byte_read...
+      * 587973 : use G_DIR_SEPARATOR_S instead of " /' " 
+      * 587976 : Fix for gst-inspect and gst-launch when option parsing is...
+      * 588744 : [check] Stream consistency checker utility
+      * 588745 : [basesrc] Serialize tags in the dataflow
+      * 589127 : gsttask leaks the pool
+      * 590056 : [collectpads] race resulting in double flush-stop being o...
+      * 590622 : [bytereader] buffer size checks subject to wrap-around ov...
+      * 579177 : GstInfo: maintain ABI compatibility
+      * 581321 : typefind element leaks force-caps property
+      * 584118 : [gstadapter][doc] Improve documentation of gst_adapter_ma...
+      * 585433 : [queue] Can lock down if min-threshold conflicts with max...
+      * 585569 : rtsp/rtp streaming fails when skipping explicit PAUSED st...
+      * 585834 : Support for GstBufferList in ghostpads
+      * 585960 : Support for GstBufferList in gstbasesink
+      * 587052 : [filesink.c] Support for files > 4GB on windows makes file...
+
+API added since 0.10.23:
+     
+      * GST_DEBUG_CATEGORY_GET() macro
+      * gst_byte_reader_dup_data
+      * gst_byte_reader_dup_string
+      * gst_byte_reader_dup_string_utf8
+      * gst_byte_reader_dup_string_utf16
+      * gst_byte_reader_dup_string_utf32
+      * gst_byte_reader_skip_string
+      * gst_byte_reader_skip_string_utf8
+      * gst_byte_reader_skip_string_utf16
+      * gst_byte_reader_skip_string_utf32
+      * gst_byte_reader_peek_string
+      * gst_byte_reader_peek_string_utf8
+      * gst_byte_reader_get_string
+      * gst_byte_reader_get_string_utf8
+      * add gst_tag_list_new_full()
+      * add gst_tag_list_new_full_valist()
+      * add gst_byte_reader_masked_scan_uint32()
+      * add gst_plugin_get_cache_data, gst_plugin_set_cache_data
+      * gst_structure_get()
+      * gst_structure_id_get()
+      * gst_structure_get_valist()
+      * gst_structure_id_get_valist()
+      * GstSegment::gst_segment_set_running_time()
+      * Add GST_MESSAGE_SRC_NAME() macro
+      * GstSegment::gst_segment_to_position()
+      * GstEvent::gst_event_new_step()
+      * GstEvent::gst_event_parse_step()
+      * GstMessage::gst_message_new_step_done()
+      * GstMessage::gst_message_parse_step_done()
+      * gst_structure_id_new()
+      * Add gst_message_{new,parse}_tag_full() to get/set the source pad
+      * GstAdapter::gst_adapter_masked_scan_uint32()
+      * GstElement::gst_element_lost_state_full()
+      * GstAdapter::gst_adapter_prev_timestamp()
+      * gst_plugin_register_static_full()
+      * gst_tag_list_add_value()
+      * gst_tag_setter_add_tag_value()
+      * add GST_TAG_CONTAINER_FORMAT tag
+      * GstTask::gst_task_set_state()
+      * GstObject::gst_object_ref_sink()
+
+Changes since 0.10.22:
+      * Support files > 4GB on Windows
+      * Controller interpolation fixes
+      * Add timer support to GstPoll and use it for clocking
+      * Attempt to typefind contents from the file extension if all else fails
+      * GStreamer revision control switched to Git
+      * Many other bug fixes and improvements
+
+Bugs fixed since 0.10.22:
+     
+      * 579177 : GstInfo: maintain ABI compatibility
+      * 163577 : [RFC] Interlaced/progressive media support in GStreamer.
+      * 574160 : collectpads does not reliably eos when last pad is removed
+      * 575598 : hierarchical pipelines accumulate segment-done wrongly
+      * 575922 : disabling subsystems cause API break
+      * 576842 : loading a broken registry file can crash
+      * 555978 : [ladspa] no elements exposed/found on Cygwin
+      * 565607 : Broken macros in gsturi.h and gstinterface.h
+      * 566936 : [ghostpads] unlink function wrongly called on target
+      * 567692 : gstinfo.h header not compatible with C++
+      * 567725 : [qtdemux] stopping at a time sometimes shows a different ...
+      * 568289 : gst_pad_template_new() leaks caps it's supposed to take o...
+      * 568438 : gst_poll_wait calling read() on control socket
+      * 568481 : GStreamer linking failures.
+      * 568632 : __MSVCRT_VERSION__ not defined with mingw, causing " stora...
+      * 568678 : filesrc doesn't logs offsets
+      * 570910 : Removing the target of a ghostpad does not re-target the ...
+      * 571227 : Add home page tag
+      * 571559 : [API] add GST_PARAM_MUTABLE_PLAYING etc. to indicate vali...
+      * 572480 : unref and copy functions should not be macros
+      * 573623 : [API] Array binary search utility function
+      * 574024 : [GstAdapter] gst_adapter_push should not accept empty buf...
+      * 574211 : gst_poll_*_control always returns FALSE on Windows
+      * 574213 : [gstcheck] fix for libcheck > 0.9.6
+      * 574241 : gst_tag_list_add and gst_tag_list_add_values behave incon...
+      * 574484 : [patch] Make caps in DOT debug graphs more readable
+      * 574623 : [dot_file_with_ts] ':' not a valid character for a filename
+      * 574805 : [capsfilter] Doesn't reset the internal suggestion with A...
+      * 575695 : build fails on OpenSolaris due to incorrect header file i...
+      * 575814 : flag for EOS on gst-launch when exiting with ctrl-c
+      * 576381 : [basesink] QoS: emergency rendering not always done
+      * 576563 : pidgin crashes on exit in gst_plugin_ext_dep_free()
+      * 576582 : A patch to enable the use of 'name' in Enum parameters
+      * 577887 : Missing GST_DISABLE_GST_DEBUG in gstregistrybinary.c
+      * 577891 : add alloc-pad property on tee
+      * 578114 : API: add two new log levels: FIXME and MEMDUMP
+      * 578201 : _gst_plugin_fault_handler_is_setup undefined under HAVE_W...
+      * 579127 : gst-launch: disable CLOCK_LOST message handling
+      * 580121 : race condition in GStreamer state changes causes problems...
+      * 361155 : Add monotonic clock
+      * 517231 : threadsafe/colored windows logging
+      * 572591 : Another batch of " differs in signedness " warnings
+      * 573823 : pad block callback if it is re-blocked while the previous...
+      * 574163 : Fix gst_pad_activate_pull deactivation with unlinked element
+      * 575682 : Add gst_pad_is_compatible()
+      * 575988 : On Windows filesink can't write files longer than 2-4 GiB...
+
+API additions since 0.10.22:
+    
+      * New FIXME and MEMDUMP debug levels
+      * gst_tag_list_get_buffer() and gst_tag_list_get_buffer_index()
+      * New tags: GST_TAG_SUBTITLE_CODEC, GST_TAG_HOMEPAGE
+      * gst_util_array_binary_search()
+      * gst_message_new_request_state(), gst_message_parse_request_state(), GST_MESSAGE_REQUEST_STATE
+      * GstPoll::gst_poll_new_timer()
+      * GstPoll::gst_poll_write_control()
+      * GstPoll::gst_poll_read_control()
+
+Changes since 0.10.21:
+
+      * GstController improvements
+      * Extensions to the latency setting behaviours
+      * Ability for plugins to register dependencies to trigger re-scanning
+      * Optimisations in some common operations on caps and values and elsewhere
+      * Add sequence numbers to events so dependent events can be associated with
+        the event that caused them
+      * New macros for reading and writing float values
+      * Many improvements in the basesink base class
+      * Support non-default main contexts for GstBus watches
+      * Improvements in pull-mode scheduling of sinks
+      * Fixes for alignment issues on sparc
+      * Ghost pad fixes
+      * New bit-reader assistance API
+      * Many other bug fixes and improvements
+      
+Bugs fixed since 0.10.21:
+
+      * 567002 : --gst-disable-registry-update also skips registry creation
+      * 350477 : [Registry] Provide a way for plugins to delegate the 'cha...
+      * 510354 : post GST_MESSAGE_STRUCTURE_CHANGE when linking and unlink...
+      * 526044 : Crash if there is more than one watcher for a GstBus
+      * 539108 : gst_ghost_pad_new() does more than call g_object_new()
+      * 544003 : [parse] Links to wrong pad if no padtemplate name is given
+      * 544293 : rtspsrc / gstpoll regression
+      * 545714 : GST_READ_UINT_* and GST_WRITE_UINT_* are not always safe ...
+      * 548786 : [win32] search for plugins based on location of DLL
+      * 551676 : Small Memleak fix in gst_pad_link_check_compatible_unlocked
+      * 552778 : add free_func in gstbuffer instances
+      * 553554 : [base] Add a generic bit reader
+      * 553874 : query_position broken during seek
+      * 555196 : Move floating point endian conversion macros into core
+      * 555307 : Need to push latency event into the pipeline
+      * 555631 : Banshee crashes; gstreamer GST_CAPS GST_IS_CAPS warnings
+      * 556091 : libtool-2.2 and old gettext don't mix
+      * 556900 : a copy & paste bug in helloworld example
+      * 557154 : Allow totem to run without write-access to home directory
+      * 557300 : libgstnet needs to link against $(WIN32_LIBS)
+      * 557438 : Gstreamer crashes when Banshee supposed to change track
+      * 557649 : GstBaseTransform can cause ivalid memory references
+      * 559250 : segments need identifiers.
+      * 560301 : Add --plugin to gst-inspect
+      * 560360 : Excessive statting when reading binary cache
+      * 560399 : Unnecessary CRC checksum for binary registry cache
+      * 560442 : GNOME Goal: Remove deprecated GLib symbols
+      * 561501 : g_type_class_ref without unref
+      * 562170 : GstBus watch doesn't work with non-default main context
+      * 562949 : [API] Add an URI query type for querying the source/sink URI
+      * 564863 : Caps are not propagated from a ghostpad's target to the g...
+      * 567225 : volatile gonce_data in BOILERPLATE not initialized to 0
+      * 566393 : [deadlock] Setting index on a pipeline
+
+API added since 0.10.21:
+
+      * Add bit reader and byte reader classes.
+      * gst_message_new_structure_change()
+      * gst_message_parse_structure_change()
+      * GST_BUFFER_FREE_FUNC()
+      * Add GST_READ_UINT24_(LE|BE) and GST_WRITE_UINT24_(LE|BE).
+      * GstBaseSrc::gst_base_src_set_blocksize()
+      * GstBaseSrc::gst_base_src_get_blocksize()
+      * GstBaseSink::gst_base_sink_set_blocksize()
+      * GstBaseSink::gst_base_sink_get_blocksize()
+      * GstBaseSink::blocksize
+      * GstBaseSink::gst_base_sink_do_preroll()
+      * Add gst_byte_reader_get_data and gst_byte_reader_peek_data 
+      * Move float endianness conversion macros from libgstfloatcast to core
+      * gst_util_seqnum_next, gst_util_seqnum_compare
+      * gst_event_get_seqnum, gst_event_set_seqnum
+      * gst_message_get_seqnum, gst_message_set_seqnum
+      * GstSeekFlags::GST_SEEK_FLAG_SKIP 
+      * gst_bin_recalculate_latency()
+      * GstBin::do-latency
+      * gst_tag_setter_reset_tags()
+      * gst_query_new_uri, gst_query_set_uri, gst_query_parse_uri
+      * add gst_plugin_add_dependency()
+      * add gst_plugin_add_dependency_simple()
+
+
+Changes since 0.10.20:
+
+      * Basetransform rework
+      * Basesink synchronisation extensions
+      * New documentation
+      * Many bug fixes, enhancements and optimisations
+
+Bugs fixed since 0.10.20:
+
+      * 481169 : [tag] add support for geo tags (gps location etc.)
+      * 520694 : adding GST_TAG_KEYWORDS
+      * 538201 : deleting the control point at ts=0 does not lower the con...
+      * 544855 : fakesrc and fakesink should call super::event()
+      * 339795 : [GstBaseTransform] Reverse negotiation issues in passthro...
+      * 348114 : [PPC64?] [gcc-4.1.2?] GST_BUFFER_IN_CAPS flag should have...
+      * 361718 : [basetransform] needs API to force renegotiation
+      * 533856 : gst_buffer_join() documentation is unclear
+      * 536978 : GTKDOC_CFLAGS should include CFLAGS
+      * 537804 : [multiqueue] wrongly reporting that the queue is full.
+      * 537812 : [check] add api to setup a pad by name
+      * 538568 : Add GST_TAG_ATTACHMENT
+      * 539772 : gst_pad_template_new() does more than call g_object_new()
+      * 542175 : gst-inspect --gst-plugins-path fails with multiple direct...
+      * 543444 : gst_base_sink_get_position can return 0 unexpectedly
+      * 543853 : Bison version check failure on OSX 10.4 Tiger
+      * 544174 : [basesrc] allow dynamic value of the seekable value.
+      * 544776 : [win32] binary registry may fail if glib is using a diffe...
+      * 545352 : gsturi is too restrictive
+      * 545603 : gst-inspect: don't print uri handler when compiled withou...
+      * 545605 : gstelementfactory: don't use uri handler code without uri...
+      * 545607 : gst: include gstconfig when using macros defined therein
+      * 545853 : [basetransform] rewrite
+      * 546328 : fractions with G_MAXINT cause failure for fixation
+      * 546822 : gstreamer doesn't tell gettext to output its translations...
+      * 547277 : filesrc detect if a file is seekable using SEEK_SET and n...
+      * 547728 : [basetransform] fail on buffer_alloc 
+      * 548394 : basesink should ignore EOS during flushing
+      * 548652 : [Inconsistency] GST_TAG_LOCATION is used for different me...
+      * 549504 : Thread-safe version of gst_pad_get_internal_links()
+      * 551952 : Need 'check' package when compile
+      * 551978 : Memleak in gst_element_sync_state_with_paren
+      * 547835 : tee release_request_pad while buffer_alloc racyness
+      * 538628 : Patch: added a timeout property to fdsrc used in gst_poll...
+      * 546883 : [basetransform] ximagesink fails when resizing video window
+      * 551509 : gst_base_transform_prepare_output_buffer: assertion faile...
+
+API added since 0.10.20:
+
+      * Add GST_TAG_ATTACHMENT for generic file attachments to streams.
+      * Add gst_base_sink_set_render_delay()
+      * Add gst_base_sink_get_render_delay()
+      * Add gst_check_setup_src_pad_by_name
+      * Add gst_check_setup_sink_pad_by_name
+      * Add gst_check_teardown_pad_by_name
+      * Add GstBaseTransform::gst_base_transform_suggest()
+      * GstBaseTransform::gst_base_transform_reconfigure()
+      * GstPad::gst_pad_set_iterate_internal_links_function()
+      * GstPad::GstPadIterIntLinkFunction
+      * GstPad::gst_pad_iterate_internal_links()
+      * GstPad::gst_pad_iterate_internal_links_default()
+
+API deprecated since 0.10.20:
+
+      * gst_pad_get_internal_links()
+      * gst_pad_set_internal_link_function()
+      * gst_pad_get_internal_links_default()
+
+Changes since 0.10.19:
+
+      * Add the Presets interface
+      * Use the binary registry by default
+      * Deprecate gst_element_get_pad and don't use it anywhere any more.
+      * Reverse playback fixes
+      * API to get missing element messages from parse_launch parsing.
+      * Fixes in latency calculations
+      * BaseTransform negotiation fixes
+      * New Buffering query and messages
+      * Fix multiqueue deadlocks when changing limits
+      * Remove pre-generated parser hacks and require newer flex/bison
+      * Use GSlice in more places
+      * Use static strings in property declarations everywhere to save memory
+        allocations
+      * Fix unaligned memory accesses with the binary registry and add CRC
+        checks
+      * Lots of other bug fixes
+
+Bugs fixed since 0.10.19:
+
+      * 535069 : basesrc no longer support non-flushing seeks on itself
+      * 522882 : Add a configure option to enable/disable OPTION_PARSING i...
+      * 396779 : Preset interface for elements
+      * 359653 : GStreamer Binary Registry patch
+      * 401456 : [API] Rename gst_bin_find_unconnected_pad to gst_bin_find...
+      * 446763 : [identity] leaks events in single segment mode
+      * 459862 : typefinding coud be more efficient
+      * 461253 : Crash when gst_base_transform_prepare_output_buffer is se...
+      * 489269 : valgrind option parameter invalid for valgrind 2.2 
+      * 508070 : gstreamer crashes whilst trying to read .so files in .deb...
+      * 512577 : GstTagMergeMode doc has slightly incorrect explanation
+      * 512578 : gst_tag_setter_merge_tags can mess up with KEEP_ALL merge...
+      * 514507 : gst-xmlinspect outputs text instead of xml for plugins
+      * 518022 : [libgstnet] MSVC 6.0 compile error due to socklen_t
+      * 518932 : Expose gst_segment_copy() to facilitate wrapping of GstSe...
+      * 520468 : Add a Env to enable/disable scan_and_update_registry for ...
+      * 522326 : use of 'char*' instead of 'const char*' in gst_caps_set_s...
+      * 523798 : [API] Some GstMiniObject enhancements
+      * 523806 : Should use G_PARAM_STATIC_(NAME|NICK|BLURB) when possible
+      * 523978 : Documentation fixes. 
+      * 523985 : [PATCH] [identity] meta-writes buffers without meta-writa...
+      * 524659 : Add specific error code for encrypted streams (e.g. WMA/A...
+      * 525532 : [fakesink/fakesrc/identity] Uses GObject marshallers for ...
+      * 526042 : [identity] check-imperfect-timestamp doesn't handle new s...
+      * 526236 : mingw32 gstpoll compilation fix
+      * 526247 : Actually build dlls when cross-compiling with mingw32
+      * 526705 : GstIndexResolver uses nickname field as description field
+      * 526768 : Basetransform bufferalloc passing through too easily
+      * 526814 : [API] add gst_pad_add_{data,event,buffer}_probe_full() wi...
+      * 527967 : gst_gerror_get_type is not thread safe
+      * 528187 : Get missing elements from gst_parse_launch()
+      * 528868 : URI schemes/protocols should be handled case insensitive
+      * 529148 : Make gstqueue give the right min latency
+      * 530317 : GType registration error - race condition when parallel c...
+      * 530637 : queue leak on capacity change
+      * 531538 : Race between gst_bus_set_flushing and async bus watches
+      * 533490 : gst_message_new_warning() should take const gchar*
+      * 533635 : gst_event_new_tag() documentation should say it takes own...
+      * 533740 : [API] add gst_typefind_suggest_simple()
+      * 533865 : gst_element_get_pad() should really be deprecated
+      * 534258 : basesink not accumulated time in some cases.
+      * 535218 : gst_base_src_send_event will block if basesrc is blocking...
+      * 536723 : Misspelled word in error string
+      * 536744 : Must link to libdl if dladdr() is used
+      * 536780 : gcc 4.3.0 compile warnings
+      * 536857 : DATADIR definition conflicts with windows headers
+      * 525961 : Build fails on darwin
+      * 535285 : Correct reference to GST_URI_UNKNOWN in gst_element_facto...
+
+API added since 0.10.19:
+
+      * Add GST_IS_PARAM_SPEC_MINI_OBJECT, GST_PARAM_SPEC_MINI_OBJECT
+        GST_TYPE_PARAM_MINI_OBJECT and gst_value_dup_mini_object
+      * typefind::force-caps
+      * gst_message_set_buffering_stats()
+      * gst_message_parse_buffering_stats()
+      * GST_QUERY_BUFFERING
+      * GstBufferingMode
+      * gst_query_new_buffering()
+      * gst_query_set_buffering_percent()
+      * gst_query_parse_buffering_percent()
+      * gst_query_set_buffering_stats()
+      * gst_query_parse_buffering_stats()
+      * gst_query_set_buffering_range()
+      * gst_query_parse_buffering_range()
+      * GST_STREAM_ERROR_DECRYPT
+      * GST_STREAM_ERROR_DECRYPT_NOKEY
+      * gst_segment_copy()
+      * gst_pad_add_data_probe_full()
+      * gst_pad_add_buffer_probe_full()
+      * gst_pad_add_event_probe_full()
+      * GstEvent::gst_event_has_name()
+      * GstFakeSrc:format
+      * gst_type_find_suggest_simple()
+      * GstBaseSink::gst_base_sink_wait_clock()
+      * gst_parse_launch_full()
+      * gst_parse_launchv_full()
+      * gst_parse_bin_from_description_full()
+      * gst_parse_context_new()
+      * gst_parse_context_free()
+      * gst_parse_context_get_missing_elements()
+      * gst_bin_find_unlinked_pad()
+      * GstPreset interface
+
+API deprecated since 0.10.19:
+
+      * gst_element_get_pad -
+        use gst_element_get_static_pad or gst_element_get_request_pad
+      * gst_atomic_int_set() - g_atomic_int_set from GLib
+      * gst_bin_find_unconnected_pad()
+
+Changes since 0.10.18:
+
+      * Fix a regression in raw fd handling
+
+Bugs fixed since 0.10.18:
+     
+      * 524041 : gstfdsrc broken in 0.10.18
+
+Changes since 0.10.17:
+        
+      * New GstPoll abstraction simplifies operations on multiple fd's/sockets
+      * Various bug fixes and corrections
+      
+Bugs fixed since 0.10.17:
+      
+      * 516187 : adding gst_collect_pads_read_buffer () collectpads
+      * 516395 : gst_buffer_create_sub does not copy flags
+      * 520756 : different registry backend configurations cause build errors
+      * 498222 : configure improvements
+      * 499127 : [multiqueue] has no documentation
+      * 505417 : Add GstPoll to core
+      * 509559 : [gstinfo]_gst_debug_init() memory leak
+      * 510194 : segmentation fault when trying to link elements.
+      * 511783 : [API] [check] add gst_check_element_push_buffer_list() etc.
+      * 513964 : [GstPad] gst_pad_get_caps don't return a copy of the caps
+      * 515469 : patch to add gst_index_set_resolver_full
+      * 519584 : gst_element_implements_interface() segfaults with 'filesr...
+      * 519698 : g_free/xmlFree mismatches in gstregistryxml
+      * 520152 : Core uses non-portable size_t and ssize_t
+      * 520671 : GstPoll needs to be ported to Windows
+      * 520808 : GstPoll's API could need some changes for Windows
+      * 520877 : registrybinary.c doesn't build cleanly on Windows/MSVC
+      * 521740 : libgstreamer.def exports not up to date
+      * 522741 : regression: gst_index_entry_free() frees string it does n...
+
+Changes since 0.10.16:
+
+      * Fix compilation on environments that have POSIX timers but not
+        monotonic clocks
+
+Bugs fixed since 0.10.16:
+      
+      * 512715 : gst/gstutils.c and HAVE_MONOTONIC_CLOCK
 
 Changes since 0.10.15: