Release 0.10.32
[glsdk/gstreamer0-10.git] / NEWS
diff --git a/NEWS b/NEWS
index fa542e3b5e785fbcdb7e40b6b6afdcbf521e16ea..1c40a3723fd7be225eb7fb31f489017c235cb919 100644 (file)
--- a/NEWS
+++ b/NEWS
@@ -1,4 +1,68 @@
-This is GStreamer 0.10.31 "Safety Pins"
+This is GStreamer 0.10.32 "Take Me to the Bonus Level"
+
+Changes since 0.10.31:
+
+      * GLib requirement is now >= 2.22
+      * New core element: valve (moved from -bad)
+      * New core element: input-selector (N.B. without "select-all" property,
+        use fsfunnel instead) (moved from -bad)
+      * New core element: output-selector (N.B. with different negotiation
+        behaviour by default, set pad-negotiation-mode=active for previous
+        behaviour) (moved from -bad)
+      * Performance improvements for many heavily-used code paths: GstPad,
+        GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue
+      * gobject-introspection: add annotations for most core API
+      * clock: make sync clock wait lockfree
+      * fdsrc/fdsink: reenable on MSVC
+      * registry: fix GStatBuf definition for win32 when building against older
+        glib (fixes unnecessary rescanning of plugins at start-up)
+      * element: add a more flexible way to get request pads from elements
+      * multiqueue: return upon input when already eos
+      * object: fix creation of default name (when creating more than 100000 elements)
+      * pluginloader: fix hangs on OSX
+      * poll: fixes for (p)select backend (used e.g. on OSX)
+      * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
+      * registry: don't replace valid existing plugins by blacklisted ones
+      * tags: don't produce duplicated entries when merging same value twice
+      * basesink: preroll fixes for async=false case
+      * basesink: rework position reporting code
+      * basetransform: handle downstream giving a buffer with new caps but invalid size
+
+Bugs fixed since 0.10.31:
+
+      * 635785 : basesrc: fix deadlock
+      * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
+      * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
+      * 564056 : Protect against umask(0177)
+      * 607513 : input-selector segfaults in g_object_notify()
+      * 632168 : [gsttask] MSVC thread names for task debugging
+      * 632447 : reduce static memory allocated by the registry
+      * 632557 : [macros] Define restrict keyword if not available
+      * 632778 : Optimisations to GstBaseSink
+      * 632779 : gstdataqueue: Only emit g_cond_signal when needed
+      * 632780 : queue: Remove useless checks from e406f7
+      * 633918 : [fakesink] [PATCH] print sink-message events like a  message and its structure
+      * 634965 : sinks render buffers in state PAUSED when async is FALSE
+      * 635001 : basesink: fix position reporting in PAUSED
+      * 636268 : configure test fails on FreeBSD
+      * 636455 : basesrc: Avoid taking object locks for just checking tag presence
+      * 637057 : [plugin-scanner] gstpoll fails with select backend
+      * 637300 : [API] request pad based on caps
+      * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
+      * 637776 : merging the same tag values again produces lists containing duplicates
+      * 638381 : {input,output}-selector: double-check API before release
+      * 638399 : a few typos in GStreamer
+      * 638900 : [GstPoll] Doesn't compile with MinGW
+      * 638941 : registry scan/loading race and inconsistency
+
+API additions since 0.10.31:
+
+      * gst_clock_single_shot_id_reinit()
+      * gst_element_request_pad()
+      * GstElementClass::request_new_pad_full()
+      * gst_poll_get_read_gpollfd()
+      * gst_value_list_merge()
+      * GST_CLOCK_DONE
 
 Changes since 0.10.30: