index 908386dbcaf43e5a8457bd6b57bc85b8d308d8bb..554653dfe97f642ddeb162f17b0bf41ed7aee86e 100644 (file)
--- a/README
+++ b/README
- MacOSX is reported to work; specific audio and video sinks have been written
- Windows support is experimental but improving. Output sinks have been
written but are not yet included in the code. We support
- - MSys/MingW builds
+ - MSys/MinGW builds
- Microsoft Visual Studio 6 builds (see win32/README.txt)
INSTALLING FROM PACKAGES
- want to hack on GStreamer
- want to verify that a bug has been fixed
- do not have a sane distribution
-should you choose to build from source tarballs or CVS.
+should you choose to build from source tarballs or git.
Find more information about the various packages at
http://gstreamer.freedesktop.org/download/
functionality you're probably looking for by now, so go on and read
that README.
-COMPILING FROM CVS
+COMPILING FROM GIT
------------------
-When building from CVS sources, you will need to run autogen.sh to generate
+When building from git sources, you will need to run autogen.sh to generate
the build system files.
-You will need a set of additional tools typical for building from CVS,
+You will need a set of additional tools typical for building from git,
including:
- autoconf
- automake
After the autogen.sh stage, you can follow the directions listed in
"COMPILING FROM SOURCE"
-You can also run your whole cvs stack uninstalled. The script in
-the gstreamer module /docs/faq/gst-uninstalled) is helpful in setting
+You can also run your whole git stack uninstalled. The script in
+the gstreamer module /scripts/gst-uninstalled) is helpful in setting
up your environment for this.
PLUG-IN DEPENDENCIES AND LICENSES