]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blobdiff - RELEASE
Release 0.10.32
[glsdk/gstreamer0-10.git] / RELEASE
diff --git a/RELEASE b/RELEASE
index 0fda09b15a4415a22ed9490b0417a97d444a4b32..698ad4e2f96e58078de28a755417a9542bf872ad 100644 (file)
--- a/RELEASE
+++ b/RELEASE
@@ -1,5 +1,5 @@
 
-Release notes for GStreamer 0.10.8 "Soepeke, ik zie ou nog altijd nie"
+Release notes for GStreamer 0.10.32 "Take Me to the Bonus Level"
         
 
 
@@ -9,12 +9,6 @@ core of the GStreamer streaming media framework.
 
 
 The 0.10.x series is a stable series targeted at end users.
-It is not API or ABI compatible with the stable 0.8.x series.
-It is, however, parallel installable with the 0.8.x series.
-
-
-The 0.10.x series has been reworked for threadsafety.  It also features
-various feature additions and enchancements.
 
 
 This module, gstreamer, only contains core functionality.
@@ -34,15 +28,67 @@ contains a set of less supported plug-ins that haven't passed the
 
 
   
+
 Features of this release
     
-      * Parallel installability with 0.8.x series
-      * Threadsafe design and API
-      * Important fix for registry update causing applets not to load
+      * GLib requirement is now >= 2.22
+      * New core element: valve (moved from -bad)
+      * New core element: input-selector (N.B. without "select-all" property, use fsfunnel instead) (moved from -bad)
+      * New core element: output-selector (with different negotiation behaviour by default, set pad-negotiation-mode=active for previous behaviour) (moved from -bad)
+      * Performance improvements for many heavily-used code paths: GstPad, GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue (use atomic ops make many code-paths
+      * gobject-introspection: add annotations for most core API
+      * clock: make sync clock wait lockfree
+      * fdsrc/fdsink: reenable on MSVC
+      * registry: fix GStatBuf definition for win32 when building against older glib (fixes unnecessary rescanning of plugins at start-up)
+      * element: add a more flexible way to get request pads from elements
+      * multiqueue: return upon input when already eos
+      * object: fix creation of default name (when creating more than 100000 elements)
+      * pluginloader: fix hangs on OSX
+      * poll: fixes for (p)select backend (used e.g. on OSX)
+      * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
+      * registry: don't replace valid existing plugins by blacklisted ones
+      * tags: don't produce duplicated entries when merging same value twice
+      * basesink: preroll fixes for async=false case
+      * basesink: rework position reporting code
+      * basetransform: handle downstream giving a buffer with new caps but invalid size
 
 Bugs fixed in this release
+     
+      * 635785 : basesrc: fix deadlock
+      * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
+      * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
+      * 564056 : Protect against umask(0177)
+      * 607513 : input-selector segfaults in g_object_notify()
+      * 632168 : [gsttask] MSVC thread names for task debugging
+      * 632447 : reduce static memory allocated by the registry
+      * 632557 : [macros] Define restrict keyword if not available
+      * 632778 : Optimisations to GstBaseSink
+      * 632779 : gstdataqueue: Only emit g_cond_signal when needed
+      * 632780 : queue: Remove useless checks from e406f7
+      * 633918 : [fakesink] [PATCH] print sink-message events like a  message and its structure
+      * 634965 : sinks render buffers in state PAUSED when async is FALSE
+      * 635001 : basesink: fix position reporting in PAUSED
+      * 636268 : configure test fails on FreeBSD
+      * 636455 : basesrc: Avoid taking object locks for just checking tag presence
+      * 637057 : [plugin-scanner] gstpoll fails with select backend
+      * 637300 : [API] request pad based on caps
+      * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
+      * 637776 : merging the same tag values again produces lists containing duplicates
+      * 638381 : {input,output}-selector: double-check API before release
+      * 638399 : a few typos in GStreamer
+      * 638900 : [GstPoll] Doesn't compile with MinGW
+      * 638941 : registry scan/loading race and inconsistency
+
+API changed in this release
+     
+- API additions:
     
-      * 344474 : Gnome Mixer Applet doesn't want to load
+      * gst_clock_single_shot_id_reinit()
+      * gst_element_request_pad()
+      * GstElementClass::request_new_pad_full()
+      * gst_poll_get_read_gpollfd()
+      * gst_value_list_merge()
+      * GST_CLOCK_DONE
 
 Download
 
@@ -61,23 +107,37 @@ http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
 
 Developers
 
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
 Interested developers of the core library, plug-ins, and applications should
 subscribe to the gstreamer-devel list. If there is sufficient interest we
 will create more lists as necessary.
 
         
-Applications
-
-Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
-Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
-Let us know if you want to be added to this list.
-
-  
 Contributors to this release
     
+      * Andoni Morales Alastruey
+      * Benjamin Gaignard
+      * Benjamin Otte
+      * David Hoyt
+      * David Schleef
       * Edward Hervey
-      * Thomas Vander Stichele
+      * Havard Graff
+      * Jan Schmidt
+      * Kipp Cannon
+      * Koop Mast
+      * Lasse Laukkanen
+      * Mark Nauwelaerts
+      * Michael Smith
+      * Olivier Crete
+      * Olivier Crête
+      * Raimo Järvi
+      * Sebastian Dröge
+      * Stefan Kost
+      * Thiago Santos
       * Tim-Philipp Müller
+      * Tommi Myöhänen
+      * Wim Taymans
+      * Zhang Wanming
+      * Christian Schaller
+      * Sjoerd Simons
  
\ No newline at end of file