index 50544c856538a0debcf38f4801305f56afb60c68..698ad4e2f96e58078de28a755417a9542bf872ad 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-Release notes for GStreamer 0.10.22 "I heard a disturbing sound"
+Release notes for GStreamer 0.10.32 "Take Me to the Bonus Level"
The 0.10.x series is a stable series targeted at end users.
-It is not API or ABI compatible with the stable 0.8.x series.
-It is, however, parallel installable with the 0.8.x series.
-
-
-The 0.10.x series has been reworked for threadsafety. It also features
-various feature additions and enhancements.
This module, gstreamer, only contains core functionality.
Features of this release
- * GstController improvements
- * Extensions to the latency setting behaviours
- * Ability for plugins to register dependencies to trigger re-scanning
- * Optimisations in some common operations on caps and values and elsewhere
- * Add sequence numbers to events so dependent events can be associated with the event that caused them
- * New macros for reading and writing float values
- * Many improvements in the basesink base class
- * Support non-default main contexts for GstBus watches
- * Improvements in pull-mode scheduling of sinks
- * Fixes for alignment issues on sparc
- * Ghost pad fixes
- * New bit-reader assistance API
- * Many other bug fixes and improvements
+ * GLib requirement is now >= 2.22
+ * New core element: valve (moved from -bad)
+ * New core element: input-selector (N.B. without "select-all" property, use fsfunnel instead) (moved from -bad)
+ * New core element: output-selector (with different negotiation behaviour by default, set pad-negotiation-mode=active for previous behaviour) (moved from -bad)
+ * Performance improvements for many heavily-used code paths: GstPad, GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue (use atomic ops make many code-paths
+ * gobject-introspection: add annotations for most core API
+ * clock: make sync clock wait lockfree
+ * fdsrc/fdsink: reenable on MSVC
+ * registry: fix GStatBuf definition for win32 when building against older glib (fixes unnecessary rescanning of plugins at start-up)
+ * element: add a more flexible way to get request pads from elements
+ * multiqueue: return upon input when already eos
+ * object: fix creation of default name (when creating more than 100000 elements)
+ * pluginloader: fix hangs on OSX
+ * poll: fixes for (p)select backend (used e.g. on OSX)
+ * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
+ * registry: don't replace valid existing plugins by blacklisted ones
+ * tags: don't produce duplicated entries when merging same value twice
+ * basesink: preroll fixes for async=false case
+ * basesink: rework position reporting code
+ * basetransform: handle downstream giving a buffer with new caps but invalid size
Bugs fixed in this release
- * 567002 : --gst-disable-registry-update also skips registry creation
- * 350477 : [Registry] Provide a way for plugins to delegate the 'cha...
- * 510354 : post GST_MESSAGE_STRUCTURE_CHANGE when linking and unlink...
- * 526044 : Crash if there is more than one watcher for a GstBus
- * 539108 : gst_ghost_pad_new() does more than call g_object_new()
- * 544003 : [parse] Links to wrong pad if no padtemplate name is given
- * 544293 : rtspsrc / gstpoll regression
- * 545714 : GST_READ_UINT_* and GST_WRITE_UINT_* are not always safe ...
- * 548786 : [win32] search for plugins based on location of DLL
- * 551676 : Small Memleak fix in gst_pad_link_check_compatible_unlocked
- * 552778 : add free_func in gstbuffer instances
- * 553554 : [base] Add a generic bit reader
- * 553874 : query_position broken during seek
- * 555196 : Move floating point endian conversion macros into core
- * 555307 : Need to push latency event into the pipeline
- * 555631 : Banshee crashes; gstreamer GST_CAPS GST_IS_CAPS warnings
- * 556091 : libtool-2.2 and old gettext don't mix
- * 556900 : a copy & paste bug in helloworld example
- * 557154 : Allow totem to run without write-access to home directory
- * 557300 : libgstnet needs to link against $(WIN32_LIBS)
- * 557438 : Gstreamer crashes when Banshee supposed to change track
- * 557649 : GstBaseTransform can cause ivalid memory references
- * 559250 : segments need identifiers.
- * 560301 : Add --plugin to gst-inspect
- * 560360 : Excessive statting when reading binary cache
- * 560399 : Unnecessary CRC checksum for binary registry cache
- * 560442 : GNOME Goal: Remove deprecated GLib symbols
- * 561501 : g_type_class_ref without unref
- * 562170 : GstBus watch doesn't work with non-default main context
- * 562949 : [API] Add an URI query type for querying the source/sink URI
- * 564863 : Caps are not propagated from a ghostpad's target to the g...
- * 567225 : volatile gonce_data in BOILERPLATE not initialized to 0
- * 566393 : [deadlock] Setting index on a pipeline
+ * 635785 : basesrc: fix deadlock
+ * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
+ * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
+ * 564056 : Protect against umask(0177)
+ * 607513 : input-selector segfaults in g_object_notify()
+ * 632168 : [gsttask] MSVC thread names for task debugging
+ * 632447 : reduce static memory allocated by the registry
+ * 632557 : [macros] Define restrict keyword if not available
+ * 632778 : Optimisations to GstBaseSink
+ * 632779 : gstdataqueue: Only emit g_cond_signal when needed
+ * 632780 : queue: Remove useless checks from e406f7
+ * 633918 : [fakesink] [PATCH] print sink-message events like a message and its structure
+ * 634965 : sinks render buffers in state PAUSED when async is FALSE
+ * 635001 : basesink: fix position reporting in PAUSED
+ * 636268 : configure test fails on FreeBSD
+ * 636455 : basesrc: Avoid taking object locks for just checking tag presence
+ * 637057 : [plugin-scanner] gstpoll fails with select backend
+ * 637300 : [API] request pad based on caps
+ * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
+ * 637776 : merging the same tag values again produces lists containing duplicates
+ * 638381 : {input,output}-selector: double-check API before release
+ * 638399 : a few typos in GStreamer
+ * 638900 : [GstPoll] Doesn't compile with MinGW
+ * 638941 : registry scan/loading race and inconsistency
API changed in this release
- API additions:
-* Add bit reader and byte reader classes.
-* gst_message_new_structure_change()
-* gst_message_parse_structure_change()
-* GST_BUFFER_FREE_FUNC()
-* Add GST_READ_UINT24_(LE|BE) and GST_WRITE_UINT24_(LE|BE).
-* GstBaseSrc::gst_base_src_set_blocksize()
-* GstBaseSrc::gst_base_src_get_blocksize()
-* GstBaseSink::gst_base_sink_set_blocksize()
-* GstBaseSink::gst_base_sink_get_blocksize()
-* GstBaseSink::blocksize
-* GstBaseSink::gst_base_sink_do_preroll()
-* Add gst_byte_reader_get_data and gst_byte_reader_peek_data
-* Move float endianness conversion macros from libgstfloatcast to core
-* gst_util_seqnum_next, gst_util_seqnum_compare
-* gst_event_get_seqnum, gst_event_set_seqnum
-* gst_message_get_seqnum, gst_message_set_seqnum
-* GstSeekFlags::GST_SEEK_FLAG_SKIP
-* gst_bin_recalculate_latency()
-* GstBin::do-latency
-* gst_tag_setter_reset_tags()
-* gst_query_new_uri, gst_query_set_uri, gst_query_parse_uri
-* add gst_plugin_add_dependency()
-* add gst_plugin_add_dependency_simple()
+ * gst_clock_single_shot_id_reinit()
+ * gst_element_request_pad()
+ * GstElementClass::request_new_pad_full()
+ * gst_poll_get_read_gpollfd()
+ * gst_value_list_merge()
+ * GST_CLOCK_DONE
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
-Applications
-
-Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
-Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
-Let us know if you want to be added to this list.
-
-
Contributors to this release
- * Alessandro Decina
- * Andrew Feren
- * Andy Wingo
- * Antoine Tremblay
- * Cygwin Ports maintainer
+ * Andoni Morales Alastruey
+ * Benjamin Gaignard
+ * Benjamin Otte
+ * David Hoyt
* David Schleef
- * Dig Ge
* Edward Hervey
+ * Havard Graff
* Jan Schmidt
- * Jan Schmidt - Sun Microsystems
- * Jonas Holmberg
+ * Kipp Cannon
+ * Koop Mast
+ * Lasse Laukkanen
+ * Mark Nauwelaerts
* Michael Smith
* Olivier Crete
- * Peter Kjellerstedt
+ * Olivier Crête
+ * Raimo Järvi
* Sebastian Dröge
- * Simon Holm Thøgersen
* Stefan Kost
- * Thijs Vermeir
- * Thomas Vander Stichele
+ * Thiago Santos
* Tim-Philipp Müller
+ * Tommi Myöhänen
* Wim Taymans
- * 이문형
+ * Zhang Wanming
+ * Christian Schaller
+ * Sjoerd Simons
\ No newline at end of file