index b6381544ccfb962e2a6205764effbb337c99cf6a..698ad4e2f96e58078de28a755417a9542bf872ad 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-GStreamer: Release notes for GStreamer 0.8.8 "I'll Take Care Of You"
+Release notes for GStreamer 0.10.32 "Take Me to the Bonus Level"
-The GStreamer team is happy to announce a new release
-in the 0.8.x stable series of the GStreamer streaming-media framework.
+The GStreamer team is proud to announce a new release
+in the 0.10.x stable series of the
+core of the GStreamer streaming media framework.
-The 0.8.x series is a stable series aimed at end users.
-It is not API or ABI compatible with the stable 0.6.x series.
-It is, however, parallel installable with the 0.6.x series.
+
+The 0.10.x series is a stable series targeted at end users.
+
+
+This module, gstreamer, only contains core functionality.
+For actual media playback, you will need other modules.
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-ugly
+contains a set of well-supported plug-ins, but might pose problems for
+ distributors
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+ rigorous quality testing we expect
-This module only contains core functionality. For actual media playback,
-you will need other modules. GStreamer Plugins contains a huge set of
-additional plugins. GStreamer FFmpeg contains a plugin based on the popular
-FFmpeg decoding library. These modules need not have the same source version
-as the core, as long as they are in the 0.8.x series.
+
Features of this release
- * Parallel installability with 0.6.x series
- * Internationalization
- * Threading fixes
- * Opt scheduler fixes
- * Documentation updates
- * New translation: Norwegian Bokmaal (Kjartan Maraas)
- * New translation: Italian (Luca Ferretti)
- * New scheduler: fair
+ * GLib requirement is now >= 2.22
+ * New core element: valve (moved from -bad)
+ * New core element: input-selector (N.B. without "select-all" property, use fsfunnel instead) (moved from -bad)
+ * New core element: output-selector (with different negotiation behaviour by default, set pad-negotiation-mode=active for previous behaviour) (moved from -bad)
+ * Performance improvements for many heavily-used code paths: GstPad, GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue (use atomic ops make many code-paths
+ * gobject-introspection: add annotations for most core API
+ * clock: make sync clock wait lockfree
+ * fdsrc/fdsink: reenable on MSVC
+ * registry: fix GStatBuf definition for win32 when building against older glib (fixes unnecessary rescanning of plugins at start-up)
+ * element: add a more flexible way to get request pads from elements
+ * multiqueue: return upon input when already eos
+ * object: fix creation of default name (when creating more than 100000 elements)
+ * pluginloader: fix hangs on OSX
+ * poll: fixes for (p)select backend (used e.g. on OSX)
+ * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
+ * registry: don't replace valid existing plugins by blacklisted ones
+ * tags: don't produce duplicated entries when merging same value twice
+ * basesink: preroll fixes for async=false case
+ * basesink: rework position reporting code
+ * basetransform: handle downstream giving a buffer with new caps but invalid size
Bugs fixed in this release
-
- * 144804 : opt scheduler breaks on playing a pipeline
- * 148787 : clocks are not distributed correctly
- * 149936 : [PATCH] [build] GStreamer without registry support do not...
- * 150051 : fakesrc needs a data rate parameter that timestamps the d...
- * 151605 : impossible to play .mpg or avi files with gst-launch-ext
- * 153882 : [PATCH] The win32 version of gstenumtypes is not up to date
- * 154061 : optimal scheduler doesn't get freed
- * 156063 : infinite loop and 100% CPU with some MP3
- * 156179 : gstreamer typefind plugin information from gst-inspect is...
- * 157127 : Cleanup of issues reported by sparse
- * 157263 : use G_SIGNAL_TYPE_STATIC_SCOPE for GstBuffers in handoff ...
- * 158018 : gstreamer typefind stalls on these JPEG files
- * 158162 : opt deadlock
- * 158163 : [api] Problem querying on ghostpads
- * 159852 : [PATCH] [api] g_signal_emit thread safety issues
- * 160019 : segfault when error occurs playback of uri containing per...
- * 160220 : gst_pad_set_explicit_caps of a NULL caps doesn't work
+
+ * 635785 : basesrc: fix deadlock
+ * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
+ * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
+ * 564056 : Protect against umask(0177)
+ * 607513 : input-selector segfaults in g_object_notify()
+ * 632168 : [gsttask] MSVC thread names for task debugging
+ * 632447 : reduce static memory allocated by the registry
+ * 632557 : [macros] Define restrict keyword if not available
+ * 632778 : Optimisations to GstBaseSink
+ * 632779 : gstdataqueue: Only emit g_cond_signal when needed
+ * 632780 : queue: Remove useless checks from e406f7
+ * 633918 : [fakesink] [PATCH] print sink-message events like a message and its structure
+ * 634965 : sinks render buffers in state PAUSED when async is FALSE
+ * 635001 : basesink: fix position reporting in PAUSED
+ * 636268 : configure test fails on FreeBSD
+ * 636455 : basesrc: Avoid taking object locks for just checking tag presence
+ * 637057 : [plugin-scanner] gstpoll fails with select backend
+ * 637300 : [API] request pad based on caps
+ * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
+ * 637776 : merging the same tag values again produces lists containing duplicates
+ * 638381 : {input,output}-selector: double-check API before release
+ * 638399 : a few typos in GStreamer
+ * 638900 : [GstPoll] Doesn't compile with MinGW
+ * 638941 : registry scan/loading race and inconsistency
API changed in this release
-
- API additions:
-* A new function, gst_plugin_get_version, has been added.
+ * gst_clock_single_shot_id_reinit()
+ * gst_element_request_pad()
+ * GstElementClass::request_new_pad_full()
+ * gst_poll_get_read_gpollfd()
+ * gst_value_list_merge()
+ * GST_CLOCK_DONE
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
-Applications
-
-Applications already ported to use GStreamer 0.8.x include the GNOME
-desktop components like gnome-media and nautilus-media, as well as other
-GNOME applications including sound-juicer, totem and RhythmBox.
-
-
Contributors to this release
+ * Andoni Morales Alastruey
+ * Benjamin Gaignard
* Benjamin Otte
- * Christian Schaller
- * Christophe Fergeau
- * Daniel Gazard
+ * David Hoyt
* David Schleef
* Edward Hervey
- * Johan Dahlin
- * Luca Ferretti
- * Kjartan Maraas
- * Martin Soto
- * Matt Kraai
- * Ronald Bultje
- * Sebastien Cote
+ * Havard Graff
+ * Jan Schmidt
+ * Kipp Cannon
+ * Koop Mast
+ * Lasse Laukkanen
+ * Mark Nauwelaerts
+ * Michael Smith
+ * Olivier Crete
+ * Olivier Crête
+ * Raimo Järvi
+ * Sebastian Dröge
* Stefan Kost
- * Stephane Loeuillet
- * Steve Lhomme
- * Thomas Vander Stichele
- * William Jon McCann
+ * Thiago Santos
+ * Tim-Philipp Müller
+ * Tommi Myöhänen
* Wim Taymans
- * Zaheer Abbas Merali
-
+ * Zhang Wanming
+ * Christian Schaller
+ * Sjoerd Simons
+
\ No newline at end of file