index befad0d326568bca0fd3bb9ad35fafbc71844700..698ad4e2f96e58078de28a755417a9542bf872ad 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-Release notes for GStreamer 0.10.13 "With or without you"
+Release notes for GStreamer 0.10.32 "Take Me to the Bonus Level"
The 0.10.x series is a stable series targeted at end users.
-It is not API or ABI compatible with the stable 0.8.x series.
-It is, however, parallel installable with the 0.8.x series.
-
-
-The 0.10.x series has been reworked for threadsafety. It also features
-various feature additions and enhancements.
This module, gstreamer, only contains core functionality.
Features of this release
- * Latency handling infrastructure for live playback scenarios
- * State change handling changes
- * GstController property handling improved
- * Various bug fixes and improvements
- * Parallel installability with 0.8.x series
- * Threadsafe design and API
+ * GLib requirement is now >= 2.22
+ * New core element: valve (moved from -bad)
+ * New core element: input-selector (N.B. without "select-all" property, use fsfunnel instead) (moved from -bad)
+ * New core element: output-selector (with different negotiation behaviour by default, set pad-negotiation-mode=active for previous behaviour) (moved from -bad)
+ * Performance improvements for many heavily-used code paths: GstPad, GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue (use atomic ops make many code-paths
+ * gobject-introspection: add annotations for most core API
+ * clock: make sync clock wait lockfree
+ * fdsrc/fdsink: reenable on MSVC
+ * registry: fix GStatBuf definition for win32 when building against older glib (fixes unnecessary rescanning of plugins at start-up)
+ * element: add a more flexible way to get request pads from elements
+ * multiqueue: return upon input when already eos
+ * object: fix creation of default name (when creating more than 100000 elements)
+ * pluginloader: fix hangs on OSX
+ * poll: fixes for (p)select backend (used e.g. on OSX)
+ * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
+ * registry: don't replace valid existing plugins by blacklisted ones
+ * tags: don't produce duplicated entries when merging same value twice
+ * basesink: preroll fixes for async=false case
+ * basesink: rework position reporting code
+ * basetransform: handle downstream giving a buffer with new caps but invalid size
Bugs fixed in this release
- * 440682 : gst/gstsystemclock unit test occasionally fails
- * 342564 : Configure options causing compilation to fail
- * 378255 : Swedish translation updated
- * 392804 : [API] add GST_CORE_ERROR_DISABLED
- * 412648 : [filesink] reports wrong (byte) position after seeking
- * 413123 : No XML dependency patch
- * 415394 : [identity] post message for imperfect streams if check-pe...
- * 417992 : Quickly playing/pausing messes up synchronization
- * 420106 : [basetransform] race on shutdown: setcaps func called aft...
- * 420206 : Collectpads causes a segv. when stopping after a pad remove
- * 421480 : Make it possible to build without libxml2 with --disable-...
- * 421543 : [GstPad] Doesn't check if pad accepts caps after caps change
- * 422295 : GstController crashes with quadratic and cubic interpolat...
- * 425400 : Multiqueue leaks memory when releasing sink pads
- * 431150 : compilation fails with flex 2.5.4
- * 431940 : [API] add gst_buffer_try_new_and_alloc()
- * 432876 : current time level in queue
- * 434926 : Multilib conflicts with gst-launch-0.10 man page
- * 435880 : [GstBin] Property to allow bins to handle child async cha...
- * 437563 : URIs with upper-case protocol don't play
- * 440463 : gstbin unit test sometimes hangs waiting for ASYNC_DONE m...
- * 441159 : Regression in state change handling
- * 349180 : gst_parse_launch is not reentrant (or recursively callable)
- * 414986 : Don't start the async thread for the system clock until n...
- * 393099 : GstBuffer copy vfunc broken?
- * 419851 : pad-added and pad-removed signals parameter type incorrect
- * 420133 : gst_element_sync_state_with_parent should look at pending...
- * 421177 : Possible deadlock if pad eventfunc is not specified
+ * 635785 : basesrc: fix deadlock
+ * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
+ * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
+ * 564056 : Protect against umask(0177)
+ * 607513 : input-selector segfaults in g_object_notify()
+ * 632168 : [gsttask] MSVC thread names for task debugging
+ * 632447 : reduce static memory allocated by the registry
+ * 632557 : [macros] Define restrict keyword if not available
+ * 632778 : Optimisations to GstBaseSink
+ * 632779 : gstdataqueue: Only emit g_cond_signal when needed
+ * 632780 : queue: Remove useless checks from e406f7
+ * 633918 : [fakesink] [PATCH] print sink-message events like a message and its structure
+ * 634965 : sinks render buffers in state PAUSED when async is FALSE
+ * 635001 : basesink: fix position reporting in PAUSED
+ * 636268 : configure test fails on FreeBSD
+ * 636455 : basesrc: Avoid taking object locks for just checking tag presence
+ * 637057 : [plugin-scanner] gstpoll fails with select backend
+ * 637300 : [API] request pad based on caps
+ * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
+ * 637776 : merging the same tag values again produces lists containing duplicates
+ * 638381 : {input,output}-selector: double-check API before release
+ * 638399 : a few typos in GStreamer
+ * 638900 : [GstPoll] Doesn't compile with MinGW
+ * 638941 : registry scan/loading race and inconsistency
API changed in this release
- API additions:
-* gst_element_change_state()
-* GST_STATE_TARGET
-* GST_BASE_TRANSFORM_LOCK/UNLOCK
-* GstClock::gst_clock_unadjust_unlocked()
-* fakesink::num-buffers property
-* GST_CORE_ERROR_DISABLED
-* basesrc::prepare_seek_segment vmethod
-* gst_buffer_try_new_and_alloc()
-* gst_uri_protocol_is_supported()
-* gst_base_src_query_latency()
-* GstQueue::pushing
-* gst_controller_suggest_next_sync()
-* gst_object_suggest_next_sync()
-* basesrc::unlock_stop
-* basesink::unlock_stop
+ * gst_clock_single_shot_id_reinit()
+ * gst_element_request_pad()
+ * GstElementClass::request_new_pad_full()
+ * gst_poll_get_read_gpollfd()
+ * gst_value_list_merge()
+ * GST_CLOCK_DONE
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
-Applications
-
-Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
-Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
-Let us know if you want to be added to this list.
-
-
Contributors to this release
- * Ville Syrjala
+ * Andoni Morales Alastruey
+ * Benjamin Gaignard
+ * Benjamin Otte
+ * David Hoyt
* David Schleef
* Edward Hervey
- * Evan Nemerson
+ * Havard Graff
* Jan Schmidt
- * Jeroen Wouters
- * Marc-Andre Lureau
+ * Kipp Cannon
+ * Koop Mast
+ * Lasse Laukkanen
* Mark Nauwelaerts
* Michael Smith
- * Mogens Jaeger
* Olivier Crete
- * Peter Kjellerstedt
+ * Olivier Crête
+ * Raimo Järvi
* Sebastian Dröge
- * Sebastien Moutte
* Stefan Kost
- * Thomas Vander Stichele
+ * Thiago Santos
* Tim-Philipp Müller
* Tommi Myöhänen
* Wim Taymans
- * Zaheer Abbas Merali
+ * Zhang Wanming
+ * Christian Schaller
+ * Sjoerd Simons
\ No newline at end of file