index 1f92eed18b2d45063426ab6fdcf2536783741210..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-GStreamer: Release notes for GStreamer 0.8.5 "Stuttgart"
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
-The GStreamer team is happy to announce a new release
-in the 0.8.x stable series of the GStreamer streaming-media framework.
+The GStreamer team is proud to announce a new release
+in the 0.10.x stable series of the
+core of the GStreamer streaming media framework.
-The 0.8.x series is a stable series aimed at end users.
-It is not API or ABI compatible with the stable 0.6.x series.
-It is, however, parallel installable with the 0.6.x series.
+The 0.10.x series is a stable series targeted at end users.
+It is not API or ABI compatible with the stable 0.8.x series.
+It is, however, parallel installable with the 0.8.x series.
-This is the first GStreamer release that compiles with MSVC7 with full
-debug support. Installation of the binaries and the locales are also handled.
+
+The 0.10.x series has been reworked for threadsafety. It also features
+various feature additions and enhancements.
+
+
+This module, gstreamer, only contains core functionality.
+For actual media playback, you will need other modules.
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-ugly
+contains a set of well-supported plug-ins, but might pose problems for
+ distributors
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+ rigorous quality testing we expect
-This module only contains core functionality. For actual media playback,
-you will need other modules. GStreamer Plugins contains a huge set of
-additional plugins. GStreamer FFmpeg contains a plugin based on the popular
-FFmpeg decoding library. These modules need not have the same source version
-as the core, as long as they are in the 0.8.x series.
+
Features of this release
- * Parallel installability with 0.6.x series
- * Internationalization
- * New Translation: Albanian (sq), Laurent Dhima
- * Translations: af, az, cs, en_GB, fr, nl, sq, sr, sv, tr, uk
- * first release that works on Windows with MSVC7
- * fixed lists can now be intersected
- * transform functions from fraction to double added
- * optimal scheduler fixes
- * fixation fixes
- * filesrc fixes
- * typefind fixes
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
Bugs fixed in this release
-
- * 145100 : segfault in gst_pad_call_get_function
- * 147889 : gst_element_link_pads_filtered may ignore named dest pad ...
- * 148692 : GstQueue binary compatibility breakage
- * 149981 : Win32 not included in the source distribution
- * 150242 : GStreamer doesn't copy some buffer flags correctly
-
-API changed in this release
-
-- API additions:
-
-* A new function, gst_scheduler_register, has been added.
-* A new enum member of GstBufferFlag, GST_BUFFER_DELTA_UNIT has been added.
-
-- API depreciations:
-
-* GstBufferFlag has a deprecated enum member, GST_BUFFER_KEY_UNIT.
-Buffers should be marked with GST_BUFFER_DELTA_UNIT when they're not
-key units instead, since key units are the more common case.
+ * 652211 : Use const instead G_CONST_RETURN
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Applications
-Applications already ported to use GStreamer 0.8.x include the GNOME
-desktop components like gnome-media and nautilus-media, as well as other
-GNOME applications including sound-juicer, totem and RhythmBox.
+Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
+Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
+Let us know if you want to be added to this list.
Contributors to this release
- * Benjamin Otte
- * Colin Walters
* David Schleef
- * Laurent Dhima
- * Ronald Bultje
- * Steve Lhomme
- * Thomas Vander Stichele
- * Wim Taymans
- * Zaheer Abbas Merali
+ * Javier Jardón
+ * Руслан Ижбулатов
\ No newline at end of file