index 4049de4fd3d5777b94931f55fbd8584192acf8be..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-GStreamer: Release notes for GStreamer 0.7.6 "Almost"
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
-The GStreamer team is happy to announce a new release in the
-0.7.x development series of the GStreamer streaming-media framework.
-The goal of this release series is to stabilize towards a 0.8
-release series which will be part of the GNOME 2.6 releases
-and hopefully eventually KDE 4.x.
+The GStreamer team is proud to announce a new release
+in the 0.10.x stable series of the
+core of the GStreamer streaming media framework.
-0.7.6 is a Release Candidate for GStreamer 0.8.0
-It is released to shake out the last bugs that might be still present
-due to major/minor number differences.
+
+The 0.10.x series is a stable series targeted at end users.
+It is not API or ABI compatible with the stable 0.8.x series.
+It is, however, parallel installable with the 0.8.x series.
+
+
+The 0.10.x series has been reworked for threadsafety. It also features
+various feature additions and enhancements.
+
+
+This module, gstreamer, only contains core functionality.
+For actual media playback, you will need other modules.
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-ugly
+contains a set of well-supported plug-ins, but might pose problems for
+ distributors
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+ rigorous quality testing we expect
-The 0.7 series is a development series and is aimed at developers.
-It is NOT API or ABI compatible with the stable 0.6.x series or
-with other releases in the series. This means you can not use this
-release to upgrade your current GStreamer installation and expect your
-GStreamer applications to keep working without a recompile.
-It is, however, parallel installable with the 0.6.x series.
+
Features of this release
- * uses 0.8 as the major/minor number
- * opt scheduler fixes
- * don't link non-versioned tools to gstreamer
- * bindings-related fixes and additions
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
+
+Bugs fixed in this release
+
+ * 652211 : Use const instead G_CONST_RETURN
Download
-You find source releases of gstreamer in the download directory:
+You can find source releases of gstreamer in the download directory:
http://gstreamer.freedesktop.org/src/gstreamer/
GStreamer Homepage
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Applications
-Applications are supposed to update their pkg-config checks for GStreamer,
-and start checking for 0.8 as the major/minor number.
+Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
+Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
+Let us know if you want to be added to this list.
Contributors to this release
- * Christian Schaller
- * Thomas Vander Stichele
* David Schleef
- * Johan Dahlin
- * Benjamin Otte
- * Christophe Fergeau
- * Andy Wingo
- * Ronald Bultje
- * Jan Schmidt
-
+ * Javier Jardón
+ * Руслан Ижбулатов
+
\ No newline at end of file