index 42e1db02dc0d56096761d2fdf1c677997e5d143e..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-Release notes for GStreamer 0.10.30 "Safety First"
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
Features of this release
- * GLib requirement was bumped to 2.20, automake requirement to 1.10
- * bin: unlock gst_element_get_state() on error, instead of hanging forever if no timeout is given
- * clock: fix refcounting bug in gst_clock_set_master
- * caps: make sure _normalize() is applied on all structures
- * info: add new TRACE log level and move refcounting there from LOG level
- * pad: don't check twice for changed caps per push
- * pad: fix iterator aggregation of all pads in the internal links fallback
- * tagsetter: protect tagsetter operations with a lock
- * value: support short fourccs (esp. serialisation/deserialisation)
- * adapter: fix _try_to_merge_up(); optimize progressive masked scans
- * basesink: implement percentage position and duration queries
- * basesink: fix segment query return value
- * basetransform: add accept_caps vmethod
- * basetransform: re-evaluate proxy_alloc when reconfigured
- * basetransform: assume in_size equals out_size if there's no transform_size/get_unit_size vfunc
- * fdsink, filesink: make sync property work correctly
- * typefind: make sure buffers' metadata is writable before setting caps on them
- * queue2: fix merging of ranges
- * queue2: don't wait for data when EOS
- * queue2: don't ignore failure to open the temporary file location
- * tools: make gst-launch print things correctly to stderr/stdout and make --quiet work correctly
- * introspection: add many more gobject-introspection annotations
- * xml: serialisation/deserialisation to/from XML has been deprecated, since it's always been broken
- for all but the most trivial pipelines, and will likely never be fixed
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
Bugs fixed in this release
- * 623586 : gst/tagsetter check fails
- * 463435 : Skip #include < libxml/parser.h > in gstconfig.h.in when not needed
- * 505770 : gst_element_get_state() should unblock if element posts an error
- * 615820 : implement percentage position and duration queries
- * 615941 : [tags] Add GST_TAG_DEVICE_MANUFACTURER and GST_TAG_DEVICE_MODEL
- * 616586 : Use GObject's boxed type for GError
- * 617223 : [tags] Add tags for direction of capture and movement
- * 617625 : Commandline utility wrappers (gst-run) don't work on Windows
- * 618644 : gst_pad_get_caps() Return pad template if parent element is in GST_STATE_NULL
- * 619508 : [tag] Add image orientation tag
- * 619815 : GST_PLUGIN_LOADING_WHITELIST env var for unit tests
- * 619828 : [API] adapter: add masked_scan_uint32_peek
- * 620460 : info: add new TRACE log level and move refcounting there from LOG level
- * 620490 : [basesink] segment query unconditionally returns FALSE
- * 621006 : Deprecate unused gst_object_{get|set}_name_prefix()
- * 621282 : Display of short fourccs is in hex instead of text
- * 621332 : BaseTransform should disable proxy alloc if downstream changes caps
- * 621334 : GstBaseTransform should not require a transform_size function
- * 621505 : Disable memory poisoning by default for releases
- * 621527 : gstcaps: New gst_caps_steal_structure() method
- * 621530 : filesink ignores sync=true
- * 621595 : --quiet doesnt make gst-launch be completely quiet, also messages should not go to stdout
- * 621773 : Add introspection annotations
- * 621867 : gst-launch: rename new --no-play command line option
- * 621896 : [API][taglist] Add gst_tag_list_peek_string_index
- * 622504 : [GstPad] Provide more fine-grained linking methods
- * 622546 : distcheck fails in docs/plugins/
- * 622685 : [GstXml] Deprecate GstXml
- * 622967 : [queue2] Problems with progressive downloading
- * 623301 : gst_caps_normalize : doesn't normalize completely
- * 623589 : Fix races/refcounting bugs with slave clocks
- * 624113 : [tags] wrong behaviour in merge function for strings
- * 622025 : Can't build gstreamer due to Gst-0.10.gir: error: Can't resolve type 'PadIntLinkFunction' for field Gst.Pad.intlinkfunc
-
-API changed in this release
-
-- API additions:
-
-* gst_caps_steal_structure()
-* gst_clock_id_wait_async_full()
-* gst_element_link_pads_full()
-* GstPadLinkCheck
-* gst_pad_link_check_get_type()
-* gst_pad_link_full()
-* gst_structure_fixate_field_string()
-* GST_TAG_DEVICE_MANUFACTURER
-* GST_TAG_DEVICE_MODEL
-* GST_TAG_IMAGE_ORIENTATION
-* GST_TAG_GEO_LOCATION_CAPTURE_DIRECTION
-* GST_TAG_GEO_LOCATION_MOVEMENT_DIRECTION
-* GST_TAG_GEO_LOCATION_MOVEMENT_SPEED
-* gst_tag_list_peek_string_index()
-* GST_TRACE
-* GST_TRACE_OBJECT
-* GST_CAT_TRACE
-* GST_CAT_TRACE_OBJECT
-* GST_LEVEL_TRACE
-* gst_adapter_masked_scan_uint32_peek
-* GstBaseSink::enable-last-buffer
-* gst_base_sink_is_last_buffer_enabled()
-* gst_base_sink_set_last_buffer_enabled()
-* GstBaseTransform::accept_caps()
-- API deprecations:
-
-* gst_object_get_name_prefix()
-* gst_object_set_name_prefix()
-* gst_caps_load_thyself()
-* gst_caps_save_thyself()
-* gst_class_signal_emit_by_name()
-* gst_object_save_thyself()
-* gst_object_restore_thyself()
-* gst_pad_load_and_link()
-* gst_xml_get_element()
-* gst_xml_get_topelements()
-* gst_xml_get_type()
-* gst_xml_make_element()
-* gst_xml_new()
-* gst_xml_parse_doc()
-* gst_xml_parse_file()
-* gst_xml_parse_memory()
-* gst_xml_write()
-* gst_xml_write_file()
+ * 652211 : Use const instead G_CONST_RETURN
Download
Contributors to this release
- * Alessandro Decina
- * Alexander Saprykin
- * Benjamin Gaignard
- * Benjamin Otte
* David Schleef
- * Eduardo Dobay
- * Edward Hervey
- * Johan Dahlin
- * Mark Nauwelaerts
- * Martin Bisson
- * Olivier Crête
- * Philippe Normand
- * Sebastian Dröge
- * Stefan Kost
- * Thiago Santos
- * Tim-Philipp Müller
- * Tristan Matthews
- * Wim Taymans
- * Zaheer Abbas Merali
+ * Javier Jardón
* Руслан Ижбулатов
\ No newline at end of file