]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blobdiff - RELEASE
g_thread_create() is deprecated in GLib master, use g_thread_try_new() instead
[glsdk/gstreamer0-10.git] / RELEASE
diff --git a/RELEASE b/RELEASE
index 5174d26c59149b16010cdabbd784a375a545f41d..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
 
-                GStreamer "30 Second Frenchman" 0.3.4 released
-
-                                 RELEASE NOTES
-
-   The  GStreamer  team  is  happy  to  announce  another  release of the
-   GStreamer streaming-media framework.
-
-Focus of this release
-
-   This release fixes a few developer usability issues.
-
-   A  few  of  the  API  functions  have  been  changed  to  offer better
-   functionality  and  to  be  more consistent with other toolkits (GLib,
-   GTK).
-   Sample changes:
-     * gst_elementfactory_make to gst_element_factory_make
-     * GST_PADTEMPLATE_* to GST_PAD_TEMPLATE_*
-
-   This  release  of  GStreamer  has  been  primarily  made in support of
-   RhythmBox. It should really work with their upcoming 0.2.0 release.
-
-   The gst-launch parsing has been bisonified. This allows for better and
-   more consistent command-line parsing. Accordingly, some changes in the
-   dynamic pad treatment have been made as well.
-   The registry handling has been changed. gst-register will now write to
-   a  local  registry  (in  ~/.gstreamer/reg.xml)  if  it  does  not have
-   permissions  to  write to the global registry. Normal applications not
-   running as root will prefer this local registry if it exists, and fall
-   back to the global otherwise.
-   Also,  a --gst-registry option has been added to all gst applications.
-   If  this  is  specified,  then  the  application  will  ONLY  use this
-   registry.  This  is  useful  for testsuites inside the core as well as
-   general testing of plugins.
-
-   GStreamer  is  now  in  Gnome's  Bugzilla. Please file bugs against us
-   there whenever you find them !
-
-Changes in the 0.3.x tree
-
-   The  0.3.x  tree  is  our first tree using GLib 2.0 and libxml2 as the
-   sole  compile  platform.  We  have  also  started  including  all  our
-   documentation  in our RPMS starting this tree. People wanting to build
-   GStreamer themselves with documentation should look at the DOCBUILDING
-   file  for  some  information on what packages are needed to build that
-   successfully.
-
-   Another  new  feature  of  this  release  tree  is  the gst-launch-ext
-   command-line  application.  It  uses predefined pipelines to play back
-   media  files  based on their file extension. This means that you don't
-   need  to construct your own pipelines using gst-launch if all you want
-   to  do  is  play  a  file. Just type gst-launch-ext [filename] and the
-   audiofile  or movie plays for you. This of course also being a work in
-   progress  means  that sometimes it might decide on the wrong pipeline,
-   or cause jitter, as well as random headaches.
-
-   For help building GStreamer, take a look at our [1]build help document
-   .
-
-Updates and Enhancements in this release
-
-     * Improved API naming
-     * New  registry  handling,  allowing  for global, local or specified
-       registry
-     * bison parser
-     * gst-launch-ext dynamic pad fixes
-     * various fixes in mad and vorbisdec for RhythmBox
-
-Previously, in the 0.3.x tree
-
-     * devhelp documentation
-     * New and improved Props API
-     * New master clock system
-     * dxr3 plugin
-     * libcolorspace plugin
-     * Full dparams documentation
-     * All functions documented (551 functions documented)
-     * Python bindings
-     * Portability fixes (no more C++ // style comments)
-     * a52dec plugin updated to a52dec 0.7.3 API
-     * gnome-vfs plugin updated to new seek api
-     * Misc bug and caps fixes
-     * SPEC files improvements
-
-   More  details on these features can be found on the project's website,
-   [2]http://gstreamer.net/.   Source   tarballs  are  also  mirrored  at
-   [3]http://gstreamer.net/releases/current/src/.  If you use Red Hat (or
-   possibly  other  RPM-based  systems),  RPMs for both GStreamer itself,
-   external  libraries and development tools not included in the standard
-   reference    distribution    (RedHat    7.2)    can    be   found   in
-   [4]http://gstreamer.net/releases/current/redhat.
-
-   GStreamer  is  hosted on SourceForge, so support requests and bugs may
-   be filed as usual. Interested developers of the core library, plugins,
-   and  applications  should  subscribe  to  the gstreamer-devel list. If
-   there is sufficient interest we will create more lists as necessary.
-
-   We  are  still  looking for people with access to Solaris, HP-UX, Irix
-   and  True64  that  would  be  willing  to  try  building  and  testing
-   GStreamer. Patches fixing such problems are also more than welcome.
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
+        
 
-Contributors to this release
 
-  Core
+The GStreamer team is proud to announce a new release
+in the 0.10.x stable series of the
+core of the GStreamer streaming media framework.
+
+
+The 0.10.x series is a stable series targeted at end users.
+It is not API or ABI compatible with the stable 0.8.x series.
+It is, however, parallel installable with the 0.8.x series.
+
+
+The 0.10.x series has been reworked for threadsafety.  It also features
+various feature additions and enhancements.
+
+
+This module, gstreamer, only contains core functionality.
+For actual media playback, you will need other modules.
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-ugly
+contains a set of well-supported plug-ins, but might pose problems for
+    distributors
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+    rigorous quality testing we expect
+
 
-     * Erik Walthinsen <omega@temple-baptist.com>
-     * Wim Taymans <wim.taymans@chello.be>
-     * Thomas Vander Stichele <thomas@apestaart.org>
-     * Andy Wingo <wingo@pobox.com>
-     * Benjamin Otte <in7y118@public.uni-hamburg.de>
 
-  Plugins and Sample Applications
+  
 
-     * Richard Boulton <richard@tartarus.org>
-     * David Lehn <dlehn@vt.edu>
-     * Ronald Bultje <rbultje@ronald.bitfreak.net>
-     * Bastien Nocera <hadess@hadess.net>
-     * Martin Enlund <martin@enlund.net>
-     * Arik Devens <arik@gnome.org>
-     * Jérémy Simon <jsimon13@yahoo.fr>
-     * Zeeshan Ali Khattak <zak147@yahoo.com>
-     * Steve Baker <stevebaker_org@yahoo.co.uk>
-     * Rehan Khwaja <rehankhwaja@yahoo.com>
+Features of this release
+    
+      * work around GLib atomic ops API change
+      * some minor win32/mingw fixes
+      * don't use G_CONST_RETURN in public headers
 
-  Misc
+Bugs fixed in this release
+     
+      * 652211 : Use const instead G_CONST_RETURN
 
-     * Christian Schaller <christian.schaller@linuxrising.org>
-     * Calum Selkirk <cselkirk@panix.com>
+Download
 
-References
+You can find source releases of gstreamer in the download directory:
+http://gstreamer.freedesktop.org/src/gstreamer/
 
-   1. http://gstreamer.net/releases/current/buildhelp.php
-   2. http://gstreamer.net/
-   3. http://gstreamer.net/releases/current/src/
-   4. http://gstreamer.net/releases/current/redhat/
+GStreamer Homepage
+
+More details can be found on the project's website:
+http://gstreamer.freedesktop.org/
+
+Support and Bugs
+
+We use GNOME's bugzilla for bug reports and feature requests:
+http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
+
+Developers
+
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
+Interested developers of the core library, plug-ins, and applications should
+subscribe to the gstreamer-devel list. If there is sufficient interest we
+will create more lists as necessary.
+
+        
+Applications
+
+Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
+Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
+Let us know if you want to be added to this list.
+
+  
+Contributors to this release
+    
+      * David Schleef
+      * Javier Jardón
+      * Руслан Ижбулатов
\ No newline at end of file