index a1ec4d68b5e54c334df97f9a7e01a05df37308b5..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-Release notes for GStreamer 0.10.10 "Pais"
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
The 0.10.x series has been reworked for threadsafety. It also features
-various feature additions and enchancements.
+various feature additions and enhancements.
This module, gstreamer, only contains core functionality.
Features of this release
- * Parallel installability with 0.8.x series
- * Threadsafe design and API
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
Bugs fixed in this release
- * 349180 : gst_parse_launch is not reentrant (or recursively callable)
- * 348455 : [filesrc] should not use mmap() by default, since it migh...
- * 340674 : marry gst-debugs & plot-timeline.py
- * 350449 : [GstBaseTransform] buffer_alloc should alway try downstream
- * 352580 : implement proper caps merging
- * 345444 : Linking to an audioconvert (pad-added callback) multiple ...
- * 347293 : GstValueList comparison is flawed
- * 347311 : element_unlink leaks its iterator wich will leak the src ...
- * 348179 : gst_parse_lauch is not reentrant
- * 348354 : failure in bison version detection breaks build
- * 350419 : API: GST_SEGMENT_FORMAT printf extension for GstSegments
- * 350879 : [init] Mark gstreamer as being initialized during registr...
- * 350935 : API: add GST_TAG_EXTENDED_COMMENT
- * 353976 : asssertion about element sanity in gst_registry_xml_write...
- * 350432 : micro-optimising quarks
- * 341029 : Ghostpads internal and target should be linked from the b...
- * 345295 : [PATCH] gstreamer/libs/gst/net for Windows
- * 347756 : Allow --disable-trace without --disable-parse
- * 347794 : Do not reset SIGSEGV handler when --gst-disable-segtrap i...
- * 348918 : application should decide whether or not to use fork() to...
- * 349943 : [QOS] documentation/code mismatch
- * 351768 : Unwanted concurent buffer modifications
- * 352958 : pad_alloc_buffer and stream lock
- * 353121 : gst_query_new_segment should initialize all structure fields
- * 353122 : gst_element_get_bus refs the bus unconditionally
- * 347385 : [ghostpad] gst_ghost_pad_new_from_template() method
- * 348677 : Upgrade to 0.10.9 breaks existing applications (failed se...
-
-API changed in this release
-
-- API additions:
-
-* gst_segtrap_is_enabled
-* gst_segtrap_set_enabled
-* gst_registry_fork_is_enabled
-* gst_registry_fork_set_enabled
-* gst_ghost_pad_new_from_template
-* gst_ghost_pad_new_no_target_from_template
-* gst_caps_merge
-* GST_TAG_EXTENDED_COMMENT
-* GstClockCLass:wait_jitter
-* GST_SEGMENT_FORMAT
-* gst_structure_id_set
-* gst_structure_id_set_valist
+ * 652211 : Use const instead G_CONST_RETURN
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Contributors to this release
- * Andy Wingo
- * Antoine Tremblay
- * Edward Hervey
- * Jan Schmidt
- * Marc-Andre Lureau
- * Michael Smith
- * Peter Kjellerstedt
- * Stefan Kost
- * Thomas Vander Stichele
- * Tim-Philipp Müller
- * Torsten Schoenfeld
- * Wim Taymans
+ * David Schleef
+ * Javier Jardón
+ * Руслан Ижбулатов
\ No newline at end of file