index aad1b0a3704dbec0affb4c059292111c95ff906d..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-Release notes for GStreamer 0.10.17 "Due Negligence"
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
Features of this release
- * Fix compilation on environments that have POSIX timers but not monotonic clocks
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
Bugs fixed in this release
- * 512715 : gst/gstutils.c and HAVE_MONOTONIC_CLOCK
+ * 652211 : Use const instead G_CONST_RETURN
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Contributors to this release
- * Jan Schmidt
- * Cygwin Ports Maintainer
- * Sebastian Dröge
+ * David Schleef
+ * Javier Jardón
+ * Руслан Ижбулатов
\ No newline at end of file