index b6381544ccfb962e2a6205764effbb337c99cf6a..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-GStreamer: Release notes for GStreamer 0.8.8 "I'll Take Care Of You"
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
-The GStreamer team is happy to announce a new release
-in the 0.8.x stable series of the GStreamer streaming-media framework.
+The GStreamer team is proud to announce a new release
+in the 0.10.x stable series of the
+core of the GStreamer streaming media framework.
-The 0.8.x series is a stable series aimed at end users.
-It is not API or ABI compatible with the stable 0.6.x series.
-It is, however, parallel installable with the 0.6.x series.
+
+The 0.10.x series is a stable series targeted at end users.
+It is not API or ABI compatible with the stable 0.8.x series.
+It is, however, parallel installable with the 0.8.x series.
+
+
+The 0.10.x series has been reworked for threadsafety. It also features
+various feature additions and enhancements.
+
+
+This module, gstreamer, only contains core functionality.
+For actual media playback, you will need other modules.
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-ugly
+contains a set of well-supported plug-ins, but might pose problems for
+ distributors
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+ rigorous quality testing we expect
-This module only contains core functionality. For actual media playback,
-you will need other modules. GStreamer Plugins contains a huge set of
-additional plugins. GStreamer FFmpeg contains a plugin based on the popular
-FFmpeg decoding library. These modules need not have the same source version
-as the core, as long as they are in the 0.8.x series.
+
Features of this release
- * Parallel installability with 0.6.x series
- * Internationalization
- * Threading fixes
- * Opt scheduler fixes
- * Documentation updates
- * New translation: Norwegian Bokmaal (Kjartan Maraas)
- * New translation: Italian (Luca Ferretti)
- * New scheduler: fair
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
Bugs fixed in this release
-
- * 144804 : opt scheduler breaks on playing a pipeline
- * 148787 : clocks are not distributed correctly
- * 149936 : [PATCH] [build] GStreamer without registry support do not...
- * 150051 : fakesrc needs a data rate parameter that timestamps the d...
- * 151605 : impossible to play .mpg or avi files with gst-launch-ext
- * 153882 : [PATCH] The win32 version of gstenumtypes is not up to date
- * 154061 : optimal scheduler doesn't get freed
- * 156063 : infinite loop and 100% CPU with some MP3
- * 156179 : gstreamer typefind plugin information from gst-inspect is...
- * 157127 : Cleanup of issues reported by sparse
- * 157263 : use G_SIGNAL_TYPE_STATIC_SCOPE for GstBuffers in handoff ...
- * 158018 : gstreamer typefind stalls on these JPEG files
- * 158162 : opt deadlock
- * 158163 : [api] Problem querying on ghostpads
- * 159852 : [PATCH] [api] g_signal_emit thread safety issues
- * 160019 : segfault when error occurs playback of uri containing per...
- * 160220 : gst_pad_set_explicit_caps of a NULL caps doesn't work
-
-API changed in this release
-
-- API additions:
-
-* A new function, gst_plugin_get_version, has been added.
+ * 652211 : Use const instead G_CONST_RETURN
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Applications
-Applications already ported to use GStreamer 0.8.x include the GNOME
-desktop components like gnome-media and nautilus-media, as well as other
-GNOME applications including sound-juicer, totem and RhythmBox.
+Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
+Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
+Let us know if you want to be added to this list.
Contributors to this release
- * Benjamin Otte
- * Christian Schaller
- * Christophe Fergeau
- * Daniel Gazard
* David Schleef
- * Edward Hervey
- * Johan Dahlin
- * Luca Ferretti
- * Kjartan Maraas
- * Martin Soto
- * Matt Kraai
- * Ronald Bultje
- * Sebastien Cote
- * Stefan Kost
- * Stephane Loeuillet
- * Steve Lhomme
- * Thomas Vander Stichele
- * William Jon McCann
- * Wim Taymans
- * Zaheer Abbas Merali
-
+ * Javier Jardón
+ * Руслан Ижбулатов
+
\ No newline at end of file