index c4f7a65904609cc38391568cd9135d95a48aa351..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-GStreamer 0.3.2 "Do-B-day" released
-
-Release Notes
-
- The GStreamer team is happy to announce another release of the
- GStreamer streaming-media framework. GStreamer now contains close to
- 100 plugins for reading, writing and manipulating audio and video. We
- are rapidly approaching a stable set of libraries. Our sample
- applications are, however, still under development.
-
- We now have a gst-all module prepared that includes all of our source
- modules in one easy-to-compile package.
-
-Future Plans
-
- Our goal for the next release is stabilizing and improving the current
- feature set of GStreamer further, including introducing an improved
- autoplugger module for even better handling of media formats. We will
- also focus more attention at our media player sample application as
- this is the application most users and developers probably will use to
- get aquinted with the framework.
-
- For help building GStreamer, take a look at our build help document.
-
-Updates and Enhancements
-
- * new capabilities negotiation system
- * xml support bugfixes
- * sdlvideosink enhancements
- * gst-xmllaunch added
- * fixes in avi plugin
- * fli plugin now works again
- * fixes to old gstmediaplayer making it work
- * lots of fixes on the v4l plugin
- * new cdxa plugin
- * new mjpeg encoder and decoder plugins
- * new example plugin using GOB
- * partial update of documentation and examples
- * miscellaneous bugfixes
-
- More details on these features can be found, along with the release
- tarballs and some RPMs, on the project's website,
- http://gstreamer.net/.
-
- GStreamer is hosted on SourceForge, so support requests and bugs may
- be filed as usual. Interested developers of the core library, plugins,
- and applications should subscribe to the gstreamer-devel list. If
- there is sufficient interest we will create more lists as necessary.
-
- We are still looking for people with access to Solaris, HP-UX, Irix
- and True64 that would be willing to try building and testing
- GStreamer. Patches fixing such problems are also more than welcome.
-Contributors to this release
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
+
+
+
+The GStreamer team is proud to announce a new release
+in the 0.10.x stable series of the
+core of the GStreamer streaming media framework.
+
+
+The 0.10.x series is a stable series targeted at end users.
+It is not API or ABI compatible with the stable 0.8.x series.
+It is, however, parallel installable with the 0.8.x series.
+
+
+The 0.10.x series has been reworked for threadsafety. It also features
+various feature additions and enhancements.
+
+
+This module, gstreamer, only contains core functionality.
+For actual media playback, you will need other modules.
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-ugly
+contains a set of well-supported plug-ins, but might pose problems for
+ distributors
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+ rigorous quality testing we expect
-Core
- * Erik Walthinsen <omega@temple-baptist.com>
- * Wim Taymans <wim.taymans@chello.be>
- * Thomas Vander Stichele <thomas@apestaart.org>
- * Andy Wingo <wingo@pobox.com>
- * David Lehn <dlehn@vt.edu>
-Plugins and Sample Applications
+
- * Ronald Bultje <rbultje@ronald.bitfreak.net>
- * Bastien Nocera <hadess@hadess.net>
- * Martin Enlund <martin@enlund.net>
- * Benjamin Otte <bj>
+Features of this release
+
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
-Misc
+Bugs fixed in this release
+
+ * 652211 : Use const instead G_CONST_RETURN
- * Christian Schaller <christian.schaller@linuxrising.org>
- * wrobell <wrobell@ite.pl>
+Download
+You can find source releases of gstreamer in the download directory:
+http://gstreamer.freedesktop.org/src/gstreamer/
+
+GStreamer Homepage
+
+More details can be found on the project's website:
+http://gstreamer.freedesktop.org/
+
+Support and Bugs
+
+We use GNOME's bugzilla for bug reports and feature requests:
+http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
+
+Developers
+
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
+Interested developers of the core library, plug-ins, and applications should
+subscribe to the gstreamer-devel list. If there is sufficient interest we
+will create more lists as necessary.
+
+
+Applications
+
+Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
+Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
+Let us know if you want to be added to this list.
+
+
+Contributors to this release
+
+ * David Schleef
+ * Javier Jardón
+ * Руслан Ижбулатов
+
\ No newline at end of file